Solid Edge Draft Type Library
DVEdgeStyleName Property
Description
Gets or sets the drawing view edge styles for the specified edge type.
Property type
Read-write property
Syntax
Visual Basic
Public Property DVEdgeStyleName( _
   ByVal Element As DrawingViewEdgeStyleMappingEdgeType _
) As String
Parameters
Element
ValueDescription
seDVEdgeStyleMapping_CoordinateSystemEdge 
seDVEdgeStyleMapping_HiddenEdge 
seDVEdgeStyleMapping_ReferenceHiddenEdge 
seDVEdgeStyleMapping_ReferenceTangentEdge 
seDVEdgeStyleMapping_ReferenceVisibleEdge 
seDVEdgeStyleMapping_TangentEdge 
seDVEdgeStyleMapping_VisibleEdge 
Example
Imports System.Runtime.InteropServices
Public Class Form1

    Private Sub Button1_Click(sender As Object, e As EventArgs) Handles Button1.Click
        Dim objApp As SolidEdgeFramework.Application
        Dim objDoc As SolidEdgeDraft.DraftDocument
        Dim objFilePrefs As SolidEdgeDraft.DraftFilePreferences
        Dim objEdgeStyleName As String
        Try
            objApp = Marshal.GetActiveObject("SolidEdge.Application")
            objDoc = objApp.ActiveDocument()
            objFilePrefs = objDoc.FilePreferences()

            '// Visible
            objEdgeStyleName = objFilePrefs.DVEdgeStyleName(SolidEdgeConstants.DrawingViewEdgeStyleMappingEdgeType.seDVEdgeStyleMapping_VisibleEdge)
            objFilePrefs.DVEdgeStyleName(SolidEdgeConstants.DrawingViewEdgeStyleMappingEdgeType.seDVEdgeStyleMapping_VisibleEdge) = "Phantom"

            '// Hidden
            objEdgeStyleName = objFilePrefs.DVEdgeStyleName(SolidEdgeConstants.DrawingViewEdgeStyleMappingEdgeType.seDVEdgeStyleMapping_HiddenEdge)

            objFilePrefs.DVEdgeStyleName(SolidEdgeConstants.DrawingViewEdgeStyleMappingEdgeType.seDVEdgeStyleMapping_HiddenEdge) = "Phantom"

            '// Tangent
            objEdgeStyleName = objFilePrefs.DVEdgeStyleName(SolidEdgeConstants.DrawingViewEdgeStyleMappingEdgeType.seDVEdgeStyleMapping_TangentEdge)

            objFilePrefs.DVEdgeStyleName(SolidEdgeConstants.DrawingViewEdgeStyleMappingEdgeType.seDVEdgeStyleMapping_TangentEdge) = "Phantom"

            '// COMANDCS
            objEdgeStyleName = objFilePrefs.DVEdgeStyleName(SolidEdgeConstants.DrawingViewEdgeStyleMappingEdgeType.seDVEdgeStyleMapping_CoordinateSystemEdge)

            objFilePrefs.DVEdgeStyleName(SolidEdgeConstants.DrawingViewEdgeStyleMappingEdgeType.seDVEdgeStyleMapping_CoordinateSystemEdge) = "Phantom"

            '// Reference Visible
            objEdgeStyleName = objFilePrefs.DVEdgeStyleName(SolidEdgeConstants.DrawingViewEdgeStyleMappingEdgeType.seDVEdgeStyleMapping_ReferenceVisibleEdge)

            objFilePrefs.DVEdgeStyleName(SolidEdgeConstants.DrawingViewEdgeStyleMappingEdgeType.seDVEdgeStyleMapping_ReferenceVisibleEdge) = "Phantom"

            '// Reference Hidden
            objEdgeStyleName = objFilePrefs.DVEdgeStyleName(SolidEdgeConstants.DrawingViewEdgeStyleMappingEdgeType.seDVEdgeStyleMapping_ReferenceHiddenEdge)

            objFilePrefs.DVEdgeStyleName(SolidEdgeConstants.DrawingViewEdgeStyleMappingEdgeType.seDVEdgeStyleMapping_ReferenceHiddenEdge) = "Phantom"

            '// Reference Tangent
            objEdgeStyleName = objFilePrefs.DVEdgeStyleName(SolidEdgeConstants.DrawingViewEdgeStyleMappingEdgeType.seDVEdgeStyleMapping_ReferenceTangentEdge)

            objFilePrefs.DVEdgeStyleName(SolidEdgeConstants.DrawingViewEdgeStyleMappingEdgeType.seDVEdgeStyleMapping_ReferenceTangentEdge) = "Phantom"
        Catch ex As Exception
            MsgBox(ex.ToString)
        End Try
    End Sub
End Class
See Also

DraftFilePreferences Object  | DraftFilePreferences Members