Solid Edge Draft Type Library
DefaultView Property
Collapse All
Expand All
Solid Edge Draft Type Library
>
Block Object
: DefaultView Property
Description
Gets or sets the default view associated with a block.
Property type
Read-write property
Syntax
Visual Basic
Public Property DefaultView As
BlockView
Remarks
Note that this is the "value" method, so it will be the default when working with a block without specifying a view.
See Also
Block Object
|
Block Members
|
Solid Edge V19 - What's New