Imports System.Runtime.InteropServices
Public Class AddByActiveSheet
Private Sub Button1_Click(sender As System.Object, e As System.EventArgs) Handles Button1.Click
Dim objApplication As SolidEdgeFramework.Application = Nothing
Dim objDraftDoc As SolidEdgeDraft.DraftDocument = Nothing
Dim DrawingView As SolidEdgeDraft.DrawingView = Nothing
Dim DrawingViews As SolidEdgeDraft.DrawingViews = Nothing
Dim BlockTables As SolidEdgeDraft.BlockTables = Nothing
Dim BlockTable As SolidEdgeDraft.BlockTable = Nothing
Dim objType As Type = Nothing
Dim Balloons As SolidEdgeFrameworkSupport.Balloons = Nothing
Try
' Create/get the application with specific settings
objApplication = Marshal.GetActiveObject("SolidEdge.Application")
If objApplication Is Nothing Then
' Get the type from the Solid Edge ProgID
objType = Type.GetTypeFromProgID("SolidEdge.Application")
' Start Solid Edge
objApplication = Activator.CreateInstance(objType)
' Make Solid Edge visible
objApplication.Visible = True
End If
'Get reference to active document
objDraftDoc = objApplication.ActiveDocument
DrawingViews = objDraftDoc.ActiveSheet.DrawingViews
BlockTables = objDraftDoc.BlockTables
Balloons = objDraftDoc.ActiveSheet.Balloons
'Add Method- ByActiveSheet
BlockTable = BlockTables.AddByActiveSheet("ISO", 1)
'Update Method
For Each BlockTable In BlockTables
BlockTable.Update()
Next
Catch ex As Exception
MsgBox(ex.ToString)
End Try
End Sub
End Class