Public Methods
BringForward | Changes the display order of the referenced object by moving it in front of the first object that obscures it. |
BringToFront | Changes the display order of the referenced object by moving it in front of all other overlapping objects. |
Copy | Places a copy of the referenced object on the clipboard. |
Cut | Moves the referenced object to the system clipboard. |
Delete | Deletes the referenced object. |
Duplicate | Copies the referenced object to a specified location, creating a new instance of the object with the same property values as the original. |
GetOrigin | Gets origin of block label |
Mirror | Copies the referenced object about an axis. |
Move | Moves the referenced object. |
Range | Returns the high and low range values for the referenced object. |
Rotate | Rotates the referenced object about the point specified by the angle in radians. |
Scale | Scales the referenced object by a specified factor. |
Select | Selects the referenced object in the active window. |
SendBackward | Changes the display order of visible objects by moving the referenced object so that it is in back of the first object behind it. |
SendToBack | Changes the display order of visible objects by moving the referenced object behind all overlapping objects. |
SetOrigin | Sets origin of block label |
Public Properties
Angle | Angle of text string in radians |
Application | Returns the active application object. |
Description | Description of block label |
Document | Returns the document to which the referenced object belongs. |
Global | Whether or not a label has the same value in all block occurrences |
Index | Returns the numeric index for the active object. |
Key | Returns a key (a string) to find the object relative to its owning parents. |
Layer | Sets and returns the named layer on which the referenced object resides. |
Name | Returns the name of the referenced object. |
OriginLocation | Specifies the location of the origin with respect to the label text. |
Parent | Returns the parent object for the referenced object. |
PositionLocked | Whether or not the label origin can be changed in the context of a block occurrence |
Prompt | Whether or not user should be prompted for label value on creation of block occurrence |
style | For collection objects, Body objects, RefPlane objects, Sketch objects, CoordinateSystem objects, CommandBarButton objects, SmartFrame2d objects, View objects, and TextCharStyle objects, Style is read-write. For all other objects, Style is read-only. |
Type | Specifies the type of the object being referenced. |
value | Default value of label |
VisibleInOccurrence | Whether or not a label displays in the context of a block occurrence |
ZOrder | Specifies the front-to-back order in which an object is displayed relative to other objects. |
See Also