Solid Edge Constants Type Library
SizeModeConstants Enumeration
Description
Predefined Values for when links are updated
Members
MemberValueDescription
igFrameChangesSize2The frame size changes to match the extents of the object.
igFrameCrops1The frame keeps its size and the object gets cropped or fits within the frame.
igObjectScaled3The object is scaled so that the entire object can be viewed within the frame.