Solid Edge Constants Type Library
SECommandBarModeConstants Enumeration
Description
Command mode display, command bar or quick bar
Members
MemberValueDescription
seApplicationGlobalShowCommandBarMode1Command Bar Mode
seApplicationGlobalShowQuickBarMode2Quick Bar Mode
Example
Imports System.IO
Imports System.Runtime.InteropServices

Module Example
    <STAThread()> _
    Sub Main()
        Dim objApplication As SolidEdgeFramework.Application = Nothing
        Dim currentCommandBarMode As Object = Nothing

        Try
            OleMessageFilter.Register()

            ' Start Solid Edge
            objApplication = Marshal.GetActiveObject("SolidEdge.Application")

            ' Determine the current command user interface mode.
            objApplication.GetGlobalParameter(SolidEdgeFramework.ApplicationGlobalConstants.seApplicationGlobalCommandBarMode, currentCommandBarMode)

            Select Case currentCommandBarMode
                Case SolidEdgeConstants.SECommandBarModeConstants.seApplicationGlobalShowCommandBarMode
                    ' CommandBarMode = seApplicationGlobalShowCommandBarMode
                Case SolidEdgeConstants.SECommandBarModeConstants.seApplicationGlobalShowQuickBarMode
                    ' CommandBarMode = seApplicationGlobalShowQuickBarMode
            End Select

            ' Set the command user interface mode to Command Bar Mode.
            objApplication.SetGlobalParameter( _
                SolidEdgeFramework.ApplicationGlobalConstants.seApplicationGlobalCommandBarMode, _
                SolidEdgeConstants.SECommandBarModeConstants.seApplicationGlobalShowCommandBarMode)

            ' Set the command user interface mode to Quick Bar Mode.
            objApplication.SetGlobalParameter( _
                SolidEdgeFramework.ApplicationGlobalConstants.seApplicationGlobalCommandBarMode, _
                SolidEdgeConstants.SECommandBarModeConstants.seApplicationGlobalShowQuickBarMode)

        Catch ex As Exception
            Console.WriteLine(ex.Message)
        Finally
            OleMessageFilter.Revoke()
        End Try
    End Sub

End Module
See Also

Solid Edge ST3 - What's New