Solid Edge Constants Type Library
InterferenceOptionsConstants Enumeration
Description
Interference Options Constants
Members
MemberValueDescription
seIntfOptIgnoreSameNominalDia1If constant is passed in and an interference exists with the same nominal diameter, it is ignored. If the constant is not passed in, the interference is considered.
seIntfOptIgnoreThreadVsNonThreaded2If constant is passed in and an interference exists between threaded fasteners and non-threaded holes, it is ignored. If the constant is not passed in, the interference is passed.
See Also

Solid Edge V20 - What's New