Solid Edge Constants Type Library
DimDispTypeConstants Enumeration
Description
Dimension Display Types
Members
MemberValueDescription
igDimDisplayTypeBasic5Dimension Basic
igDimDisplayTypeBlank8Dimension Blank
igDimDisplayTypeClassfit3Dimension Class Fit
igDimDisplayTypeClassPlusMinus9Dimension Class Plus Minus
igDimDisplayTypeFitWithLimits11Display the tolerance class along with the tolerance values in parentheses.
igDimDisplayTypeHoleCallout12Dimension Hole Callout.
igDimDisplayTypeHoleShaft10Display Hole and Shaft tolerance classes as Hole/Shaft.
igDimDisplayTypeHoleShaftTolOnly13Display Hole and Shaft tolerance classes as tolerance values.
igDimDisplayTypeHoleShaftWithTol14Display Hole and Shaft tolerance classes along with tolerance values in parentheses.
igDimDisplayTypeLimits4Dimension Limits
igDimDisplayTypeNominal1Dimension Nominal
igDimDisplayTypeReference6Dimension Reference
igDimDisplayTypeTolerance2Dimension Tolerance
igDimDisplayTypeUnitTolerance15Dimension Unit Tolerance.
See Also

Solid Edge ST5 - What's New  | Solid Edge ST4 - What's New  | Solid Edge ST2 - What's New