Solid Edge Revision Manager Object Library
SetInterPartLinkOption Method
Description
Sets interpart link option in registry.
Syntax
Visual Basic
Public Function SetInterPartLinkOption( _
   ByVal enumInterPartLinkOption As InterPartLinkOption _
) As Long
Parameters
enumInterPartLinkOption
ValueDescription
eCopyAllLinkedDocsCreates copies of the direct and indirect documents. The Action on the original document is Unchanged.
eInterPartLinkUnknownThis is added just for initialization purpose.
eOutOfContextWithNewDoc

Creates a new direct document, but links from the indirect document(s) remain with the original parent document, and Out of Context with the new document. The Action on the original parent document is set to Copy and the linked indirect document(s) is set to Do not update.

eUpdateLinksToNewDocUpdates all the indirect documents to the new parent. The Action on the original parent document is set to Copy and the linked indirect document(s) is set to Update Document.
See Also

IRMgrApp Object  | IRMgrApp Members