Solid Edge Revision Manager Object Library
Insight Property
Description
This read-only property returns the Insight object.
Property type
Read-only property
Syntax
Visual Basic
Public Property Insight As Object
Example
Imports RevisionManager
Imports System.Runtime.InteropServices

Module Example

    Sub Main()
        Dim objApplication As RevisionManager.Application = Nothing
        Dim objInsight As RevisionManager.Insight = Nothing

        Try
            ' Start Revision Manager.
            objApplication = New RevisionManager.Application
            objInsight = objApplication.Insight
        Catch ex As Exception
            ' Write any errors to console.
            Console.WriteLine(ex.Message)
        Finally
            ' Release COM Objects.
            If Not (objInsight Is Nothing) Then
                Marshal.ReleaseComObject(objInsight)
                objInsight = Nothing
            End If
            If Not (objApplication Is Nothing) Then
                objApplication.Quit()
                Marshal.ReleaseComObject(objApplication)
                objApplication = Nothing
            End If
        End Try
    End Sub

End Module
See Also

IRMgrApp Object  | IRMgrApp Members