Solid Edge Revision Manager Object Library
IsDocumentFOP Method
MemberValue
FOPMasterAndChild6
FOPMasterDocument2
FOPMemberDocument4
FopStatusUnknown0
NotInvolvedInFOP1
Syntax
Visual Basic
Public Function IsDocumentFOP( _
   ByRef FOPStatus As Long _
) As Long
Parameters
FOPStatus
MemberValue
FOPMasterAndChild6
FOPMasterDocument2
FOPMemberDocument4
FopStatusUnknown0
NotInvolvedInFOP1
Example
Imports RevisionManager
Imports System.Runtime.InteropServices

Module Example

    Sub Main()
        Dim objApplication As RevisionManager.Application = Nothing
        Dim objDocument As RevisionManager.Document = Nothing
        Dim iFOPStatus As Integer
        Dim iRetVal As Integer

        Try
            ' Start Revision Manager.
            objApplication = New RevisionManager.Application
            objDocument = objApplication.Open("C:\Part1.par")
            iRetVal = objDocument.IsDocumentFOP(iFOPStatus)
        Catch ex As Exception
            ' Write any errors to console.
            Console.WriteLine(ex.Message)
        Finally
            ' Release COM Objects.
            If Not (objDocument Is Nothing) Then
                Marshal.ReleaseComObject(objDocument)
                objDocument = Nothing
            End If
            If Not (objApplication Is Nothing) Then
                objApplication.Quit()
                Marshal.ReleaseComObject(objApplication)
                objApplication = Nothing
            End If
        End Try
    End Sub

End Module
See Also

IDocAuto Object  | IDocAuto Members