Solid Edge Revision Manager Object Library : ApplicationGlobalConstants Enumeration |
Member | Value | Description |
---|---|---|
seApplicationGlobalAdminFileLocation | 18 | |
seApplicationGlobalApplyStatusToLinks | 9 | |
seApplicationGlobalAvailableRootFolder | 12 | |
seApplicationGlobalBaselinedRootFolder | 17 | |
seApplicationGlobalCheckInOnClose | 0 | |
seApplicationGlobalExcludedCharactersFromRevision | 22 | |
seApplicationGlobalInReviewRootFolder | 16 | |
seApplicationGlobalInsightCacheLocation | 2 | |
seApplicationGlobalInsightFolderMappingFileLocation | 3 | |
seApplicationGlobalInWorkRootFolder | 14 | |
seApplicationGlobalLogFilesLocation | 1 | |
seApplicationGlobalLookAheadVersion | 6 | |
seApplicationGlobalMakeRevisionsObsolete | 11 | |
seApplicationGlobalMaximumCharactersInRevision | 21 | |
seApplicationGlobalObsoleteRootFolder | 13 | |
seApplicationGlobalOfflineMode | 5 | |
seApplicationGlobalReleasedRootFolder | 15 | |
seApplicationGlobalRevisionDelimiter | 8 | |
seApplicationGlobalSearchScope | 4 | |
seApplicationGlobalStartingRevisionValue | 20 | |
seApplicationGlobalTeamcenterFormula | 19 | |
seApplicationGlobalUpdateDraft | 10 | |
seApplicationGlobalUploadOnClose | 7 |