![]() |
T4S
18.2 C7549 A21431
Teamcenter Gateway for SAP Business Suite API Reference
|
Functions | |
checkSAPDocumentKey DatasetTypeName | |
This convenient function checks if the document key is completely specified and fills out the missing key attribute with the predefined defaults. The document key default configuration can be defined by the corresponding Teamcenter preference set starting with the prefix T4S_DocumentInfoRecordDefaultDocumentKey4<DataType> or by using the T4S::DIR::CONFIG::setDocumentInfoRecordKeyDefaults API. More... | |
getDocumentInfoRecordOriginals ObjectTypeName | |
This convenient function fills the needed API input fields that are needed to transfer original file to SAP Which means the ::SAPDat(Document:Files:*) and ::SAPDat(Document:FileNames:*) attributes are filled based on the configuration information for a given object type name. The configuration can be defined by the corresponding Teamcenter preference set starting with the prefix T4S_DocumentInfoRecordMappingNamedFileList4<DataType> and the related set of. More... | |
T4S::DIR::MAPPING::checkSAPDocumentKey | DatasetTypeName | ||
This convenient function checks if the document key is completely specified and fills out the missing key attribute with the predefined defaults.
The document key default configuration can be defined by the corresponding Teamcenter preference set starting with the prefix T4S_DocumentInfoRecordDefaultDocumentKey4<DataType>
or by using the T4S::DIR::CONFIG::setDocumentInfoRecordKeyDefaults
API.
ObjectTypeName | Internal Teamcenter object type name (e.g. ItemRevision, Text) |
References T4X::CORE::getSessionLogChannel(), and tpwrite().
Referenced by T4S::PROP::CUSTOM::MAPPING::GetDIRData(), and T4S::DIR::CUSTOM::MAPPING::TC_Object2SAP_DocumentInfoRecord().
T4S::DIR::MAPPING::getDocumentInfoRecordOriginals | ObjectTypeName | ||
This convenient function fills the needed API input fields that are needed to transfer original file to SAP Which means the ::SAPDat(Document:Files:*) and ::SAPDat(Document:FileNames:*) attributes are filled based on the configuration information for a given object type name. The configuration can be defined by the corresponding Teamcenter preference set starting with the prefix T4S_DocumentInfoRecordMappingNamedFileList4<DataType>
and the related set of.
T4S_DIR_WorkstationApplication4<NamedFileRealtionInfo>
T4S_DIR_FileExtension4<NamedFileRealtionInfo>
T4S_DIR_DataCarrierName4<NamedFileRealtionInfo>
T4S_DIR_DataCarrierPath4<NamedFileRealtionInfo>
T4S_DIR_KproName4<NamedFileRealtionInfo>
::T4S::DIR::setDocumentInfoRecordOriginalsConfig
APIObjectTypeName | Internal Teamcenter object type name (e.g. ItemRevision, Text) |
References T4X::CORE::getSessionLogChannel(), and tpwrite().