Version |
PR Number |
Description |
Application |
Function |
Sub Function |
1880 |
7774710 |
Request to create the scanning path while rotating table. |
CMM_INSPECTION |
PATH |
ALL |
1880 |
7917454 |
Want to control Datum Letter so that greater than 2 characters are inputted. |
CMM_INSPECTION |
TOLERANCES |
ALL |
1880 |
8331747 |
ER - Parallel Generate - Temporary filename incremented from existing part file |
CAM |
TC_MFG |
OTHER |
1880 |
8404327 |
Durability for 402 |
CAE |
ADV_SIMULATION |
DURABILITY |
1880 |
8414690 |
Update of NX-Continuous Release over Mapped Drive will destroy UGII_BASE_DIR |
SYSTEM |
WNT_INSTALL |
ALL |
1880 |
8420160 |
NX 11.0.1 MP2 fem file cannot be opened in NX 12.0.x or later versions. |
CAE |
ADV_SIMULATION |
FIELDS |
1880 |
8423195 |
NX Installation Guide needs correction for regsvr32 /u advise |
SYSTEM |
WNT_INSTALL |
ALL |
1880 |
8423519 |
Pre-solver crashes when doing mesh mapping using LMS file |
CAE |
ADV_SIMULATION |
SYSNOISE_SOLVER |
1880 |
8425165 |
Not able to open saved part with CAM data * URGENT |
CAM |
BASIC_FUNCTIONS |
UNDETERMINED |
1880 |
8559410 |
Cannot execute NX Nastran with severe (174): SIGSEGV segmentation fault occur |
CAE |
ADV_SIMULATION |
SYSNOISE_SOLVER |
1880 |
8562108 |
GSO: not to make Mass connections |
CAE |
ADV_SIMULATION |
CONNECTIONS_UNI |
1880 |
9021178 |
Not possible to create manual support |
ADD_FIXED_PLANE |
NESTING |
OTHER |
1880 |
9093818 |
Calculation Method as Optional on Tolerance Operation of type Distance Between |
CMM_INSPECTION |
ANALYZE |
ALL |
1880 |
9094071 |
Using create region support surface and support area not shown & redundant |
ADD_FIXED_PLANE |
SUPPORTS |
OTHER |
1880 |
9317205 |
ER: Support Bracket symbols on drawing |
SHIP_DESIGN |
STEEL_FEATURES |
BRACKET |
1880 |
9326196 |
FBM - first run of Create Feature Process has bad performance |
CAM |
FEATURE_BASED |
RULES_OOTB |
1880 |
9373903 |
error when adding friction to a joint |
CAE |
MOTION |
JOINT |
1880 |
9384160 |
thread depth not displayed correctly on model |
DESIGN |
FEATURE_MODEL |
HOLE |
1880 |
9388348 |
Texts length become longer origin after translated to dwg. |
TRANSLATOR |
DXF_DWG |
ALL |
1880 |
9428539 |
FBM - MRL - Initial Caching of Tools takes too long. |
CAM |
FEATURE_BASED |
FEATURE_RECOGNI |
1880 |
9479667 |
NXOpen.CAE.AfuManager.ListRecordInformation not writing to a file correctly |
CAE |
ADV_SIMULATION |
NXOPEN |
1880 |
9480559 |
NX-CAM Contour toolpaths generate with gouges |
CAM |
SURFACE_CONTOUR |
FASC_FIX_PROJ |
1880 |
9487926 |
Section drawing feature causes modeler error while creating a section view |
SHIP_DESIGN |
DRAFTING |
SHIP_SECTN_DRWG |
1880 |
9495116 |
NXOpen.UF.UFLib.ExecuteQuery fails in managed NX mode for INCLASS_get_count |
CAM |
LIBRARIES |
MECHANISM |
1880 |
9499520 |
ER: Need an indicator to show profile cutout is right handed or left handed |
SHIP_DESIGN |
CONCEPT |
CUTOUT |
1880 |
9499652 |
Electrode Drafting Naming Rule disregards MW_EW_DRAWING_PART_NAME_RULE |
KDA |
ELECTRODE_DESGN |
DRAWING |
1880 |
9501415 |
CSE does not work with waved blank and suppressed component in NX 12 |
CAM |
ISV |
MACH_CODE_BASED |
1880 |
9502262 |
Force sensor error when there is friction in a link |
CAE |
MOTION |
JOINT |
1880 |
9502689 |
step ap242 translator export geometry of excluded layers |
TRANSLATOR |
STEP_AP242 |
UG_TO_STEP |
1880 |
9504068 |
Error opening sim file (new/old) in Simcenter 3D - Portuguese language |
CAE |
ADV_SIMULATION |
CONNECTIONS_UNI |
1880 |
9505397 |
Enter Manufacturing throws internal error after deleting Program Group by NXOpen |
CAM |
USER_INTERFACE |
OTHER |
1880 |
9507187 |
Penetration Management - The Displayed part must be a valid work-set |
SHIP_DESIGN |
TOOLS |
PENETRATION_MGT |
1880 |
9507671 |
ISV Model slows NXOpen script dramatically in NX 12 |
CAM |
ISV |
TOOL_PATH_BASED |
1880 |
9508805 |
Different German translations in Ribbon and Dialog for Move Object command |
DESIGN |
FEATURE_MODEL |
MOVE_OBJECT |
1880 |
9512158 |
PTS part remains work part after added to assembly making it an assembly. |
KDA |
REUSE_LIBRARY |
ADD_REUSE_COMP |
1880 |
9524646 |
Cannot edit routing pipe bend table while NX open. |
ROUTING_MECH |
TOOLS |
BEND_REPORT |
1880 |
9526146 |
Electrode EDM drawing does not use electrode name as advertised |
KDA |
ELECTRODE_DESGN |
DRAWING |
1880 |
9527250 |
Simcenter - Ansys time domain import |
CAE |
ADV_SIMULATION |
UNIF_DATA_VIE |
1880 |
9528968 |
CAM Japanese translation of Linear is wrong. |
CAM |
USER_INTERFACE |
CAM_SESSION |
1880 |
9532310 |
Part file will not open |
CAM |
PART_CORRUPTION |
ALL |
1880 |
9532880 |
SC30590 Icon Discrete Drivetrain is greyed out |
CAE |
MOTION |
DISC_DRV_TRAIN |
1880 |
9537908 |
Error when open CAM Part File (Severe error 580009 index 223 out of range) |
CAM |
BASIC_FUNCTIONS |
UNDETERMINED |
1880 |
9541473 |
Translated Japanese of NX1872/1876 Start menu icon name is wrong |
SYSTEM |
WNT_INSTALL |
ALL |
1880 |
9542451 |
No Shortcuts for Quality Dashboard and Validation Rule Editor found anymore |
SYSTEM |
WNT_INSTALL |
ALL |
1880 |
9550941 |
CAM-Part cannot be opened after saving in NX 1876 array Attribute out of range |
CAM |
BASIC_FUNCTIONS |
UNDETERMINED |
1880 |
9551016 |
Not able to open saved part with CAM data |
CAM |
BASIC_FUNCTIONS |
UNDETERMINED |
1880 |
9555146 |
Problem with opening file after save in NX 1876 - Severe error 580009 |
CAM |
BASIC_FUNCTIONS |
UNDETERMINED |
1876 |
1986895 |
Step file cannot be imported - Invalid toroidal surface definition. |
TRANSLATOR |
STEP_AP214 |
IMPORT_GEOMETRY |
1876 |
8387207 |
Bumper pendulum placed at wrong contact point |
KDA |
GENERAL_PACKAGE |
BUMPER |
1876 |
8396322 |
STEP Import abort |
TRANSLATOR |
STEP_AP214 |
IMPORT_ASSEMBLY |
1876 |
8408779 |
Misleading deprecated notes in NX12 Routing APV XML and README files |
ROUTING_GENERAL |
ADMINISTRATION |
NXOPEN |
1876 |
8418943 |
Suppress Beta version of NX message |
BETA_EAP |
ARCHITECTURE |
ALL |
1876 |
8560541 |
HTML report does not work for an assembly with bundles |
FLEXIBLE_PIPE |
GENERAL |
ALL |
1876 |
9064202 |
Different Position between Tool_Tip and Tool_Mount is not honored inside Sys-Tr |
TC_FEATURES |
RESOURCE_MGR |
AUTO_ASSEMBLY |
1876 |
9071549 |
FPC Design App - Attach bodies to flex and bring them along when flattening |
FLEX_PC_DESIGN |
PREFERENCES |
ALL |
1876 |
9213628 |
Flange: Corner Relief partly removes Bend from opposite side |
NX_SHEET_METAL |
FLANGE |
ALL |
1876 |
9281984 |
Internal error with Make Unique |
NXMANAGER |
MAKE_UNIQUE |
ALL |
1876 |
9287087 |
After Flange creation the Flange width is no more the same (-0 002 mm) |
NX_SHEET_METAL |
FLANGE |
ALL |
1876 |
9314631 |
Sheet Metal Flange is always too small in the model |
NX_SHEET_METAL |
FLANGE |
ALL |
1876 |
9326801 |
CAE JT missing faces |
CAE |
ADV_SIMULATION |
POST_JT |
1876 |
9327215 |
Sheet Metal Flange is always too small in the model |
NX_SHEET_METAL |
FLANGE |
ALL |
1876 |
9329203 |
By adding a flange, the bend on the other side of the part almost vanished |
NX_SHEET_METAL |
FLANGE |
ALL |
1876 |
9348613 |
Error during multi-flange depending on the selection sequence. |
NX_SHEET_METAL |
FLANGE |
ALL |
1876 |
9358567 |
Selection Scope in Routing Qualify Part limited to Within Work Part Only |
ROUTING_GENERAL |
PART |
QUALIFY_PART |
1876 |
9364407 |
insert multiple flange failed |
NX_SHEET_METAL |
FLANGE |
ALL |
1876 |
9364527 |
Qualify Part does not allow selection in Entire Assembly anymore |
ROUTING_GENERAL |
PART |
QUALIFY_PART |
1876 |
9365209 |
Wrong result with Multi-flange feature in NX 12.0.2 |
NX_SHEET_METAL |
FLANGE |
ALL |
1876 |
9375954 |
Measuring width of Flanges not accurate |
NX_SHEET_METAL |
FLANGE |
ALL |
1876 |
9383478 |
Regression: selection scope cannot be changed anymore |
ROUTING_GENERAL |
PART |
QUALIFY_PART |
1876 |
9384160 |
thread depth not displayed correctly on model |
DESIGN |
FEATURE_MODEL |
HOLE |
1876 |
9417958 |
Internal error memory access violation when opening NX assembly |
ASSEMBLIES |
ASSEMBLY_MODEL |
COMP_REPLACE |
1876 |
9462163 |
Connected Ports are displayed when selecting a run |
ROUTING_GENERAL |
RUN_NAVIGATOR |
FIND_RUN |
1876 |
9462264 |
MFK (Remove object type from non-default domain) |
NXMANAGER |
FILE_SAVE_AS |
NEW_ITEM |
1876 |
9466471 |
Components do not highlight in Component Navigator after changing applications. |
ROUTING_ELEC |
COMPONENT_LIST |
SELECT_ALL |
1876 |
9475101 |
NC: NXMGR: On save NX is creating second ug part named reference |
NXMANAGER |
FILE_SAVE |
ALL |
1876 |
9479055 |
Display node numbers |
CAE |
ADV_SIMULATION |
NODE_OPERATIONS |
1876 |
9489746 |
RCPs get deleted at corners in logical routing. |
ROUTING_GENERAL |
PATH |
SIMPLIFY_PATH |
1876 |
9498486 |
Plate type Edge reinforcement loses central Alignment |
SHIP_DESIGN |
STEEL_FEATURES |
EDGE_RNFC |
1876 |
9502378 |
Activating Solutions takes long time NX had to be killed from Task Manager |
CAE |
ADV_SIMULATION |
ELEMENT_PROPS |