Version |
PR Number |
Description |
Application |
Function |
Sub Function |
1876 |
1986895 |
Step file cannot be imported - Invalid toroidal_surface definition. |
TRANSLATOR |
STEP_AP214 |
IMPORT_GEOMETRY |
1876 |
8387207 |
Bumper pendulum placed at wrong contact point |
KDA |
GENERAL_PACKAGE |
BUMPER |
1876 |
8396322 |
STEP Import abort |
TRANSLATOR |
STEP_AP214 |
IMPORT_ASSEMBLY |
1876 |
8408779 |
Misleading deprecated notes in NX12 Routing APV XML and README files |
ROUTING_GENERAL |
ADMINISTRATION |
NXOPEN |
1876 |
8418943 |
Suppress Beta version of NX message |
BETA_EAP |
ARCHITECTURE |
ALL |
1876 |
8560541 |
HTML report does not work for an assembly with bundles |
FLEXIBLE_PIPE |
GENERAL |
ALL |
1876 |
9064202 |
Different Position between Tool_Tip and Tool_Mount is not honored inside Sys-Tr |
TC_FEATURES |
RESOURCE_MGR |
AUTO_ASSEMBLY |
1876 |
9071549 |
FPC Design App - Attach bodies to flex and bring them along when flattening |
FLEX_PC_DESIGN |
PREFERENCES |
ALL |
1876 |
9213628 |
Flange: Corner Relief partly removes Bend from opposite side |
NX_SHEET_METAL |
FLANGE |
ALL |
1876 |
9281984 |
Internal error with Make Unique |
NXMANAGER |
MAKE_UNIQUE |
ALL |
1876 |
9287087 |
After Flange creation the Flange width is no more the same (-0 002 mm) |
NX_SHEET_METAL |
FLANGE |
ALL |
1876 |
9314631 |
Sheet Metal Flange is always too small in the model |
NX_SHEET_METAL |
FLANGE |
ALL |
1876 |
9326801 |
CAE JT missing faces |
CAE |
ADV_SIMULATION |
POST_JT |
1876 |
9327215 |
Sheet Metal Flange is always too small in the model |
NX_SHEET_METAL |
FLANGE |
ALL |
1876 |
9329203 |
By adding a flange a bend on the others side of the part is almost vanished |
NX_SHEET_METAL |
FLANGE |
ALL |
1876 |
9348613 |
Error during multi-flange depending on the selection sequence. |
NX_SHEET_METAL |
FLANGE |
ALL |
1876 |
9358567 |
Selection Scope in Routing Qualify Part limited to Within Work Part Only |
ROUTING_GENERAL |
PART |
QUALIFY_PART |
1876 |
9364407 |
insert multiple flange failed |
NX_SHEET_METAL |
FLANGE |
ALL |
1876 |
9364527 |
Qualify Part does not allow selection in Entire Assembly anymore |
ROUTING_GENERAL |
PART |
QUALIFY_PART |
1876 |
9365209 |
Wrong result with Multi-flange feature in NX 12.0.2 |
NX_SHEET_METAL |
FLANGE |
ALL |
1876 |
9375954 |
Measuring width of Flanges not accurate |
NX_SHEET_METAL |
FLANGE |
ALL |
1876 |
9383478 |
Regression: selection scope cannot be changed anymore |
ROUTING_GENERAL |
PART |
QUALIFY_PART |
1876 |
9384160 |
thread depth not displayed correctly on model |
DESIGN |
FEATURE_MODEL |
HOLE |
1876 |
9417958 |
Internal error memory access violation when opening NX assembly |
ASSEMBLIES |
ASSEMBLY_MODEL |
COMP_REPLACE |
1876 |
9462163 |
Connected Ports are displayed when selecting a run |
ROUTING_GENERAL |
RUN_NAVIGATOR |
FIND_RUN |
1876 |
9462264 |
MFK (Remove object type from non-default domain) |
NXMANAGER |
FILE_SAVE_AS |
NEW_ITEM |
1876 |
9466471 |
Components do not highlight in Component Navigator after changing applications. |
ROUTING_ELEC |
COMPONENT_LIST |
SELECT_ALL |
1876 |
9475101 |
NC: NXMGR: On save NX is creating second ug part named reference |
NXMANAGER |
FILE_SAVE |
ALL |
1876 |
9479055 |
Display node numbers |
CAE |
ADV_SIMULATION |
NODE_OPERATIONS |
1876 |
9489746 |
RCPs get deleted at corners in logical routing. |
ROUTING_GENERAL |
PATH |
SIMPLIFY_PATH |
1876 |
9498486 |
Plate type Edge reinforcement loses central Alignment |
SHIP_DESIGN |
STEEL_FEATURES |
EDGE_RNFC |
1876 |
9502378 |
Activating Solutions takes long time NX had to be killed from Task Manager |
CAE |
ADV_SIMULATION |
ELEMENT_PROPS |