/*
uf_wave.h
File Description:
This is the Open API interface to WAVE. These routines allow you to
manipulate linked features and delayed update control.
These routines are typically used with routines in uf_so.h. In particular,
assy_ctxt_xforms are smart objects created using routines in that file.
Linked features rely on data from other parts. In some cases, therefore,
the UF_WAVE_xxx routines may require data from parts that are not loaded.
Where the data is being created or modified, the part is automatically
loaded first. However, where the data is only needed for an enquiry
routine, memory considerations mean it may not be appropriate to load the
part, if it is not already loaded. Hence the enquiry routines have been
provided with an allow_load argument, which controls whether parts are
loaded if necessary to supply the data wanted, or if an error
(UF_WAVE_data_not_loaded) is given instead.
****************************************************************************/
#ifndef UF_WAVE_INCLUDED
#define UF_WAVE_INCLUDED
/****************************************************************************
***************************************************************************/
#include <uf_defs.h>
#include <uf_retiring.h>
#include <uf_wave_types.h>
#include <libufun_exports.h>
/****************************************************************************
Definitions and Prototypes for the Open API interface routines for
the WAVE extract features functionality.
Note on Error Handling: All functions return a failure code of non zero
if an error is encountered. A descriptive message associated with
a failure code can be obtained by calling UF_get_fail_message with
the failure code as the argument.
***************************************************************************=*/
/******************************************************************************
* P R O T O T Y P E D E F I N I T I O N S *
******************************************************************************/
/*****************************************************************************
Create a linked body feature, and its associated body. The source
body must not be an occurrence, but can be in any part. It can be
either a solid body or a sheet body. Its part is fully loaded if
necessary, as is the destination part of the feature.
In order to avoid the potential performance issue when multiple linked
features are being created, it is required that the application call UF_MODL_update()
once after the linked features have been created using UF_WAVE_xxx
function calls.
Environment: Internal and External
See Also:
History:
******************************************************************************/
extern UFUNEXPORT int UF_WAVE_create_linked_body (
const tag_t body ,/* <I>
The body which is the source geometry of
the new linked body feature.
*/
const tag_t xform ,/* <I>
The transform which determines the position of the linked
feature relative to its source geometry. Must be NULL_TAG
(create position independent link) or an assy_ctxt_xform in the
same part as object_in_part whose to_part_occ contains body.
*/
const tag_t object_in_part ,/* <I>
Determines the part within which the new
feature is made.
*/
const logical update_at_timestamp ,/* <I>
If update_at_timestamp is true, the linked
body feature updates at a time determined
by its creation timestamp. If it is false, it
updates after its source body is completely
generated.
*/
tag_t * linked_feature /* <O>
The tag of the new linked body feature.
*/
);
/*****************************************************************************
Create a linked datum feature, and its associated datum in the same
part as object_in_part. The source datum must not be an occurrence,
but can be in any part, except that linked datum features must be
interpart. It can be a datum axis or a datum plane. Its part is fully
loaded if necessary, as is the destination part of the feature.
Note that a datum is not affected by the update of later features, so an
update_at_timestamp argument would not affect the behavior of a
linked datum.
It is required that the application call UF_MODL_update() once after the
linked datum features have been created. See UF_WAVE_create_linked_body for
more clarification.
Environment: Internal and External
See Also:
History:
******************************************************************************/
extern UFUNEXPORT int UF_WAVE_create_linked_datum (
const tag_t datum ,/* <I>
The datum plane or axis which is the source
geometry of the new linked datum feature.
*/
const tag_t xform ,/* <I>
The transform which determines the
position of the linked feature relative to its
source geometry. Must be NULL_TAG
(create position independent link) or an
assy_ctxt_xform in the same part as
object_in_part whose to_part_occ contains
datum. Linked datums must be interpart.
*/
const tag_t object_in_part ,/* <I>
Determines the part within which the new
feature is made.
*/
tag_t * linked_feature /* <O>
The tag of the new linked datum feature.
*/
);
/*****************************************************************************
Create a linked sketch feature, and its associated sketch, in the same
part as object_in_part. The source sketch must not be an occurrence,
and must not have been created using the old (pre-v13) sketcher, but
can be in any part, except that linked sketch features must be
interpart. Its part is fully loaded if necessary, as is the destination part
of the feature.
Note that a sketch is not affected by the update of later features, so an
update_at_timestamp argument would not affect the behavior of a
linked sketch.
It is required that the application call UF_MODL_update() once after the
linked sketch features have been created. See UF_WAVE_create_linked_body for
more clarification.
Environment: Internal and External
See Also:
History:
******************************************************************************/
extern UFUNEXPORT int UF_WAVE_create_linked_sketch (
const tag_t sketch ,/* <I>
The sketch which is the source geometry of
the new linked sketch feature.
*/
const tag_t xform ,/* <I>
The transform which determines the
position of the linked feature relative to its
source geometry. Must be NULL_TAG
(create position independent link) or an
assy_ctxt_xform in the same part as
object_in_part whose to_part_occ contains
sketch. Linked sketches must be interpart.
*/
const tag_t object_in_part ,/* <I>
Determines the part within which the new
feature is made.
*/
tag_t * linked_feature /* <O>
The tag of the new linked sketch feature.
*/
);
/*****************************************************************************
Create a linked string feature, and its associated curves, in the same
part as object_in_part. The source must either be an intersection curve
feature, a projection curve feature, an offset curve feature, or a solid
face. It can be in any part, except that linked string features must be
interpart. Its part is fully loaded if necessary, as is the destination part
of the feature.
A string feature's definition is not affected by the update of
later features, so an update_at_timestamp argument would not affect
the behavior of a linked string.
It is required that the application call UF_MODL_update() once after the
linked string features have been created. See UF_WAVE_create_linked_body for
more clarification.
Environment: Internal and External
See Also:
History: In V15.0, this function was enhanced to accept a solid face for the
source string.
******************************************************************************/
extern UFUNEXPORT int UF_WAVE_create_linked_string (
const tag_t string ,/* <I>
The string feature whose curves are the
source geometry of the new linked string
feature.
*/
const tag_t xform ,/* <I>
The transform which determines the
position of the linked feature relative to its
source geometry. Must be NULL_TAG
(create position independent link) or an
assy_ctxt_xform in the same part as
object_in_part whose to_part_occ contains
string. Linked strings must be interpart.
*/
const tag_t object_in_part ,/* <I>
Determines the part within which the new
feature is made.
*/
tag_t * linked_feature /* <O>
The tag of the new linked string feature.
*/
);
/*****************************************************************************
Create a linked face feature, and its associated sheet body in the same
part as object_in_part. The source face must not be an occurrence, but
can be in any part. Its part is fully loaded if necessary, as is the
destination part of the feature.
Environment: Internal and External
See Also:
History:
******************************************************************************/
extern UFUNEXPORT int UF_WAVE_create_linked_face (
const tag_t face ,/* <I>
The face which is the source geometry of
the new linked face feature.
*/
const tag_t xform ,/* <I>
The transform which determines the
position of the linked feature relative to its
source geometry. Must be NULL_TAG
(create position independent link) or an
assy_ctxt_xform in the same part as
object_in_part whose to_part_occ contains
face.
*/
const tag_t object_in_part ,/* <I>
Determines the part within which the new
feature is made.
*/
const logical update_at_timestamp ,/* <I>
If update_at_timestamp is true, the linked
face feature updates at a time determined
by its creation timestamp.
If it is false, it updates after its source
face's body is completely generated.
*/
tag_t * linked_feature /* <O>
The tag of the new linked face feature.
*/
);
/*****************************************************************************
Create a linked curve feature, and its associated curve in the same
part as object_in_part. The source curve must not be an occurrence,
but can be in any part. It can be a solid edge. Its part is fully loaded
if necessary, as is the destination part of the feature.
It is required that the application call UF_MODL_update() once after the
linked curve features have been created. See UF_WAVE_create_linked_body for
more clarification.
Environment: Internal and External
See Also:
History:
******************************************************************************/
extern UFUNEXPORT int UF_WAVE_create_linked_curve (
const tag_t curve ,/* <I>
The curve which is the source geometry of
the new linked curve feature.
*/
const tag_t xform ,/* <I>
The transform which determines the
position of the linked feature relative to its
source geometry. Must be NULL_TAG
(create position independent link) or an
assy_ctxt_xform in the same part as
object_in_part whose to_part_occ contains
curve.
*/
const tag_t object_in_part ,/* <I>
Determines the part within which the new
feature is made.
*/
const logical update_at_timestamp ,/* <I>
If true, the linked curve feature updates at
a time determined by its creation timestamp.
If it is false, it updates after its source
curve is completely generated.
*/
tag_t * linked_feature /* <O>
The tag of the new linked curve feature.
*/
);
/*****************************************************************************
Create a linked region feature, and its associated sheet body, in the
same part as object_in_part. The region includes all faces in the
seed_faces array, and all faces on the same solid that can be reached
from them without crossing any face in the boundary_faces array. All
faces in both arrays must be on the same solid, which can be in any
part. They cannot be occurrences. The source solid's part is fully
loaded if necessary, as is the destination part of the feature.
Boundary faces are not normally part of the created region, but if a
boundary face is a seed face as well, it is added to the region, though
it does not cause any of its adjacent faces to be added to the region. If
n_boundary_faces is 0, then all faces on the seed faces' solid are part
of the region. At present, there must only be one face in the
seed_faces array.
It is required that the application call UF_MODL_update() once after the
linked region features have been created. See UF_WAVE_create_linked_body for
more clarification.
Environment: Internal and External
See Also:
UF_WAVE_ask_link_region_sources
UF_WAVE_set_link_region_data
History:
******************************************************************************/
extern UFUNEXPORT int UF_WAVE_create_linked_region (
const int n_seed_faces ,/* <I>
The number of seed faces.
*/
const tag_t * seed_faces ,/* <I>
The array of seed faces.
*/
const int n_boundary_faces ,/* <I>
The number of boundary faces.
*/
const tag_t * boundary_faces ,/* <I>
The array of boundary faces.
*/
const tag_t xform ,/* <I>
The transform which determines the position of the linked
feature relative to its source geometry. Must be NULL_TAG
(apply no transformation) or an assy_ctxt_xform in the same
part as object_in_part whose to_part_occ contains the body.
*/
const tag_t object_in_part ,/* <I>
Determines the part within which the new
feature is made.
*/
const logical update_at_timestamp ,/* <I>
If true, the linked region feature updates at
a time determined by its creation timestamp.
If false, the feature updates after its
source faces body is completely generated.
*/
const logical traverse_interior_edges ,/* <I>
If true, the traversal algorithm passes
through holes in the body.
if false, it only passes over the outside
surface of the body.
*/
const logical delete_openings ,/* <I>
If true, any holes in the resulting sheet are
closed up; if false they are left.
*/
tag_t *linked_feature /* <O>
The tag of the new linked region feature.
*/
);
/*****************************************************************************
Creates a linked mirror body feature, and its associated body, in the
same part as object_in_body. The source body and mirror datum
plane must not be occurrences, but can be in any part or parts. Their
parts are fully loaded if necessary, as is the destination part of the
feature. The source body can be either a solid body or a sheet body.
It is required that the application call UF_MODL_update() once after the
linked mirror body features have been created. See UF_WAVE_create_linked_body for
more clarification.
Environment: Internal and External
See Also:
UF_WAVE_ask_link_mirror_data
UF_WAVE_set_link_mirror_data
History:
******************************************************************************/
extern UFUNEXPORT int UF_WAVE_create_linked_mirror (
const tag_t body ,/* <I>
The body which is the source geometry of
the new linked mirror body feature.
*/
const tag_t body_xform ,/* <I>
The transform which determines the
position of the linked feature relative to its
source body, before the reflection is
applied. Must be NULL_TAG (apply no
transformation) or an assy_ctxt_xform in
the same part as object_in_part whose
to_part_occ contains body.
*/
const tag_t datum_plane ,/* <I>
The datum plane which provides the plane
of reflection of the new linked mirror body
feature.
*/
const tag_t datum_xform ,/* <I>
The transform which determines the
position of the plane of reflection of the
linked feature relative to its source datum
plane. Must be NULL_TAG (apply no
transformation) or an assy_ctxt_xform
whose to_part_occ contains datum_plane.
*/
const tag_t object_in_part ,/* <I>
Determines the part within which the new
feature is made.
*/
const logical update_at_timestamp ,/* <I>
If true, the feature updates at its creation
timestamp. If false, the feature updates
after its source geometry is completely
generated.
*/
tag_t * linked_feature /* <O>
The tag of the new linked mirror feature.
*/
);
/*****************************************************************************
Create a linked routing port with its associated characteristics in the same
part as object_in_part. The parent/source port must not be an occurrence,
but can be in any part. The port to be linked can be of fitting, fixture,
multi or fabrication stock port type. The linked port will show up as a
LINKED_PORT feature and will always be positioned using the provided
assembly context xform object with respect to its parent. The source part
is fully loaded as necessary, as is the destination part.
Return :
Return code :
= 0 : sucessful
!= 0 : linking/extracting error
Environment: Internal and External
See Also:
History: New in V18.
******************************************************************************/
extern UFUNEXPORT int UF_WAVE_create_linked_route_port
(
const tag_t port , /* <I>
The port which is the source geometry of
the new linked port.
*/
const tag_t xform , /* <I>
The transform which determines the
position of the linked object relative to its
source geometry. Must be NULL_TAG
(apply no transformation) or an
assy_ctxt_xform in the same part as
object_in_part whose to_part_occ contains
curve.
*/
const tag_t object_in_part ,/* <I>
Determines the part within which the new
linked port copy is made.
*/
tag_t * linked_port_feature /* <O>
The tag of the new linked port feature.
*/
);
/*****************************************************************************
Create a linked routing segment, and its associated end control points
in the same part as object_in_part. The parent/source segment must not
be an occurrence, but can be in any part. This function extracts a
LINKED_CURVE feature in the work part from the parent segment and then
creates a routing segment as following the extracted LINKED_CURVE feature.
The end control points of the linked segment will be derived from
the end points of this extracted LINKED_CURVE feature. The "linked" segment
will always be positioned using the provided assembly context xform object
with respect to its parent. The source part is fully loaded as necessary,
as is the destination part.
NOTE: The actual linked geometry for a "linked" segment is the LINKED_CURVE.
The linked segment is just a smart segment in the work part that follows
the extracted LINKED_CURVE.
Return :
Return code :
= 0 : sucessful
!= 0 : linking/extracting error
Environment: Internal and External
See Also:
History: New in V18.
******************************************************************************/
extern UFUNEXPORT int UF_WAVE_create_linked_route_segment
(
const tag_t segment , /* <I>
The segment which is the source geometry of
the new linked segment.
*/
const tag_t xform , /* <I>
The transform which determines the
position of the linked object relative to its
source geometry. Must be NULL_TAG
(apply no transformation) or an
assy_ctxt_xform in the same part as
object_in_part whose to_part_occ contains
curve.
*/
const tag_t object_in_part ,/* <I>
Determines the part within which the new
linked segment copy is made.
*/
tag_t *linked_curve_feature,/* <O>
The tag of the LINKED_CURVE feature which the
linked segment follows.
*/
tag_t *linked_segment /* <O>
The tag of the segment that follows the
LINKED_CURVE
*/
);
/*****************************************************************************
Create a linked point feature, and its associated point, in the same
part as object_in_part, in a position corresponding to the source point.
The source point must not be an occurrence, but can be in any part,
except that linked point features must be interpart. Its part is fully
loaded if necessary.
The source point can either be an ordinary "dumb" point, or a smart
point, such as one created with an UF_SO_create_point_xxx routine.
The linked point updates after the source point has completely
updated.
Environment: Internal and External
See Also:
UF_WAVE_set_linked_pt_point
History:
******************************************************************************/
extern UFUNEXPORT int UF_WAVE_create_linked_pt_point (
const tag_t point ,/* <I>
The point which is the source geometry of
the new linked point feature.
*/
const tag_t xform ,/* <I>
Gives the transformation that is applied to
the source point to generate the linked
point. It must be NULL_TAG (create position
independent link) or an assy_ctxt_xform in
the same part as object_in_part whose
to_part_occ contains point.
*/
const tag_t object_in_part ,/* <I>
Determines the part within which the new
feature is made.
*/
tag_t * linked_feature /* <O>
The tag of the new linked point feature.
*/
);
/*****************************************************************************
Creates a linked point feature, and its associated point, in the same
part as object_in_part, in a position corresponding to the point on
curve indicated by the parameter (prm). The source curve
must not be an occurrence, but can be in any part, except that linked
point features must be interpart. Its part is fully loaded if necessary.
The linked point updates after the source curve (and its underlying
body, if any) has completely updated.
Environment: Internal and External
See Also:
UF_WAVE_set_linked_pt_curve
History:
******************************************************************************/
extern UFUNEXPORT int UF_WAVE_create_linked_pt_curve (
const tag_t curve ,/* <I>
The curve which defines the source
geometry of the new linked point feature.
*/
const tag_t prm ,/* <I>
The parameter (smart scalar) which defines
the position of the new linked point feature
along curve. It must be in the same part as
object_in_part.
*/
const tag_t xform ,/* <I>
Gives the transformation that is applied to
the point on the source curve to generate
the linked point. It must be NULL_TAG
(create position independent link) or an
assy_ctxt_xform in the same part as
object_in_part whose to_part_occ contains
curve.
*/
const tag_t object_in_part ,/* <I>
Determines the part within which the new
feature is made.
*/
tag_t * linked_feature /* <O>
The tag of the new linked point feature.
*/
);
/*****************************************************************************
Create a linked point feature, and its associated point, in the same
part as object_in_part, at the center of a source conic. The source
conic must not be an occurrence, but can be in any part, except that
linked point features must be interpart. Its part is fully loaded if
necessary, as is the destination part.
The linked point updates after the source conic (and its underlying
solid, if any) has completely updated.
Environment: Internal and External
See Also:
UF_WAVE_set_linked_pt_center
History:
******************************************************************************/
extern UFUNEXPORT int UF_WAVE_create_linked_pt_center (
const tag_t conic ,/* <I>
The conic whose center is the source
geometry of the new linked point feature.
*/
const tag_t xform ,/* <I>
Gives the transformation that is applied to
the center of the source curve to generate
the linked point. It must be NULL_TAG
(create position independent link) or an
assy_ctxt_xform in the same part as
object_in_part whose to_part_occ contains
conic.
*/
const tag_t object_in_part ,/* <I>
Determines the part within which the new
feature is made.
*/
tag_t * linked_feature /* <O>
The tag of the new linked point feature.
*/
);
/*****************************************************************************
Create a linked point feature, and its associated point, in the same
part as object_in_part, from a source arc and an angle (smart scalar)
along it. The source arc must not be an occurrence, but can be in any
part, except that linked point features must be interpart. Its part is
fully loaded if necessary.
The linked point updates after the source arc (and its underlying
body, if any) has completely updated.
Environment: Internal and External
See Also:
UF_WAVE_set_linked_pt_angle
History:
******************************************************************************/
extern UFUNEXPORT int UF_WAVE_create_linked_pt_angle (
const tag_t arc ,/* <I>
The arc which defines the source geometry
of the new linked point feature.
*/
const tag_t angle ,/* <I>
The angle (smart scalar) which defines the
position of the new linked point feature
around arc. It must be in the same part as
object_in_part. Its value is in radians.
*/
const tag_t xform ,/* <I>
The transform which determines the
position of the linked feature relative to its
source geometry. Must be NULL_TAG
(create position independent link) or an
assy_ctxt_xform in the same part as
object_in_part whose to_part_occ contains arc.
*/
const tag_t object_in_part ,/* <I>
Determines the part within which the new
feature is made.
*/
tag_t * linked_feature /* <O>
The tag of the new linked point feature.
*/
);
/*****************************************************************************
Creates a linked part of the specified name whose contents are all the
entities in the given smart part contained in ref_set. The linked part
has the same units as the source part. ref_set can be NULL_TAG, in
which case the entire contents of start_part are copied into the linked
part. ref_set cannot be the empty reference set. start_part is fully
loaded if necessary. This routine only runs if a WAVE licence is
available, but it does not use up that license.
Environment: Internal and External
See Also:
History: This function was originally released in V15.0.
******************************************************************************/
extern UFUNEXPORT int UF_WAVE_create_linked_part(
const tag_t start_part, /* <I>
Start part from which the linked part
is to be made.
*/
const tag_t ref_set, /* <I>
The reference set defining the entities
to be linked into the new linked part.
*/
char *linked_part_name, /* <I>
The name of the new linked part.
*/
tag_t *linked_part /* <O>
The tag of the new linked part.
*/
);
/*****************************************************************************
Given a linked feature, ask if the link is broken (i.e. does not have
access to all its source geometry, and hence cannot update). For
linked mirror features, lack of access to either the source solid or the
mirror datum plane means the link is broken.
A link can lack access to its source geometry because the source
geometry has been deleted, because the connecting xform's assembly
has been altered, or because the link has been explicitly broken,
including by reparenting it using UF_WAVE_set_link_data. A link is
NOT broken just because its source geometry is currently unloaded.
Environment: Internal and External
See Also:
UF_WAVE_set_link_data
UF_WAVE_accept_link_broken
UF_WAVE_ask_link_accept_broken
History:
******************************************************************************/
extern UFUNEXPORT int UF_WAVE_is_link_broken (
const tag_t linked_feature ,/* <I>
The linked feature whose broken status is
to be checked.
*/
logical * is_broken /* <O>
True if the feature is broken, false
otherwise.
*/
);
/***********************************************************************
Ask the current source entity (parent) of a linked feature. If the
source entity's part is not already fully loaded, it is fully loaded if
allow_load is true; otherwise, NULL_TAG is returned and an
appropriate error code is given. If the linked feature is broken, and
the source cannot be identified, NULL_TAG is returned. This
routine cannot be called for region or mirror linked features, which
have multiple source entities. It works for curves, sketches, strings,
datums, faces, bodies, and points; for points, the relevant point,
curve, conic or arc is returned.
Environment: Internal and External
See Also:
UF_WAVE_set_link_data
History:
******************************************************************************/
extern UFUNEXPORT int UF_WAVE_ask_link_source (
const tag_t linked_feature ,/* <I>
The linked feature whose source geometry
is wanted.
*/
const logical allow_load ,/* <I>
True if the source geometry's part can be
loaded, false otherwise.
*/
tag_t * source_entity /* <O>
The tag of the source geometry entity.
*/
);
/*****************************************************************************
Given a linked feature, ask the xform associated with it. This can be
NULL_TAG, a dumb xform (only possible for broken linked features), or an
assy_ctxt_xform. On a linked mirror feature, this returns the xform of the
reflected solid: use UF_WAVE_ask_link_mirror_data if the mirror datum plane's
xform is wanted. The xform is in the same part as the linked feature, and is
always loaded if the feature is.
Environment: Internal and External
See Also:
UF_WAVE_set_link_data
UF_WAVE_ask_link_mirror_data
History:
******************************************************************************/
extern UFUNEXPORT int UF_WAVE_ask_link_xform (
const tag_t linked_feature ,/* <I>
The linked feature whose xform is wanted.
*/
tag_t * xform /* <O>
The transform of the linked feature relative
to its source entity.
*/
);
/*****************************************************************************
Set the source entity, xform and update behavior of a linked feature.
This reparents it if the new source entity is different. The new source
entity must be of the same type as the previous source entity of the
linked feature, but it can be in a different part. It cannot be an
occurrence. It can be NULL_TAG, in which case the feature's link is
broken (and xform must also be NULL_TAG); this also accepts the
link as broken. The source entity's part is fully loaded if it is not
already fully loaded. The xform can be set to NULL_TAG (for an
identity transform) or any assy_ctxt_xform in the same part as the
linked feature. update_at_timestamp sets the update behavior of the
feature, in the same way as it does when a linked feature is created. It
has no effect if the link is being broken, or if the link is one of the link
types (sketches, strings, datums) with no update_at_timestamp option
at creation.
Linked datum axis features cannot be reparented to datum planes,
nor vice versa. This routine cannot be called for region or mirror
linked features, which have multiple source entities, nor for point
linked features, which have multiple definitions. It works for curves,
sketches, strings, datums, faces and bodies. Intersection curve strings,
projection curve strings, offset curve and face edge(s) strings can be
reparented to one another.
Environment: Internal and External
See Also:
UF_WAVE_ask_link_source
UF_WAVE_ask_link_xform
UF_WAVE_ask_link_update_time
History: In V15.0, this function was enhanced to allow reparenting for face
edge strings.
******************************************************************************/
extern UFUNEXPORT int UF_WAVE_set_link_data (
const tag_t linked_feature ,/* <I>
The linked feature whose properties are to
be set.
*/
const tag_t source_entity ,/* <I>
The tag of the new source geometry; can be
NULL_TAG, in which case the link is
broken.
*/
const tag_t xform ,/* <I>
The new transform which determines the
position of the linked feature relative to its
source geometry. Must be NULL_TAG
(identity transform) or an assy_ctxt_xform
in the same part as linked_feature whose
to_part_occ contains source_entity.
*/
const logical update_at_timestamp /* <I>
If true, the linked feature now updates at
its timestamp. If false, the feature now
updates after its source geometry has
updated.
*/
);
/*****************************************************************************
Ask the current seed faces and boundary faces of a linked region
feature, and the current values of the traverse_interior_edges and
delete_openings logicals. seed_faces and boundary_faces are allocated
arrays, and should both be freed afterwards with UF_free. If the part
containing the source faces is not already fully loaded, it is fully
loaded if allow_load is true; otherwise n_seed_faces and
n_boundary_faces are set to 0, seed_faces and boundary_faces are
empty, the logicals are set to false, and an appropriate error is given.
If the link is currently broken and the source data is not available, the
same default argument values are returned, though with an return
value of 0.
Environment: Internal and External
See Also:
UF_WAVE_create_linked_region
UF_WAVE_set_link_region_data
History:
******************************************************************************/
extern UFUNEXPORT int UF_WAVE_ask_link_region_sources (
const tag_t linked_feature ,/* <I>
The linked region feature whose source
geometry is wanted.
*/
const logical allow_load ,/* <I>
True if the source geometry's part can be
loaded, false otherwise.
*/
int * n_seed_faces ,/* <O>
The number of seed faces.
*/
tag_t ** seed_faces ,/* <OF>
The array of tags of the seed faces. This must
be freed by calling UF_free.
*/
int * n_boundary_faces ,/* <O>
The number of boundary faces.
*/
tag_t ** boundary_faces ,/* <OF>
The array of tags of the boundary faces. This must
be freed by calling UF_free.
*/
logical * traverse_interior_edges ,/* <O>
True if the traversal algorithm passes
through holes in the body; false if it only
passes over the outside surface of the body.
*/
logical * delete_openings /* <O>
True if any holes in the resulting sheet are
closed up; false if they are left.
*/
);
/*****************************************************************************
Sets the seed faces, boundary faces, xform and
traverse_interior_edges and delete_openings logicals of a linked
region feature. This reparents it if the faces are changed.
n_seed_faces is the length of the array seed_faces, which gives the new
seed faces for the region feature. n_boundary_faces is the length of
the array boundary_faces, which gives the new boundary faces for the
region feature. All faces in the input arrays have to be in the same
body, which need not be in the same part as the previous sources of
the feature. The part containing the body is fully loaded if it is not
already fully loaded. The xform can be set to NULL_TAG or any
assy_ctxt_xform in the same part as the linked_feature whose
to_part_occ contains the body. If n_seed_faces and n_boundary_faces
are both 0, the feature's link is broken (and xform must also be
NULL_TAG). This also accepts the link as broken. The
update_at_timestamp argument sets the update behavior of the
feature, in the same way as it does when a linked feature is created. It
is ignored if the link is being broken. At present, there must only be
one face in the seed_faces array, unless the link is being broken.
Environment: Internal and External
See Also:
UF_WAVE_create_linked_region
UF_WAVE_ask_link_region_sources
History:
******************************************************************************/
extern UFUNEXPORT int UF_WAVE_set_link_region_data (
const tag_t linked_feature ,/* <I>
The linked region feature whose properties
are to be set.
*/
const int n_seed_faces ,/* <I>
The number of seed faces; can be 0, in
which case the link is broken.
*/
const tag_t * seed_faces ,/* <I>
The array of seed faces.
*/
const int n_boundary_faces ,/* <I>
The number of boundary faces.
*/
const tag_t * boundary_faces ,/* <I>
The array of boundary faces.
*/
const tag_t xform ,/* <I>
The new transform which determines the
position of the linked region feature
relative to its source geometry. Must be
NULL_TAG (identity transform) or an
assy_ctxt_xform in the same part as
linked_feature.
*/
const logical update_at_timestamp ,/* <I>
If true, the linked region feature now
updates at its timestamp. If false, the
feature now updates after its source
geometry has updated.
*/
const logical traverse_interior_edges ,/* <I>
If true, the traversal algorithm now
pass es through holes in the body; if
false, it now only passes over the
outside surface of the body.
*/
const logical delete_openings /* <I>
If true, any holes in the resulting sheet are
now closed up, if false they are now left.
*/
);
/*****************************************************************************
Ask the current source body and mirror datum plane of a linked
mirror feature, and the associated xform of each. If the source body's
part is not already fully loaded, it is fully loaded if allow_load is true;
otherwise, NULL_TAG is returned for all arguments and an
appropriate error is given. The same applies to the mirror datum
plane's part. If the link is currently broken, NULL_TAG may be
returned in one or more of the arguments, and the body_xform and
datum_xform arguments may be dumb xforms.
Environment: Internal and External
See Also:
UF_WAVE_create_linked_mirror
UF_WAVE_set_link_mirror_data
History:
******************************************************************************/
extern UFUNEXPORT int UF_WAVE_ask_link_mirror_data (
const tag_t linked_feature ,/* <I>
The linked mirror feature whose source
geometry and xforms are wanted.
*/
const logical allow_load ,/* <I>
True if the source geometry's part can be
loaded, false otherwise.
*/
tag_t * source_body ,/* <O>
The body which is the source geometry of
the linked mirror body feature.
*/
tag_t * body_xform ,/* <O>
The transform which determines the
position of the linked feature relative to its
source body.
*/
tag_t * datum_plane ,/* <O>
The datum plane which provides the plane
of reflection of the linked mirror body
feature.
*/
tag_t * datum_xform /* <O>
The transform which determines the
position of the plane of reflection of the
linked feature relative to its source datum
plane.
*/
);
/*****************************************************************************
Set the source body, mirror datum plane and associated xforms of a
linked mirror feature. This reparents it if the body or plane are
different. The new source entities can be in different parts from the
old ones, and need not be in the same part as one another. Their
parts are fully loaded if they are not already fully loaded. body_xform
and datum_xform can be set to NULL_TAG or any assy_ctxt_xform in
the same part as the linked_feature. If source_body and datum_plane
are both NULL_TAG, the links to the previous source body and
mirror datum plane are broken (and body_xform and datum_xform
must both also be NULL_TAG). This also accepts the link as broken.
It is not possible to set only one of source_body and datum_plane to
NULL_TAG. The update_at_timestamp argument sets the update
behavior of the feature, in the same way as it does when a linked
feature is created. It is ignored if the link is being broken.
Environment: Internal and External
See Also:
UF_WAVE_ask_link_mirror_data
UF_WAVE_create_linked_mirror
History:
******************************************************************************/
extern UFUNEXPORT int UF_WAVE_set_link_mirror_data (
const tag_t linked_feature ,/* <I>
The linked mirror feature whose properties
are to be set.
*/
const tag_t source_body ,/* <I>
The body which is the new source geometry
of the linked mirror body feature; can be
NULL_TAG, in which case the link is
broken.
*/
const tag_t body_xform ,/* <I>
The new transform which determines the
position of the linked feature relative to its
source body, before the reflection is
applied. Must be NULL_TAG (identity
transform) or an assy_ctxt_xform in the
same part as linked_feature whose
to_part_occ contains source_body.
*/
const tag_t datum_plane ,/* <I>
The datum plane which provides the new
plane of reflection of the linked mirror
body feature; can be NULL_TAG, in which
case the link is broken.
*/
const tag_t datum_xform ,/* <I>
The new transform which determines the
position of the plane of reflection of the
linked feature relative to its source datum
plane. Must be NULL_TAG (identity
transform) or an assy_ctxt_xform in the
same part as linked_feature whose
to_part_occ contains datum_plane.
*/
const logical update_at_timestamp /* <I>
If true, the feature updates at its
timestamp. If false, the feature updates
after its source geometry has updated.
*/
);
/*****************************************************************************
Sets a linked point feature to be based on an existing point and an
xform. This reparents it if the point is different. The existing point
can be in a different part from the previous parent. The existing
point's part is fully loaded if it is not already fully loaded. xform can
be set to NULL_TAG or any assy_ctxt_xform in the same part as the
linked point feature. If point is NULL_TAG, the link to the previous
parent is broken (and xform must also be NULL_TAG). This also
accepts the link as broken. Note that any linked point can be
reparented with this routine, even if its previous parent was not an
existing point.
Environment: Internal and External
See Also:
UF_WAVE_create_linked_pt_point
History:
******************************************************************************/
extern UFUNEXPORT int UF_WAVE_set_linked_pt_point (
const tag_t linked_feature ,/* <I>
The linked point feature whose properties
are to be set.
*/
const tag_t point ,/* <I>
The point which is the new source geometry
of the linked point feature; can be
NULL_TAG, in which case the link is
broken.
*/
const tag_t xform /* <I>
The new transform which determines the
position of the linked point feature relative
to its source geometry. Must be
NULL_TAG or an assy_ctxt_xform in the
same part as linked_feature whose
to_part_occ contains point.
*/
);
/*****************************************************************************
Sets a linked point feature to be based on a parameterized point on a
curve and an xform. This reparents it if the curve is different. The
curve can be in a different part from the previous parent. The curve's
part will be fully loaded if it is not already fully loaded. The
parameter is given by a smart scalar, which must be in the same part
as the linked point feature. xform can be set to NULL_TAG or any
assy_ctxt_xform in the same part as the linked point feature whose
to_part_occ contains curve. If curve is NULL_TAG, the link to the
previous parent is broken (and xform and t must also be
NULL_TAG). This also accepts the link as broken. Note that any
linked point can be reparented with this routine, even if its previous
parent was not a point on a curve.
Environment: Internal and External
See Also:
UF_WAVE_create_linked_pt_curve
History:
******************************************************************************/
extern UFUNEXPORT int UF_WAVE_set_linked_pt_curve (
const tag_t linked_feature ,/* <I>
The linked point feature whose properties
are to be set.
*/
const tag_t curve ,/* <I>
The curve which defines the new source
geometry of the linked point feature.
*/
const tag_t prm ,/* <I>
The parameter (smar scalar) which defines
the position of the linked point feature
along curve. It must be in the same part as
linked_feature.
*/
const tag_t xform /* <I>
The new transform which determines the
position of the linked point feature relative
to its source geometry. Must be
NULL_TAG or an assy_ctxt_xform in the
same part as linked_feature whose
to_part_occ contains curve.
*/
);
/*****************************************************************************
Sets a linked point feature to be based on the center of a conic and an
xform. This reparents it if the conic is different. The conic can be in a
different part from the previous parent. The conic's part will be fully
loaded if it is not already fully loaded. xform can be set to
NULL_TAG or any assy_ctxt_xform in the same part as the linked
point feature whose to_part_occ contains conic. If conic is
NULL_TAG, the link to the previous parent is broken (and xform
must also be NULL_TAG). This also accepts the link as broken. Note
that any linked point can be reparented with this routine, even if its
previous parent was not the center of a conic.
Environment: Internal and External
See Also:
UF_WAVE_create_linked_pt_center
History:
******************************************************************************/
extern UFUNEXPORT int UF_WAVE_set_linked_pt_center (
const tag_t linked_feature ,/* <I>
The linked point feature whose properties
are to be set.
*/
const tag_t conic ,/* <I>
The conic whose center is the new source
geometry of the linked point feature.
*/
const tag_t xform /* <I>
The new transform which determines the
position of the linked point feature relative
to its source geometry. Must be
NULL_TAG or an assy_ctxt_xform in the
same part as linked_feature whose
to_part_occ contains conic.
*/
);
/*****************************************************************************
Sets a linked point feature to be based on an angle on an arc and an
xform. This reparents it, if the arc is different. The arc can be in a
different part from the previous parent. The arc's part is fully loaded
if it is not already fully loaded. The angle is given (in radians) by a
smart scalar, which must be in the same part as the linked point
feature. xform can be set to NULL_TAG or any assy_ctxt_xform in
the same part as the linked point feature whose to_part_occ contains
arc. If arc is NULL_TAG, the link to the previous parent is broken
(and xform and angle must also be NULL_TAG). This will also
accept the link as broken. Note that any linked point can be
reparented with this routine, even if its previous parent was not an
angle on an arc.
Environment: Internal and External
See Also:
UF_WAVE_create_linked_pt_angle
History:
******************************************************************************/
extern UFUNEXPORT int UF_WAVE_set_linked_pt_angle (
const tag_t linked_feature ,/* <I>
The linked point feature whose properties
are to be set.
*/
const tag_t arc ,/* <I>
The arc which defines the new source
geometry of the linked point feature.
*/
const tag_t angle ,/* <I>
The angle (smart scalar) which defines the
position of the linked point feature around
arc. It must be in the same part as
linked_feature. Its value is in radians.
*/
const tag_t xform /* <I>
The new transform which determines the
position of the linked point feature relative
to its source geometry. Must be
NULL_TAG (identity transform) or an
assy_ctxt_xform in the same part as
linked_feature whose to_part_occ contains
arc.
*/
);
/*****************************************************************************
Ask the parameter of a linked point feature that is positioned with a
parameter on a curve. Any other linked point, including a broken
linked point, returns NULL_TAG as the parameter.
Environment: Internal and External
See Also:
UF_WAVE_create_linked_pt_curve
UF_WAVE_set_linked_pt_curve
History: This function was originally released in V15.0
******************************************************************************/
extern UFUNEXPORT int UF_WAVE_ask_linked_pt_curve_prm(
const tag_t linked_feature, /* <I>
The linked point feature whose parameter is
wanted.
*/
tag_t *prm /* <O>
The tag of the parameter (smart scalar)
which defines the position of the linked point
feature along its defining curve.
*/
);
/*****************************************************************************
Returns the angle of a linked point feature that is positioned with an
angle on an arc. Any other linked point, including a broken linked
point, will return NULL_TAG as the angle.
Environment: Internal and External
See Also:
UF_WAVE_create_linked_pt_angle
UF_WAVE_set_linked_pt_angle
History: This function was originally released in V15.0
******************************************************************************/
extern UFUNEXPORT int UF_WAVE_ask_linked_pt_angle(
const tag_t linked_feature, /* <I>
The linked point feature whose angle is
wanted.
*/
tag_t *angle /* <O>
The tag of the angle (smart scalar) which
defines the position of the linked point
feature around its defining arc.
*/
);
/*****************************************************************************
Queries when a linked feature updates. For linked features which
update at a particular timestamp (update_at_timestamp set to true at
creation or reparenting), the tag of the feature after which the linked
feature updates is returned. For linked features which update after
their source has updated completely (update_at_timestamp set to false
at creation or reparenting), and for linked features whose type has no
specified update behavior (sketches, strings, datums and points),
NULL_TAG is returned. If the timestamp feature is not loaded, the
behavior is controlled by the allow_load argument. If it is true, the
timestamp feature's part is fully loaded; if it is false, an appropriate
error code is returned.
Environment: Internal and External
See Also:
UF_WAVE_set_link_update_time
History:
******************************************************************************/
extern UFUNEXPORT int UF_WAVE_ask_link_update_time (
const tag_t linked_feature ,/* <I>
The linked feature whose timestamp
feature is wanted.
*/
const logical allow_load ,/* <I>
True if the source geometry's part can be
loaded, false otherwise.
*/
tag_t * timestamp_feature /* <O>
The timestamp feature of the linked
feature.
*/
);
/*****************************************************************************
Given a linked feature, sets when it is to update. Pass in NULL_TAG
as timestamp_feature to specify that the linked feature update after its
source has updated completely. Pass in a feature tag as
timestamp_feature to specify the feature after which the linked feature
is to update. For those linked features whose type has no specified
update behavior (sketches, strings, datums and points), this routine
can be called, but has no effect. For solid, face, region, mirror and
edge-based curve linked features, the timestamp feature must be
part of the same solid as the source geometry, and must have a
timestamp later than the feature that created that geometry. This
routine cannot be called for extractions (linked features linked within
a single part), nor for linked features whose source is unavailable. If
the linked feature is later reparented, its timestamp feature is
overridden.
Environment: Internal and External
See Also:
UF_WAVE_ask_link_update_time
History:
******************************************************************************/
extern UFUNEXPORT int UF_WAVE_set_link_update_time (
const tag_t linked_feature ,/* <I>
The linked feature whose timestamp
feature is to be set.
*/
const tag_t timestamp_feature /* <I>
The new timestamp feature of the linked
feature.
*/
);
/*****************************************************************************
Accept that a linked feature is broken. This routine cannot be called
on unbroken linked features, and returns an error if this is attempted.
Once this routine has been called, the linked feature continues to be
accepted as broken until it is no longer broken at some later time;
when the feature becomes unbroken, its accepted-as-broken status
is automatically removed.
Environment: Internal and External
See Also:
UF_WAVE_set_link_data
UF_WAVE_is_link_broken
UF_WAVE_ask_link_accept_broken
History:
******************************************************************************/
extern UFUNEXPORT int UF_WAVE_accept_link_broken (
const tag_t linked_feature /* <I>
The linked feature to be accepted as
broken.
*/
);
/*****************************************************************************
Ask if a linked feature is broken and has been accepted as such, either
by UF_WAVE_accept_link_broken or from the WAVE user interface.
Returns false for any unbroken linked feature. Also returns false for a
feature that had been accepted, but has since become unbroken and
then rebroken again.
Environment: Internal and External
See Also:
UF_WAVE_set_link_data
UF_WAVE_is_link_broken
UF_WAVE_accept_link_broken
History:
******************************************************************************/
extern UFUNEXPORT int UF_WAVE_ask_link_accept_broken (
const tag_t linked_feature ,/* <I>
The linked feature whose
accepted-as-broken status is wanted.
*/
logical * is_accepted /* <O>
The accepted status of the given linked feature.
*/
);
/*****************************************************************************
Returns the tag of the linked entity created by the given linked
feature. For linked bodies, faces, mirrors, and regions the linked sheet
or solid body is returned. For linked sketches, the linked sketch entity
is returned. For linked points, curves and datums the linked entity is
returned. For linked strings, which do not create a single linked
entity, NULL_TAG is returned. This routine works even if the link is
currently broken.
Environment: Internal and External
See Also:
UF_WAVE_ask_link_source
History: This function was originally released in V15.0
******************************************************************************/
extern UFUNEXPORT int UF_WAVE_ask_linked_feature_geom(
const tag_t linked_feature, /* <I>
The linked feature whose geometry is
wanted.
*/
tag_t *linked_geom /* <O>
The tag of the entity created by the
linked feature.
*/
);
/*****************************************************************************
Returns arrays of the source geometry used by the linked feature and
the linked geometry created by it when given a linked feature. The
arrays are in the same order, so can be used to find the linked
geometry corresponding to specific source geometry, or vice versa.
n_map_items gives the total length of each array.
The arrays should both be freed afterwards with UF_free(). For
linked bodies, faces, mirrors and regions all the linked faces and edges
are mapped, except for any that no longer have associated geometry
in the linked feature. For features that create a sheet body, the linked
faces and all the edges joining or bounding them are mapped. The
arrays list all the faces first and then all the edges. For linked
sketches and strings, all the curves in the source sketch or string are
mapped. This routine returns an appropriate error code if passed a
linked point, datum, or curve. If the link is currently broken and the
source data is not available, n_map_items is set to 0. If the source
data's part is not already fully loaded, it is fully loaded if allow_load is
true; otherwise, 0 or NULL is returned for all arguments and an
appropriate error code is given.
Instead of making repeated calls to UF_WAVE_map_source_to_link_geom or
UF_WAVE_map_link_geom_to_source, it is more efficient to use this
routine and use qsort and bsearch to look through the returned arrays.
Environment: Internal and External
See Also:
UF_WAVE_map_source_to_link_geom
UF_WAVE_map_link_geom_to_source
History: This function was originally released in V15.0
******************************************************************************/
extern UFUNEXPORT int UF_WAVE_ask_linked_feature_map(
const tag_t linked_feature, /* <I>
The linked feature whose geometry map
is wanted.
*/
const logical allow_load, /* <I>
True if the source geometry's part can
be loaded, false otherwise.
*/
int *n_map_items, /* <O>
The number of source and linked
entities in the arrays
*/
tag_t **source_geom, /* <OF>
The tags of the entities composing the
source geometry. This array must be
freed by calling UF_free.
*/
tag_t **linked_geom /* <OF>
The corresponding tags of the entities
created by the linked feature. This
array must be freed by calling UF_free.
*/
);
/*****************************************************************************
Given a linked feature and geometry belonging to its source, return
the corresponding linked geometry created by the linked feature. For
linked bodies, faces, mirrors and regions any of the faces or edges can
be mapped. For linked sketches and strings, any of the source curves
can be mapped. This routine returns an appropriate error code if
passed a linked point, datum, or curve. If geometry that does not form
part of the source of the linked feature is passed in, NULL_TAG is
returned. NULL_TAG is also returned if the geometry is part of the
source, but its associated linked geometry no longer exists in the
linked feature (for instance, it has been removed by a later feature
applied to the linked geometry).
Environment: Internal and External
See Also:
UF_WAVE_ask_linked_feature_map
UF_WAVE_map_link_geom_to_source
History: This function was originally released in V15.0
******************************************************************************/
extern UFUNEXPORT int UF_WAVE_map_source_to_link_geom(
const tag_t linked_feature, /* <I>
The linked feature whose linked
geometry is wanted.
*/
const tag_t source_geom, /* <I>
The tag of the entity contained in the
source geometry
*/
tag_t *linked_geom /* <O>
The tag of the corresponding entity
created by the linked feature.
*/
);
/*****************************************************************************
Given a linked feature and geometry created by it, return the
corresponding geometry in its source. For linked bodies, faces,
mirrors and regions any of the faces or edges can be mapped. For
linked sketches and strings, any of the source curves can be mapped.
This routine returns an appropriate error code if passed a linked
point, datum, or curve. If geometry that does not form part of the
linked feature is passed in, or if the link is currently broken and the
source data is not available, NULL_TAG is returned. This routine is
likely to be slower than UF_WAVE_map_source_to_link_geom, and so
should be used with caution. If the source data's part is not already
fully loaded, it is fully loaded if allow_load is true; otherwise,
NULL_TAG is returned and an appropriate error code is given.
Environment: Internal and External
See Also:
UF_WAVE_ask_linked_feature_map
UF_WAVE_map_source_to_link_geom
History: This function was originally released in V15.0
******************************************************************************/
extern UFUNEXPORT int UF_WAVE_map_link_geom_to_source(
const tag_t linked_feature, /* <I>
The linked feature whose source geometry
is wanted.
*/
const tag_t linked_geom, /* <I>
The tag of the entity created by the
linked feature.
*/
const logical allow_load, /* <I>
True if the source geometry's part can
be loaded, false otherwise.
*/
tag_t *source_geom /* <O>
The tag of the corresponding entity
contained in the source geometry.
*/
);
/******************************************************************************
Functions for controlling interpart update.
******************************************************************************/
/****************************************************************************
Assigns the delay status to the current NX session. Setting
session delay to true means that interpart objects do not update in the
current session. Setting session delay to false updates any
non-frozen, out of date parts in the session. This may require
loading of partially loaded out of date parts.
Environment: Internal and External
See Also:
History:
****************************************************************************/
extern UFUNEXPORT int UF_WAVE_set_session_delay(
logical delayed /* <I>
True if you want the session to be delayed false if
you want it to be undelayed.
*/
);
/***************************************************************************
Determines if the session has interpart update delayed, and sets the
delayed parameter to true if so, false otherwise.
Environment: Internal and External
See Also:
History:
****************************************************************************/
extern UFUNEXPORT int UF_WAVE_ask_session_delay(
logical * delayed /* <O>
True if the session is currently delayed.
*/
);
/****************************************************************************
Updates non-frozen, out of date parts in the session. If an out of date
part is partially loaded, it is fully loaded and updated.
Environment: Internal and External
See Also:
History:
****************************************************************************/
extern UFUNEXPORT int UF_WAVE_update_session( void );
/***************************************************************************
Returns the parts currently loaded in the session that are out of date.
Environment: Internal and External
See Also:
History:
****************************************************************************/
extern UFUNEXPORT int UF_WAVE_ask_out_of_date_parts(
int * n_parts ,/* <O>
Number of out of date parts in session.
*/
tag_t ** parts /* <OF>
Array of tags of parts that are out of date. Use
UF_free to deallocate memory.
*/
);
/***************************************************************************
Gets an array of objects that are out of date in the given part.
Environment: Internal and External
See Also:
History:
****************************************************************************/
extern UFUNEXPORT int UF_WAVE_ask_out_of_date_objects(
tag_t part ,/* <I>
The part that may contain out of date objects
*/
int * n_objects ,/* <O>
Number of out of date objects in the part.
*/
tag_t ** objects /* <OF>
Array of tags of objects that are out of date. Use
UF_free to deallocate memory when done.
*/
);
/****************************************************************************
Updates a set of out of date parts. This updates frozen parts. If a part
in the array is partially loaded (and it's out of date) it is fully loaded in
order to allow for the update.
In order to run, this routine requires the existence of at least
one WAVE license. The function does not use a license, but requires
that one is installed. If a WAVE license is not installed, this function
returns an error.
Environment: Internal and External
See Also:
History:
****************************************************************************/
extern UFUNEXPORT int UF_WAVE_update_parts(
int n_parts ,/* <I>
Number of parts to update.
*/
tag_t * parts /* <I>
Array of tags of parts to update.
*/
);
/***************************************************************************
Freezes a set of parts from interpart update in the current session.
Environment: Internal and External
See Also:
History:
***************************************************************************/
extern UFUNEXPORT int UF_WAVE_freeze(
int n_parts ,/* <I>
Number of parts to freeze
*/
tag_t * parts /* <I>
Array of tags of parts to freeze.
*/
);
/*****************************************************************************
Freezes a set of parts from interpart update persistently. Persistently
frozen parts are marked frozen so that they do not update (once saved
in this state) in any session they are subsequently loaded into.
Environment: Internal and External
See Also:
History:
*****************************************************************************/
extern UFUNEXPORT int UF_WAVE_freeze_persistently(
int n_parts ,/* <I>
Number of parts to freeze persistently.
*/
tag_t * parts /* <I>
Array of tags of parts to freeze persistently.
*/
);
/****************************************************************************
Unfreezes a set of frozen parts. If parts in the array are not frozen,
they are not changed. This function works on both frozen and
persistently frozen parts.
Environment: Internal and External
See Also:
History:
****************************************************************************/
extern UFUNEXPORT int UF_WAVE_unfreeze(
int n_parts ,/* <I>
Number of parts to unfreeze.
*/
tag_t * parts /* <I>
Array of tags of parts to unfreeze.
*/
);
/*
enum for the delay status of a part.
*/
enum UF_WAVE_delay_status_e
{
UF_WAVE_not_delayed = 0, /* The part is not delayed. */
UF_WAVE_session_delayed, /* The part is delayed because geometry and expressions are delayed. */
UF_WAVE_session_frozen, /* The part is frozen in this session. */
UF_WAVE_persistent_frozen, /* The part is frozen for all sessions. */
UF_WAVE_not_in_assembly_delayed, /* The part is delayed because it's not in the displayed assembly */
UF_WAVE_assembly_constraints_delayed /* The part is delayed because assembly constraints are delayed */
};
typedef enum UF_WAVE_delay_status_e UF_WAVE_delay_status_t;
/****************************************************************************
Determines the delay status assigned to a given part.
Environment: Internal and External
See Also:
UF_WAVE_delay_status_t
History:
*****************************************************************************/
extern UFUNEXPORT int UF_WAVE_ask_delay_status(
tag_t part ,/* <I>
Tag of part for which to get delay status.
*/
UF_WAVE_delay_status_t * delay_status /* <O>
Delay status of the part.
*/
);
/*****************************************************************************
Load find and load the WAVE parent parts of a given part file. This will also
load parent parts for any Mating Conditions of Interpart Expressions
Environment: Internal and External
See Also:
******************************************************************************/
extern UFUNEXPORT int UF_WAVE_load_parents(
tag_t part, /* <I>
Tag of the part for which to load the parts of
*/
int parent_option, /* <I>
This is the WAVE load option as described in
uf_assem_types.h
UF_ASSEM_none Don't load any non-loaded parents, but
fully load partially loaded parents.
UF_ASSEM_immediate Only load the immediate parents
(First-level parents)
UF_ASSEM_all Recursively load parents, and parents of
parents until there are no more parents
left to load.
*/
int *n_failures, /* <O>
Number of parent parts that failed to load
*/
char ***failing_parts, /* <OF>
Names of the parts that failed to load
Use UF_free_string_array to deallocate memory when done.
*/
int **failing_statuses /* <OF>
Error codes for the failures in corresponding order
Use UF_free to deallocate memory when done.
*/
);/* */
/*****************************************************************************
This routine makes a copy of the parent part as the new part name in the same
assembly as the parent part. Any linked features that are in the parent part
will still be maintained in the new part.
This routine is similar to performing a save-as except that the linked objects
will not become dumb to assembly position.
An update is required after the call to UF_WAVE_copy_component_as to position
the new component and resolve the links.
Environment: Internal and External
See Also:
******************************************************************************/
extern UFUNEXPORT int UF_WAVE_copy_component_as (
const tag_t source_part_occurrence, /* <I>
The part occurrence that is being copied
*/
const char *source_part_name, /* <I>
The component part name that is to be copied
*/
const char *new_part_name, /* <I>
The new component part name that will exist in the
current assembly.
*/
const char *reference_set_name, /* <I>
Name of reference set to use from component
parts. The refset_name cannot exceed 30
characters, cannot include a directory path,
and should not have a file extension.
*/
const char *instance_name, /* <I>
Name of new instance The instance_name cannot
exceed 30 characters, cannot include a
directory path, and should not have a file
extension.
*/
double transform[4][4], /* <I>
The transform to apply to the new component
*/
tag_t *new_instance, /* <O>
The new instance tag created in the assembly
*/
tag_t *new_part /* <O>
The new part tag that is a copy of parent part.
*/
);
/*****************************************************************************
This routine gets the part file name for the broken link's source part, if it
is available.
A link may be broken either because the relation to the source geometry is severed (e.g. the source geometry
is deleted or the link becomes non-associative to the source geometry by hitting the "break link" icon") or
the link's context has changed. In the latter case, the source geometry information still exists. Therefore,
it can be returned provided that the source part is either fully or partially loaded in the session.
This function will return the source part for a broken link provided that (1) the break occurred only because
the link's context changed and (2) the source part is at least partially loaded. In all other other cases, no
source part is returned. The absence of this information is not an error.
Environment: Internal and External
See Also:
*****************************************************************************/
extern UFUNEXPORT int UF_WAVE_ask_broken_link_source_part( tag_t broken_link, /* <I> */
char **part_name, /* The part name for the source of the link <OF> */
char ** source_object_handle /* The handle for the source part <OF>*/ );
/***********************************************************************
Initialize UF_WAVE_linked_feature_info_s data structure.
Environment: Internal and External
See Also:
UF_WAVE_free_linked_feature_info
History: New in NX3.0.2 after the Release
******************************************************************************/
extern UFUNEXPORT int UF_WAVE_init_linked_feature_info(
UF_WAVE_linked_feature_info_p_t name_store /* <I>
Pointer to the data structure.
*/
);
/***********************************************************************
Free memory allocated in UF_WAVE_linked_feature_info_s data structure.
Environment: Internal and External
See Also:
UF_WAVE_free_linked_feature_info
History: New in NX3.0.2 after the Release
******************************************************************************/
extern UFUNEXPORT int UF_WAVE_free_linked_feature_info(
UF_WAVE_linked_feature_info_p_t name_store /* <I>
Pointer to the data structure.
*/
);
/***********************************************************************
Given the tag of a linked geometry, ask the name of its associated feature,
the name of its owning part, and the name of its source part if the link
is not broken. If the link is broken then the source_part_name field
in the UF_WAVE_linked_feature_info_s structure will be NULL. Also note that for
linked mirrors the source_part_name consists of both the owning part name
of the parent feature and the owning part name of the mirror plane.
Environment: Internal and External
See Also:
UF_WAVE_init_linked_feature_info
UF_WAVE_free_linked_feature_info
UF_WAVE_ask_link_source
History: New in NX3.0.2 after the Release
******************************************************************************/
extern UFUNEXPORT int UF_WAVE_ask_linked_feature_info(
const tag_t linked_geom , /* <I>
Tag of the linked geometry.
*/
UF_WAVE_linked_feature_info_p_t name_store /* <OF>
The names of the associated feature, owning part,
and the source part.
Use UF_WAVE_init_linked_feature_info to initailize before
calling this function.
Use UF_WAVE_free_linked_feature_info to free the memory.
*/
);
/***********************************************************************
Given the tag of a xform, this routine will return whether the xform is
PILO(Position Independent) or not.
Environment: Internal and External
See Also:
History: New in NX5.0
******************************************************************************/
extern UFUNEXPORT logical UF_WAVE_is_pilo_xform(
tag_t xform /* <I>
Tag of the xform.
*/
);
/******************************************************************************
Convert legacy (before NX9) linked features and linked expressions to use new
functionality of Product Interface object.
This function will also convert the legacy Product Interface objects in the
assembly or used by the linked objects if the source part is not a component
of the assembly.
User needs to fully load all their assembly parts and the source parts and turn
off interpart update delay before calling this function to convert.
This is temporary and will be retired in NX11.
Environment: Internal
See Also:
History: NX9.0.3
******************************************************************************/
extern UFUNEXPORT int UF_WAVE_convert_links_to_use_product_interface();
#undef EXPORTLIBRARY
#endif /* UF_WAVE_INCLUDED */