UF_UGMGR_clone_auto_trans_f_t (view source)
Defined in: uf_ugmgr.h
Overview
Purpose: An autotranslate function suitable for use during Clone based
Import/Export. The function receives the name to be translated
in old_name. If this is a cli form name, the function should
return a corresponding native part file name in new_name,
otherwise it should return a cli style name in new_name.
The return value of the function should be an error status,
currently recogni ed error statuses are:
0 - Success
5 - Invalid File Name
6 - Part name Exceeds maximum length
int UF_UGMGR_clone_auto_trans_f_t
(
const char [ MAX_FSPEC_BUFSIZE ] ,
char [ MAX_FSPEC_BUFSIZE ]
)
const char[MAX_FSPEC_BUFSIZE] | | Input | : receives the name to be translated, which will be either an NX Manager CLI form name (indicating an export operation) or a native file system specification (indicating an import operation) |
char[MAX_FSPEC_BUFSIZE] | | Output | : Returns the translated name, if old_name was an NX Manager CLI form name, this should be a native file system name, if old_name was a native file system specification, this should be a NX Manager CLI form name. |
UF_UGMGR_new_alternate_part_no_fn_t (view source)
Defined in: uf_ugmgr_types.h
int UF_UGMGR_new_alternate_part_no_fn_t
(
UF_UGMGR_new_alternate_part_no_p_t
)
UF_UGMGR_new_alternate_part_no_p_t | | Input | |
UF_UGMGR_new_dataset_name_fn_t (view source)
Defined in: uf_ugmgr_types.h
int UF_UGMGR_new_dataset_name_fn_t
(
UF_UGMGR_new_dataset_name_p_t
)
UF_UGMGR_new_dataset_name_p_t | | Input | |
UF_UGMGR_new_id_fn_t (view source)
Defined in: uf_ugmgr_types.h
int UF_UGMGR_new_id_fn_t
(
UF_UGMGR_new_id_p_t
)
UF_UGMGR_new_part_no_fn_t (view source)
Defined in: uf_ugmgr_types.h
int UF_UGMGR_new_part_no_fn_t
(
UF_UGMGR_new_part_no_p_t
)
UF_UGMGR_new_part_no_p_t | | Input | |
UF_UGMGR_new_part_rev_fn_t (view source)
Defined in: uf_ugmgr_types.h
int UF_UGMGR_new_part_rev_fn_t
(
UF_UGMGR_new_part_rev_p_t
)
UF_UGMGR_new_part_rev_p_t | | Input | |
UF_UGMGR_saveas_dataset_info_fn_t (view source)
Defined in: uf_ugmgr_types.h
int UF_UGMGR_saveas_dataset_info_fn_t
(
UF_UGMGR_saveas_dataset_info_p_t
)
UF_UGMGR_saveas_dataset_info_p_t | | Input | |
UF_UGMGR_validate_dataset_name_fn_t (view source)
Defined in: uf_ugmgr_types.h
int UF_UGMGR_validate_dataset_name_fn_t
(
UF_UGMGR_validate_dataset_name_p_t
)