UF_PLOT_cmp_color_width_e (view source)
Defined in: uf_plot.h
Also known as:
- UF_PLOT_cmp_color_width_t
Data Members
UF_PLOT_CMP_COLOR_WIDTH = 1
UF_PLOT_CMP_NO_COLOR_WIDTH
UF_PLOT_colors_e (view source)
Defined in: uf_plot_types.h
Also known as:
- UF_PLOT_colors_t
- UF_PLOT_colors_p_t
Overview
This enumerated type provides the selection of what colors are to be used
to render the display, drawing sheets without custom colors, and drawing
sheets when use_drawing_sheet_colors is FALSE.
Data Members
UF_PLOT_AS_DISPLAYED_COLORS
UF_PLOT_PART_COLORS
UF_PLOT_CUSTOM_PALETTE_COLORS
UF_PLOT_BLACK_ON_WHITE
UF_PLOT_LEGACY_COLORS
UF_PLOT_COLOR_BY_WIDTH
UF_PLOT_create_cmp_result_plot_e (view source)
Defined in: uf_plot.h
Also known as:
- UF_PLOT_create_cmp_result_plot_t
Overview
This enum is used as an option for when to create a results plot
when calling UF_PLOT_compare_ughpgl_files. The results plot will
always contain the entire image, regardless of which option is selected.
Data Members
UF_PLOT_CREATE_CMP_PLOT = 1
UF_PLOT_CREATE_CMP_PLOT_DIFF_ONLY
UF_PLOT_CREATE_CMP_NO_PLOT
UF_PLOT_diff_cmp_status_e (view source)
Defined in: uf_plot.h
Also known as:
- UF_PLOT_diff_cmp_status_t
Data Members
UF_PLOT_CMP_NO_DIFF_FOUND = 0
UF_PLOT_CMP_DIFF_FOUND
UF_PLOT_format_e (view source)
Defined in: uf_plot_types.h
Also known as:
- UF_PLOT_format_t
- UF_PLOT_format_p_t
Overview
This enumerated type provides the selection of the type of file to create
when converting files.
Data Members
UF_PLOT_CGM_FORMAT
UF_PLOT_EMF_FORMAT
UF_PLOT_TIFF_FORMAT
UF_PLOT_JPEG_FORMAT
UF_PLOT_PNG_FORMAT
UF_PLOT_rotation_e (view source)
Defined in: uf_plot_types.h
Also known as:
- UF_PLOT_rotation_t
- UF_PLOT_rotation_p_t
Overview
This enumerated type provides the selection of the rotation a plot is to
have when placed in the layout.
Data Members
UF_PLOT_ROTATION_0
UF_PLOT_ROTATION_90
UF_PLOT_ROTATION_180
UF_PLOT_ROTATION_270
UF_PLOT_units_e (view source)
Defined in: uf_plot_types.h
Also known as:
- UF_PLOT_units_t
- UF_PLOT_units_p_t
Overview
This enumerated type provides the units selection where needed. It is
initialized to be cognate to the values of UF_PART_METRIC and UF_PART_ENGLISH.
Data Members
UF_PLOT_MILLIMETERS = 1
UF_PLOT_INCHES
UF_PLOT_widths_e (view source)
Defined in: uf_plot_types.h
Also known as:
- UF_PLOT_widths_t
- UF_PLOT_widths_p_t
Overview
This enumerated type provides the selection of what line widths are to be used
to render the display, drawing sheets without custom widths, and drawing sheets
when use_drawing_sheet_widths is FALSE.
Data Members
UF_PLOT_STANDARD_WIDTHS
UF_PLOT_SINGLE_WIDTH
UF_PLOT_CUSTOM_3_WIDTHS
UF_PLOT_CUSTOM_PALETTE_WIDTHS