UF_PART_export_exp_mode_e (view source)
 
Defined in: uf_part_types.h
 
Also known as:
 
Overview
Type which describes how expressions should be processed during an
export operation:


Data Members

UF_PART_copy_exp_deeply
Expressions will be copied deeply.
If an expression references another
expression in the same part, then
that referenced expression will also
be copied. (However any referenced
expressions in a different part will
not be copied.)

UF_PART_copy_exp_shallowly
Expressions will be copied shallowly.
If an expression references another
expression, the copy of the
referencing expression will reference
the same referenced expression. This
happens for both inter-part and
intra-part references to expressions.

 


 
UF_PART_export_params_mode_e (view source)
 
Defined in: uf_part_types.h
 
Also known as:
 
Overview
Type which describes how solid parameters should be processed during
an export operation,
NOTE: UF_PART_maintain_all_params is a newly introduced option in V15.0.

The behaviours of UF_PART_maintain_params and UF_PART_remove_params
are the same in V15.0 as in earlier releases.


Data Members

UF_PART_maintain_params
Solid parameters should be maintained
during the export operation. Note that
with this option, solid parameters will
NOT be copied if they depend upon other
objects for their validity unless those
other objects are going to be copied
anyway.

UF_PART_remove_params
Solid parameters will be removed during
the export operation. Solids copied
into the destination part will have no
solid parameters.

UF_PART_maintain_all_params
All solid parameters should be
maintained during the export
operation. All solid parameters in
the source objects will be copied into
the destination objects. Note that
extra objects which are required to
maintain the validity of the
parameters will be copied too.

 


 
UF_PART_load_state_e (view source)
 
Defined in: uf_part_types.h
 
Also known as:
 
Overview
Type which describes the part load state.


Data Members

UF_PART_not_loaded = 0
Part is not loaded

UF_PART_fully_loaded
Part is fully loaded

UF_PART_partially_loaded
Part is partially loaded

UF_PART_minimally_loaded
Part is minimally loaded