/*
uf_modl_trex.h
File description:
Open API modeling routines to create, edit and inquire about blends.
*****************************************************************************/
#ifndef UF_MODL_TREX_H_INCLUDED
#define UF_MODL_TREX_H_INCLUDED
/***************************************************************************
***************************************************************************/
#include <uf_defs.h>
#include <uf_modl_types.h>
#include <libufun_exports.h>
enum UF_MODL_TREX_algorithm_e
{
UF_MODL_TREX_ALGORITHM_NONE=0,
UF_MODL_TREX_ALGORITHM_COUNT, /* Insert new versions above this line */
UF_MODL_TREX_ALGORITHM_CURRENT=UF_MODL_TREX_ALGORITHM_COUNT - 1
};
enum UF_MODL_TREX_extend_method_e
{
UF_MODL_TREX_C2=0,
UF_MODL_TREX_LINEAR,
UF_MODL_TREX_REFLECTED,
UF_MODL_TREX_NATURAL
};
typedef enum UF_MODL_TREX_extend_method_e
UF_MODL_TREX_extend_method_t;
enum UF_MODL_TREX_to_option_e
{
UF_MODL_TREX_DISTANCE=0,
UF_MODL_TREX_PERCENT,
UF_MODL_TREX_SURFACE
};
typedef enum UF_MODL_TREX_to_option_e
UF_MODL_TREX_to_option_t;
enum UF_MODL_TREX_region_option_e
{
UF_MODL_TREX_KEEP=0,
UF_MODL_TREX_REMOVE
};
typedef enum UF_MODL_TREX_region_option_e
UF_MODL_TREX_region_option_t;
/*
* Trim extend target/tool dataset
*/
struct UF_MODL_TREX_data_set_s
{
tag_t collector;
double extend_val;
double offset_val;
int reversed;
};
typedef struct UF_MODL_TREX_data_set_s
UF_MODL_TREX_data_set_t, *UF_MODL_TREX_data_set_p_t;
/*
* Trim extend application data
*/
struct UF_MODL_TREX_appl_data_s
{
int num_targets; /* Number of target data sets */
UF_MODL_TREX_data_set_p_t *targets; /* Array of target data sets */
int num_tools; /* Number of tool data sets */
UF_MODL_TREX_data_set_p_t *tools; /* Array of tool data sets */
UF_MODL_TREX_extend_method_t extend_method; /* Extend method */
UF_MODL_TREX_to_option_t to_option; /* To option */
UF_MODL_TREX_region_option_t region_option; /* Region option */
int make_corner; /* Make corner flag */
int keep_boundaries; /* Keep boundaries flag */
int extract_sheets; /* Extract sheets flag */
double dist_tol; /* Distance Tolerance */
int algorithm_version; /* Future Use */
};
typedef struct UF_MODL_TREX_appl_data_s
UF_MODL_TREX_appl_data_t, *UF_MODL_TREX_appl_data_p_t;
/********************************************************************
Creates a trim and extend feature.
This is a complete interface to create a trim/extend feature. Extends the
target by a given distance or until a target. If extended until a tool then
the target will be trimmed by the tool and optionally can modify the tool
also to make a corner between the target and the tool.
Following types of collectors allowed for a target and tool.
1. A connected set of free edges
2. A connected set of faces
a) Could be a whole sheet body
b) A connected set of faces of a sheet body
The collector is a Smart Container. For edges the collector should be created
with UF_MODL_create_smart_wireframe_container. For faces the collector should
be created with UF_MODL_create_smart_face_container.
For now only "Body Faces" are allowed for face collectors.
In case of "connected set of free edges" required extension distances are
computed internally. No extensions are done if they are "a set of faces".
If successful, it returns the tag for the feature created. If not successful,
it returns a valid error code.
Return:
0 : if successful
!=0 : if there is a failure. Refer to TREX_* error codes in in uf_modl_error.h.
Environment: Internal and External
See Also: UF_MODL_TREX_ask_trim_extend
History: Originally released in NX 2.0.1
********************************************************************/
extern UFUNEXPORT int UF_MODL_TREX_create_trex_feature
(
UF_MODL_TREX_appl_data_p_t feature_data, /* <I> : Pointer to the structure
containing defining data for
the trim extend operation
*/
tag_t* feature /* <O> : trim extend feature identifier
*/
);
/********************************************************************
Edits a trim and extend feature.
Edits the parameters of a trim/extend feature. All the creation parameters are available
for editing also. One can query for the creation parameters by calling UF_MODL_TREX_ask_trim_extend.
Return:
0 : if successful
!=0 : if there is a failure. Refer to TREX_* error codes in in uf_modl_error.h.
Environment: Internal and External
See Also: UF_MODL_TREX_ask_trim_extend
History: Originally released in NX 2.0.1
********************************************************************/
extern UFUNEXPORT int UF_MODL_TREX_edit_trex_feature
(
UF_MODL_TREX_appl_data_p_t feature_data, /* <I> Pointer to the structure
containing defining data
for the trimextend operation
*/
tag_t feature /* <I> Offset curve on face
identifier
*/
);
/********************************************************************
Queries a trim and extend feature.
Returns the creation data for a trim / extend feature. Refer to UF_MODL_trex_input_p_t for
detailed information on the contents.
If successful, it returns the input data associated with the feature. If not successful,
it returns a valid error code.
Return:
0 : if successful
!=0 : if there is a failure. Refer to TREX_* error codes in in uf_modl_error.h.
Environment: Internal and External
See Also: UF_MODL_TREX_edit_trex_feature
UF_MODL_TREX_free_trex_data
History: Originally released in NX 2.0.1
********************************************************************/
extern UFUNEXPORT int UF_MODL_TREX_ask_trim_extend
(
tag_t feature, /* <I> The trim/extend feature tag */
UF_MODL_TREX_appl_data_p_t feature_data /* <OF> The feature data */
);
/********************************************************************
Initializes the trim and extend feature input data.
Return:
0 : if successful
!=0 : if there is a failure. Refer to TREX_* error codes in in uf_modl_error.h.
Environment: Internal and External
See Also: UF_MODL_TREX_ask_trim_extend
History: Originally released in NX 2.0.1
********************************************************************/
extern UFUNEXPORT int UF_MODL_TREX_init_trex_data
(
UF_MODL_TREX_appl_data_p_t feature_data
);
/********************************************************************
Initializes the trim and extend target tool data set.
Return:
0 : if successful
!=0 : if there is a failure. Refer to TREX_* error codes in in uf_modl_error.h.
Environment: Internal and External
History:
********************************************************************/
extern UFUNEXPORT int UF_MODL_TREX_init_trex_data_set
(
UF_MODL_TREX_data_set_p_t feature_data_set
);
/********************************************************************
Frees the trim and extend feature input data.
Return:
0 : if successful
!=0 : if there is a failure. Refer to TREX_* error codes in in uf_modl_error.h.
Environment: Internal and External
See Also: UF_MODL_TREX_ask_trim_extend
History: Originally released in NX 2.0.1
********************************************************************/
extern UFUNEXPORT int UF_MODL_TREX_free_trex_data
(
UF_MODL_TREX_appl_data_p_t feature_data
);
#undef EXPORTLIBRARY
#endif /* UF_MODL_TREX_H_INCLUDED */