UF_DRF_begin_line_fn_t (view source)
Defined in: uf_drf_types.h
Overview
Callbacks for UF_DRF_render_text. Default set is used for other functions.
Each return either UF_DRF_RENDER_OK or
UF_DRF_RENDER_CANNOT_RENDER_CHAR (UF_DRF_draw_char_fn_t only) or
UF_DRF_RENDER_CANNOT_RENDER_SYMBOL (UF_DRF_draw_user_symbol_fn_t only).
If a cannot render or not drawn status is returned for a user symbol or an
individual character, the resultant object will be stroked.
Lines are output as polyline segments bracketed by calls to
the begin and end line functions.
UF_DRF_render_text_status_t UF_DRF_begin_line_fn_t
(
void * client
)
void * | client | Input | client data |
UF_DRF_draw_arc_fn_t (view source)
Defined in: uf_drf_types.h
UF_DRF_render_text_status_t UF_DRF_draw_arc_fn_t
(
double center [ 3 ] ,
double radius,
double start_param,
double end_param,
void * client
)
double | center [ 3 ] | Input | center point in coord system of annotation |
double | radius | Input | radius of arc |
double | start_param | Input | start angle in radians |
double | end_param | Input | end angle in radians |
void * | client | Input | client data |
UF_DRF_draw_char_fn_t (view source)
Defined in: uf_drf_types.h
UF_DRF_render_text_status_t UF_DRF_draw_char_fn_t
(
double origin [ 3 ] ,
unsigned char character,
void * client
)
double | origin [ 3 ] | Input | text_origin coord system of annotation |
unsigned char | character | Input | character (possibly multi-byte)to be drawn |
void * | client | Input | client data |
UF_DRF_draw_standard_font_string_fn_t (view source)
Defined in: uf_drf_types.h
Overview
Function called to render a text string using a standard font for UF_DRF_render_table_t
when the use_standard_font_string_fn UF_DRF_render_table_t flag is set.
This function should be used with the text mode set to UF_TEXT_ALL_UTF8.
Data returned by this function may be outside the user's locale mode.
UF_DRF_render_text_status_t UF_DRF_draw_standard_font_string_fn_t
(
const char* textString,
const double origin [ 3 ] ,
int fontId,
double textAngle,
double fontSize,
double gapSize,
double aspectRatio,
logical suppressKerning,
logical vertical,
logical bold,
logical italic,
void * client
)
const char* | textString | Input | Text string to display. If the text mode is UF_TEXT_LOCALE then the '#' character will be returned for each character that is outside the user's locale mode. Note that text control sequence symbols displayed using standard fonts may return characters that are defined outside the user's locale. |
const double | origin [ 3 ] | Input | Origin of text baseline |
int | fontId | Input | Standard font number |
double | textAngle | Input | Text angle |
double | fontSize | Input | Character height to use for standard font. This is the actual size used when using the FreeType Font library. Note that this differs from the NX character height. |
double | gapSize | Input | Size of spacing between characters |
double | aspectRatio | Input | Aspect ratio to use for display |
logical | suppressKerning | Input | True to not use kerning when rendering |
logical | vertical | Input | True to draw in vertical direction |
logical | bold | Input | True if using bold style |
logical | italic | Input | True if using italic style |
void * | client | Input | Client data |
UF_DRF_draw_to_position_fn_t (view source)
Defined in: uf_drf_types.h
Overview
The input parameter 'last_out_point' will be set to the 'out_point' output
argument of the previous UF_DRF_set_to_position_fn_t or UF_DRF_draw_to_position_fn_t
call. It is up to the client to decide what the 'out_point' means to the
UF_DRF_set_position_fn_t and UF_DRF_draw_to_position_fn_t that they have
implemented.
The input parameter 'last_status' will be set to the 'out_status' output
argument of the previous UF_DRF_set_to_position_fn_t or UF_DRF_draw_to_position_fn_t
call. It is up to the client to decide what the 'out_status' means to the
UF_DRF_set_position_fn_t and UF_DRF_draw_to_position_fn_t that they have
implemented.
UF_DRF_render_text_status_t UF_DRF_draw_to_position_fn_t
(
double in_point [ 3 ] ,
double last_out_point [ 3 ] ,
logical last_status,
void * client,
double out_point [ 3 ] ,
logical * out_status
)
double | in_point [ 3 ] | Input | 3d point in coord system of annotation |
double | last_out_point [ 3 ] | Input | 'out_point' from the previous UF_DRF_set_to_position_fn_t or UF_DRF_draw_to_position_fn_t call |
logical | last_status | Input | 'out_status' from the previous UF_DRF_set_to_position_fn_t or UF_DRF_draw_to_position_fn_t call |
void * | client | Input | client data |
double | out_point [ 3 ] | Output | passed into the next UF_DRF_draw_to_position_fn_t call as the 'last_out_point' input argument. This argument will only be returned if UF_DRF_RENDER_OK or UF_DRF_RENDER_DRAWN is returned by this function |
logical * | out_status | Output | passed into the next UF_DRF_draw_to_position_fn_t call as the 'last_status' input argument. This argument will only be returned if UF_DRF_RENDER_OK or UF_DRF_RENDER_DRAWN is returned by this function |
UF_DRF_draw_user_symbol_fn_t (view source)
Defined in: uf_drf_types.h
UF_DRF_render_text_status_t UF_DRF_draw_user_symbol_fn_t
(
char * symbol_name,
double origin [ 3 ] ,
void * symbol_params,
void * client
)
char * | symbol_name | Input | name of user defined symbol to render |
double | origin [ 3 ] | Input | |
void * | symbol_params | Input | |
void * | client | Input | client data |
UF_DRF_end_line_fn_t (view source)
Defined in: uf_drf_types.h
UF_DRF_render_text_status_t UF_DRF_end_line_fn_t
(
void * client
)
void * | client | Input | client data |
UF_DRF_fill_region_fn_t (view source)
Defined in: uf_drf_types.h
UF_DRF_render_text_status_t UF_DRF_fill_region_fn_t
(
int num_points,
double * points,
double fill_dist,
double last_pt [ 3 ] ,
logical * was_drawn,
void * client
)
int | num_points | Input | number of points in region |
double * | points | Input | array of 3d points |
double | fill_dist | Input | fill distance |
double | last_pt [ 3 ] | Output | last on screen point |
logical * | was_drawn | Output | return TRUE if anything drawn |
void * | client | Input | client data |
UF_DRF_pop_orientation_fn_t (view source)
Defined in: uf_drf_types.h
UF_DRF_render_text_status_t UF_DRF_pop_orientation_fn_t
(
void * client
)
void * | client | Input | client data |
UF_DRF_push_orientation_fn_t (view source)
Defined in: uf_drf_types.h
UF_DRF_render_text_status_t UF_DRF_push_orientation_fn_t
(
double matrix [ 9 ] ,
void * client
)
double | matrix [ 9 ] | Input | orientation matrix |
void * | client | Input | client data |
UF_DRF_set_cfw_fn_t (view source)
Defined in: uf_drf_types.h
UF_DRF_render_text_status_t UF_DRF_set_cfw_fn_t
(
UF_DRF_cfw_p_t cfw,
void * client
)
UF_DRF_cfw_p_t | cfw | Input | new color, line font and line width |
void * | client | Input | client data |
UF_DRF_set_to_position_fn_t (view source)
Defined in: uf_drf_types.h
UF_DRF_render_text_status_t UF_DRF_set_to_position_fn_t
(
double in_point [ 3 ] ,
void * client,
double out_point [ 3 ] ,
logical * out_status
)
double | in_point [ 3 ] | Input | 3d point in coord system of annotation |
void * | client | Input | client data |
double | out_point [ 3 ] | Output | passed into the next UF_DRF_draw_to_position_fn_t call as the 'last_out_point' input argument. This argument will only be returned if UF_DRF_RENDER_OK or UF_DRF_RENDER_DRAWN is returned by this function |
logical * | out_status | Output | passed into the next UF_DRF_draw_to_position_fn_t call as the 'last_status' input argument. This argument will only be returned if UF_DRF_RENDER_OK or UF_DRF_RENDER_DRAWN is returned by this function |