/*
uf_cutter.h
* File description:
*
* This file contains documentation for the UF_CUTTER module. This module
* allows the Open API programmer to interface with the cutting tools that NX
* uses in its CAM operations. The programmer can perform functions
* such as retrieving a cutter into NX from an external library and creating
* a cutter based upon a template object.
*
******************************************************************************/
#ifndef UF_CUTTER_H_INCLUDED
#define UF_CUTTER_H_INCLUDED
/***************************** Include Files **********************************/
#include <uf_defs.h>
#include <uf_cam.h>
#include <libufun_cam_exports.h>
#include <uf_obj_types.h>
/******************************** Defines *************************************/
/**** CUTTER types *************/
#define UF_CUTTER_TYPE_MILL 1
#define UF_CUTTER_TYPE_DRILL 2
#define UF_CUTTER_TYPE_TURN 3
#define UF_CUTTER_TYPE_GROOVE 4
#define UF_CUTTER_TYPE_THREAD 5
#define UF_CUTTER_TYPE_BARREL 7
#define UF_CUTTER_TYPE_T 8
#define UF_CUTTER_TYPE_FORM 9
#define UF_CUTTER_TYPE_SOLID 11
#define UF_CUTTER_TYPE_LASER 12
#define UF_CUTTER_TYPE_SOFT UF_CUTTER_TYPE_LASER
/**** Cutter subtypes *********/
/*** Subtypes valid for type UF_CUTTER_TYPE_MILL ****/
#define UF_CUTTER_SUBTYPE_MILL_5 1
#define UF_CUTTER_SUBTYPE_MILL_7 2
#define UF_CUTTER_SUBTYPE_MILL_10 3
#define UF_CUTTER_SUBTYPE_MILL_BALL 4
#define UF_CUTTER_SUBTYPE_MILL_CHAMFER 5
#define UF_CUTTER_SUBTYPE_MILL_SPHERICAL 6
/*** Subtypes valid for type UF_CUTTER_TYPE_DRILL ****/
#define UF_CUTTER_SUBTYPE_DRILL_STD 0
#define UF_CUTTER_SUBTYPE_DRILL_CENTER_BELL 1
#define UF_CUTTER_SUBTYPE_DRILL_COUNTERSINK 2
#define UF_CUTTER_SUBTYPE_DRILL_SPOT_FACE 3
#define UF_CUTTER_SUBTYPE_DRILL_SPOT_DRILL 4
#define UF_CUTTER_SUBTYPE_DRILL_BORE 5
#define UF_CUTTER_SUBTYPE_DRILL_REAM 6
#define UF_CUTTER_SUBTYPE_DRILL_COUNTERBORE 7
#define UF_CUTTER_SUBTYPE_DRILL_TAP 8
#define UF_CUTTER_SUBTYPE_DRILL_THREAD_MILL 10
#define UF_CUTTER_SUBTYPE_DRILL_STEP 12
/*** Subtypes valid for type UF_CUTTER_TYPE_TURN ****/
#define UF_CUTTER_SUBTYPE_TURN_STD 1
#define UF_CUTTER_SUBTYPE_TURN_BUTTON 2
#define UF_CUTTER_SUBTYPE_TURN_BORING_BAR 3
/*** Subtypes valid for type UF_CUTTER_TYPE_GROOVE ****/
#define UF_CUTTER_SUBTYPE_GROOVE_STD 1
#define UF_CUTTER_SUBTYPE_GROOVE_RING 2
#define UF_CUTTER_SUBTYPE_GROOVE_FNR 3
#define UF_CUTTER_SUBTYPE_GROOVE_USER 4
/*** Subtypes valid for type UF_CUTTER_TYPE_THREAD ****/
#define UF_CUTTER_SUBTYPE_THREAD_STD 1
#define UF_CUTTER_SUBTYPE_THREAD_TRAP 4
/*** Subtypes valid for type UF_CUTTER_TYPE_SOLID ****/
#define UF_CUTTER_SUBTYPE_GENERIC 0
#define UF_CUTTER_SUBTYPE_PROBE 1
#define UF_CUTTER_SUBTYPE_HARDENING_LASER 2
#define UF_CUTTER_SUBTYPE_STAMPING 3
/*** Subtypes valid for type UF_CUTTER_TYPE_SOFT ****/
#define UF_CUTTER_SUBTYPE_STD_LASER 0
#define UF_CUTTER_SUBTYPE_COAXIAL_LASER 1
#define UF_CUTTER_SUBTYPE_LASER UF_CUTTER_SUBTYPE_STD_LASER
/*** Subtypes valid for type UF_CUTTER_TYPE_BARREL ****/
#define UF_CUTTER_SUBTYPE_STANDARD_BARREL 0
#define UF_CUTTER_SUBTYPE_TANGENT_BARREL 1
#define UF_CUTTER_SUBTYPE_TAPER_BARREL 2
/* Defines for TURN CUTTER inserttypes */
#define UF_TURN_INSERTTYPE_PARALLEL_85 0 /* ISO A */
#define UF_TURN_INSERTTYPE_PARALLEL_82 1 /* ISO B */
#define UF_TURN_INSERTTYPE_DIAMOND_80 2 /* ISO C */
#define UF_TURN_INSERTTYPE_DIAMOND_100 3 /* ISO C turned 90deg */
#define UF_TURN_INSERTTYPE_DIAMOND_55 4 /* ISO D */
#define UF_TURN_INSERTTYPE_DIAMOND_75 5 /* ISO E */
#define UF_TURN_INSERTTYPE_HEXAGON 6 /* ISO H */
#define UF_TURN_INSERTTYPE_PARALLEL_55 7 /* ISO K */
#define UF_TURN_INSERTTYPE_RECTANGLE 8 /* ISO L */
#define UF_TURN_INSERTTYPE_DIAMOND_86 9 /* ISO M */
#define UF_TURN_INSERTTYPE_OCTAGON 10 /* ISO O */
#define UF_TURN_INSERTTYPE_PENTAGON 11 /* ISO P */
#define UF_TURN_INSERTTYPE_ROUND 12 /* ISO R */
#define UF_TURN_INSERTTYPE_SQUARE 13 /* ISO S */
#define UF_TURN_INSERTTYPE_TRIANGLE 14 /* ISO T */
#define UF_TURN_INSERTTYPE_DIAMOND_35 15 /* ISO V */
#define UF_TURN_INSERTTYPE_TRIGON 16 /* ISO W */
#define UF_TURN_INSERTTYPE_USER 17 /* User defined */
#define UF_TURN_INSERTTYPE_GRV_STD 0 /* Standard grooving tool */
#define UF_TURN_INSERTTYPE_GRV_FNR 1 /* Full nose radius grooving tool */
#define UF_TURN_INSERTTYPE_GRV_RTJ 2 /* Ring type joint grooving tool */
#define UF_TURN_INSERTTYPE_GRV_USER 3 /* User defined grooving tool */
#define UF_TURN_INSERTTYPE_THREAD_STD 0 /* Standard threading tool */
#define UF_TURN_INSERTTYPE_THREAD_TRAP 1 /* Trapezoidal threading tool */
/* Defines for TURN CUTTER thickness types */
#define UF_TURN_THICKNESS_TYPE_01 0
#define UF_TURN_THICKNESS_TYPE_T1 1
#define UF_TURN_THICKNESS_TYPE_02 2
#define UF_TURN_THICKNESS_TYPE_T2 3
#define UF_TURN_THICKNESS_TYPE_03 4
#define UF_TURN_THICKNESS_TYPE_T3 5
#define UF_TURN_THICKNESS_TYPE_04 6
#define UF_TURN_THICKNESS_TYPE_05 7
#define UF_TURN_THICKNESS_TYPE_06 8
#define UF_TURN_THICKNESS_TYPE_07 9
#define UF_TURN_THICKNESS_TYPE_09 10
#define UF_TURN_THICKNESS_TYPE_11 11
#define UF_TURN_THICKNESS_TYPE_12 12
#define UF_TURN_THICKNESS_TYPE_USER 13
/* Defines for TURN CUTTER relief angle types */
#define UF_TURN_RELIEF_ANGLE_TYPE_A 0 /* A (3) */
#define UF_TURN_RELIEF_ANGLE_TYPE_B 1 /* B (5) */
#define UF_TURN_RELIEF_ANGLE_TYPE_C 2 /* C (7) */
#define UF_TURN_RELIEF_ANGLE_TYPE_D 3 /* D (15) */
#define UF_TURN_RELIEF_ANGLE_TYPE_E 4 /* E (20) */
#define UF_TURN_RELIEF_ANGLE_TYPE_F 5 /* F (25) */
#define UF_TURN_RELIEF_ANGLE_TYPE_G 6 /* G (30) */
#define UF_TURN_RELIEF_ANGLE_TYPE_N 7 /* N (0) */
#define UF_TURN_RELIEF_ANGLE_TYPE_P 8 /* P (11) */
#define UF_TURN_RELIEF_ANGLE_TYPE_O 9 /* O (other) */
/* Defines for TURN CUTTER insert position types */
/* If the insert position is topside,
the spindle have to rotate in clockwise direction,
if the tool works above the centerline */
#define UF_TURN_INSERT_POSITION_TYPE_TOPSIDE 1
/* If the insert position is underside,
the spindle have to rotate in counterclockwise direction,
if the tool works above the centerline */
#define UF_TURN_INSERT_POSITION_TYPE_UNDERSIDE 2
/*
| Integral constants for tracking point location on a turning cutter
|
| Y
| ^
| |
| |
| TL 2 TM 6 1 TR
| x--------x--------x
| | | |
| | | |
| ML 7| MM 9 |5 MR
| x--------x--------x--------->X
| | | |
| | | |
| | | |
| x--------x--------x
| BL 3 BM 8 4 BR
|
| Abbreviations: T = Top, M = Middle, B = Bottom, L = Left, R = Right
*/
#define UF_TURN_CUTTER_TRACKING_POINT_TL 2
#define UF_TURN_CUTTER_TRACKING_POINT_TM 6
#define UF_TURN_CUTTER_TRACKING_POINT_TR 1
#define UF_TURN_CUTTER_TRACKING_POINT_ML 7
#define UF_TURN_CUTTER_TRACKING_POINT_MM 9
#define UF_TURN_CUTTER_TRACKING_POINT_MR 5
#define UF_TURN_CUTTER_TRACKING_POINT_BL 3
#define UF_TURN_CUTTER_TRACKING_POINT_BM 8
#define UF_TURN_CUTTER_TRACKING_POINT_BR 4
/***************************** Public Typedefs ********************************/
/* tracking point data structure for a Milling Cutter tracking point */
struct UF_CUTTER_tracking_point_data_s
{
double diameter; /* The output diameter of the point */
double distance; /* The distance of the point along the tool axis */
double zoff; /* The postprocessor Z offset of the point */
int adjust; /* The adjust register to use with this point */
int cutcom; /* The cutcom register to use with this point */
int zoff_status; /* The active/inactive status of the Z offset */
int adjust_status; /* The active/inactive status of the adjust register */
int cutcom_status; /* The active/inactive status of the cutcom register */
char name[ UF_OBJ_NAME_BUFSIZE ]; /* The name of the tracking point */
};
typedef struct UF_CUTTER_tracking_point_data_s
UF_CUTTER_tracking_point_data_t, *UF_CUTTER_tracking_point_data_p_t;
/* tracking point data structure for a Turning Cutter tracking point */
struct UF_CUTTER_turn_tracking_point_data_s
{
double tlangl; /* The tool angle of the point */
double radius; /* The radius value of the point */
double xoff; /* The postprocessor X offset of the point */
double yoff; /* The postprocessor Y offset of the point */
int adjust; /* The adjust register to use with this point */
int cutcom; /* The cutcom register to use with this point */
int radiusid; /* The radius id of this point */
int cluster; /* The P value of this point */
char name[ UF_OBJ_NAME_BUFSIZE ]; /* The name of the tracking point */
};
typedef struct UF_CUTTER_turn_tracking_point_data_s
UF_CUTTER_turn_tracking_point_data_t, *UF_CUTTER_turn_tracking_point_data_p_t;
/*
Data structure to hold parameters for a holder section
*/
struct UF_CUTTER_holder_section_s
{
double diameter; /* diameter of the cylindrical section */
double length; /* height of the cylindrical section */
double taper; /* taper angle of the cylindrical section in radians */
double corner; /* corner radius at bottom of section */
};
typedef struct UF_CUTTER_holder_section_s
UF_CUTTER_holder_section_t, *UF_CUTTER_holder_section_p_t;
/************************* Public Function Definitions ************************/
/*****************************************************************************
* This function retrieves a Cutter from the current Cutter Library (as
* defined in cam_config.dat) and creates an NX Cutter Object based upon
* the values received from the library.
*
* Environment : Internal and External
* See Also:
* History : Released in V16.0
****************************************************************************/
extern UFUN_CAMEXPORT int UF_CUTTER_retrieve
(
const char *libref, /* <I> - the library reference of the desired
* cutter. Can be gotten from a record
* set or an existing NX object
*/
tag_t *tool_tag /* <O> - the NX object created as a result of the
* retrieval
*/
);
/*****************************************************************************
* This function updates the data of an already existing Cutter from the current
* Cutter Library (as defined in cam_config.dat).
*
* Environment : Internal and External
* See Also:
* History : Released in V18.0
****************************************************************************/
extern UFUN_CAMEXPORT int UF_CUTTER_update_from_lib
(
tag_t tool_tag /* <I> - the NX object which shall be updated
*
*/
);
/*****************************************************************************
* This function creates a Cutter based upon the Cutter template object
* specified. All parameters of the newly created Cutter are derived from
* the specified Cutter template object.
*
* Environment : Internal and External
* See Also:
* History : Released in V16.0
****************************************************************************/
extern UFUN_CAMEXPORT int UF_CUTTER_create
(
char *type_name, /* <I> - the template type name of the desired Cutter
* template object.
*/
char *subtype_name, /* <I> - the template subtype name of the desired
* Cutter template object.
*/
tag_t *new_object /* <O> - the tag of the newly created Cutter object */
);
extern UFUN_CAMEXPORT int UF_CUTTER_ask_type_and_subtype(
tag_t object_id ,/* <I>
Object identifier of CUTTER
*/
int * type , /* <O>
CUTTER Type
*/
int * subtype /* <O>
CUTTER Subtype
*/
);
/***************************************************************
* Create a new tracking point and add it to the input Cutter.
*
* Return :
* UF_CAM_ERROR_TAG_NOT_CORRECT_TYPE
* The input tag is not a cutter
*
* Environment: Internal and External
*
* See Also:
* History: Released in NX2.0
*************************************************************/
extern UFUN_CAMEXPORT int UF_CUTTER_create_tracking_point
(
tag_t object_tag, /* <I> the parent of the point */
UF_CUTTER_tracking_point_data_t *data /* <I> the data of the point */
);
/***************************************************************
* Create a new turn tracking point and add it to the input Cutter.
*
* Return :
* UF_CAM_ERROR_TAG_NOT_CORRECT_TYPE
* The input tag is not a cutter
*
* Environment: Internal and External
*
* See Also:
* History: Released in NX5.0
*************************************************************/
extern UFUN_CAMEXPORT int UF_CUTTER_create_turn_tracking_point
(
tag_t object_tag, /* <I> the parent of the point */
UF_CUTTER_turn_tracking_point_data_t *data /* <I> the data of the point */
);
/***************************************************************
* Query the number of tracking points in the Cutter.
*
* Return :
* UF_CAM_ERROR_TAG_NOT_CORRECT_TYPE
* The input tag is not a cutter
*
* Environment: Internal and External
*
* See Also:
* UF_CUTTER_ask_tracking_point_data
*
* History: Released in NX2.0
*************************************************************/
extern UFUN_CAMEXPORT int UF_CUTTER_ask_tracking_point_count
(
tag_t object_tag, /* <I> the parent object of the points */
int *count /* <O> the number of tracking points */
);
/***************************************************************
* Query the tracking point data for a cutter.
*
* Return :
* UF_CAM_ERROR_TAG_NOT_CORRECT_TYPE
* The input tag is not a cutter
*
* Environment: Internal and External
*
* See Also:
* History: Released in NX2.0
*************************************************************/
extern UFUN_CAMEXPORT int UF_CUTTER_ask_tracking_point_data
(
tag_t object_tag, /* <I> the parent of the point */
int *count, /* <O> number of tracking points */
UF_CUTTER_tracking_point_data_t ***data /* <OF> count
the data for the points */
);
/***************************************************************
* Query the turn tracking point data for a cutter.
*
* Return :
* UF_CAM_ERROR_TAG_NOT_CORRECT_TYPE
* The input tag is not a cutter
*
* Environment: Internal and External
*
* See Also:
* History: Released in NX5.0
*************************************************************/
extern UFUN_CAMEXPORT int UF_CUTTER_ask_turn_tracking_point_data
(
tag_t object_tag, /* <I> the parent of the point */
int *count, /* <O> number of tracking points */
UF_CUTTER_turn_tracking_point_data_t ***data /* <OF> count
the data for the points */
);
/***************************************************************
* Modify the tracking point data for a specified point.
*
* Return :
* UF_CAM_ERROR_TAG_NOT_CORRECT_TYPE
* The input tag is not a cutter
* UF_CAM_ERROR_INVALID_INDEX
* No tracking point with this index exists in the cutter.
*
* Environment: Internal and External
*
* See Also:
* History: Released in NX2.0
*************************************************************/
extern UFUN_CAMEXPORT int UF_CUTTER_set_tracking_point_data
(
tag_t object_tag, /* <I> the parent object of the point */
int index, /* <I> index of tracking point in parent (from 0 to
the number of tracking points - 1) */
UF_CUTTER_tracking_point_data_t *data /* <I> the modified data of the point */
);
/***************************************************************
* Modify the turn tracking point data for a specified point.
*
* Return :
* UF_CAM_ERROR_TAG_NOT_CORRECT_TYPE
* The input tag is not a cutter
* UF_CAM_ERROR_INVALID_INDEX
* No turn tracking point with this index exists in the cutter.
*
* Environment: Internal and External
*
* See Also:
* History: Released in NX2.0
*************************************************************/
extern UFUN_CAMEXPORT int UF_CUTTER_set_turn_tracking_point_data
(
tag_t object_tag, /* <I> the parent object of the point */
int index, /* <I> index of tracking point in parent (from 0 to
the number of tracking points - 1) */
UF_CUTTER_turn_tracking_point_data_t *data /* <I> the modified data of the point */
);
/***************************************************************
* Delete a specified tracking point from the specified cutter.
*
* Return :
* UF_CAM_ERROR_TAG_NOT_CORRECT_TYPE
* The input tag is not a cutter
*
* Environment: Internal and External
*
* See Also:
* History: Released in NX2.0
*************************************************************/
extern UFUN_CAMEXPORT int UF_CUTTER_delete_tracking_point
(
tag_t cutter_tag, /* <I> the parent cutter of the point */
int index /* <I> index of tracking point in parent (from 0 to the
number of tracking points -1) */
);
/***************************************************************
* Create a new holder section and append it to the holder definition
*
* Return :
* UF_CAM_ERROR_TAG_NOT_CORRECT_TYPE
* The input tag is not a cutter
* UF_CAM_ERROR_INVALID_RADIUS
* UF_CAM_ERROR_INVALID_DIAMETER
* UF_CAM_ERROR_INVALID_LENGTH
* UF_CAM_ERROR_INVALID_TAPER
* The input structure contains invalid data
*
* Environment: Internal and External
*
* See Also:
* History: Released in NX2.0
*************************************************************/
extern UFUN_CAMEXPORT int UF_CUTTER_create_holder_section
(
tag_t object_tag, /* <I> the tag of the cutter */
UF_CUTTER_holder_section_t *data /* <I> the data of the section */
);
/***************************************************************
* Query a cutter for the number of cylindrical sections defining the holder
*
* Return :
* UF_CAM_ERROR_TAG_NOT_CORRECT_TYPE
* The input tag is not a cutter
*
* Environment: Internal and External
*
* See Also:
* History: Released in NX2.0
*************************************************************/
extern UFUN_CAMEXPORT int UF_CUTTER_ask_section_count
(
tag_t object_tag, /* <I> the tag of the cutter */
int *count /* <O> the number of cylindrical sections */
);
/***************************************************************
* Query a cutter for the data of a tool cylindrical section holder
*
* Return :
* UF_CAM_ERROR_TAG_NOT_CORRECT_TYPE
* The input tag is not a cutter
*
* Environment: Internal and External
*
* See Also:
* History: Released in NX2.0
*************************************************************/
extern UFUN_CAMEXPORT int UF_CUTTER_ask_holder_data
(
tag_t object_tag, /* <I> the tag of the cutter */
int *count, /* <O> number of holder sections */
UF_CUTTER_holder_section_t ***data /* <OF> count
array of structure pointers
for each cylindrical section */
);
/***************************************************************
* Modify the data for a specific tool cylindrical section
*
* Return :
* UF_CAM_ERROR_TAG_NOT_CORRECT_TYPE
* The input tag is not a cutter
*
* Environment: Internal and External
*
* See Also:
* History: Released in NX2.0
*************************************************************/
extern UFUN_CAMEXPORT int UF_CUTTER_edit_holder_section
(
tag_t object_tag, /* <I> the tag of the cutter */
int index, /* <I> index to desired section to modify */
UF_CUTTER_holder_section_t *data /* <I> modified section data */
);
/***************************************************************
* Delete a specific tool cylindrical section
*
* Return :
* UF_CAM_ERROR_TAG_NOT_CORRECT_TYPE
* The input tag is not a cutter
* UF_CAM_ERROR_INVALID_INDEX
* No holder section with this index exists in the cutter.
*
* Environment: Internal and External
*
* See Also:
* History: Released in NX2.0
*************************************************************/
extern UFUN_CAMEXPORT int UF_CUTTER_delete_holder_section
(
tag_t object_tag, /* <I> the tag of the cutter */
int index /* <I> index to desired section to delete */
);
#undef EXPORTLIBRARY
#endif /* UF_CUTTER_H_INCLUDED */