UF_ASSEM_expl_status_e (view source)
 
Defined in: uf_assem.h
 
Also known as:
 


Data Members

UF_ASSEM_unexploded


UF_ASSEM_exploded


UF_ASSEM_revert_exploded


 


 
UF_ASSEM_level_option_e (view source)
 
Defined in: uf_assem_types.h
 
Also known as:
 
Overview
UF_ASSEM_level_option_t is used to control the results of an operation
to modify a part occurrence, when the part occurrence chosen
cannot be modified directly for some reason. It is currently
used for reposition.


Data Members

UF_ASSEM_use_strict_level
If the given part occurrence can't be
modified, the operation will fail and return
UF_ASSEM_err_operation_requires_override

UF_ASSEM_use_existing_level
If the given part occurrence can't be
modified, the operation will instead transform
the corresponding part occurrence at the
nearest level down in the assembly where an
appropriate override exists. If none exists
then the instance will be modified.

UF_ASSEM_establish_override
If the given part occurrence can't be
modified, the operation will create an override
in the part of the given part occurrence and
then perform the transform.

 


 
UF_ASSEM_part_load_option_e (view source)
 
Defined in: uf_assem_types.h
 
Also known as:
 
Overview
UF_ASSEM_part_load_option_t is used to control the part load option.
The first four settings are equivalent to the four possible
combinations of the partial loading and lightweight representations.
The final setting is reserved for future use.


Data Members

UF_ASSEM_part_load_option_fully_load = 0
partial load : off, use lightweight : off

UF_ASSEM_part_load_option_partially_load = 1
partial load : on, use lightweight : off

UF_ASSEM_part_load_option_fully_load_lightweight_display = 2
partial load : off, use lightweight : on

UF_ASSEM_part_load_option_partially_load_lightweight_display = 3
partial load : on, use lightweight : on

UF_ASSEM_part_load_option_minimally_load_lightweight_display = 4
reserved for future use

 


 
UF_ASSEM_seq_playback_e (view source)
 
Defined in: uf_assem.h
 
Also known as:
 


Data Members

UF_ASSEM_seq_step_forward


UF_ASSEM_seq_step_backward


UF_ASSEM_seq_play_forward


UF_ASSEM_seq_play_backward