/*
uf.h
File Description :
Open C API general interface. These are general purpose functions that
will be common to most Open C API programs, as well as specialized functions
that do not belong to any of the other interfaces.
Note: UF_free/UF_free_string_array is applicable for C/C++ only
***************************************************************************/
#ifndef UF_INCLUDED
#define UF_INCLUDED
/***************************************************************************
***************************************************************************/
#include <uf_defs.h>
#include <uf_cfi_types.h>
#include <uf_ugopenint.h>
#include <uf_cfi_types.h>
#include <uf_retiring.h>
#include <libufun_exports.h>
#define NONE 0
#define METRIC 1
#define ENGLISH 2
/*****************************************************************************
Unique identifiers for standard NX applications
*****************************************************************************/
#define UF_APP_NONE (0) /* No App Module (may be in External UF)*/
#define UF_APP_DRAFTING (1) /* Drafting */
#define UF_APP_MECHANISMS (14) /* CAE - Mechanisms */
#define UF_APP_CAM (16) /* Manufacturing */
/* obsoleted in NX 3 (38) ICAD - Generative Modeling */
#define UF_APP_MODELING (40) /* Modeling */
#define UF_APP_VALISYS (47) /* Valisys - Quality Control */
#define UF_APP_GATEWAY (48) /* Gateway */
/* UGMX retired in V18.0.0.12 */
#define UF_APP_UGMX (50) /* UGMX Interface */
#define UF_APP_HARNESS (51)
#define UF_APP_FLAT (60) /* Sheet Metal Design - Flat Patterns */
#define UF_APP_SHTNEST (61) /* Sheet Metal Design - Nesting */
#define UF_APP_PUNCH (62) /* Sheet Metal Design - Punch Press */
#define UF_APP_MPG (63) /* Sheet Metal Design - Multipart Gridding */
#define UF_APP_SSL (64) /* Sheet Metal Design - Surface Layout */
#define UF_APP_SHTFAB (65) /* Sheet Metal Design - Fabrication */
#define UF_APP_SMD (66) /* Sheet Metal Design Application */
#define UF_APP_BUILDER (67) /* UI Builder */
#define UF_APP_SFEM (68) /* CAE Advanced Simulation */
#define UF_APP_ROUTE (69) /* PSA - Routing Applications */
/* obsoleted (70) PSA - Virtual Mockup (Division) */
#define UF_APP_PIPE (71) /* PSA - Routing - Piping */
#define UF_APP_TUBE (72) /* PSA - Routing - Tubing */
#define UF_APP_STEEL (73) /* PSA - Routing - Steel */
#define UF_APP_CONDUIT (74) /* PSA - Routing - Conduit */
#define UF_APP_RACEWAY (75) /* PSA - Routing - Raceway */
#define UF_APP_SHOPS (76) /* Manufacturing - Shop floor app */
#define UF_APP_WIRE (77) /* PSA - Routing - Wiring */
#define UF_APP_MTB (78) /* Manufacturing - Machine Tool Builder */
#define UF_APP_SKETCHER (79) /* Sketcher Task Environment */
#define UF_APP_NOPART (80) /* No Part loaded menubar */
/* obsoleted (81) CAE - Advanced FEM */
#define UF_APP_ROUTE_MECH (82) /* PSA - Routing - Mechanical */
#define UF_APP_ROUTE_ELEC (83) /* PSA - Routing - Electrical */
#define UF_APP_ROUTE_LGCL (84) /* PSA - Routing - Logical */
#define UF_APP_SBSM (85) /* SBSM - Straight Break Sheet Metal */
#define UF_APP_SEQUENCING (86) /* Sequencing Task Environment */
#define UF_APP_UFUN (87) /* UFUN app */
#define UF_APP_STUDIO (88) /* Shape Studio */
#define UF_APP_DESFEM (89) /* CAE - Design Simulation */
#define UF_APP_SHIP (90) /* PSA - Ship Building */
#define UF_APP_AEROSM (91) /* PSA - Aerospace Sheet Metal Application */
#define UF_APP_FLEX_PCB (92) /* Flexible Printed Circuit Design */
#define UF_APP_INSPECTION (93) /* CMM Inspection Programming */
#define UF_APP_MECHATRONICS (94) /* Mechatronics Designer */
#define UF_APP_STYLER (95) /* Block Styler */
#define UF_APP_SUBSET_DEFINITION (96) /* Subset Definition task environment */
#define UF_APP_TRUE_STUDIO (97) /* True Studio Task Environment */
#define UF_APP_SHIP_BASICDESIGN (98) /* Ship Building */
#define UF_APP_SHIP_DETAILSDESIGN (99)/* Ship Building */
#define UF_APP_SHIP_MANUFACTURE (100) /* Ship Building */
#define UF_APP_SINUCAST (101) /* SinuCAST */
#define UF_APP_SUBDIVISION_MODELING (102) /* Subdivision Modeling Task Environment */
/* Codesets supported by NX. This is returned by the
function UF_ask_codeset. */
enum UF_codeset_e
{
UF_CODESET_NOT_INITIALIZED=-2, /* This is an error condition. */
UF_CODESET_NOT_SUPPORT=-1, /* This is an error condition. */
UF_CODESET_ASCII, /* Only ASCII characters are supported.
If NX does not recognize a
codeset, then it will revert to
UF_CODESET_ASCII. */
UF_CODESET_ISO8859_1, /* Western European standard */
UF_CODESET_EUC, /* Japanese EUC codeset */
UF_CODESET_SJIS, /* Japanese SJIS codeset */
UF_CODESET_ISO8859_4, /* Finnish, Latvian, Norwegian, Swedish
and other European languages. */
UF_CODESET_ISO8859_5, /* Russian, Ukrainian, Bulgarian and other
Eastern European languages. */
UF_CODESET_ISO8859_8, /* Hebrew codeset */
UF_CODESET_BIG5, /* Traditional Chinese for Taiwan */
UF_CODESET_NT_866, /* No longer used, placeholder only */
UF_CODESET_ISO8859_2, /* Czech, Polish, Slovak and other
Eastern European languages. */
UF_CODESET_NT_852, /* No longer used, placeholder only */
UF_CODESET_NT_862, /* No longer used, placeholder only */
UF_CODESET_KSC5601, /* Korean codeset */
UF_CODESET_GB2312, /* Simplified Chinese for Mainland China */
UF_CODESET_NT_1251, /* Windows NT Russian codeset */
UF_CODESET_NT_1255, /* Windows NT Hebrew codeset */
UF_CODESET_NT_1250, /* Windows NT Eastern European codeset */
UF_CODESET_NT_1252, /* Windows NT Western European and US
codeset */
UF_CODESET_ISO8859_15, /* Western European codeset including
EURO */
UF_CODESET_NT_1253, /* Windows NT Greek codeset */
UF_CODESET_ISO8859_7, /* Greek Codeset */
UF_CODESET_UTF8, /* UTF-8 Codeset */
UF_CODESET_NT_1254, /* Windows NT Turkish codeset */
UF_CODESET_NT_1257, /* Windows NT Baltic codeset */
UF_CODESET_NT_1256, /* Windows NT Arabic codeset */
UF_CODESET_ISO8859_6, /* Arabic Codeset */
UF_CODESET_ISO8859_11, /* Thai Unix and Windows (CP 874) */
UF_CODESET_NT_1258 /* Vietnamese codeset */
};
typedef enum UF_codeset_e UF_codeset_t;
/*
This type is used to hold information about a timer in NX. You
can have more than one timer active at a time, each active timer requires
a UF_timer_t variable.
*/
typedef unsigned short UF_timer_t, *UF_timer_p_t;
/*
The structure UF_timer_values_t below is used to get the values from the
timer. The routine UF_end_timer fills the fields of this structure, when the
timer is closed. The timer is initiated by the routine UF_begin_timer.
*/
struct UF_timer_values_s
{
double cpu_time; /* Total CPU time (User + System) for this process */
double real_time; /* Total elapsed time */
};
typedef struct UF_timer_values_s
UF_timer_values_t, *UF_timer_values_p_t;
/*
The structure UF_system_info_t below is used to get the information about
the current process. The routine UF_ask_system_info retrieves the
information about the process and fills the structure. Once the data is used,
the memory allocated to these fields should be freed by calling the routine,
UF_free_system_info.
*/
struct UF_system_info_s
{
char *date_buf; /* Current date and time info */
char *user_name; /* User, who is running this process */
char *program_name; /* The current program name */
char *node_name; /* Machine, on which this process is running */
char *machine_type; /* Hardware type on which the machine is running */
char *os_name; /* Operating system, on which this process is running
*/
char *os_version; /* Version and release level of this Operating System
*/
long physical_memory; /* Returns the number of bytes of physical memory
on this machine. */
char **bundles_used; /* Array of the names of the bundles currently in use. */
int number_of_bundles; /* The number of bundles currently in use */
};
typedef struct UF_system_info_s
UF_system_info_t, *UF_system_info_p_t;
/****************************************************************************
* Get the information about an Open C Program
*
* This routine can be used to gather the system information of an Open C
* program, like the machine name, Operating System information etc., and is
* useful in benchmarking, where you want to record the information about
* the machine the benchmark was run on.
*
* This routine outputs the data through the structure UF_system_info_t.
*
* Once the data is no longer needed, the memory allocated to the fields
* of this structure should be freed by a corresponding call to the routine
* UF_free_system_info.
*
* Environment: Internal and External
*
* See Also:
* UF_free_system_info
* UF_system_info_t
*
* History: Released in V18.0, modified in NX 6.0 to return used bundles
****************************************************************************/
extern UFUNEXPORT int UF_ask_system_info(
UF_system_info_p_t info /* <OF>
structure to hold the process information.
The allocated fields should be freed by
calling UF_free_system_info
*/
);
/****************************************************************************
* Free the fields of the structure UF_system_info_t, containing the process
* information
*
* This structure is filled earlier by a call to the routine UF_ask_system_info
*
* Environment: Internal and External
*
* See Also:
* UF_ask_system_info
* UF_system_info_t
*
* History: Released in V18.0
****************************************************************************/
extern UFUNEXPORT int UF_free_system_info(
UF_system_info_p_t info /* <I>
structure whose fields are to be freed
*/
); /* */
/****************************************************************************
* Start a timer.
*
* This routine can be used to gather timing information about an Open C
* program, and is useful in benchmarking. This routine will start a timer.
* The timer will be stopped with a corresponding call to UF_end_timer.
*
* More than one timer can be active at any time, this is useful when you
* have one overall timer, and then several sub-timers timing individual
* sub-operations.
*
* Environment: Internal and External
*
* See Also:
* UF_end_timer
* UF_timer_values_t
*
* History: Released in V18.0
****************************************************************************/
extern UFUNEXPORT int UF_begin_timer (
UF_timer_p_t timer /* <O>
* Timer id that is created
*/
);
/****************************************************************************
* Stop the timer and get the timer values
*
* This routine is used to gather timing information about an Open C program,
* and is useful in benchmarking. This routine will stop the timer created by
* a corresponding UF_begin_timer call, and output the timing information in
* the structure UF_timer_values_t.
*
* Environment: Internal and External
*
* See Also:
* UF_begin_timer
* UF_timer_values_t
*
* History: Released in V18.0
****************************************************************************/
extern UFUNEXPORT int UF_end_timer (
UF_timer_t timer, /* <I>
* Timer to be stopped
*/
UF_timer_values_p_t values /* <O>
* Timer values when it is
* stopped
*/
);
/*****************************************************************************
* Frees the memory allocated and returned by an Open C API routine.
*
* Note: UF_free/UF_free_string_array is applicable for C/C++ only
*
* Return: void
*
* Environment: Internal and External
*
* See Also:
*
* History:
*****************************************************************************/
extern UFUNEXPORT void UF_free (
void *data /* <I> Pointer to data item to free */
);
/*****************************************************************************
* Allocates a block of storage and returns a pointer to it. Use UF_free
* to free the allocated memory when no longer required.
*
* Return:
* void * - a pointer to the block of storage, aligned so
* that any data type can be stored in it.
* when error occur or nbytes = 0, a NULL pointer
* is returned
*
* Environment: Internal and External
*
* See Also:
*
* History: This function was originally released in V15.0
*****************************************************************************/
extern UFUNEXPORT void *UF_allocate_memory(
unsigned int nbytes, /* <I>
The number of bytes to be allocated.
If 0, NULL is returned
*/
int *error_code /*<O>
NX standard error code
0 success
!=0 failure
*/
);
/*****************************************************************************
* Reallocates a block of storage and returns a pointer to it. Use UF_free
* to free the allocated memory when no longer required.
*
* Return:
* void * - a pointer to the block of storage, aligned so
* that any data type can be stored in it.
* when error occur or nbytes = 0, a NULL pointer
* is returned
*
* Environment: Internal and External
*
* See Also:
*
* History: This function was originally released in V16.0
*****************************************************************************/
extern UFUNEXPORT void *UF_reallocate_memory(
void *data, /* <I>
Pointer to previously allocated memory
*/
unsigned int nbytes, /* <I>
The number of bytes to be allocated.
If 0, NULL is returned
*/
int *error_code /* <O>
NX standard error code
*/
);
/*****************************************************************************
* Frees the memory allocated for an array of pointers and frees the
* strings within the array. You must pass in the number of pointer in
* the array. Various Open C API routines malloc space for an array
* of pointers, and then allocate space for each of the pointers.
*
* Note: UF_free/UF_free_string_array is applicable for C/C++ only
*
* Return: void
*
* Environment: Internal and External
*
* See Also:
*
* History:
*****************************************************************************/
extern UFUNEXPORT void UF_free_string_array (
int n_strings , /* <I>
number of pointers
*/
char **string_array /*<I> n_strings
pointer to the array of pointers to free
*/
);/**/
/*****************************************************************************
* Returns the message string associated with an error code.
*
* Environment: Internal and External
*
* See Also:
*
* History:
*****************************************************************************/
extern UFUNEXPORT int UF_get_fail_message (
int fail_code , /* <I>
the failure code to translate
*/
char message[ 133 ] /* <O>
the message corresponding to the fail code
*/
);
/*****************************************************************************
* Returns the message string associated with an error code in current user interface language.
*
* Environment: Internal and External
*
* See Also:
*
* History: Originally released in NX 10.0
*****************************************************************************/
extern UFUNEXPORT int UF_get_translated_fail_message(
int fail_code , /* <I>
the failure code to translate
*/
char ** message /* <O>
the message corresponding to the fail code
*/
);
/***************************************************************************
* Explanation: In UG V9, when an entity had a known Entity IDentifier *
* (EID), that EID was saved with the part and would be the same the next *
* time the part was loaded. In V10, because multiple parts can be loaded *
* at once, the Tag (ie, EID) of an object can not be guaranteed between *
* sessions. For this reason, "Handles" were created to identify objects *
* between sessions. To aid applications where the EID was saved in some *
* data file between sessions, UF_ask_new_tag_of_entity() was created to *
* return the V10 tag corresponding to the EID of an entity in a V9 part *
***************************************************************************/
/***************************************************************************
* This function replaces UF_TAG_ask_handle_of_tag.
*
* Return the persistent HANDLE for an object tag.
*
* Multiple parts can be loaded into NX during a single session, and
* the Tag (i.e. Object Identifier) cannot be guaranteed between sessions.
* Consequently, "handles" were created to identify objects between sessions.
* This handle is persistent between sessions once the object is saved to a part file.
* A handle of a new object in this session which is never saved is not guaranteed
* to stay the same until the object is saved. Recreating the same object in a new
* session may not be the same even if seemingly identical steps were taken to create
* the object. This is particularly true across versions of software.
*
* Handles should not be compared directly for checking identity as they contain
* version information. Handles should be broken apart using UF_TAG_decompose_handle
* and the file_data strings compared and the sub_file_id integers compared but the
* version should be ignored.
*
* Operations which change the name of the part will change the handle as well - so
* "Save As" will cause handles to change.
*
* This function will return an error when the part data of the handle
* contains a character that cannot be represented. For this reason
* it is suggested that UF_TEXT_set_text_mode(UF_TEXT_ALL_UTF8) be
* set when you are working with handles that may come from parts that have
* characters that are outside of your locale (e.g. parts with Japanese
* characters on an english system).
*
* Output:
* The name of handle for object tag. This string must be freed by calling UF_free.
*
* Environment: Internal and External
* See Also: UF_TAG_ask_tag_of_handle
* History: Originally released in NX 10.0
***************************************************************************/
extern UFUNEXPORT int UF_TAG_ask_handle_from_tag (
tag_t object_tag, /* <I>
tag of object to query for persistent handle
*/
char **handle /* <OF>
Output handle for the tag.
*/
);
/****************************************************************************
* Return the object tag of a persistent HANDLE.
*
* Return:
* Returns object tag of object handle
*
* Environment: Internal and External
*
* See Also: UF_TAG_ask_handle_from_tag
*
* History:
****************************************************************************/
extern UFUNEXPORT tag_t UF_TAG_ask_tag_of_handle (
char *object_handle /* <I>
Name of persistent handle
*/
);/* */
#define UF_ask_new_tag_of_entity UF_TAG_ask_new_tag_of_entity
/****************************************************************************
* Returns the new tag of the object corresponding to the known object
* ID in the V9 part. This only works for the Object IDs of the last V9
* part loaded into this session.
* NOTE: This was renamed from UF_ask_new_tag_of_entity()
*
* Return:
* New tag
*
* Environment: Internal and External
* See Also: UF_TAG_ask_handle_from_tag
* History:
****************************************************************************/
extern UFUNEXPORT tag_t UF_TAG_ask_new_tag_of_entity (
tag_t v9_eid /* <I>
Known Object ID (EID) of V9 part
*/
);/* */
/*****************************************************************************
* Given the constituent parts of data manager, filename, subfile id and
* version, this function returns the resulting handle.
*
* Environment: Internal and External
*
* See Also:
*
* History:
******************************************************************************/
extern UFUNEXPORT int UF_TAG_compose_handle (
const char *file_data , /* <I>
Data about the file. This string would come
from a call to UF_TAG_decompose_handle.
*/
unsigned int sub_file_id , /* <I>
sub_file identifier. The sub_file is
an internal file in the part file database.
*/
unsigned int version , /* <I>
Version of part
*/
char **handle /* <OF>
String containing the composed handle
*/
);
/*****************************************************************************
* Given the handle, the constituent parts of data manager, filename, subfile
* id and version are returned.
*
* Note this function will return an error if you have UF_TEXT_set_text_mode()
* set to locale and the file that the data is coming from has characters
* outside of your locale. It is suggested that you set your text mode to
* UF_TEXT_ALL_UTF8 when you are working with handles.
*
* Environment: Internal and External
*
* See Also: UF_TAG_ask_new_tag_of_entity
* UF_TAG_ask_handle_from_tag
*
* History:
******************************************************************************/
extern UFUNEXPORT int UF_TAG_decompose_handle(
char *handle , /* <I>
Handle to decompose
*/
char **file_data , /* <OF>
Data about the file. This can be used by
UF_TAG_compose_handle. This argument
must be freed by calling UF_free.
*/
unsigned int *sub_file_id , /* <O>
Sub-file identifier for handle. The
sub_file is an internal file in the part
file database.
*/
unsigned int *version /* <O>
Version of part in which handle is located.
*/
);
#define UF_set_program_name UF_MISC_set_program_name
/****************************************************************************
* Each part file has an internal history storage area where the program
* name can be stored when the system saves the part file. This function
* enables you to specify either the entire program name (External
* mode) or append a name to the program name (Internal mode). You
* should call this routine before you call UF_PART_open since it does
* not set the program name on parts that are already opened. A utility
* called ug_inspect enables you to read the program name stored in the
* history area.
*
* Interactively (Internal mode), when you are in NX, the program
* name will take the version of NX currently being run (e.g. NX9.0.0.19)
* and append the string being passed into UF_MISC_set_program_name. For
* example, if you specify "XYZ version 9.0" as the name string to this
* routine, then the program name in the history would look like:
* NX 9.0.0.19XYZ version 9.0
* To separate the version and string, put a leading space in the name being
* passed into this routine. " XYZ version 9.0" passed in will create:
* NX 9.0.0.19 XYZ version 9.0
*
* Once UF_terminate is called, the appended string is removed and it will
* default back to the NX version number the next time the part is saved.
*
* In External mode, the program name is what you specify in the name
* string. From our previous example this would be XYZ version 9.0.
* The limitation for the length of the name string depends on which
* mode you are in, Internal or External. The maximum length of the
* entire program name is 128 characters. In Internal mode, because the
* name string is concatenated to the program name you are limited to
* 64 characters. In External mode, since the name string you specify
* becomes the program name you are limited to 128 characters. In
* either mode, if you specify a name that is to long, the name is
* truncated to either 64 or 128 characters (Internal and External mode
* respectively).
*
* The internal history area is like a log file. If you resave the part file
* with a different program a new history entry is added to the part file.
* That is, the history grows larger. Thus you are likely to see two lines of
* history if you have saved the part file twice and specified a name with
* each save.
*
* Return: void
*
* Environment: Internal and External
*
* See Also:
*
* History:
****************************************************************************/
extern UFUNEXPORT void UF_MISC_set_program_name (
const char *name /* <I>
Name of program to store in the internal history
*/
);
/****************************************************************************
* Translates environment variables to their equivalence strings. You
* must supply the complete name of the variable argument. The pointer passed
* back points to an operating system string. This string must not be changed.
*
* Environment: Internal and External
*
* See Also: See the example
*
* History:
****************************************************************************/
extern UFUNEXPORT int UF_translate_variable (
const char *variable , /* <I>
Environment Variable to Translate
*/
char **translation /* <O>
Translated variable name or NULL if nonexistent.
*/
);
/****************************************************************************
* Sets an environment variable to the string specified in value. You must
* supply the complete name of variable.
*
* Environment: Internal and External
*
* See Also: See the example
*
* History:
****************************************************************************/
extern UFUNEXPORT int UF_set_variable (
const char *variable , /* <I>
Environment Variable to set in Operating System
*/
const char *value /* <I>
Value or equivalence string for the variable.
*/
);
/****************************************************************************
* Initializes the Open C API environment and allocates an Open C
* API execute license. If you do not call UF_initialize, then subsequent
* calls to Open C API fail with an error code of
* UF_err_program_not_initialized. This function must be the first
* function you call after you have declared your variables.
*
* In external mode, you may only call UF_initialize once. Once
* UF_terminate is called, there is no way to reconnect to the Open C environment.
*
* Programs need to call UF_terminate before exiting to ensure licenses are
* released and avoid errors in downstream NXOpen programs.
*
* Environment: Internal and External
*
* See Also:
* Refer to the UGII_UGOPEN_SESSION variable
*
* History:
****************************************************************************/
extern UFUNEXPORT int UF_initialize (
void
);/**/
/****************************************************************************
* Same as UF_initialize with the addition that Direct Model is also initialized.
*
* Environment: Internal and External
*
* See Also:
*
* History:
****************************************************************************/
extern UFUNEXPORT int UF_initialize_dm (
void
);
/****************************************************************************
* Checks if the Open C API environment has been successfully
* initialized.
*
* Return:
* return code:
* 0 = Open C API is not initialized.
* 1 = Open C API has been properly
* initialized.
*
* Environment: Internal and External
*
* See Also:
*
* History:
****************************************************************************/
extern UFUNEXPORT int UF_is_initialized (
void
);/* */
/****************************************************************************
* Terminates the Open C API environment and deallocates a
* Open C API execute license. If UF_terminate is not called, the
* Open C API execute license may not be freed. Once UF_terminate
* is called in an external Open C API program, the program will
* exit. You will not be able to call UF_initialize again and continue
* operation.
*
* Calling this method will release all licenses in the default context.
*
* Once UF_terminate has completed in an external program, you can no
* longer write to the console window. It must be reinitialized with system
* calls.
*
* Environment: Internal and External
*
* See Also:
* Refer to the UGII_UGOPEN_SESSION variable
* History:
****************************************************************************/
extern UFUNEXPORT int UF_terminate (
void
);
/****************************************************************************
* Reserve a license against the specified license context.
* If the specified user-defined context does not already exist it will be created.
*
* Environment: Internal and External
*
* See Also:
*
* History:
****************************************************************************/
extern UFUNEXPORT int UF_reserve
(
const char* license , /* <I>
License feature name to be reserved
*/
const char* context_name /* <I>
Name of context to reserve license against. Will use the default context if NULL is specified.
*/
);
/****************************************************************************
* Release a license against the specified license context.
*
* Environment: Internal and External
*
* See Also:
*
* History:
****************************************************************************/
extern UFUNEXPORT int UF_release
(
const char* license , /* <I>
License feature name to be released
*/
const char* context_name /* <I>
Name of context to release license against. Will use the default context if NULL is specified.
*/
);
/****************************************************************************
* Release all licenses against the specified license context. If
* the context specified is a user-defined context it will be deleted.
*
* Environment: Internal and External
*
* See Also:
*
* History:
****************************************************************************/
extern UFUNEXPORT int UF_release_all
(
const char* context_name /* <I>
Name of context release to release. Will use the default context if NULL is specified.
*/
);
/****************************************************************************
* Returns the licenses that are currently reserved against a context.
* This method will also output the licenses reserved against the default context in the syslog.
*
* Environment: Internal and External
*
* See Also:
*
* History:
****************************************************************************/
extern UFUNEXPORT int UF_get_reserved_licenses
(
const char* context_name, /* <I>
Name of context to release against. Will use the default context if NULL is specified.
*/
int *n_licenses, /* <O>
The number of licenses.
*/
char*** licenses /* <OF>
The list of license reserved against the specified context. This must be
freed by calling UF_free_string_array.
*/
);
/***************************************************************************
* Encodes an input authorization file using an integer value for
* perturbation.
*
* Environment: Internal
*
* See Also:
*
* History:
*************************************************************************/
extern UFUNEXPORT int UF_encode_auth_file (
int key , /* <I>
Value used to perturb the input file
*/
char *input_file , /* <I>
Input authorization file name
*/
char *output_file /* <I>
Output encoded authorization file name
*/
);
/***************************************************************************
* Decodes an input authorization file using an integer key value that
* matches the original key for perturbation.
*
* NOTE: See %UGII_BASE_DIR%\UGALLIANCE\alliance_readme.txt for more information
*
* Environment: Internal
*
* See Also:
*
* History:
**************************************************************************/
extern UFUNEXPORT int UF_decode_auth_file (
int key , /* <I>
Integer valued key for decoding the input file
*/
char *input_file, /* <I>
Input authorization file to decode
Use the leaf name of a file located under the folder %UGALLIANCE%\auth_files.
Entering the full path will return an error of -5 "Invalid file name".
*/
void **out_mem /* <OF>
Pointer to decoded contents of the authorization
file. Use UF_free to deallocate the memory.
*/
);
/*****************************************************************************
* Returns the current application module. The value that is returned
* maps to a string defined constant. You can find the string in the
* header file uf.h. The strings are of the form UF_APP_<module>.
* For example, UF_APP_DRAFTING represents the drafting module.
*
* Note - if this function is called from an external program it will
* always return a FALSE and an app id of APP_NONE.
*
* Environment: Internal and External
* See Also:
* History:
*****************************************************************************/
extern UFUNEXPORT int UF_ask_application_module(
int *module_id /* <O>
The module identification value of the
current application.
*/
);
/*****************************************************************************
* Calls and executes a GRIP program. Your GRIP program must be written,
* compiled, linked, and ready to run.
*
* While a GRIP program executes, it can have access to an Open C API function
* arguments and their contents. Argument passing to the GRIP program occurs
* through UFARGS. After GRIP program termination, the Open C API program has
* access to any assignments made by the GRIP program. The GRIP program
* completes its execution and then UF_call_grip outputs a return value.
*
* Note: If the path is omitted in the grip_executable string passed to
* UF_call_grip, NX will look in the current directory for the grip program.
* It will not look in the directory of the ufunc program or use any
* environment variables, including UGII_INITIAL_GRIP_DIR, to search for the
* GRIP program.
*
* UF_translate_variable can be used to extract an environment variable and
* concatenate it with the program name.
*
* The following GRIP commands are not
* supported in External mode when calling GRIP:
* ALL OF GRIP NC
* PLNOTE EDTXHT CHAIN
* BLANK UNBLNK RVBLNK
* If any of these commands are encountered, an error is written to the
* batch log file.
*
* Environment: Internal and External
*
* See Also: See the example
* which calls the grip program.
*
* History:
****************************************************************************/
extern UFUNEXPORT int UF_call_grip (
char *grip_executable, /* <I>
Name of GRIP program to execute (file name
or full path name).
*/
int count, /* <I>
Count of arguments to pass to GRIP executable
*/
UF_args_p_t UFARGS /* <I>
An array of structures where each element in
the array is a structure that contains an
arguments type, size, and address. Note that
if an argument is type UF_TYPE_CHAR, the array
must be initialized prior to the UF_call_grip
call.
*/
);
/*****************************************************************************
* This routine retrieves a customer default value from the database.
* There are several different conditions that can arise from querying
* the database:
* 1) The record was found and its units match. The function
* returns SUCCESS(0)
* 2) The record was not found. If units given was ENGLISH or METRIC
* nothing is returned and the function returns a FAILED(1). If
* the units given was NONE a second and/or third attempt is made
* with units ENGLISH THEN METRIC used instead. The results of
* these attempts can be any of the conditions outlined above.
*
* If you specify either METRIC or ENGLISH for units, this function
* automatically appends _MU or _EU to the input name. For example, if you
* specify METRIC and input the name "UG_gridSpacingY", the function searches
* for "UG_gridSpacingY_MU".
*
* If you specify NONE for units, the function searches for the name
* as specified. If the name is not found it searches again with _EU
* appended to the name. If the name is still not found, then it
* appends _MU to the name for its final search.
*
* Return:
* return code:
* 0 = Success
* 1 = Record not found
* <0 or >1 = Use UF_get_fail_message to get error.
*
* Environment: Internal and External
*
* See Also: See the example
*
* History:
*****************************************************************************/
extern UFUNEXPORT int UF_get_customer_default(
char * name , /* <I>
Name of Module ID and default
*/
int units , /* <I>
Units are enumerated as follows:
0 = NONE
1 = METRIC
2 = ENGLISH
*/
char ** default_value /* <OF>
String containing default value. If
*default_value is NULL then the value was
not found or an error occurred. Use UF_free
to deallocate memory when no longer required.
*/
);
/**************************************************************************
* Returns the compatible base release version number. For example, if
* you call this function from 1847, it returns NX V1847.
* For monthly release this function returns its compatible base release version. For example,
* if you call this function from 1851, it returns NX V1847
* You must use UF_free to deallocate space used by release.
*
* Environment: Internal and External
*
* See Also:
*
* History:
****************************************************************************/
extern UFUNEXPORT int UF_get_release(
char ** release /* <OF>
Major release version number
*/
);
typedef void (*UF_load_f_p_t)( void );
/**********************************************************************
* Loads the shared library specified by library_name and finds the entry
* point specified by symbol_name in that library. The reference to the
* specified entry point is output as a function pointer declared to accept
* and return void (i.e. type UF_load_f_p_t).
*
* For the entry point to be found on Windows NT, you must declare it with
* the DllExport macro, e.g.
*
* extern DllExport int my_function(...
*
* without the DllExport, the name will not be exported. Since the DllExport
* also works on Unix systems, the best practice is just to always use the
* DllExport macro for routines you want exported.
*
* If library_name is found but symbol_name is not, an appropriate error
* code returns, but the loaded library may not be unloaded. The user
* should call UF_unload_library to explicitly unload library_name on
* failure, if appropriate.
*
* To load a shared library into an external application - the library must
* not be linked against any interactive libraries. This can be accomplished
* by using the "-noui" option on Unix.
*
* NOTE: UF_load_library is intended for function (i.e. "text" entry
* point) lookup only. It should NOT be used for data symbol lookup.
*
* Environment: Internal and External
*
* See Also: UF_unload_library
* The UF_load_library example is split into an, internal program
* which is loaded by the external program.
*
* History:
**********************************************************************/
extern UFUNEXPORT int UF_load_library(
const char * library_name ,/* <I>
Name of shared library to load.
*/
const char * symbol_name ,/* <I>
Name of symbol (function) to find.
*/
UF_load_f_p_t *function_ptr /* <O>
Pointer to symbol (function) in library.
*/
);/**/
/**********************************************************************
* Unloads the shared library specified by library_name. UF_unload_library
* unloads the library unconditionally, effectively invalidating all function
* pointers previously set by calls to UF_load_library for the specified
* library.
*
* Environment: Internal and External
*
* See Also: UF_load_library
* The two UF_load_library example one and
* example two use UF_unload_library.
*
* History:
*
*********************************************************************/
extern UFUNEXPORT int UF_unload_library(
char * library_name /* <I>
Name of shared library to unload.
*/
);
/****************************************************************************
* Force NX to shut down immediately. This is a substitute for the standard
* c function: exit(0)
*
* Warning: depending on the current state of NX, forcing a shutdown
* may produce warnings/errors as NX attempts to close itself.
*
* Environment: Internal and External
*
* History: NX 6.0.1
****************************************************************************/
extern UFUNEXPORT void UF_sys_exit( void );/**/
/*****************************************************************************
* Checks to see if an NX Manager process is
* active. It returns true if NX Manager is active.
*
* Environment: Internal and External
*
* See Also:
*
* History:
*****************************************************************************/
extern UFUNEXPORT int UF_is_ugmanager_active(
logical *is_active /* <O>
Returns true if NX Manager is active
*/
);
/****************************************************************************
* Returns the code set identifier supported by a machine. The code set
* identifier can be any one of the enumerated constants in UF_codeset_e.
*
* Environment: Internal and External
*
* See Also: UF_codeset_t
*
* History:
****************************************************************************/
extern UFUNEXPORT int UF_ask_codeset(
UF_codeset_t *codeset /*<O>
Pointer to the codeset identifier.
*/
);
/*
* These are the reasons against which call backs can be registered.
*
* The registered callbacks will be called whenever the specific reason occurs
* in interactive NX.
*
* For all the reasons, except for UF_close_part_reason, the callbacks will be
* called towards the end of that particular operation. For example, the
* callbacks registered against UF_create_part_reason will be called when a
* new part is created, after almost all the process of creating this new part
* is completed.
*
* The UF_change_work_part_reason call back will be called after a work part change
* has occurred. It should be noted that this callback may be called at times where the
* old work part (which is passed as the part tag data to the call back routine) may
* not necessarily be different from the new work part. For example, this call back is
* also called if the display part has changed but the new work part is still the same tag
* and now represents a component in a different display part. This call back may be
* called more than once as part of a single operation.
*
* An attempt to query the work or display part in a UF_save_part_reason_callback
* may return unexpected results.
*
* The callbacks registered against UF_close_part_reason will be called at the
* beginning of part close.
*
* The callbacks registered against UF_modified_part_reason will be called
* when the part is modified for the first time after opening it or after a
* save operation.
*
* These callbacks give a handle to the user to do some extra processing, in
* addition to the processing that NX does, during that particular operation.
*
* In NX Manager mode, when a new part is being created it first loads the
* template part (seed part), changes the template part to be the work part
* and then renames the work part to the new part name given. So, the following callbacks are being called:
* UF_modified_part_reason, UF_open_part_reason, UF_change_work_part_reason,
* UF_rename_part_reason and UF_create_part_reason.
*/
enum UF_callback_reason_e
{
UF_create_part_reason, /* Callback when a new part is created. */
UF_open_part_reason, /* Callback when an existing part is opened.
The part opened callback is called just after the "target parts
of the load operation" (e.g. the top level part of an assembly
and its component parts have been loaded), but is only issued
for the "target parts of the load operation". This callback may
be called if more data is loaded for an already partially
loaded part.*/
UF_save_part_reason, /* Callback when a part is saved. */
UF_save_as_part_reason, /* Callback when a part is saved-as. */
UF_close_part_reason, /* Callback when a part is closed. */
UF_modified_part_reason, /* Callback when a part is modified. */
UF_rename_part_reason, /* Callback when a part is renamed. */
UF_change_work_part_reason, /* Callback when there is a new work part.
The part returned is of the old work part.
Use UF_ASSEM_ask_work_part to get new work part. */
UF_post_save_as_part_reason, /* Callback reason for adding parts for
Save As at the end of in progress Save As operation
of selected part/parts, it's like nested Save As.
Only issued in managed mode. */
UF_max_reason /* Do not use - not a valid reason */
};
typedef enum UF_callback_reason_e UF_callback_reason_e_t;
/* Definition of a callback function prototype. */
typedef void (*UF_callback_fn_t)(
UF_callback_reason_e_t, /* <I> reason the callback has been called */
const void*, /* <I> This is the pointer to the part tag that
caused the callback. For UF_change_work_part_reason
the part returned is of the old work part.
Use UF_ASSEM_ask_work_part to get new work part.
*/
void* /* <I> This is a user supplied pointer. Typically
this will be a structure pointer of data
that your callback function will need.
*/
);
typedef struct UF_registered_fn_s *UF_registered_fn_p_t;
/****************************************************************************
* Registers the callback to be called whenever the reason specified
* occurs within NX.
*
* Please note the following:
*
* Once a routine is registered as a callback, the shared library it
* resides in should not be unloaded until it is deregistered.
*
* The callback function must call UF_initialize and UF_terminate, if
* it makes any Open C function calls
*
* The callback function receives three arguments:
* argument 1 - The reason the callback has been called
* argument 2 - A pointer to the part tag that caused the callback.
* argument 3 - A user supplied pointer. Typically this will be a
* structure pointer of data that the callback function
* will need.
*
* The callback will be called towards the end of the processing for that
* particular reason. For example, the callback registered against
* UF_create_part_reason will be called when a new part is created, after
* almost all the process of creating this new part is completed.
*
* The only exception to the above is UF_close_part_reason, for which
* the callback will be called at the beginning of closing the part.
*
* NOTE: For the new and open part reasons the callback is run at a time
* when the newly created or opened part has not been set as the work part.
* Also operations such as create part, open part, save part or change display part
* should not be called from callbacks fired by any of these same operations.
*
* Environment: Internal and External
*
* See Also: UF_remove_callback_function
* UF_callback_reason_e
* Refer to the example of setting up a callback.
*
* History: V16 was changed to require the callback to call UF_initialize
****************************************************************************/
extern UFUNEXPORT int UF_add_callback_function (
UF_callback_reason_e_t reason, /* <I>
Reason to call callback
*/
UF_callback_fn_t fn, /* <I>
Function to call. Note this function
must call UF_initialize if it
makes any Open C function calls. It
should also call UF_terminate.
*/
void *user_data, /* <I>
User data. This pointer will be passed
to your callback function as the third
argument. It will typically be a
structure pointer with information that
your callback function will require.
*/
UF_registered_fn_p_t *function_id /* <O>
Identifier to use to remove callback
*/
);
/****************************************************************************
* Deregisters the callback specified by the identifier.
*
* Environment: Internal and External
*
* See Also: UF_add_callback_function
*
* History:
****************************************************************************/
extern UFUNEXPORT int UF_remove_callback_function (
UF_registered_fn_p_t function_id /* <I>
Identifier from UF_add_callback_function
*/
);
/****************************************************************************
* The following set of routines allow the registration of routines to be
* called when tags are created and deleted. This allows synchronisation of
* data structures outside of NX with NX. Note that the routines registered
* can not call any other UF routines themselves. Also the implementation
* of any routine so registered must be very efficient as it will be called
* very many times.
*
* Also it should be remembered that tags get reused. This means that the
* order of events is important so the event is interpreted with respect
* to the right incarnation of the tag.
****************************************************************************/
/****************************************************************************
* This enum identifies the type of an event that occurred on a tag.
****************************************************************************/
enum UF_TAG_event_e
{ UF_TAG_EVENT_NORMAL_CREATE, /* The tag was created. */
UF_TAG_EVENT_UNDO_OVER_CREATE, /* An undo occurred over the tag's
creation and so is now invalid. */
UF_TAG_EVENT_NORMAL_DELETE, /* The tag was deleted. */
UF_TAG_EVENT_UNDO_OVER_DELETE, /* An undo occurred over the tag's
deletion and so has come back to
life. */
UF_TAG_EVENT_UNDO_DELETE_EXPIRED, /* NX will now never undo over
the deletion so it will never come back
to life. */
UF_TAG_EVENT_UNDO_CREATE_EXPIRED /* NX will now never undo over
the tags creation. */
};
typedef enum UF_TAG_event_e UF_TAG_event_t;
/****************************************************************************
* Type of the event notification callback.
*****************************************************************************/
typedef void (*UF_TAG_event_fn_t)(UF_TAG_event_t reason, /* <I> */
tag_t tag, /* <I> */
void *closure /* <I> */);
/*****************************************************************************
* Register a new tag event callback. All callbacks are called on all tags
* for all events. This returns an identifier for the callback which is
* used to allow it removal.
*
* Please note the following items:
* . The routines registered can not call any other Open C routines
* In particular, the tag cannot be queried or edited in any way.
* . The implementation of any routine so registered must be very
* efficient as it is called many times.
* . Recall that tags get reused. This means that the order of events is
* important so the event is interpreted with respect to the right
* "incarnation" of the tag.
*
* Environment: Internal and External
*
* See Also: UF_TAG_unregister_event_cb
*
* History: This function was originally released in V15.0.
****************************************************************************/
extern UFUNEXPORT int UF_TAG_register_event_cb(
UF_TAG_event_fn_t callback, /* <I>
Callback function
*/
void *closure, /* <I>
Pointer passed to callback on
each call
*/
int *callback_id /* <O>
Identifier for callback
*/
);
/****************************************************************************
* Unregister a previously registered callback.
*
* Environment: Internal and External
*
* See Also: UF_TAG_register_event_cb
*
* History: This function was originally released in V15.0.
****************************************************************************/
extern UFUNEXPORT int UF_TAG_unregister_event_cb(
int callback_id /* <I> - identifier of callback */
);
/****************************************************************************
* Set a flag that determines if an Open C executable will issue
* warnings when a function that is scheduled to be retired is called.
* This can be used to alert the NX Open programmer that modification to
* their program is required.
*
* When routines are planned to be removed from the NX Open interface, the
* prototype will be moved to uf_retiring.h, along with a description of
* what the NX Open programmer should do. A warning can be issued when
* any of these routines are called by an NX Open application. This routine
* allows the NX Open programmer to set the value of this flag.
*
* This routine overrides the environment variable
* UGII_USING_RETIRING_FUNCTIONS which can be set by the user to get
* the same warnings. This routine is meant to be used when the programmer
* wants to force a particular value for a program.
*
* Environment: Internal and External
*
* See Also:
*
* History: Released in V16.0
****************************************************************************/
extern UFUNEXPORT int UF_set_retiring_flag(
int value /* <I>
0 = Don't warn user at all, this is the default
1 = Output a single message if any function is called
that is planned to be obsoleted
2 = Output a message for each function called that
is planned to be obsoleted. The message will include
the routine name, and the number of times called.
*/
);
/****************************************************************************
* Output a message to the syslog.
*
* This message can be used to print run time information about the NX Open
* program to the syslog and is useful for state checking, validation and
* debugging.
*
* Printing the trace is especially useful while debugging and reporting a
* problem.
*
* Environment: Internal and External
*
* See Also:
*
* History: Released in V18.0
****************************************************************************/
extern UFUNEXPORT int UF_print_syslog(
char *message, /* <I>
Message to be output to the syslog
*/
logical trace /* <I>
TRUE = Print the stack trace along with the message
FALSE = Print only the message
*/
);
/****************************************************************************
* Get name of the current syslog
*
* Environment: Internal and External
*
* See Also:
*
* History: Released in NX2.0.5
****************************************************************************/
extern UFUNEXPORT int UF_ask_syslog_filename(
char **filename /* <OF>
pointer to dynamically allocated path
filename must be freed with UF_free()
*/
);
/****************************************************************************
* Find a given subdirectory and file. This routine will traverse all the
* directories specified in the file custom_dirs.dat and ug_custom_dirs.dat
* looking for the file specified by the given subdirectory and filename.
* This routine will return the first file found.
*
* Environment: Internal and External
*
* See Also: UF_find_all_subdirectories
*
* History: Released in NX 1.0
****************************************************************************/
extern UFUNEXPORT int UF_find_file(
const char *subdirectory, /* <I>
The subdirectory in which to look for the
given file.
*/
const char *filename, /* <I>
The filename to look for, including any extension.
*/
char **path /* <OF>
The filename found. If no file is found, **path will
be NULL. The path must be freed by calling UF_free.
*/
);
/****************************************************************************
* Find all subdirectories of a given name in the directories specified in
* the file custom_dirs.dat and ug_custom_dirs.dat. Since the same
* subdirectory may be in multiple directories, an array of path names
* will be returned. As an example searching for the subdirectory "startup"
* will return almost all of the directories, since this is a standard
* subdirectory.
*
* Environment: Internal and External
*
* See Also: UF_find_file
*
* History: Released in NX 1.0
****************************************************************************/
extern UFUNEXPORT int UF_find_all_subdirectories(
const char *subdirectory, /* <I>
The subdirectory to look for.
*/
int *num_found, /* <O>
The number of subdirectories found.
*/
char ***path /* <OF>
The list of subdirectories found. This must be
freed by calling UF_free_string_array.
*/
);
/****************************************************************************
* Select the listing device. The listing device can be set to a file,
* the listing window, or both file and listing window. The listing
* device can also be set to no output.
*
* Return:
* 0 = Success
* 2 = Listing device is unavailable
* otherwise an error code
*
* Environment: Internal and External
*
* See Also: UF_UI_open_listing_window
* UF_UI_close_listing_window
* UF_UI_write_listing_window
*
* History:
****************************************************************************/
extern UFUNEXPORT int uc4400(
int listing_device, /*<I>
The listing device to use:
= 0 standard listing window
= 4 output to a file
= 8 output to both file and listing window
= 9 No output is written
*/
char *file_spec, /*<I>
This is only used for output to a file. This is
the file specification for the output file, and
must be less than MAX_FSPEC_NCHARS characters.
*/
int ip3 /*<I>
This is no longer used.
*/
);
/****************************************************************************
* Query the current disposition of the listing device.
*
* Environment: Internal and External
*
* Returns:
* 0 = Listing device is set to the listing window
* 4 = Listing device is set to a file
* 8 = Listing device is set to both file and the listing window
* 9 = Listing device is set to NULL
* otherwise the return is an error code.
*
* See Also: UF_UI_open_listing_window
* UF_UI_close_listing_window
* UF_UI_write_listing_window
* uc4400
*
* History:
****************************************************************************/
extern UFUNEXPORT int uc4409(
char file_name[ MAX_FSPEC_BUFSIZE ], /* <O>
For return code 4 or 8, this is the file specification
of the listing device file.
*/
int *ir3 /* <O>
Unused.
*/
);
/****************************************************************************
* Query the current NX Open program environment for the current image.
*
* Note: This value is updated during initialization so it is set for
* each image and won't remember the information from previous images.
*
* Environment: Internal and External
*
* Returns:
* Void
*
* History:
****************************************************************************/
extern UFUNEXPORT void uf3192(
int *ir1 /* <O>
The environment that the NX Open program is running in.
0 is External Open, 1 is Internal Open.
*/
);
/******************************************************************************
******************************************************************************
***** WARNING: The routines that follow will be obsoleted soon. *****
***** Do not use them! Use their indicated replacements. *****
******************************************************************************
******************************************************************************
*/
/* uf4401 opens the listing device set by uc4400 for output
if you only need to open the listing window for output
(and not a particular listing device set by uc4400)
this function may be replaced with UF_UI_open_listing_window */
extern UFUNEXPORT void uf4401(int *ir1);
/* uf4402 closes listing device set by uc4400
if you only need to close the listing window
(and not a particular device set by uc4400)
this function may be replaced by UF_UI_close_listing_window */
extern UFUNEXPORT void uf4402(void);
/* uc4403 write character string to listing device set by call to uc4400
if you only need to write to the listing window
(as opposed to a listing device set by uc4400)
this function may be replaced with UF_UI_write_listing_window */
extern UFUNEXPORT int uc4403(const char *cp1/* <I> */);
/* uc4404 write character string and integer to listing device set by uc4400
if you only need to write the data to the listing window
(and not a particular device set by uc4400)
this function may be replaced by UF_UI_write_listing_window */
extern UFUNEXPORT int uc4404(const char *cp1/* <I> */, int ip2);
/* uc4406 write character string and real to listing device set by uc4400
if you only need to write the data to the listing window
(and not a particular listing device set by uc4400)
this function may be replaced by UF_UI_write_listing_window */
extern UFUNEXPORT int uc4406(const char *cp1/* <I> */, double rp2);
/***************************************************************************
***************************************************************************/
#undef EXPORTLIBRARY
#endif /* UF_INCLUDED */