/*
uf_ui_types.h
File description:
These are the types required for the Open C API interface to the NX user
interface. The descriptions and typdef's here will only be usable by Internal
Open API programs.
******************************************************************************/
#ifndef UF_UI_TYPES_H_INCLUDED
#define UF_UI_TYPES_H_INCLUDED
/***************************************************************************
***************************************************************************/
#include <uf_part_types.h>
/* Data structure that controls standard button configuration on message
dialogs */
struct UF_UI_message_buttons_s{
logical button1; /* flag that specifies whether or not button1
(OK) is required */
logical button2; /* flag that specifies whether or not button2
(BACK) is required */
logical button3; /* flag that specifies whether or not button3
(CANCEL) is required */
char *label1; /* label for button1 (OK by default) */
char *label2; /* label for button2 (BACK by default) */
char *label3; /* label for button3 (CANCEL by default) */
int response1; /* Response value for button1 */
int response2; /* Response value for button2 */
int response3; /* Response value for button3 */
};
typedef struct UF_UI_message_buttons_s UF_UI_message_buttons_t, *UF_UI_message_buttons_p_t;
enum UF_UI_MESSAGE_DIALOG_TYPE
{
UF_UI_MESSAGE_ERROR,
UF_UI_MESSAGE_WARNING,
UF_UI_MESSAGE_INFORMATION,
UF_UI_MESSAGE_QUESTION
};
/***************************************************************************
User responses by selecting objects (UF_UI_PICK_RESPONS) or clicking the
button which is labeled ok, cancel, back, apply or help.
****************************************************************************/
#define UF_UI_PICK_RESPONSE 1 /* User response was a selection of objects.*/
#define UF_UI_OK 2 /* OK button was selected. */
#define UF_UI_CANCEL 3 /* Cancel button was selected. */
#define UF_UI_BACK 4 /* Back button was selected. */
#define UF_UI_APPLY 5 /* Apply button was selected. */
#define UF_UI_HELP 6 /* Help button was selected. */
#define UF_UI_OBJECT_SELECTED 7 /* Object was selected. */
#define UF_UI_OBJECT_SELECTED_BY_NAME 8 /* Object was selected by name. */
#define UF_UI_CB_TERMINATE 9 /* Callback routine has terminated. */
/* Constants for saving state info with custom menu */
#ifndef UF_UI_FROM_CUSTOM
#define UF_UI_NO_LOCK (0)
#define UF_UI_FROM_CUSTOM (1)
#endif
#define UF_UI_SUCCESS 0
#define UF_UI_FAILURE 1
#define UF_UI_LOCK 2
#define UF_UI_UNLOCK 3
#define UF_UI_ERROR 4
#define UF_UI_LOCK_SET 5
#define UF_UI_LOCK_EXISTS 6
#define UF_UI_LOCK_ERROR 7
#define UF_UI_UNLOCK_SET 8
#define UF_UI_NO_LOCK_EXISTED 9
#define UF_UI_UNLOCK_ERROR 10
#define UF_UI_LOCK_UNNECESSARY 11
typedef int (*UF_UI_change_state_fn_t) (int new_state /* <I> */);
/* Constants for selection scope */
#define UF_UI_SEL_SCOPE_NO_CHANGE 0
#define UF_UI_SEL_SCOPE_WORK_PART 1 /* Allows you to select only objects
which belong to the work part.
This includes immediate
components of the work part. If
you select an object occurrence,
the prototype is returned. */
#define UF_UI_SEL_SCOPE_ANY_IN_ASSEMBLY 3 /* Allows you to select any object
or object occurrence in the
assembly. No scope restrictions
are applied. */
#define UF_UI_SEL_SCOPE_WORK_PART_AND_OCC 4 /* Allows you to select objects
which belong to the work part or
its subassembly. If you select
an object occurrence, the
prototype is returned. */
#define UF_UI_SEL_SCOPE_WORK_PART_AND_WP_OCC 5 /* Allows you to select objects
which belong to the work part or
its subassembly. If you select
an object occurrence, the
occurrence of the work part is returned. */
/* selection mask actions to be used as input to
UF_UI_set_sel_mask
*/
enum UF_UI_sel_mask_action_e{
UF_UI_SEL_MASK_ENABLE_ALL,
UF_UI_SEL_MASK_ENABLE_SPECIFIC,
UF_UI_SEL_MASK_DISABLE_SPECIFIC,
UF_UI_SEL_MASK_CLEAR_AND_ENABLE_SPECIFIC,
UF_UI_SEL_MASK_ALL_AND_DISABLE_SPECIFIC,
UF_UI_SEL_MASK_COUNT /* Do not use - not a valid input as a selection mask action */
} ;
typedef enum UF_UI_sel_mask_action_e UF_UI_sel_mask_action_t;
/* selection types to be used as input to UF_UI_set_sel_type */
#define UF_UI_SEL_TYPE_INACTIVE_SELECTION (0)
#define UF_UI_SEL_TYPE_SINGLE_POSITION (1 << 0)
#define UF_UI_SEL_TYPE_RECTANGLE_POSITION (1 << 1)
#define UF_UI_SEL_TYPE_SINGLE_SELECTION (1 << 2)
#define UF_UI_SEL_TYPE_SINGLE_DESELECTION (1 << 7)
#define UF_UI_SEL_TYPE_ROBUST_SELECTION (1 << 5)
/* Note: ROBUST_SELECTION includes single select, single deselect,
* rectangle select, rectangle deselect, reselect last and chaining */
/* selection descriptors to be used with UF_UI_ask_sel_descriptor */
#define UF_UI_SEL_DESC_SELECTION (1 << 0)
#define UF_UI_SEL_DESC_DESELECTION (1 << 1)
#define UF_UI_SEL_DESC_RESELECTION (1 << 2)
#define UF_UI_SEL_DESC_SINGLE (1 << 3)
#define UF_UI_SEL_DESC_MULTIPLE (1 << 4)
#define UF_UI_SEL_DESC_SINGLE_POSITION (1 << 5)
#define UF_UI_SEL_DESC_RECTANGLE_POSITION (1 << 6)
#define UF_UI_SEL_DESC_NAME_SELECTION (1 << 7)
#define UF_UI_SEL_DESC_RECTANGLE (1 << 8)
#define UF_UI_SEL_FAILURE 0
#define UF_UI_SEL_SUCCESS 1
#define UF_UI_CB_EXIT_DIALOG 1
#define UF_UI_CB_CONTINUE_DIALOG 0
#define UF_UI_CB_CONTINUE_SWITCH 0
#define UF_UI_CB_REJECT_SWITCH 1
#define UF_UI_SEL_REJECT 0
#define UF_UI_SEL_ACCEPT 1
/* User Tool routine defines */
#define UF_UI_HIDE FALSE
#define UF_UI_SHOW TRUE
/* Non-Modal Message Dialog's positioning methods */
#define UF_UI_MSG_POS_CURSOR 0
#define UF_UI_MSG_POS_CASCADE 1
#define UF_UI_MSG_POS_BOTTOM_RIGHT 2
#define UF_UI_MSG_POS_TOP_LEFT 3
#define UF_UI_MSG_POS_DA1 4
#define UF_UI_MSG_POS_DA2 5
/* Temporary display flag setting for UF_UI_select_conehead */
#define UF_UI_DISP_NONE 0
#define UF_UI_DISP_SELECTED 1
#define UF_UI_DISP_ALL 2
/* Temporary display flag setting for UF_UI_specify_vector */
#define UF_UI_DISP_NO_VECTOR 0
#define UF_UI_DISP_TEMP_VECTOR 1
/* Mode settings for UF_UI_specify_vector
* (Note: see unsupported modes below) */
#define UF_UI_TWO_POINTS 2
#define UF_UI_TANGENT_TO_CURVE 3
#define UF_UI_XC_AXIS 7
#define UF_UI_NEGATIVE_XC_AXIS 8
#define UF_UI_YC_AXIS 9
#define UF_UI_NEGATIVE_YC_AXIS 10
#define UF_UI_ZC_AXIS 11
#define UF_UI_NEGATIVE_ZC_AXIS 12
#define UF_UI_INFERRED 13
#define UF_UI_AT_ANGLE 14
#define UF_UI_EDGE_CURVE 15
#define UF_UI_FACE_NORMAL 16
#define UF_UI_DATUM_PLANE 17
#define UF_UI_DATUM_AXIS 18
/* Mode settings for the old UF_UI_specify_vector subfunction.
* These options are no longer supported in their orignal form.
* When input, the option will be mapped to the closest mode in
* the new vector subfunction. Output mode will always be from
* current modes as listed above */
#define UF_UI_ENABLE_OK_NO_DEFAULT (-1)
#define UF_UI_NO_DEFAULT 0
#define UF_UI_LINE_ENDPOINT 1
#define UF_UI_IJK_COMPONENTS 4
#define UF_UI_SPHERICAL_COORDS 5
#define UF_UI_COORD_SYSTEM_AXIS 6
/* Mode settings for UF_UI_ask_iw_decimal_places */
#define UF_UI_SYSTEM_DECIMAL_PLACES 0
#define UF_UI_USER_DECIMAL_PLACES 1
/* Units settings for UF_UI_ask_info_units */
#define UF_UI_POUNDS_INCHES 0
#define UF_UI_POUNDS_FEET 1
#define UF_UI_GRAMS_MILLIMETERS 2
#define UF_UI_GRAMS_CENTIMETERS 3
#define UF_UI_KILOS_METERS 4
#define UF_UI_KILOS_MILLIMETERS 5
#define UF_UI_DEFAULT_UNITS 1000
/* Constants for FSD directory filter access
Refer to the enumerated constants
*/
enum UF_UI_dialog_filter_id_e{
UF_UI_EXPORT_PART_FLTR, /* Specifies *.prt */
UF_UI_EXPORT_PARASOLID_FLTR, /* Specifies *.xmt_txt */
UF_UI_EXPORT_CGM_FLTR, /* Specifies *.cgm */
UF_UI_EXPORT_DIAGRAM_FLTR, /* Specifies *.* */
UF_UI_EXPORT_RPT_FLTR, /* Specifies *.stl */
UF_UI_EXPORT_INV_FLTR, /* Specifies *.iv */
UF_UI_SYM_FLTR, /* Specifies *.sym */
UF_UI_IMPORT_PART_FLTR, /* Specifies *.prt */
UF_UI_IMPORT_PARASOLID_FLTR, /* Specifies *.xmt_txt */
UF_UI_IMPORT_CGM_FLTR, /* Specifies *.cgm */
UF_UI_IMPORT_MARKUP_FLTR, /* Specifies *.mkp */
UF_UI_IMPORT_UDF_FLTR, /* Specifies *.udf */
UF_UI_PART_NEW_FLTR, /* Specifies *.prt */
UF_UI_PART_OPEN_FLTR, /* Specifies *.prt */
UF_UI_PART_SAVEAS_FLTR, /* Specifies *.prt */
UF_UI_PART_SAVEAS_STUDENT_FLTR, /* Specifies *.prt */
UF_UI_FILE_GRIP_FLTR, /* Specifies *.grx */
UF_UI_FILE_UFUN_FLTR, /* Specifies *.sl, *.so or *.dll depending
on the platform. */
UF_UI_IMPORT_SYMBOL_FLTR, /* Specifies *.sym,*.txt, or *.* */
UF_UI_IMPORT_BLOCK_FLTR, /* Specifies *.dwg,*.dxf,*.txt */
UF_UI_IMAGE_QS_FLTR, /* Specifies *.pix */
UF_UI_IMAGE_DISP_FLTR, /* Specifies *.tif and .pix */
UF_UI_EXPORT_EXPRESSIONS_FLTR, /* Specifies *.exp */
UF_UI_IMPORT_EXPRESSIONS_FLTR, /* Specifies *.exp */
UF_UI_MACRO_FLTR, /* Specifies *.macro */
UF_UI_LAYOUT_FLTR, /* Specifies *.win */
UF_UI_EXPORT_COMPONENT_FLTR, /* Specifies *.flt */
UF_UI_IMPORT_COMPONENT_FLTR, /* Specifies *.flt */
UF_UI_CAM_MDF_FLTR, /* Specifies *.md* */
UF_UI_CAM_GPM_FLTR, /* Specifies *.* */
UF_UI_CAM_CLS_FLTR, /* Specifies *.cls */
UF_UI_CAM_CL_FLTR, /* Specifies *.cl */
UF_UI_CAM_CLF_FLTR, /* Specifies *.clf */
UF_UI_CAM_BCL_FLTR, /* Specifies *.bcl */
UF_UI_CAM_ISO_FLTR, /* Specifies *.iso */
UF_UI_CAM_NCOUT_FLTR, /* Specifies *.* */
UF_UI_CAM_LISTOUT_FLTR, /* Specifies *.* */
UF_UI_CAM_ACL_FLTR, /* Specifies *.acl */
UF_UI_CAM_S_FLTR, /* Specifies *.*s* */
UF_UI_CAM_ARC_FLTR, /* Specifies *.arc */
UF_UI_CAM_CYC_FILE_FLTR, /* Specifies *.cyc */
UF_UI_CAM_MTK_FLTR, /* Specifies *.mtk */
UF_UI_TRAN_PART_FLTR, /* Specifies *.prt */
UF_UI_TRAN_IGS_FLTR, /* Specifies *.igs */
UF_UI_TRAN_STP_FLTR, /* Specifies *.stp */
UF_UI_TRAN_DXF_FLTR, /* Specifies *.dxf */
UF_UI_TRAN_IGES_FLTR, /* Specifies *.def */
UF_UI_TRAN_STEP203_FLTR, /* Specifies *.def */
UF_UI_TRAN_STEP214_FLTR, /* Specifies *.def */
UF_UI_TRAN_DXFTOUG_FLTR, /* Specifies *.def */
UF_UI_TRAN_UGTODXF_FLTR, /* Specifies *.def */
UF_UI_TRAN_LOG_FLTR, /* Specifies *.log */
UF_UI_MB_SYSLOG_FLTR, /* Specifies *.syslog */
UF_UI_MISC_DATA_FLTR, /* Specifies *.dat */
UF_UI_CAM_TOOLIB_FLTR, /* Specifies *.prt */
UF_UI_CAM_LIBLIST_FLTR, /* Specifies *.prt */
UF_UI_CAM_DISPAT_FLTR, /* Specifies *.prt */
UF_UI_CAM_VCUTS_FLTR, /* Specifies *.stl */
UF_UI_CAM_VCUTT_FLTR, /* Specifies *.txt */
UF_UI_CAM_TEMPSET_FLTR, /* Specifies *.opt */
UF_UI_IMPORT_VRML_FLTR, /* Specifies *.wrl and *.wrl.gz */
UF_UI_NLE_FLTR, /* */
UF_UI_RLIST_HRN_FLTR, /* */
UF_UI_RLIST_CMP_FLTR, /* */
UF_UI_IMPORT_SE_FLTR, /* */
UF_UI_IMPORT_STL_FLTR, /* Specifies *.stl and *.stl.gz */
UF_UI_IMPORT_CUST_UNIT_CELL_FLTR, /*Specifies *.xml */
UF_UI_CAM_CONFIG_FLTR, /* */
UF_UI_CAM_SETUP_PRT_FLTR, /* */
UF_UI_VDAC_CEO_FLTR, /* */
UF_UI_VDAC_CFG_FLTR, /* */
UF_UI_TBR_FLTR, /* */
UF_UI_HATCH_FLTR, /* */
UF_UI_BOOKMARK_FLTR, /* */
UF_UI_CAM_SHOP_DOC_FLTR, /* */
UF_UI_FMBD_FILE_FLTR, /* */
UF_UI_LOAD_OPT_FLTR, /* Specifies *.def */
UF_UI_TRAN_DWG_FLTR, /* Specifies *.dwg */
UF_UI_MENU_DXF_FLTR, /* Specifies *.dwg and *.dxf */
UF_UI_IMPORT_ASC_FLTR, /* Specifies *.asc and *.dwg*/
UF_UI_TRAN_CATIA_FLTR, /* Specifies *.mod and *.exp */
UF_UI_TRAN_CATMOD_FLTR, /* Specifies *.mod only */
UF_UI_CAE_RPT_TEMPLATES_FLTR, /* Specifies *.htt only */
UF_UI_CAE_RPT_IMG_FLTR, /* Specifies *.gif, jpg, mpg, vrml */
UF_UI_INTEROP_FLTR, /* Specifies files that contain plm xml context, such as .bkm */
UF_UI_DRAFTING_IMAGE_FLTR, /* Specifies *.jpg and *.tif */
UF_UI_NX2D_FLTR, /* NX2D File */
UF_UI_SPRD_FLTR, /* Specifies *.xls *.csv, *.xs6, *.tsv and *.* */
UF_UI_SPRDNT_FLTR, /* Specifies *.xls *.csv, *.tsv and *.* */
UF_UI_SPRSHT_FLTR, /* Specifies *.xlsx *xls */
UF_UI_XESS_FLTR, /* Specifies *.xs6, etc. */
UF_UI_CAE_RST_FLTR, /* Specifies *.op2 *.vdm *.rst *.rth *.des and *.fil */
UF_UI_CAE_RST_ODB_FLTR, /* Specifies *.op2 *.vdm *.rst *.rth *.des *.ssndb *.fil and *.odb */
UF_UI_CAE_ODB_FLTR, /* Specifies *.odb */
UF_UI_CAE_SAMCEF_FLTR, /* Specifies *.des *.ssndb *.op2 *.vdm *.rst *.rth and *.fil */
UF_UI_CAE_OP2_FLTR, /* Specifies *.op2 */
UF_UI_TRAN_CATIAV5_FLTR, /* Specifies *.CATPart and *.CATProduct */
UF_UI_TRAN_CATIAV5_CATPART_FLTR, /* Specifies *.CATPart */
UF_UI_IMPORT_AC_FLTR, /* Specifies *.ac */
UF_UI_PRT_PART_OPEN_FLTR, /* Specifies *.prt */
UF_UI_SFEM_PART_OPEN_FLTR, /* Specifies *.prt, *.fem *.sim */
UF_UI_FEM_PART_OPEN_FLTR, /* Specifies *.fem */
UF_UI_FEM_PART_NEW_FLTR, /* Specifies *.fem */
UF_UI_BOOKMARK_OPEN_FLTR, /* Specified for open bookmark *.bkm, *.plmxlm */
UF_UI_BOOKMARK_SAVE_FLTR, /* Specified for save bookmark *.plmxml */
UF_UI_CAE_AFU_FLTR, /* Specifies *.afu */
UF_UI_XYPLOT_DISP_TEMPLATE_FLTR, /* Specifies *.xml */
UF_UI_FEM_SAVEAS_FLTR, /* Specifies *.fem */
UF_UI_SIM_SAVEAS_FLTR, /* Specifies *.sim */
UF_UI_MOTION_IMP_EXP_FLTR, /* Specifies *.xml */
UF_UI_FTK_NAV_TREE_HISTORY_FLTR, /* Specifies *.xml */
UF_UI_SIM_PART_NEW_FLTR, /* Specifies *.sim */
UF_UI_SIM_PART_OPEN_FLTR, /* Specifies *.sim */
UF_UI_FACE_ANALYSIS_REFLECTION_FLTR, /* Specifies *.jpg, *.tif and *.png */
UF_UI_BACKGROUND_IMAGE_FLTR, /* Specifies *.jpg, *.tif and *.png */
UF_UI_TEXTURE_IMAGE_FLTR, /* Specifies *.jpg, *.tif and *.png */
UF_UI_IBL_IMAGE_FLTR, /* Specifies *.lwi, *.jpg, *.tif *.png and *.bmp *hdr and *.exr */
UF_UI_CAE_RPCIII_FLTR, /* Specifies *.rsp */
UF_UI_CAE_DAC_FLTR, /* Specifies *.dac */
UF_UI_CAE_CSV_FLTR, /* Specifies *.csv */
UF_UI_TRAN_PROE_FLTR, /*Specifies *.asm.* and *.prt.* */
UF_UI_SE_PART_ASM_FLTR, /* Specifies *.par and *.asm (Solid Edge files) */
UF_UI_CAE_EEF_FLTR, /* Specifies *.eef */
UF_UI_CAE_SEF_FLTR, /* Specifies *.sef */
UF_UI_CAE_RS2_FLTR, /* Specifies *.rs2 */
UF_UI_CAM_FEA_EXPORT_FLTR, /* Specifies *.plmxml for Manufacturing Feature export */
UF_UI_CAE_MAT_FLTR, /* Specifies *.mat */
UF_UI_MOTION_ADAMS_RES_FLTR, /* Specifies *.res */
UF_UI_MOTION_RECURDYN_RAD_FLTR, /* Specifies *.rad */
UF_UI_PDF_FLTR, /* Specifies *.pdf */
UF_UI_JPG_FLTR, /* Specifies *.jpg */
UF_UI_TIF_FLTR, /* Specifies *.tif */
UF_UI_EMF_FLTR, /* Specifies *.emf */
UF_UI_PNG_FLTR, /* Specifies *.png */
UF_UI_CAE_UNV58_FLTR, /* Specifies *.unv(dataset58) */
UF_UI_ASSY_FEM_PART_OPEN_FLTR, /* Specifies *.afm */
UF_UI_ASSY_FEM_PART_NEW_FLTR, /* Specifies *.afm */
UF_UI_ASSY_FEM_SAVEAS_FLTR, /* Specifies *.afm */
UF_UI_IFEM_PART_OPEN_FLTR, /* Specifies *.fem, *.afm */
UF_UI_KF_MISC1_FLTR, /* Specifies kf specified file type */
UF_UI_KF_MISC2_FLTR, /* Specifies kf specified file type */
UF_UI_KF_MISC3_FLTR, /* Specifies kf specified file type */
UF_UI_KF_MISC4_FLTR, /* Specifies kf specified file type */
UF_UI_KF_MISC5_FLTR, /* Specifies kf specified file type */
UF_UI_SIMULINK_MDL_FLTR, /* Simulink MDL file type */
UF_UI_SIMULINK_M_FLTR, /* Simulink M file type */
UF_UI_MOTION_EXPORT_SDK_RMD_FLTR, /* Specifies *.sdk and *.rmd */
UF_UI_STANDARD_FONTS_FLTR, /* Specifies .ttf and other standard font types */
UF_UI_SW_PART_ASM_FLTR, /* Specifies (Solid Works files) */
UF_UI_IGES_EXPORT_FLTR, /* Used by File->Export->IGES */
UF_UI_STEP_EXPORT_FLTR, /* Used by File->Export->STEP203, STEP214) */
UF_UI_MOTION_FLEXBODY_RFI_FLTR, /* Specifies *.rfi for flexible body use*/
UF_UI_IMAGE_FILE_FLTR, /* Specifies *.bmp, *.jpg, *.gif, *.png and *.tif*/
UF_UI_ATTR_CATALOG_FLTR, /* Specifies *.xml */
UF_UI_MW_FLTR, /* Specifies *.mw for Maple Worksheet*/
UF_UI_TRUMPF_GEO_FLTR, /* Specifies .geo for Trumpf bending machines */
UF_UI_TIRE_SPINDLE_FLTR, /* Specifies *.spindle */
UF_UI_STUDIO_IMAGE_FILE_FLTR, /* Specifies *.tif, *.jpg, *.png, *.gif and *.bmp */
UF_UI_MOTION_RECURDYN_RAD_RAN_FLTR, /*Specifies *.rad, *.ran for Motion RecurDyn*/
UF_UI_MECHDES_RUNTIME_CODE_FLTR, /* Specifies *.cs and *.dll file type */
UF_UI_CAE_UNV_FLTR, /* Specifies *.unv */
UF_UI_PAX_FLTR, /* Specifies *.pax */
UF_UI_HDF5_FLTR, /* Specifies *.h5 */
UF_UI_LAYUP_FLTR, /* Specifies *.Layup */
UF_UI_CAE_BROWSE_FLTR, /* Specifies *.* */
UF_UI_CAE_MDF_FLTR, /* Specifies *.mdf */
UF_UI_PART_SAVEAS_WITH_CATPRODUCT_FLTR, /* Specifies *.prt */
UF_UI_TRAN_CATIAV5_CATPRODUCT_FLTR, /* Specifies *.CATProduct */
UF_UI_JT_CONFIG_FLTR, /*Specifies *.config file*/
UF_UI_CAE_CONDSEQ_FLTR, /* Specifies *.bdd, *.* */
UF_UI_JPEG_FLTR, /* Specifies *.jpeg */
UF_UI_JPE_FLTR, /* Specifies *.jpe */
UF_UI_TIFF_FLTR, /* Specifies *.tiff */
UF_UI_RASTER_IMAGE_FLTR, /* Specifies *.jpg,*.jpeg,*.jpe,*.png,*.tif and *.tiff */
UF_UI_MOTION_LMS_MRES_FLTR, /* Specifies *.mres for LMS Motion */
UF_UI_REPORT_TEMPLATE_FLTR, /* Specifies *.docx */
UF_UI_REPORT_IMAGES_FLTR, /* Specifies *.jpg, *.tif, *.png and *.gif */
UF_UI_REPORT_ZIP_FLTR, /* Specifies *.rlfz */
UF_UI_TRAN_ACIS_IMPORT_FLTR, /*Specifies *.sat* and *.sab* */
UF_UI_TRAN_ACIS_EXPORT_FLTR, /*Specifies *.sat* and *.sab* */
UF_UI_TRAN_ACIS_SAT_FLTR, /*Specifies *.sat* */
UF_UI_TRAN_ACIS_SAB_FLTR, /*Specifies *.sab* */
UF_UI_POD_FLTR, /* Specifies *.pod */
UF_UI_IRAYPLUS_MATERIAL_FLTR, /* Specifies *.xml, *.mdl */
UF_UI_IRAYPLUS_MATERIAL_SYSTEM_SAVE_FLTR, /* Specifies *.xml */
UF_UI_IRAYPLUS_MDL_FLTR, /* Specifies *.mdl */
UF_UI_PSF_FLTR, /* Specifies *.psf* */
UF_UI_DGML_FLTR, /* Specifies *.dgml */
UF_UI_TRAN_STPX_FLTR,
UF_UI_TRAN_STPZ_FLTR,
UF_UI_TRAN_STPXZ_FLTR,
UF_UI_TRAN_STP242_FLTR,
UF_UI_TRAN_3MF_FLTR,
UF_UI_TRAN_WAVEFRONT_OBJ_FLTR,
UF_UI_CAE_LAYOUTSTATE_FLTR, /* For the layout states *.lsx */
UF_UI_MOTION_LMS_LMSMOTIONRESULTS_FLTR, /* Specifies *.lmsmotionresults for LMS Motion */
UF_UI_MOTION_LMS_OFF_FLTR, /* Specifies *.off tessellation for LMS Motion */
UF_UI_LIGHT_PROFILE_FILE_FLTR, /* Specifies light profile files *.ies */
UF_UI_CAE_APPPP_DATASOURCE_FLTR, /* For APPPP data sources */
UF_UI_CAE_RESULTSESSION_FLTR, /* For the Result Session Files *.rsfx */
UF_UI_XMCF_FLTR, /* For the *.xmcf */
UF_UI_PART_SAVEAS_WITH_PROTECTION, /* Specifies *.prt */
UF_UI_GIF_FLTR, /* Specifies *.gif */
UF_UI_BMP_FLTR, /* Specifies *.bmp */
UF_UI_XWD_FLTR, /* Sepcifies *.xwd */
UF_UI_FIELD_IMPORT_FLTR, /* Specifies *.fld, *.* */
UF_UI_XXML_FLTR, /* Speficies extended *.xml */
UF_UI_DIALOG_FILTER_COUNT /* UF_UI_DIALOG_FILTER_COUNT should
always be defined last */
} ;
typedef enum UF_UI_dialog_filter_id_e UF_UI_dialog_filter_id_t;
/*
* UF_UI_PART_OPEN_XT_FLTR was added in NX4 at the time when XT files were added
* to Part Open to be loaded into NX using the XT adapter. Shortly thereafter it
* was decided to make that case the default case for Part Open, rendering
* UF_UI_PART_OPEN_XT_FLTR unnecessary. However since the value was defined in a UF
* header there is the potential that NX/Open customers have files that reference the
* enum value. This define is to satisfy those customers. This define will be removed
* in NX6.
*/
#define UF_UI_PART_OPEN_XT_FLTR UF_UI_PART_OPEN_FLTR
/* Constants for FSD directory path access.
Refer to the enumerated constants
*/
enum UF_UI_dialog_dir_id_e{
UF_UI_EXPORT_DIR, /* This is used by File->Export->Part, File->Export->CGM,
File->Export->Parasolid, File->Export->Diagram,
File->Export->Rapid-Prototyping, and
Assemblies->Component Filters->Define Filter-> Export
*/
UF_UI_IMPORT_DIR, /* This is used by File->Import->Part, File->Import->CGM,
File->Import->Parasolid, File->Import->Markup,
Toolbox->Feature->User Defined,
Toolbox->Expression->Export,
Toolbox->Expression->Import,
Assemblies->Component Filters->Define Filter->Import
*/
UF_UI_PART_DIR, /* This is used by File->New, File->Open,
File->Save->Part As,
File->Export->Iges->Specify Part,
File->Import->Iges->Specify Part,
File->Export->Step203->Specify Part,
File->Import->Step203->Specify Part,
File->Export->Step214->Specify Part,
File->Import->Step214->Specify Part,
File->Export->Dxf->Specify Part,
File->Import->Dxf->Specify Part
*/
UF_UI_GRIP_DIR, /* This is used by File->Execute->Grip and
File->Execute-> Debug Grip. */
UF_UI_IMAGE_DIR, /* This is used by
View->Visualization->Create Quick Image->Save,
View->Visualization->Assembly Hidden Line->Save
View->Visualization->Display Image->Save
*/
UF_UI_IMPORT_SYMB_DIR,/* This is used by File->Import->Symbol Function.*/
UF_UI_IMPORT_BLOCK_DIR,/* This is used by File->Import->AutoCAD Block Function.*/
UF_UI_UFUN_DIR, /* This is used by File->Execute Open->User Function.
*/
UF_UI_MACRO_DIR, /* This is used by Macro->Playback and
Macro->Start Record.
*/
UF_UI_LAYOUT_DIR, /* This is no longer used. */
UF_UI_CAM_MDF_DIR, /* This is used by
Toolbox->CL Source File->Postprocess->GPM (Specify)
*/
UF_UI_CAM_GPM_DIR, /* */
UF_UI_CAM_CLF_DIR, /* This is used by
Toolbox->Tool Pth->Postprocess->Generate STD CLF
*/
UF_UI_CAM_CL_DIR, /* This is used by
Toolbox->Tool Path->Postprocess->Input File Name
(Specify).
*/
UF_UI_CAM_CLS_DIR, /* This is used by Applications->Manufacturing. */
UF_UI_CAM_BCL_DIR, /* This is used by
Toolbox->Tool Path->Postprocess->Output File Name
(Specify). */
UF_UI_CAM_ISO_DIR, /* This is used by
Toolbox->Tool Path->Postprocess->Generate ISO CLF
*/
UF_UI_CAM_NCOUT_DIR, /* This is used by
Toolbox->CL Source File->Postprocess->NC Output->Output File
*/
UF_UI_CAM_LISTOUT_DIR, /* */
UF_UI_CAM_ACL_DIR, /* This is used by
Toolbox->CL Source File->Postprocess->Output File Name
*/
UF_UI_CAM_S_DIR, /* This is used by
Toolbox->CL Source File->Postprocess->Input File Name
*/
UF_UI_CAM_ARC_DIR, /* This is used by
Machine Tool Builder -> Import NC Archive*/
UF_UI_CAM_CYC_DIR, /* This is used by
Program Manager -> Import Cyc Archive*/
UF_UI_CAM_MTK_DIR,/* This is used by
Machine Tool Builder -> Import Machine Tool Kit
*/
UF_UI_TRAN_IGS_DIR, /* This is used by
File->Export->Iges->Specify IGES File
File->Import->Iges->Specify IGES File
*/
UF_UI_TRAN_STP_DIR, /* This is used by
File->Export->Step203->Specify Step203 File
File->Import->Step203->Specify Step203 File
File->Export->Step214->Specify Step214 File
File->Import->Step214->Specify Step214 File
*/
UF_UI_TRAN_DXF_DIR, /* This is used by
File->Export->Dxf->Specify DXF File
File->Import->Dxf->Specify DXF File
*/
UF_UI_TRAN_IGES_DIR, /* This is used by
File->Export->Iges->Choose Defaults File
File->Import->Iges->Choose Defaults File
*/
UF_UI_TRAN_STEP203_DIR,/* This is used by
File->Export->Step203->Choose Defaults File
File->Import->Step203->Choose Defaults File
*/
UF_UI_TRAN_STEP214_DIR, /* This is used by
File->Export->Step214->Choose Defaults File
File->Import->Step214->Choose Defaults File
*/
UF_UI_TRAN_DXFTOUG_DIR, /* This is used by
File->Import->Dxf->Choose Defaults File
*/
UF_UI_TRAN_UGTODXF_DIR, /* This is used by
File->Export->Dxf->Choose Defaults File
*/
UF_UI_TRAN_LOG_DIR, /* This is used by
File->Export->Iges->Specify Log File
File->Export->Step203->Specify Log File
File->Export->Step214->Specify Log File
File->Export->Dxf->Specify Log File
File->Import->Iges->Specify Log File
File->Import->Step203->Specify Log File
File->Import->Step214->Specify Log File
File->Import->Dxf->Specify Log File
File->Export->Iges->Review Log File
File->Export->Step203->Review Log File
File->Export->Step214->Review Log File
File->Export->Dxf->Review Log File
File->Import->Iges->Review Log File
File->Import->Step203->Review Log File
File->Import->Step214->Review Log File
File->Import->Dxf->Review Log File
*/
UF_UI_MB_SYSLOG_DIR, /* This is used by
Info->Custom MenuBar->File Usage Report
*/
UF_UI_MISC_DATA_DIR, /* This is used by
Toolbox->Curve->Spline->By Poles->Points From File
Toolbox->Curve->Spline->Through Points->Points From File
Toolbox->Curve->Spline->Fit->Points From File
Toolbox->Free Form Feature->Through Points->Points From File
Toolbox->Free Form Feature->From Poles->Points From File
Toolbox->Free Form Feature->From Point Cloud->Points From File
Toolbox->Free Form Feature->Move Defining Point
Toolbox->Free Form Feature->Move Pole
Toolbox->Curve->Edit Curve->Edit Curve Parameters->
Edit Point->Points From File
Toolbox->Curve->Edit Curve->Edit Curve Parameters->
Edit Pole->Points From File
*/
UF_UI_CAM_TOOLIB_DIR, /* This is used by
Toolbox->Tool->LIbrary->Retrieve From Library
*/
UF_UI_CAM_LIBLIST_DIR, /* This is used by
Toolbox->Tool->LIbrary->List Library Entries
*/
UF_UI_CAM_DISPAT_DIR, /* This is used by
Applications->Manufacturing->Operation->
Edit Display->Specify (Pattern)->Pattern File Name
*/
UF_UI_CAM_VCUTS_DIR, /* This is used by
Preferences->General CAM->Use Vericut->Toolbox->ToolPath->
Vericut->Geometry Definition->OK
*/
UF_UI_CAM_VCUTT_DIR, /* This is used by
Preferences->General CAM->Use Vericut->Toolbox->ToolPath->
Vericut->Geometry Definitions->Output Type (Text)
*/
UF_UI_CAM_TEMPSET_DIR, /* */
UF_UI_NLE_DIR, /* */
UF_UI_RLIST_HRN_DIR, /* */
UF_UI_RLIST_CMP_DIR, /* */
UF_UI_CAM_CONFIG_DIR, /* */
UF_UI_CAM_SETUP_PRT_DIR, /* */
UF_UI_VDAC_CEO_DIR, /* */
UF_UI_VDAC_CFG_DIR, /* */
UF_UI_TBR_DIR, /* */
UF_UI_HATCH_DIR, /* */
UF_UI_BOOKMARK_DIR, /* */
UF_UI_CAM_SHOP_DOC_DIR, /* */
UF_UI_FMBD_FILE_DIR,
UF_UI_TRAN_DWG_DIR, /* This is used by
File->Export->DWG->Specify DWG File
File->Import->DWG->Specify DWG File
*/
UF_UI_MENU_DXF_DIR, /* This is used by
File->Import->DWG->Specify DWG File
*/
UF_UI_IMPORT_ASC_DIR, /* Used by File->Import->Ideas ASC/DWG */
UF_UI_TRAN_CATIA_DIR, /* This is used by
** File->Import->CATIA->Specify MOD or EXP File
*/
UF_UI_TRAN_CATMOD_DIR, /* This is used by
** File->Export->CATIA->Specify MOD File
*/
UF_UI_CAE_RPT_TEMPLATES_DIR, /* This is used by
** Structures->Tools->Report->Input to define
the htt template file of the report.
*/
UF_UI_CAE_RPT_IMG_DIR, /* This is used by
** Structures->Tools->Report->Input to define
the gif, jpg, mpg, vrml files of the report.
*/
UF_UI_INTEROP_FILE_DIR,
UF_UI_DRAFTING_IMAGE_DIR,/* This is used by
** Insert->Image in Drafting to select an image
file to create a drafting image from
*/
UF_UI_NX2D_FILE_DIR,
UF_UI_SPRD_FILE_DIR,
UF_UI_SPRDNT_FILE_DIR, /* This is used by Motion Analysis->Spreadsheet Run
** toolbar icon for selecting motion data spreadsheet
*/
UF_UI_SPRSHT_FILE_DIR,
UF_UI_XESS_FILE_DIR,
UF_UI_CAE_RST_DIR, /* This is used by
** Strutcures->Solution->Preload Result File
*/
UF_UI_CAE_RST_ODB_DIR,
UF_UI_CAE_ODB_DIR,
UF_UI_CAE_SAMCEF_DIR, /*used for *.des */
UF_UI_TRAN_CATIAV5_DIR, /* These two are used by CATIA V5 under */
UF_UI_TRAN_CATIAV5_CATPART_DIR, /* File Open, Save As, Import, and Export */
UF_UI_CAE_AFU_DIR, /* Used by *.afu File */
UF_UI_XYPLOT_DISP_TEMPLATE_DIR, /* Used by *.xml File */
UF_UI_MOTION_IMP_EXP_DIR, /* Used by *.xml File */
UF_UI_FTK_NAV_TREE_HISTORY_DIR, /* Used by *.xml File */
UF_UI_FACE_ANALYSIS_REFLECTION_DIR, /* Used by Face Analysis -> Reflections: User Specified Image */
UF_UI_BACKGROUND_IMAGE_DIR, /* Used by View -> Visualiztion -> Visual Effects: Background */
UF_UI_TEXTURE_IMAGE_DIR, /* Used by Materials Editor: Pattern: Simple Decal: Image */
UF_UI_IBL_IMAGE_DIR, /* Used by visual effects HDRI */
UF_UI_CAE_RPCIII_DIR, /* Used by *.rsp File */
UF_UI_CAE_DAC_DIR, /* Used by *.dac File */
UF_UI_CAE_CSV_DIR, /* Used by *.csv File */
UF_UI_TRAN_PROE_DIR, /* Used by PROE */
UF_UI_CAE_EEF_DIR, /* Used by *.eef File */
UF_UI_CAE_SEF_DIR, /* Used by *.sef File */
UF_UI_CAE_RS2_DIR, /* Used by *.rs2 File */
UF_UI_CAE_MAT_DIR, /* Used by *.mat File */
UF_UI_REPORT_TEMPLATE_DIR, /* Used by report template file, *.docx */
UF_UI_REPORT_IMAGES_DIR, /* Used by report images file, *.tif, *.jpg *.png and *.gif */
UF_UI_REPORT_ZIP_DIR, /* Used by *.rlfz File */
UF_UI_MOTION_ADAMS_RES_DIR, /* Used by *.res File */
UF_UI_MOTION_RECURDYN_RAD_DIR, /* Used by *.rad File */
UF_UI_PDF_DIR, /* Used by *.pdf File */
UF_UI_JPG_DIR, /* Used by *.jpg File */
UF_UI_TIF_DIR, /* Used by *.tif File */
UF_UI_EMF_DIR, /* Used by *.emf File */
UF_UI_PNG_DIR, /* Used by *.png File */
UF_UI_SYM_DIR, /* Used by *.sym File */
UF_UI_CAE_UNV58_DIR, /* Used by *.unv(dataset58) File */
UF_UI_KF_MISC1_DIR, /* Used by UI_Comp_KFSelectFile */
UF_UI_KF_MISC2_DIR, /* Used by UI_Comp_KFSelectFile */
UF_UI_KF_MISC3_DIR, /* Used by UI_Comp_KFSelectFile */
UF_UI_KF_MISC4_DIR, /* Used by UI_Comp_KFSelectFile */
UF_UI_KF_MISC5_DIR, /* Used by UI_Comp_KFSelectFile */
UF_UI_SIMULINK_MDL_DIR, /* Used by *.mdl File*/
UF_UI_SIMULINK_M_DIR, /* Used by *.m File*/
UF_UI_MOTION_EXPORT_SDK_RMD_DIR, /* Used by Export->RecurDyn Input in Motion RecurDyn */
UF_UI_STANDARD_FONTS_DIR, /* Used by DisplayUI_UICompSelectFontFile */
UF_UI_IGES_EXPORT_DIR, /* Used by File->Export->IGES */
UF_UI_STEP_EXPORT_DIR, /* Used by File->Export->STEP203, STEP214) */
UF_UI_MOTION_FLEXBODY_RFI_DIR, /* Used by *.rfi File*/
UF_UI_ATTR_CATALOG_DIR, /* Used by *.xml File*/
UF_UI_MW_DIR, /* Used by *.mw File */
UF_UI_TRUMPF_GEO_DIR, /* Used by .geo file */
UF_UI_TIRE_SPINDLE_DIR, /* Used by *.spindle File */
UF_UI_MOTION_RECURDYN_RAD_RAN_DIR, /* Used by *.ran File */
UF_UI_MECHDES_RUNTIME_CODE_DIR, /* Used by *.cs and *.dll file*/
UF_UI_CAE_UNV_DIR, /* Used by *.unv File */
UF_UI_PAX_DIR, /* Used by *.pax file */
UF_UI_HDF5_DIR, /* Used by *.h5 file */
UF_UI_LAYUP_DIR, /* Used by *.Layup file */
UF_UI_CAE_BROWSE_DIR, /*Used by Solution->Browse*/
UF_UI_CAE_MDF_DIR, /* Used for .mdf file */
UF_UI_TRAN_CATIAV5_CATPRODUCT_DIR, /* File Open, Save As, Import, and Export */
UF_UI_CAE_CONDSEQ_DIR, /* Used by *.bdd file */
UF_UI_MOTION_LMS_MRES_DIR, /* Used by *.mres file in Motion LMS */
UF_UI_CAE_RST_XDB_DIR, /* This is used by PostProcessing import Result File (to be removed) */
UF_UI_CAE_RST_XDB_ODB_DIR, /* This is used by PostProcessing import Result File (to be removed) */
UF_UI_TRAN_ACIS_DIR,
UF_UI_TRAN_ACIS_SAT_DIR,
UF_UI_TRAN_ACIS_SAB_DIR,
UF_UI_MOTION_FLEXBODY_OP2_DIR, /* Used by *.op2 File containing flexible body */
UF_UI_POD_DIR, /* Used by *.pod files Point Cloud ) */
UF_UI_DGML_DIR, /* Used by *.dgml XML-based file format for directed graphs */
UF_UI_TRAN_STPX_DIR,
UF_UI_TRAN_STPZ_DIR,
UF_UI_IRAYPLUS_MATERIAL_DIR, /* Used by IrayPlus Material Editor Export to *.xml file */
UF_UI_IRAYPLUS_MATERIAL_SYSTEM_SAVE_DIR, /* Used by IrayPlus Material Editor Save to System Studio Materials *.xml file */
UF_UI_IRAYPLUS_MDL_DIR, /* Used by Import MDL *.mdl file */
UF_UI_TRAN_STPXZ_DIR,
UF_UI_TRAN_STP242_DIR,
UF_UI_TRAN_3MF_DIR,
UF_UI_TRAN_WAVEFRONT_OBJ_DIR,
UF_UI_CAE_LAYOUTSTATE_DIR,
UF_UI_MOTION_LMS_LMSMOTIONRESULTS_DIR, /* Used by *.lmsmotionresults for motion result files in LMS */
UF_UI_CAE_APPPP_DATASOURCE_DIR, /* Used by CaeUI::APPPP::SelectDataSource */
UF_UI_LIGHT_PROFILE_FILE_DIR, /* Used to specify a light profile file */
UF_UI_XMCF_DIR, /* Used by Universal connection editor to export to *.xmcf file */
UF_UI_CAE_RESULTSESSION_DIR,
UF_UI_GIF_DIR, /* Used by *.gif File */
UF_UI_BMP_DIR, /* Used by *.bmp File */
UF_UI_XWD_DIR, /* Used by *.xwd FIle */
UF_UI_FIELD_IMPORT_DIR, /* Specifies *.fld, *.* */
UF_UI_XXML_DIR, /* Specifies extended *.xml */
/*
*/
UF_UI_DIALOG_DIR_COUNT /* UF_UI_DIALOG_DIR_COUNT should
always be last */
} ;
typedef enum UF_UI_dialog_dir_id_e UF_UI_dialog_dir_id_t;
/****************************************************************************
* Limit definitions
* Used within 'UF_UI_write_listing_window'
*
* UF_UI_MAX_STRING_LEN is being deprecated because NX is moving to support
* multibyte characters. User written programs should start using the
* new definitions for file specifications:
* UF_UI_MAX_STRING_BUFSIZE should be used for buffer allocations and memory
* allocations, e.g. char my_string[UF_UI_MAX_STRING_BUFSIZE];
* UF_UI_MAX_STRING_NCHARS should be used to limit the number of characters in
* a buffer. NX code will enforce these limits.
*
* New routines have been added which will help in this transition:
* UF_TEXT_count_characters() will count the number of characters in a buffer.
* UF_TEXT_terminate_chars() will terminate a C string after the given
* number of characters.
****************************************************************************/
#define UF_UI_MAX_STRING_NCHARS 1000 /* Maximum number of characters in a UI string excluding the trailing '\0'. These may be multi-byte characters. */
#define UF_UI_MAX_STRING_BUFSIZE NX_BUFSIZE(UF_UI_MAX_STRING_NCHARS)
/* */
#define UF_UI_MAX_STRING_LEN (UF_UI_MAX_STRING_BUFSIZE - 1)
/* */
/* structure used by
UF_UI_select_point_collection
*/
struct UF_UI_chained_points_s
{
double pt[3];
tag_t object;
} ;
typedef struct UF_UI_chained_points_s UF_UI_chained_points_t,
*UF_UI_chained_points_p_t;
/* Constants for selection solid_type */
#define UF_UI_SEL_NOT_A_FEATURE (-1)
#define UF_UI_SEL_FEATURE_BODY 0
#define UF_UI_SEL_FEATURE_ANY_EDGE 1
#define UF_UI_SEL_FEATURE_LINEAR_EDGE 2
#define UF_UI_SEL_FEATURE_CIRCULAR_EDGE 3
#define UF_UI_SEL_FEATURE_ELLIPTICAL_EDGE 4
#define UF_UI_SEL_FEATURE_INTERSECTION_EDGE 5
#define UF_UI_SEL_FEATURE_BCURVE_EDGE 6
#define UF_UI_SEL_FEATURE_SPCURVE_EDGE 7
#define UF_UI_SEL_FEATURE_FOREIGN_EDGE 8
#define UF_UI_SEL_FEATURE_CNST_PARM_EDGE 9
#define UF_UI_SEL_FEATURE_ANY_WIRE_OR_EDGE 10
/* 11 to 14 are reserved for additional solid_type use */
/*
*/
#define UF_UI_SEL_FEATURE_CONVERGENT_EDGE 15
#define UF_UI_SEL_FEATURE_CONVERGENT_FACE 16
#define UF_UI_SEL_FEATURE_CONVERGENT_SOLID_BODY 17
#define UF_UI_SEL_FEATURE_CONVERGENT_SHEET_BODY 18
#define UF_UI_SEL_FEATURE_ANY_SHEET 19 /* Do not use this, use _SHEET_BODY or _ANY_FACE */
#define UF_UI_SEL_FEATURE_ANY_FACE 20
#define UF_UI_SEL_FEATURE_PLANAR_FACE 21
#define UF_UI_SEL_FEATURE_CYLINDRICAL_FACE 22
#define UF_UI_SEL_FEATURE_CONICAL_FACE 23
#define UF_UI_SEL_FEATURE_SPHERICAL_FACE 24
#define UF_UI_SEL_FEATURE_TOROIDAL_FACE 25
#define UF_UI_SEL_FEATURE_PARAMETRIC_FACE 26
#define UF_UI_SEL_FEATURE_BLENDING_FACE 27
#define UF_UI_SEL_FEATURE_OFFSET_FACE 28
#define UF_UI_SEL_FEATURE_SWEPT_FACE 29
#define UF_UI_SEL_FEATURE_SWUNG_FACE 30
#define UF_UI_SEL_FEATURE_FOREIGN_FACE 31
#define UF_UI_SEL_FEATURE_ANY_COMPOSITE_BODY 32
#define UF_UI_SEL_FEATURE_ANY_COMPOSITE_FACE 33
#define UF_UI_SEL_FEATURE_ANY_COMPOSITE_EDGE 34
#define UF_UI_SEL_FEATURE_SHEET_BODY 35
#define UF_UI_SEL_FEATURE_SOLID_BODY 36 /* non-sheet-body */
#define UF_UI_SEL_FEATURE_MAX_FEATURE 36
/* 40-90 are reserved for feature type selection use */
/* Special features, no type or subtype is needed. */
#define UF_UI_SEL_FEATURE_ROUTING_CURVE_ONLY 91 /* This should be first of special feature types */
#define UF_UI_SEL_FEATURE_ROUTING_SOLID_ONLY 92
#define UF_UI_SEL_FEATURE_WORK_PART_COMP 93
/*
*/
#define UF_UI_SEL_FEATURE_WELD_RESIS_SPOT 94
#define UF_UI_SEL_FEATURE_WELD_ARC_SPOT 95
#define UF_UI_SEL_FEATURE_WELD_MEC_CLINCH 96
#define UF_UI_SEL_FEATURE_WELD_DOLLOP 97
#define UF_UI_SEL_FEATURE_WELD_NUT 98
#define UF_UI_SEL_FEATURE_WELD_STUD 99
#define UF_UI_SEL_FEATURE_WELD_CUSTOM1 100
#define UF_UI_SEL_FEATURE_WELD_CUSTOM2 101
#define UF_UI_SEL_FEATURE_WELD_CUSTOM3 102
#define UF_UI_SEL_FEATURE_WELD_CUSTOM4 103
#define UF_UI_SEL_FEATURE_WELD_CUSTOM5 104
#define UF_UI_SEL_FEATURE_WELD_GROOVE 105
#define UF_UI_SEL_FEATURE_WELD_FILLET 106
#define UF_UI_SEL_FEATURE_WELD_USER_DEFINED 107
#define UF_UI_SEL_FEATURE_WELD_FILL 108
#define UF_UI_SEL_FEATURE_WELD_BEAD 109
#define UF_UI_SEL_FEATURE_WELD_JOINT 110
#define UF_UI_SEL_FEATURE_WELD_EDGE 111
#define UF_UI_SEL_FEATURE_WELD_RESIS_SEAM 112
#define UF_UI_SEL_FEATURE_WELD_PLUG_SLOT 113
#define UF_UI_SEL_FEATURE_WELD_SURFACE_WELD 114
#define UF_UI_SEL_FEATURE_WELD_JOINTMARK 115
#define UF_UI_SEL_FEATURE_WELD_TRANSFORM 116
/*
*/
#define UF_UI_SEL_FEATURE_WELD_COMPOUND 117
/*
*/
#define UF_UI_SEL_FEATURE_WELD_DATUM_SURFACE 118
#define UF_UI_SEL_FEATURE_WELD_DATUM_PIN 119
#define UF_UI_SEL_FEATURE_WELD_DATUM_CUSTOM1 120
#define UF_UI_SEL_FEATURE_WELD_DATUM_CUSTOM2 121
#define UF_UI_SEL_FEATURE_WELD_DATUM_CUSTOM3 122
/*
*/
#define UF_UI_SEL_FEATURE_WELD_MEASUREMENT_SURFACE 123
#define UF_UI_SEL_FEATURE_WELD_MEASUREMENT_HOLE 124
#define UF_UI_SEL_FEATURE_WELD_MEASUREMENT_STUD 125
#define UF_UI_SEL_FEATURE_WELD_MEASUREMENT_SLOT 126
#define UF_UI_SEL_FEATURE_WELD_MEASUREMENT_TRIM 127
#define UF_UI_SEL_FEATURE_WELD_MEASUREMENT_HEMMED_EDGE 128
#define UF_UI_SEL_FEATURE_WELD_MEASUREMENT_CUSTOM1 129
#define UF_UI_SEL_FEATURE_WELD_MEASUREMENT_CUSTOM2 130
#define UF_UI_SEL_FEATURE_WELD_MEASUREMENT_CUSTOM3 131
#define UF_UI_SEL_FEATURE_MAX_SPECIAL_FEATURE 132 /* This should be last of special feature types */
/* Define UF_pseudo_object_type and corresponsing subtypes and detail types:
* UF_pseudo_object_type is used for selection only and for object types not defined in uf_object_types.h
*/
#define UF_pseudo_object_type (-1)
/* The subtypes for UF_pseudo_object_type: */
/* For CAE: */
#define UF_pseudo_CAE_subtype (1)
#define UF_pseudo_CAE_node (1) /* first CAE detail type */
#define UF_pseudo_CAE_element (2) /* second CAE detail type */
#define UF_pseudo_CAE_elemface (3) /* third CAE detail type */
#define UF_pseudo_CAE_elemedge (4) /* fourth CAE detail type */
struct UF_UI_mask_s
{
int object_type; /* This can be one of the object types that are listed in
uf_object_types.h or UF_pseudo_object_type */
int object_subtype; /* This can either be UF_all_subtype (not with UF_pseudo_object_type),
or one of the corresponding supported subtypes of the object type specified.
This is ignored for certain types like UF_solid_type */
int solid_type; /* This should be named detail_type and is only meaningful for certain object_types like
UF_solid_type, UF_feature_type or UF_pseudo_type.
This should be set to one of the corresponding detail types
of the object type and object_subtype specified.
This is ignored for UF_all_subtype. */
} ;
typedef struct UF_UI_mask_s UF_UI_mask_t, *UF_UI_mask_p_t;
/* structure used by
UF_UI_select_single
UF_UI_select_by_class
Refer to the table
*/
struct UF_UI_selection_option_s
{
int num_mask_triples;
UF_UI_mask_p_t mask_triples; /* */
int scope; /* scopes are listed in uf_ui.h */
int other_options; /* initially ignored (set to 0) */
void *reserved; /* initially ignore (set to NULL) */
} ;
typedef struct UF_UI_selection_option_s UF_UI_selection_options_t,
*UF_UI_selection_options_p_t;
/* selection ptr which is input to UF_UI selection functions.
This ptr is a unique identifier for the selection associated with
a particular dialog. It is assigned by NX and provided to the
UF programmer when needed. */
typedef void* UF_UI_selection_p_t;
/* typedef for selection initialization procedure.
This is an argument to UF_UI_select_with_class_dialog and
UF_UI_select_with_single_dialog. It is an optional procedure
which the user can provide to customize his selection */
typedef int (*UF_UI_sel_init_fn_t)(
UF_UI_selection_p_t select_, /* <I> ptr to selection */
void *user_data /* <I> ptr to user data */
);
/* typedef for application selection filter procedure.
This procedure and optional user data is specified by calling
UF_UI_set_sel_procs.
It is an optional procedure which the user can provide to perform
application specific filtering when selecting objects.
It can be used with UF_UI_select_with_single_dialog,
UF_UI_select_with_class_dialog and
dialogs created with the UI Styler. */
typedef int (*UF_UI_sel_filter_fn_t)(
tag_t object, /* <I> candidate object */
int type[3], /* <I> object type, object subtype,
solid type */
void *user_data, /* <I> ptr to user's data */
UF_UI_selection_p_t select_ /* <I> ptr to selection */);
/* typedef for application selection callback.
This procedure and optional user data is specified by calling
UF_UI_set_set_procs.
It is an optional procedure which the user can provide to perform
application specific processing for each selection.
This can be used with UF_UI_select_with_single_dialog,
UF_UI_select_with_class_dialog and
dialogs created with the UI Styler */
typedef int (*UF_UI_sel_cb_fn_t)(
int num_selected, /* <I> number of objects just selected */
tag_p_t selected_objects, /* <I>
array of selected objects */
int num_deselected, /* <I> number of objects just deselected */
tag_p_t deselected_objects, /* <I>
array of deselected objects */
void *user_data, /* <I> ptr to user's data */
UF_UI_selection_p_t select_ /* <I> ptr to selection */);
/* typedefs for motion callbacks, which can be passed to
UF_UI_specify_screen_position.
*/
struct UF_UI_motion_cb_data_s
{
tag_t view_tag; /* The tag of the current view of the
crosshairs. */
double start_position[3]; /* Screen position at the time this "gesture"
* was started. This is the position in
* Work Part Absolute Coords obtained by
* projecting the cursor position "through the
* screen" onto the XY plane of the WCS;
* if Grid Snap is on, this is the "snapped"
* position. */
tag_t start_view_tag; /* The view tag of the start position. */
} ;
typedef struct UF_UI_motion_cb_data_s UF_UI_motion_cb_data_t,
*UF_UI_motion_cb_data_p_t;
typedef void (*UF_UI_motion_fn_t)(
double screen_pos[3], /* <I> The current screen position in
* Work Part Absolute Coordinates;
* This is the crosshair position
* projected "through the screen"
* onto the XY plane of the WCS;
* if Grid Snap is on, this is the
* "snapped" position. */
UF_UI_motion_cb_data_p_t motion_cb_data,
/* <I> Ptr to a UF_UI_motion_cb_data_t
* structure. */
void *data /* <I> The client data, provided with
* the callback. */
);
/* User Function Custom Applications prototypes
constant definitions and type definitions */
#define UF_UI_END_MENU {UF_UI_END_CUSTOM_MENU,NULL,\
NULL,FALSE,NULL,NULL}
#define UF_UI_END_CASCADE_MENU {UF_UI_END_CUSTOM_CASCADE_MENU,\
NULL,NULL,FALSE,NULL,NULL}
enum UF_UI_MENU_TYPE_e{
UF_UI_MENU = 1, /* menu item */
UF_UI_CASCADE_MENU, /* cascade pulldown */
UF_UI_PUSH, /* push button */
UF_UI_TOGGLE, /* Toggle button for pulldown */
UF_UI_BUTTON_SEPARATOR, /* pulldown items separator */
UF_UI_END_CUSTOM_CASCADE_MENU, /* end of cascade pulldown */
UF_UI_END_CUSTOM_MENU /* end of menu item */
} ;
typedef enum UF_UI_MENU_TYPE_e UF_UI_MENU_TYPE;
typedef void (*UF_UI_cb_proc)(void);
struct UF_UI_menubar_item_s
{
UF_UI_MENU_TYPE type; /* may be any type in UF_UI_MENU_TYPE above */
char *text; /* label to put on the button */
char *name; /* name of the resource for button */
int state; /* state of the button */
UF_UI_cb_proc CBproc; /* activate callback procedure */
void *CBdata; /* activate callback data */
};
typedef struct UF_UI_menubar_item_s UF_UI_menubar_item_t,
*UF_UI_menubar_item_p_t;
#define UF_UI_enable_all 1
#define UF_UI_disable_all 2
#define UF_UI_enable_specific 3
#define UF_UI_disable_specific 4
/******************************************************************************
* Type definitions for UF_UI_<create|open>_part error handling routines
******************************************************************************/
/* Structure containing the user data to pass to the error handling function */
struct UF_UI_err_data_s {
int size; /* Size of 'data' in bytes */
const void *data; /* Pointer to data to pass to error handling function */
} ;
typedef struct UF_UI_err_data_s UF_UI_err_data_t,
*UF_UI_err_data_p_t;
/******************************************************************************
logical (*UF_UI_create_part_err_f_t)
Return:
TRUE - Redisplay the File-New dialog (i.e. keep trying to create a
part)
FALSE - Exit the File-New dialog (i.e. exit UF_UI_create_part)
Environment:
see also:
History:
******************************************************************************/
typedef logical (*UF_UI_create_part_err_f_t)(
UF_UI_err_data_p_t error_fn_data, /* <I>
User data
*/
char *file_name, /* <I>
File name specified in the File-New dialog
*/
int error, /* <I>
Error code associated with file_name
*/
logical *skip_error_disp /* <O>
Display standard File-New dialog error i
message indicator
TRUE - Allow File-New to display the
error message it would normally display
FALSE - Do not allow File-New to display
the message it would normally display
*/
);
/******************************************************************************
logical (*UF_UI_open_part_err_f_t)
Return:
TRUE - Redisplay the File-Open dialog (i.e. keep trying to open a
part)
FALSE - Exit the File-Open dialog (i.e. exit UF_UI_open_part)
Environment:
See also:
History:
******************************************************************************/
typedef logical (*UF_UI_open_part_err_f_t)(
UF_UI_err_data_p_t error_fn_data, /* <I>
User data
*/
char *file_name, /* <I>
File name specified in the File-Open
dialog
*/
int error, /* <I>
Error code associated with file_name
*/
UF_PART_load_status_t *error_status, /* <I>
Structure filled with names and associated
error codes of any parts that did not load
properly.
NOTE: The allocated arrays must be freed.
*/
logical *skip_error_disp /* <O>
Display standard File-Open dialog error
message indicator
TRUE - Allow File-Open to display the
error it would normally display
FALSE - Do not allow File-Open to
display the error message it would
normally display
*/
);
/* Definitions for type of error handling function */
enum UF_UI_fun_type_e{
UF_UI_create_part_fun,
UF_UI_open_part_fun
} ;
typedef enum UF_UI_fun_type_e UF_UI_fun_type_t;
/* General error handling function type */
union UF_UI_err_u {
UF_UI_create_part_err_f_t create;
UF_UI_open_part_err_f_t open;
} ;
typedef union UF_UI_err_u UF_UI_err_u_t;
/* Structure containing error handling function and the user data to pass
* to it */
struct UF_UI_err_s {
UF_UI_fun_type_t type; /* Type of function in 'fun' */
UF_UI_err_u_t fun; /* UF_UI_<create|open>_part error function */
UF_UI_err_data_t fun_data; /* Pointer to data to pass to 'fun' */
} ;
typedef struct UF_UI_err_s UF_UI_err_t, *UF_UI_err_p_t;
/* Toolbar id returned by UF_UI_create_toolbar() */
typedef struct UF_UI_toolbar_id_s *UF_UI_toolbar_id_t;
/* Toolbar id returned by UF_UI_create_ribbon() */
typedef struct UF_UI_toolbar_id_s *UF_UI_ribbon_id_t;
/* UF feature selection type enum */
enum UF_UI_feat_sel_type_e
{
UF_UI_FEAT_SEL_TYPE_BROWSEABLE = 0, /* General browseable feature */
UF_UI_FEAT_SEL_TYPE_NO_BOOLEAN_UDF, /* No boolean and udf features */
UF_UI_FEAT_SEL_TYPE_LAST /* Last enum mark, don't use this. */
};
typedef enum UF_UI_feat_sel_type_e UF_UI_feat_sel_type_t;
/* enum for UF_UI_point_construct */
enum UF_UI_point_base_method_e
{
UF_UI_POINT_INFERRED = 0,
UF_UI_POINT_CURSOR_POS,
UF_UI_POINT_EXISTING_PT,
UF_UI_POINT_END_PT,
UF_UI_POINT_CONTROL_PT,
UF_UI_POINT_INTERSECT_PT,
UF_UI_POINT_CENTER_PT,
UF_UI_POINT_ANGLE_PT,
UF_UI_POINT_QUADRANT_PT,
UF_UI_POINT_ON_CURVE_PT,
UF_UI_POINT_ON_SURFACE_PT,
UF_UI_POINT_OFFSET_CSYS_PT,
UF_UI_POINT_DIALOG,
UF_UI_POINT_NO_METHOD,
UF_UI_POINT_APPLICATION_METHOD
};
typedef enum UF_UI_point_base_method_e UF_UI_POINT_base_method_t, *UF_UI_POINT_base_method_p_t;
/* Defines for File Operation callback for UI Styler
created dialogs. */
#define UF_UI_FILE_NEW (0)
#define UF_UI_FILE_OPEN (1)
#define UF_UI_FILE_SAVE (2)
#define UF_UI_FILE_SAVE_AS (3)
#define UF_UI_FILE_SAVE_ALL (4)
#define UF_UI_FILE_CLOSE (5)
#define UF_UI_FILE_QUIT (6)
#define UF_UI_FILE_SAVE_AND_EXIT (7)
#define UF_UI_FILE_CHANGE_PART (8)
#define UF_UI_FILE_EXECUTE (9)
#define UF_UI_FILE_REOPEN (10)
#define UF_UI_FILE_SAVEALL_AND_CLOSE (11)
#define UF_UI_FILE_SAVE_AND_CLOSE (12)
#define UF_UI_FILE_SAVEAS_AND_CLOSE (13)
struct UF_UI_attachment_s
{
short center;
short attach_type_top;
short attach_type_left;
short attach_type_right;
short offset_top;
short offset_left;
short offset_right;
const char *item_id_top;
const char *item_id_left;
const char *item_id_right;
};
typedef struct UF_UI_attachment_s UF_UI_attachment_t, *UF_UI_attachment_p_t;
#define UF_UI_ATTACH_DIALOG (-1)
#define UF_UI_ATTACH_DEFAULT (-2)
#define UF_UI_ATTACH_NONE (-3)
#define UF_UI_ATTACH_NO_CHANGE (-4)
#define UF_UI_ATTACH_ITEM (-5)
/* Option Toggle Data */
struct UF_UI_option_toggle_s
{
int choice; /* active option */
logical is_checked; /* check box state */
};
typedef struct UF_UI_option_toggle_s UF_UI_option_toggle_t, *UF_UI_option_toggle_p_t;
#endif /* UF_UI_TYPES_H_INCLUDED */