tag_t | udo_tag | Input | -- the tag for the UDO whose attention point is being defined |
void * | display_context | Input | -- a pointer to a private structure used in display calls |
tag_t | udo_tag | Input | -- the tag for the UDO who has an associated object being deleted |
UF_UDOBJ_link_p_t | deleted_obj | Input | -- the link for the item that is deleted |
tag_t | udo_tag | Input | -- the tag for the UDO being displayed |
void * | display_context | Input | -- a pointer to a private structure used in display calls |
tag_t | udo_tag | Input | -- the tag for the UDO which is being edited in the callback |
tag_t | udo_tag | Input | -- the tag for the UDO being fit to the view |
void * | display_context | Input | -- a pointer to a private structure used in fit calls |
tag_t | udo_tag | Input | -- the tag for the UDO for which information is being requested |
tag_t | udo_tag | Input | -- the tag for the UDO being fit to the view |
logical * | is_occurrenceable | Output | -- TRUE if object can be occurrenced otherwise FALSE |
tag_t | udo_tag | Input | -- the tag for the UDO whose screen-size objects need to be fit to the view |
void * | display_context | Input | -- a pointer to a private structure used in screen-size-fit calls |
tag_t | udo_tag | Input | -- the tag for the UDO being selected |
void * | display_context | Input | -- a pointer to a private structure used in selection calls |
tag_t | udo_feat_tag | Input | -- the tag for the UDO feature which is being suppressed in the callback |
tag_t | udo_tag | Input | -- the tag for the UDO being updated |
UF_UDOBJ_link_p_t | update_cause | Input | -- the link for the item that caused the UDO to be updated |