UF_SKET_assoc_mod_e (view source)
 
Defined in: uf_sket_types.h
 
Also known as:
 


Data Members

UF_SKET_first_end_point


UF_SKET_last_end_point


 


 
UF_SKET_assoc_type_e (view source)
 
Defined in: uf_sket_types.h
 
Also known as:
 
Overview
Associativity types for sketch dimension.


Data Members

UF_SKET_assoc_type_none


UF_SKET_end_point


UF_SKET_arc_center


UF_SKET_tangency


UF_SKET_curve_point


UF_SKET_anchor_point


 


 
UF_SKET_con_class_e (view source)
 
Defined in: uf_sket_types.h
 
Also known as:
 


Data Members

UF_SKET_no_cons


UF_SKET_all_cons


UF_SKET_geo_cons


UF_SKET_dim_cons


 


 
UF_SKET_con_type_e (view source)
 
Defined in: uf_sket_types.h
 
Also known as:
 


Data Members

UF_SKET_no_con


UF_SKET_fixed


UF_SKET_horizontal


UF_SKET_vertical


UF_SKET_parallel


UF_SKET_perpendicular


UF_SKET_collinear


UF_SKET_equal_length


UF_SKET_equal_radius


UF_SKET_constant_length


UF_SKET_constant_angle


UF_SKET_coincident


UF_SKET_concentric


UF_SKET_mirror


UF_SKET_point_on_curve


UF_SKET_midpoint


UF_SKET_tangent


UF_SKET_radius_dim


UF_SKET_diameter_dim


UF_SKET_horizontal_dim


UF_SKET_vertical_dim


UF_SKET_parallel_dim


UF_SKET_perpendicular_dim


UF_SKET_angular_dim


UF_SKET_reserved_con_1
Do not use

UF_SKET_reserved_con_2
Do not use

UF_SKET_reserved_con_3
Do not use

UF_SKET_reserved_con_4
Do not use

UF_SKET_reserved_con_5
Do not use

UF_SKET_reserved_con_6
Do not use

UF_SKET_point_on_string


UF_SKET_slope


UF_SKET_uniform_scaled


UF_SKET_non_uniform_scaled


UF_SKET_assoc_trim
Limited support

UF_SKET_assoc_offset
Limited support

UF_SKET_perimeter_dim


UF_SKET_pgm_offset


UF_SKET_normal


UF_SKET_point_on_loop


UF_SKET_recipe_trim


UF_SKET_pattern


UF_SKET_rigid_set


UF_SKET_g1


UF_SKET_g2


UF_SKET_align


UF_SKET_tangent_to_string


UF_SKET_perpendicular_to_string


UF_SKET_scalable_set


UF_SKET_last_con_type
The last constraint type indicator; NOT to be used.

 


 
UF_SKET_geom_vertex_e (view source)
 
Defined in: uf_sket_types.h
 
Also known as:
 
Overview
enum and structures for createing geometric constraints


Data Members

UF_SKET_no_vertex


UF_SKET_start_vertex


UF_SKET_end_vertex


UF_SKET_center_vertex
used only for Arcs/Ellipses

UF_SKET_spline_defining_point
used only for splines

UF_SKET_anchor_vertex
used only by general conics

UF_SKET_spline_pole
used only for splineByPoles

UF_SKET_mid_vertex
used only for Arcs/Lines

 


 
UF_SKET_help_type_e (view source)
 
Defined in: uf_sket_types.h
 
Also known as:
 


Data Members

UF_SKET_no_help_data


UF_SKET_use_help_pt


UF_SKET_use_help_param


 


 
UF_SKET_reference_status_e (view source)
 
Defined in: uf_sket_types.h
 
Also known as:
 


Data Members

UF_SKET_reference


UF_SKET_active


 


 
UF_SKET_status_e (view source)
 
Defined in: uf_sket_types.h
 
Also known as:
 
Overview
As of V17, the values of these UF_SKET_status_e will be recorded in
the part file. Hence, their values cannot be arbitrarily changed.


Data Members

UF_SKET_unknown_status


UF_SKET_not_evaluated


UF_SKET_under_constrained


UF_SKET_well_constrained


UF_SKET_over_constrained


UF_SKET_inconsistently_constrained