/*
uf_sf_enums.h
File Description :
Enumeration Definitions for the Open C API interface to Advanced Simulation
*****************************************************************************/
#ifndef UF_SF_ENUMS__H_INCLUDED
#define UF_SF_ENUMS__H_INCLUDED
enum UF_SFNAS_inter_output_types_e
{
INTOUT_YES = 0,
INTOUT_NO,
INTOUT_ALL
};
typedef enum UF_SFNAS_inter_output_types_e UF_SFNAS_inter_output_types_t;
typedef enum UF_SFNAS_inter_output_types_e SFNAS_inter_output_types_t;
enum UF_SF_node_btype_e
{
UF_SF_NODE_BODYINTERIOR, /* Node on the interior of a body. */
UF_SF_NODE_EDGE, /* Node on an edge. */
UF_SF_NODE_FACEINTERIOR, /* Node on the interior of a face. */
UF_SF_NODE_INTERIOR, /* Interior node. */
UF_SF_NODE_NO_GEOMETRY, /* Node not on any geometry. */
UF_SF_NODE_POINT /* Node on point. The point could be on
Edge or Face, but the node on point
is not a part of mesh on edge/face. */
};
typedef enum UF_SF_node_btype_e UF_SF_node_btype_t,
*UF_SF_node_btype_p_t;
enum UF_SF_node_switch_e
{
UF_SF_SWITCH_ON_BOUNDARY, /* Switch to nodes only on the boundary. */
UF_SF_SWITCH_IN_INTERIOR, /* Switch to nodes only in the interior. */
UF_SF_SWITCH_ALL /* Switch to all nodes, independent of the
location. */
};
typedef enum UF_SF_node_switch_e UF_SF_node_switch_t,
*UF_SF_node_switch_p_t;
enum UF_SF_mid_node_type_e
{
UF_SF_NODE_CORNER, /* Node on the corner. */
UF_SF_NODE_DISABLED, /* Node disabled. */
UF_SF_NODE_MID, /* Node on the middle. */
UF_SF_NODE_ORIENTATION /* Node with an orientation. */
};
typedef enum UF_SF_mid_node_type_e UF_SF_mid_node_type_t,
*UF_SF_mid_node_type_p_t;
/* meshdir codes associated with mesh geometry in a mesh recipe */
enum UF_SF_mesh_geom_meshdir_e
{
UF_SF_MG_MESHDIR_UNINITIALIZED = 0, /* Uninitialized mesh direction. */
UF_SF_MG_MESHDIR_UNDEFINED, /* Undefined mesh direction. */
UF_SF_MG_MESHDIR_FROM_START, /* Mesh direction from line start */
UF_SF_MG_MESHDIR_FROM_END, /* Mesh direction from line end */
UF_SF_MG_MESHDIR_REVERSE, /* Reverse the mesh direction */
UF_SF_MG_MESHDIR_DONT_REVERSE /* Do not reverse the mesh direction. */
};
typedef enum UF_SF_mesh_geom_meshdir_e UF_SF_mesh_geom_meshdir_t,
*UF_SF_mesh_geom_meshdir_p_t;
enum UF_SF_mesh_recipe_adaptivity_e
{
UF_SF_MESH_RECIPE_ADAPT_HELMS, /* Adaptivity of elements is H-type. */
UF_SF_MESH_RECIPE_ADAPT_PELMS /* Adaptivity of elements is P-type. */
};
typedef enum UF_SF_mesh_recipe_adaptivity_e UF_SF_mesh_recipe_adaptivity_t,
*UF_SF_mesh_recipe_adaptivity_p_t;
enum UF_SF_elm_adaptivity_type_e
{
UF_SF_ELEMENT_ADAPT_HELMS = (int)UF_SF_MESH_RECIPE_ADAPT_HELMS,
/* Adaptivity of elements is H-type. */
UF_SF_ELEMENT_ADAPT_PELMS = (int)UF_SF_MESH_RECIPE_ADAPT_PELMS
/* Adaptivity of elements is P-type. */
};
typedef enum UF_SF_elm_adaptivity_type_e UF_SF_elm_adaptivity_type_t,
*UF_SF_elm_adaptivity_type_p_t;
enum UF_SF_element_type_e
{
UF_SF_UNDEFINED = 0,/* Generic undefined type. */
UF_SF_CMASS = 1, /* Concentrated mass element. */
UF_SF_BAR = 2, /* Bar element. */
UF_SF_BEAM = 3, /* Beam element. */
UF_SF_ROD = 4, /* Rod element. */
UF_SF_RBE2 = 5, /* Rigid link element. */
UF_SF_SPRING = 6, /* Spring element. */
UF_SF_MASS = 7, /* Distributed mass element. */
UF_SF_HBDY = 8, /* Heat body element. */
UF_SF_QUAD4 = 9, /* Quadrilateral element with 4 nodes. */
UF_SF_TRIA3 = 10, /* Triangular element with 3 nodes. */
UF_SF_QUAD8 = 11, /* Quadrilateral element with 8 nodes. */
UF_SF_TRIA6 = 12, /* Triangular element with 6 nodes. */
UF_SF_TET4 = 13, /* Tetrahedral element with 4 nodes. */
UF_SF_TET10 = 14, /* Tetrahedral element with 10 nodes. */
UF_SF_1D_CONTACT=15, /* 1D contact elements between 2 bodies. */
UF_SF_HEX8 = 16, /* Hexahedral element with 8 nodes. */
UF_SF_HEX20 = 17, /* Hexahedral element with 20 nodes. */
UF_SF_WDG6 = 18, /* Wedge element with 6 nodes. */
UF_SF_WDG15 = 19, /* Wedge element with 15 nodes. */
UF_SF_2D_CONTACT = 20, /* 2D Contact elements between 2 faces */
UF_SF_WELD = 21, /* weld elements */
UF_SF_EF_CONN = 22, /* Edge-Face connection element */
UF_SF_MM_FREE = 23, /* Not an element type but useful as connection. */
UF_SF_MM_GLUE = 24, /* Not an element type but useful as connection. */
UF_SF_RBE3 = 25, /* rbe3 element with 1 core node (first node) and multiple leg nodes. */
UF_SF_PYR5 = 26, /* Pyramid element with 5 nodes. */
UF_SF_PYR9 = 27, /* Pyramid element with 9 nodes. */
UF_SF_PYR13 = 28, /* Pyramid element with 13 nodes. */
UF_SF_1D_NG = 29, /* 1D Node to Ground elements with 1 node. */
UF_SF_1D_PLOTEL = 30,/* 1D plotel element with 2 nodes. */
UF_SF_1D_MASS = 31, /* 1D mass element with 2 nodes. */
UF_SF_PYR_MIXED_ORDER = 32, /* Pyramid element mixed order. */
UF_SF_TET_MIXED_ORDER = 33, /* Tetrahedral element mixed order. */
UF_SF_1D_BEARING = 34,
UF_SF_HEXCOHES8 = 35, /* cohesive element with 8 nodes. */
UF_SF_HEXCOHES20 = 36, /* cohesive element with 20 nodes. */
UF_SF_WDGCOHES6 = 37, /* cohesive element with 6 nodes. */
UF_SF_WDGCOHES15 = 38, /* cohesive element with 15 nodes. */
UF_SF_MPC = 39, /* mpc element with 1 core node (first node) and multiple leg nodes. */
UF_SF_MATRIX = 40, /* matrix element with nodes and/or scalar points. */
UF_SF_1D_JOINT = 41, /* joint element */
/*
*/
UF_SF_TOTAL_COUNT = 42 /* This last member represents the total
number of members in this enum */
};
typedef enum UF_SF_element_type_e UF_SF_element_type_t,
*UF_SF_element_type_p_t;
enum UF_SF_mesh_dimension_e
{
UF_SF_DIMENSION_0D, /* Element dimension is 0 - CMASS or MASS */
UF_SF_DIMENSION_1D, /* Element dimension is 1 - Bar, beam, rods, rigid
links, springs and contact elements. */
UF_SF_DIMENSION_2D, /* Element dimension is 2 - quad4, quad8, tri3, tri6 */
UF_SF_DIMENSION_3D, /* Element dimension is 3 - tet4, tet10. */
UF_SF_DIMENSION_MATRIX,/* Element dimension is 4 - matrix element with nodes and/or scalar points */
UF_SF_DIMENSION_ANY /* Element of any dimension. */
};
typedef enum UF_SF_mesh_dimension_e UF_SF_mesh_dimension_t,
*UF_SF_mesh_dimension_p_t;
enum UF_SF_elm_dimension_type_e
{
UF_SF_ELEMENT_POINT = (int)UF_SF_DIMENSION_0D, /* Element type is point - CMASS
or MASS. */
UF_SF_ELEMENT_BEAM = (int)UF_SF_DIMENSION_1D, /* Element type is beam - Bar,
beam, rods, rigid links,
springs and contact elements.*/
UF_SF_ELEMENT_SHELL = (int)UF_SF_DIMENSION_2D, /* Element type is shell - quad4,
quad8, tri3, tri6. */
UF_SF_ELEMENT_SOLID = (int)UF_SF_DIMENSION_3D, /* Element type is solid - tet4,
tet10. */
UF_SF_ELEMENT_MATRIX = (int)UF_SF_DIMENSION_MATRIX,/* Element type is matrix element
with nodes and/or scalar points */
UF_SF_ELEMENT_ALL = (int)UF_SF_DIMENSION_ANY /* Element of any of the above types. */
};
typedef enum UF_SF_elm_dimension_type_e UF_SF_elm_dimension_type_t,
*UF_SF_elm_dimension_type_p_t;
enum UF_SF_section_type_e
{
UF_SF_SECTION_TWREC = 0, /* Thin wall, rectangle */
UF_SF_SECTION_TWCYL, /* Thin wall, cylinder */
UF_SF_SECTION_TWCHA, /* Thin wall, channel */
UF_SF_SECTION_TWHAT, /* Thin wall, hat */
UF_SF_SECTION_TWIBE, /* Thin wall, I beam */
UF_SF_SECTION_SOCYL, /* Solid, cylinder */
UF_SF_SECTION_SOREC, /* Solid, rectangle */
UF_SF_SECTION_KEYIN, /* User defined. */
UF_SF_SECTION_USER_TW, /* User Defined TW */
UF_SF_SECTION_USER_SOLID, /* User Defined Solid */
UF_SF_SECTION_NUM_TYPES
};
typedef enum UF_SF_section_type_e UF_SF_section_type_t,
*UF_SF_section_type_p_t;
/* */
enum UF_SF_neutral_material_types_e
{
UF_SF_MATERIAL_ISOTROPIC = 0, /* Material is isotropic. */
UF_SF_MATERIAL_ORTHOTROPIC = 1, /* Material is orthotropic. */
UF_SF_MATERIAL_ANISOTROPIC = 2, /* Material is anisotropic. */
UF_SF_MATERIAL_FORMABILITY = 3, /* Formability properties. */
UF_SF_MATERIAL_FLUID = 4, /* Fluid material. */
UF_SF_MATERIAL_HYPERELASTIC = 5, /* General Hyperelastic Material */
UF_SF_MATERIAL_MOONEYRIVLIN=6, /* Mooney Rivlin */
UF_SF_MATERIAL_MOONEYRIVLINTESTDATA=7, /* Mooney Rivlin - test data option */
UF_SF_MATERIAL_POLYNOMIAL=8, /* Polynomial */
UF_SF_MATERIAL_REDUCEDPOLYNOMIAL=9, /* Reduced Polynomial */
UF_SF_MATERIAL_OGDEN=10, /* Ogden */
UF_SF_MATERIAL_OGDENTESTDATA=11, /* Ogden - test data option */
UF_SF_MATERIAL_FOAM=12, /* Foam */
UF_SF_MATERIAL_FOAMTESTDATA=13, /* Foam - test data option */
UF_SF_MATERIAL_BLATZ=14, /* Blatz-Ko */
UF_SF_MATERIAL_ARRUDABOYCE=15, /* Arruda-Boyce */
UF_SF_MATERIAL_ARRUDABOYCETESTDATA=16, /* Arruda-Boyce - test data option */
UF_SF_MATERIAL_NEOHOOKE=17, /* Neo Hooke */
UF_SF_MATERIAL_NEOHOOKETESTDATA=18, /* Neo Hooke - test data option */
UF_SF_MATERIAL_MARLOW=19, /* Marlow */
UF_SF_MATERIAL_VANDERWAALS=20, /* Van Der Waals */
UF_SF_MATERIAL_YEOH=21, /* Yeoh */
UF_SF_MATERIAL_YEOHTESTDATA=22, /* Yeoh - test data option */
UF_SF_MATERIAL_GENT=23, /* Gent */
UF_SF_MATERIAL_GASKET=24, /* Gasket */
UF_SF_MATERIAL_GASKETBEHAVIOR=25, /* Gasket Behavior */
UF_SF_MATERIAL_SHAPEMEMORYALLOY=26, /* Shape Memory Alloy */
UF_SF_MATERIAL_SUSSMANBATHE=27, /* Sussman-Bathe hyperelastic material */
UF_SF_MATERIAL_GASKETDISPLACEMENT=28, /* Gasket with length-based loading */
UF_SF_MATERIAL_DAMAGEINTERFACE=29, /* Damage interface material */
UF_SF_MATERIAL_MULTIPLEFLUID=30, /* Multiple fluid material */
UF_SF_MATERIAL_HARTSMITH=31, /* Hart-Smith material */
UF_SF_MATERIAL_ALEXANDER=32, /* Alexander material */
UF_SF_MATERIAL_CURING=33, /* Curing material */
UF_SF_MATERIAL_POROUS=35 /* Porous material */
};
typedef enum UF_SF_neutral_material_types_e UF_SF_neutral_material_types_t,
*UF_SF_neutral_material_types_p_t;
/* Extended material types. */
enum UF_SF_matl_orient_option_e
{
UF_SF_MATL_ORIENT_FIXED, /* Origin/vectors option */
UF_SF_MATL_ORIENT_WCS /* Create an orientation based
upon the current WCS. */
};
typedef enum UF_SF_matl_orient_option_e UF_SF_matl_orient_option_t,
*UF_SF_matl_orient_option_p_t;
/* Coordinate system type. */
enum UF_SF_fem_coord_type_e
{
UF_SF_RECT_COORD
};
typedef enum UF_SF_fem_coord_type_e UF_SF_fem_coord_type_t,
*UF_SF_fem_coord_type_p_t;
enum UF_SF_multi_prop_type_e
{
UF_SF_MULTI_PROP_TABLE, /* Tabular form of variable material properties.*/
UF_SF_MULTI_PROP_EXPRESSION /* Variation of material properties is through
an expression. */
};
typedef enum UF_SF_multi_prop_type_e UF_SF_multi_prop_type_t,
*UF_SF_multi_prop_type_p_t;
enum UF_SF_library_material_e
{
UF_SF_MATL_IS_READ_ONLY, /* User not allowed to edit in NX. */
UF_SF_MATL_IS_EDITABLE /* User allowed to edit within NX. */
};
typedef enum UF_SF_library_material_e UF_SF_library_material_t,
*UF_SF_library_material_p_t;
enum UF_SF_mesh_geom_usage_e
{
UF_SF_GEOM_ANY, /* all geometry */
UF_SF_GEOM_HARD, /* hard geometry */
UF_SF_GEOM_CONNECT_A, /* group1 geometry */
UF_SF_GEOM_CONNECT_B /* group2 geometry */
};
typedef enum UF_SF_mesh_geom_usage_e UF_SF_mesh_geom_usage_t,
*UF_SF_mesh_geom_usage_p_t;
enum UF_SF_edge_density_type_e
{
UF_SF_EDGE_DENSITY_SIZE, /* Edge density defined by elm size */
UF_SF_EDGE_DENSITY_NUMBER, /* Edge density defined by number of elms. */
UF_SF_EDGE_DENSITY_SMART = 4, /* Edge density defined by smart option. */
UF_SF_NOT_EDGE_DENSITY_DEFINED /* Edge density not defined. */
};
typedef enum UF_SF_edge_density_type_e UF_SF_edge_density_type_t,
*UF_SF_edge_density_type_p_t;
/* The definition method for numeric values. */
enum UF_SF_numeric_method_e
{
UF_SF_NUMERIC, /* Numeric value */
UF_SF_EXPRESSION /* Expression string used. */
};
typedef enum UF_SF_numeric_method_e UF_SF_numeric_method_t,
*UF_SF_numeric_method_p_t;
/* The smart point definition method. */
enum UF_SF_HPT_method_e
{
UF_SF_HPT_NO_METHOD, /* Smart point created with no method. */
UF_SF_HPT_ON_CURVE, /* Smart point created on curve. */
UF_SF_HPT_BASEPT_AND_OFFSET, /* Smart point created as offset to some base
point. */
UF_SF_HPT_CENTER_OF_CONIC, /* Smart point created at the center of a
conic. */
UF_SF_HPT_CURVE_INTERSECTION, /* Smart point created at the intersection of
two curves. */
UF_SF_HPT_ON_SURFACE /* Smart point created on a surface. */
};
typedef enum UF_SF_HPT_method_e UF_SF_HPT_method_t,
*UF_SF_HPT_method_p_t;
/* The 0d mesher element types. */
enum UF_SF_0D_element_type_e
{
UF_SF_0D_CONMASS = (int)UF_SF_CMASS /* 0D element type - concentrated mass. */
};
typedef enum UF_SF_0D_element_type_e UF_SF_0D_element_type_t,
*UF_SF_0D_element_type_p_t;
/* The 0d mesher element density. */
enum UF_SF_0D_density_type_e
{
UF_SF_0D_EDGE_DENSITY_SIZE, /* Edge density given as size of the
elements. */
UF_SF_0D_EDGE_DENSITY_NUMBER, /* Edge density given as number of the
elements. */
UF_SF_0D_EDGE_DENSITY_SMART = 4
};
typedef enum UF_SF_0D_density_type_e UF_SF_0D_density_type_t,
*UF_SF_0D_density_type_p_t;
/* The 1d mesher element types. */
enum UF_SF_1D_element_type_e
{
UF_SF_1D_SPRING_TYPE = (int)UF_SF_SPRING, /* Spring elements. */
UF_SF_1D_BAR_TYPE = (int)UF_SF_BAR, /* Bar elements. */
UF_SF_1D_BEAM_TYPE = (int)UF_SF_BEAM, /* Beam elements. */
UF_SF_1D_ROD_TYPE = (int)UF_SF_ROD, /* Rod elements. */
UF_SF_1D_RIGID_TYPE = (int)UF_SF_RBE2 /* Rigid link elements. */
};
typedef enum UF_SF_1D_element_type_e UF_SF_1D_element_type_t,
*UF_SF_1D_element_type_p_t;
/* The 1d mesher element density. */
enum UF_SF_1D_density_type_e
{
UF_SF_1D_EDGE_DENSITY_SIZE, /* Edge density given as a size of the
elements. */
UF_SF_1D_EDGE_DENSITY_NUMBER, /* Edge density given as number of the
elements. */
UF_SF_1D_EDGE_DENSITY_SMART = 4
};
typedef enum UF_SF_1D_density_type_e UF_SF_1D_density_type_t,
*UF_SF_1D_density_type_p_t;
/* The Load functions mode_type parameter. */
enum UF_SF_load_mode_e
{
UF_SF_LOAD_FORCE = 1, /* Force. */
UF_SF_LOAD_DISTRIBUTED = 2, /* Uniform pressure, applicable only normal
to the face. */
UF_SF_LOAD_SPACIAL = 3,
UF_SF_LOAD_GRAVITY = 4, /* Gravity load. */
UF_SF_LOAD_PRESSURE = 5, /* Pressure load, can be appied in any
direction. */
UF_SF_LOAD_MOMENT = 6, /* Moment. */
UF_SF_LOAD_SHEAR = 7, /* Edge shear. */
UF_SF_LOAD_FLUX = 8, /* Heat flux. */
UF_SF_LOAD_TEMPERATURE = 9, /* Temperature load. */
UF_SF_LOAD_CENTRIFUGAL = 10, /* Centrifugal load. */
UF_SF_LOAD_TORQUE = 11, /* Torque */
UF_SF_LOAD_BEARING = 12, /* Bearing */
UF_SF_LOAD_UNKNOWN_MODE = -99999 /* Unknown load mode type */
};
typedef enum UF_SF_load_mode_e UF_SF_load_mode_t,
*UF_SF_load_mode_p_t;
/* The Load functions load_class parameter. */
enum UF_SF_load_class_e
{
UF_SF_LOAD_NODE_ELEMENT_CLASS = 1, /* Load applied on a node. */
UF_SF_LOAD_EDGE_ELEMENT_CLASS = 2, /* Load applied on an edge. */
UF_SF_LOAD_FACE_CLASS = 3, /* Load applied on a face. */
UF_SF_LOAD_PART_CLASS = 4, /* Load applied to the whole part. */
UF_SF_LOAD_BODY_CLASS = 5, /* Load applied on a body. */
UF_SF_LOAD_CURVE_CLASS = 6 /* Load applied on a curve. */
};
typedef enum UF_SF_load_class_e UF_SF_load_class_t,
*UF_SF_load_class_p_t;
/* The BC functions class parameter. */
enum UF_SF_bc_class_e
{
UF_SF_BC_ERROR_CLASS = -1, /* To indicate error */
UF_SF_BC_NODE_ELEMENT_CLASS = 1, /* BC applied on a node. */
UF_SF_BC_EDGE_ELEMENT_CLASS = 2, /* BC applied on an edge. */
UF_SF_BC_FACE_CLASS = 3, /* BC applied on a face. */
UF_SF_BC_CURVE_CLASS = 4 /* BC applied on a curve. */
};
typedef enum UF_SF_bc_class_e UF_SF_bc_class_t,
*UF_SF_bc_class_p_t;
/* The Load functions load_disp_symbol parameter. */
enum UF_SF_load_disp_symbol_e
{
UF_SF_LOAD_SINGLE_HEADED_ARROW = 1,
UF_SF_LOAD_DOUBLE_HEADED_ARROW = 2,
UF_SF_LOAD_HALF_ARROW = 3,
UF_SF_LOAD_Q_ARROW = 4,
UF_SF_BC_PYRAMID = 101,
UF_SF_BC_ARROW = 102,
UF_SF_BC_DOUBLE_HEADED_ARROW = 103,
UF_SF_BC_SMALL_CIRCLE = 104,
UF_SF_BC_SMALL_ARROW = 105,
UF_SF_BC_S_ON_ENTITY = 106,
UF_SF_BC_M_ON_ENTITY = 107
};
typedef enum UF_SF_load_disp_symbol_e UF_SF_load_disp_symbol_t,
*UF_SF_load_disp_symbol_p_t;
/* The Load functions component_type parameter. */
enum UF_SF_LBC_component_type_e
{
UF_SF_NULL_COMP = -1,
UF_SF_LBC_XYZ = 0, /* Having XYZ components - rectangular coordinates. */
UF_SF_LBC_RTZ, /* Having RTZ components - Cylindrical coordinates. */
UF_SF_LBC_RTP, /* Having RTP components - Spherical coordinates. */
UF_SF_LBC_NORMAL_TO, /* Applicable normal to a face only. */
UF_SF_LBC_EDGE_CSYS /* Applicable along an edge only. */
};
typedef enum UF_SF_LBC_component_type_e UF_SF_LBC_component_type_t,
*UF_SF_LBC_component_type_p_t;
enum UF_SF_load_dimension_e
{
UF_SF_NULL_LOAD = 0, /* Load value is 0. */
UF_SF_SCALAR_LOAD, /* Load is a scalar - temperature. */
UF_SF_VECTOR_LOAD, /* Having RTP components - Spherical coordinates. */
UF_SF_AXIS_LOAD /* Applicable normal to a face only. */
};
typedef enum UF_SF_load_dimension_e UF_SF_load_dimension_t,
*UF_SF_load_dimention_p_t;
/* The BC functions mode parameter. */
enum UF_SF_bc_mode_e
{
UF_SF_BC_CONSTRAINT = 1, /* Both linear displacement and rotation
are available. */
UF_SF_BC_DISPLACEMENT = 2, /* Only displacement is available,
rotation is free. */
UF_SF_BC_ROTATION = 3, /* Only rotation is available,
displacement is free. */
UF_SF_BC_TEMPERATURE = 4, /* Temperature BC is available. */
UF_SF_BC_CONVECTION_COEFFICIENT = 5,/* Convection coefficient BC is
available. */
UF_SF_BC_UNKNOWN_MODE = -99999 /* Unknown BC mode type */
};
typedef enum UF_SF_bc_mode_e UF_SF_bc_mode_t,
*UF_SF_bc_mode_p_t;
/* The Durability Event mode parameter. */
enum UF_SF_dur_event_mode_e
{
UF_SF_DUR_EVENT_STATIC = 1 /* Currently we only have Static Durability Events */
};
typedef enum UF_SF_dur_event_mode_e UF_SF_dur_event_mode_t,
*UF_SF_dur_event_mode_p_t;
/* geometry types */
enum UF_SF_mesh_geometry_types_e
{
UF_SF_GEOM_OTHER, /* Geometry does not fall into any of the categories
listed below. */
UF_SF_GEOM_ASSEM, /* Geometry is an assembly. */
UF_SF_GEOM_COMPON, /* Geometry is a component. */
UF_SF_GEOM_OCC, /* Geometry is an occurrence. */
UF_SF_GEOM_BODY, /* Geometry is a body. */
UF_SF_GEOM_FACE, /* Geometry is a face. */
UF_SF_GEOM_EDGE, /* Geometry is an edge. */
UF_SF_GEOM_SURF , /* Geometry is a surface. */
UF_SF_GEOM_CURVE, /* Geometry is a curve. */
UF_SF_GEOM_POINT, /* Geometry is a point. */
UF_SF_GEOM_VERTEX, /* Geometry is a vertex. */
UF_SF_GEOM_COMPOSITE_BODY, /* Geometry is a composite body */
UF_SF_GEOM_COMPOSITE_FACE, /* Geometry is a composite face */
UF_SF_GEOM_COMPOSITE_EDGE /* Geometry is a composite edge */
};
typedef enum UF_SF_mesh_geometry_types_e UF_SF_mesh_geometry_types_t,
*UF_SF_mesh_geometry_types_p_t;
enum UF_SF_LANG_analysis_type_e
{
UF_SF_LANG_ANALYSIS_UNKNOWN = 0, /* unknown language type */
UF_SF_LANG_ANALYSIS_STRUCTURAL = 1, /* Structural analysis */
UF_SF_LANG_ANALYSIS_THERMAL = 2, /* Thermal analysis */
UF_SF_LANG_ANALYSIS_FLOW = 3, /* CFD analysis */
UF_SF_LANG_ANALYSIS_COUPLED = 4, /* Flow-Thermal analysis */
UF_SF_LANG_ANALYSIS_MAPPING = 5 /* Mapping analysis */
};
typedef enum UF_SF_LANG_analysis_type_e UF_SF_LANG_analysis_type_t,
*UF_SF_LANG_analysis_type_p_t;
enum UF_SF_LANG_problem_abstract_e
{
UF_SF_LANG_SIMPLE_PROB_ABSTRACT = 1,
UF_SF_LANG_AXISYM_PROB_ABSTRACT = 2,
UF_SF_LANG_MIXED_PROB_ABSTRACT = 3
};
typedef enum UF_SF_LANG_problem_abstract_e UF_SF_LANG_problem_abstract_t,
*UF_SF_LANG_problem_abstract_p_t;
enum UF_SF_LANG_linearity_e
{
UF_SF_LANG_LINEAR_LINEARITY = 1,
UF_SF_LANG_NONLINEAR_LINEARITY = 2
};
typedef enum UF_SF_LANG_linearity_e UF_SF_LANG_linearity_t,
*UF_SF_LANG_linearity_p_t;
enum UF_SF_LANG_time_depend_e
{
UF_SF_LANG_STEADY_TIME_DEPEND = 1 /* Analysis will be steady-state. */
};
typedef enum UF_SF_LANG_time_depend_e UF_SF_LANG_time_depend_t,
*UF_SF_LANG_time_depend_p_t;
/* Element types supported by Aries Tet Mesher */
enum UF_SF_atm_element_types_e
{
UF_SF_ATM_SYSTEM_DEFAULT_TYPE = 0, /* Element will be system default,
either tet4 or tet10, depending on the
enviroment. */
UF_SF_ATM_TETRA, /* Element will be tetrahedral, with 4
nodes. */
UF_SF_ATM_TETRA_10 /* Element will be tetrahedral, with 10
nodes. */
};
typedef enum UF_SF_atm_element_types_e UF_SF_atm_element_types_t;
/* Aries Tet Mesher edge shapes */
enum UF_SF_atm_edge_shape_types_e
{
UF_SF_ATM_LINEAR = 0, /* Type of element is linear. */
UF_SF_ATM_CURVED, /* Type of element is curved. */
UF_SF_ATM_MIXED /* Both curved and linear elements can form. */
};
typedef enum UF_SF_atm_edge_shape_types_e UF_SF_atm_edge_shape_types_t;
/********************************* ATM parameters *****************************/
enum UF_SF_sfqm_elem_type_e
{
UF_SF_SFQM_QUAD4,
UF_SF_SFQM_TRIA3,
UF_SF_SFQM_QUAD8,
UF_SF_SFQM_TRIA6
};
typedef enum UF_SF_sfqm_elem_type_e UF_SF_sfqm_elem_type_t,
*UF_SF_sfqm_elem_type_p_t;
/* Distribution type */
enum UF_SF_dist_type_t
{
UF_SF_SINUSOIDAL = 0,
UF_SF_PARABOLIC
};
/* Mating Type */
enum UF_SF_mate_type_e
{
UF_SF_NOT_SUPPORT_MATE_TYPE = 0,
UF_SF_ASSEMBLY_MESH
};
typedef enum UF_SF_mate_type_e UF_SF_mate_type_t,
*UF_SF_mate_type_p_t;
/* Assembly Mesh Type */
enum UF_SF_assembly_type_e
{
UF_SF_NOT_SUPPORT_ASSEM_TYPE = 0,
UF_SF_ASSEM_BY_GLUE,
UF_SF_ASSEM_BY_SLIDE_CONTACT,
UF_SF_ASSEM_BY_GAP_CONTACT,
UF_SF_ASSEM_FREE
};
typedef enum UF_SF_assembly_type_e UF_SF_assembly_type_t,
*UF_SF_assembly_type_p_t;
enum UF_SF_edge_matching_type_e
{
UF_SF_EDGE_MATCHING_TYPE_ND,
UF_SF_EDGE_MATCHING_BY_LOCATION,
UF_SF_EDGE_MATCHING_BY_ESIZE,
UF_SF_EDGE_MATCHING_BY_COLLAPSE,
UF_SF_EDGE_MATCHING_MM_GLUE,
UF_SF_EDGE_MATCHING_MM_FREE,
UF_SF_EDGE_MATCHING_ANY
};
typedef enum UF_SF_edge_matching_type_e UF_SF_edge_matching_type_t,
*UF_SF_edge_matching_type_p_t;
enum UF_SF_idealize_parm_exp_t
{
UF_SF_IDEALIZE_HOLE_DIAMETER,
UF_SF_IDEALIZE_BLEND_RADIUS,
UF_SF_IDEALIZE_TINY_FACE_AREA,
UF_SF_IDEALIZE_THIN_FACE_WIDTH,
UF_SF_IDEALIZE_FACE_COLLECTOR,
UF_SF_IDEALIZE_SCREEN_SELECTED_FACE
};
enum UF_SF_idealize_parm_face_t
{
UF_SF_IDEALIZE_RETAINED_FACES,
UF_SF_IDEALIZE_REMOVED_FACES
};
#define UF_SF_SEPERATE_FACES UF_SF_SEPARATE_FACES
enum UF_SF_face_subdiv_status_e
{
UF_SF_IDENTICAL_FACES_EQ_EDGES, /* Both faces identical with eq. num of edges */
UF_SF_IDENTICAL_FACES_UNEQ_EDGES,/* Both faces identical with uneq. num of edges */
UF_SF_NOT_IDENTICAL, /* Both faces are not identical */
UF_SF_OVERLAPPING_FACES, /* Both faces overlapping */
UF_SF_SEPARATE_FACES /* Both faces are separate */
};
typedef enum UF_SF_face_subdiv_status_e UF_SF_face_subdiv_status_t,
*UF_SF_face_subdiv_status_p_t;
enum UF_SFANS_algorithm_t
{
UF_SFANS_NULL_SOLVER = -1,
UF_SFANS_FRONTAL_SOLVER = 0,
UF_SFANS_PCG_SOLVER,
UF_SFANS_JCG_SOLVER,
UF_SFANS_SPARSE_SOLVER,
UF_SFANS_JCG_PCG_SOLVER,
UF_SFANS_JCG_FRONTAL_SOLVER,
UF_SFANS_SUBSPACE_MODOPT_SOLVER,
UF_SFANS_LANCZOS_MODOPT_SOLVER,
UF_SFANS_POWERDYN_MODOPT_SOLVER,
UF_SFANS_NUM_ALGORITHM_TYPES
};
typedef enum UF_SFANS_algorithm_t, *UF_SFANS_algorithm_p_t;
enum UF_SFFEA_algorithm_t
{
UF_SFFEA_AUTOMATIC = -1,
UF_SFFEA_DIRECT_IN_CORE = 0,
UF_SFFEA_DIRECT_OUT_OF_CORE = 2,
UF_SFFEA_ITERATIVE_IN_CORE = 6,
UF_SFFEA_ITERATIVE_OUT_OF_CORE = 8,
UF_SFFEA_SPARSE = 10,
UF_SFFEA_ITERATIVE = 11
};
typedef enum UF_SFFEA_algorithm_t, *UF_SFFEA_algorithm_p_t;
enum UF_SFOPT_solver_type_t
{
UF_SFOPT_NULL_SOLVER_TYPE = -1,
UF_SFOPT_GENERIC_SOLVER_TYPE = 0,
UF_SFOPT_SENSITIVITY_SOLVER_TYPE = 1,
UF_SFOPT_HYPEROPT_SOLVER_TYPE = 2,
UF_MAX_NUM_SOLVER_TYPES = 3
};
typedef enum UF_SFOPT_solver_type_t, *UF_SFOPT_solver_type_p_t;
/* The Load functions mode_type parameter. */
enum UF_SF_lv_function_mode_e
{
UF_SF_HALF_UNIT_CYCLE = 0, /* Half Unit Cycle */
UF_SF_FULL_UNIT_CYCLE = 1 /* Full Unit Cycle */
};
typedef enum UF_SF_lv_function_mode_e UF_SF_lv_function_mode_t,
*UF_SF_lv_function_mode_p_t;
enum UF_SFAS_mode_type_t
{
UF_MODE_TYPE = 0,
UF_MODE_AND_FREQUENCY_RANGE_TYPE,
UF_FREQUENCY_RANGE_TYPE,
UF_SFAS_MAX_MODE_CHOICES
};
typedef enum UF_SFAS_mode_type_t, *UF_SFAS_mode_type_p_t;
enum UF_SF_scenario_info_t
{
UF_SF_mesh_info = 0, /* export info about meshes */
UF_SF_load_info = 1, /* export info about loads */
UF_SF_solution_info = 2, /* export info about solutions */
UF_SF_step_info = 3, /* export info about steps */
UF_SF_boundary_condition_info = 4, /* export info about boundary
conditions. */
UF_SF_material_info = 5, /* export info about materials
Assigned to a specified entity. */
UF_SF_section_info = 6, /* export info about sections */
UF_SF_mesh_mating_condition_info = 7, /* export info about a mesh mating
condition. */
UF_SF_fea_summary_info = 8, /* export a summary including all
fea entities. */
UF_SF_dur_event_info = 9, /* export a summary including all
load variations for the event. */
UF_SF_load_case_info = 10, /* export info about load cases */
UF_SF_sim_summary_info = 11 /* export a summary of simulation
entities. */
};
/* FEM Property types. */
#define UF_SF_LANG_NIL_VAL_TYPE 0
#define UF_SF_LANG_INT_VAL_TYPE 1
#define UF_SF_LANG_SCALAR_VAL_TYPE 2
#define UF_SF_LANG_TEXT_VAL_TYPE 3
#define UF_SF_LANG_ENUM_VAL_TYPE 4
#define UF_SF_LANG_COORD_VAL_TYPE 5
#define UF_SF_LANG_MATERIAL_VAL_TYPE 6
#define UF_SF_LANG_SECTION_VAL_TYPE 7
#define UF_SF_LANG_VECTOR_VAL_TYPE 8
#define UF_SF_LANG_TABLE_VAL_TYPE 9
#define UF_SF_LANG_LOAD_VAL_TYPE 10
#define UF_SF_LANG_BNDCOND_VAL_TYPE 11
#define UF_SF_LANG_BOOL_VAL_TYPE 12
#define UF_SF_LANG_MULTI_STRING_VAL_TYPE 13
#define UF_SF_LANG_FILENAME_VAL_TYPE 14
#define UF_SF_LANG_DIRPATH_VAL_TYPE 15
#define UF_SF_LANG_SSMO_VAL_TYPE 16
#define UF_SF_LANG_FIELD_VAL_TYPE 17
#define UF_SF_LANG_AXIS_VAL_TYPE 18
#define UF_SF_LANG_DOF_VAL_TYPE 19
#define UF_SF_LANG_POINT_VAL_TYPE 20
/******************************************************************
================================================================= */
#define UF_SF_LANG_MULTI_STRING_ITI_VAL_TYPE 23
#define UF_SF_LANG_CAE_SECTION_VAL_TYPE 24
#define UF_SF_LANG_EDGES_ON_FACE_VAL_TYPE 25
#define UF_SF_LANG_SFEM_VECTOR_VAL_TYPE 26
#define UF_SF_LANG_SCALAR_ARRAY_VAL_TYPE 27
#define UF_SF_LANG_ACTION_VAL_TYPE 28
#define UF_SF_LANG_PPT_VAL_TYPE 29
#define UF_SF_LANG_SSMO_ARRAY_VAL_TYPE 30
#define UF_SF_LANG_TIME_VAL_TYPE 31
#define UF_SF_LANG_PLYMAT_VAL_TYPE 32
#define UF_SF_LANG_INT_ARRAY_VAL_TYPE 33
#define UF_SF_LANG_EXT_MENU_VAL_TYPE 34
#define UF_SF_LANG_CATALOG_VAL_TYPE 35
#define UF_SF_LANG_GENERAL_FIELD_VAL_TYPE 36
#define UF_SF_LANG_SCALAR_FIELD_VAL_TYPE 37
#define UF_SF_LANG_VECTOR_FIELD_VAL_TYPE 38
#define UF_SF_LANG_MATRIX_VAL_TYPE 39
#define UF_SF_LANG_REGION_VAL_TYPE 40
#define UF_SF_LANG_GROUPREF_VAL_TYPE 41
#define UF_SF_LANG_SELECTREF_VAL_TYPE 42
#define UF_SF_LANG_CAE_SECTION_ORIENT_VAL_TYPE 43
#define UF_SF_LANG_CAE_SECTION_OFFSET_VAL_TYPE 44
#define UF_SF_LANG_TARGETSET_VAL_TYPE 45
#define UF_SF_LANG_CAE_SECTION_REF_VAL_TYPE 46
#define UF_SF_LANG_DOFSETREF_VAL_TYPE 47
/******************************************************************
================================================================= */
#define UF_SF_LANG_LBCREF_VAL_TYPE 49
#define UF_SF_LANG_PHYSICAL_ARRAY_VAL_TYPE 50
#define UF_SF_LANG_SOLUTIONREF_VAL_TYPE 51
#define UF_SF_LANG_GROUPREF_ARRAY_VAL_TYPE 52
#define UF_SF_LANG_SCALAR_FIELD_TABLE_VAL_TYPE 53
#define UF_SF_LANG_COMPLEX_SCALAR_FIELD_VAL_TYPE 54
#define UF_SF_LANG_SOLUTIONSTEPREF_VAL_TYPE 55
#define UF_SF_LANG_POINT_ARRAY_VAL_TYPE 56
#define UF_SF_LANG_COMPONENTREF_VAL_TYPE 57
#define UF_SF_LANG_COMPONENTREF_ARRAY_VAL_TYPE 58
#define UF_SF_LANG_SOLVER_DRIVEN_STRING_ARRAY_VAL_TYPE 59
#define UF_SF_LANG_IMAGE_VAL_TYPE 60
#define UF_SF_LANG_COMPLEX_VECTOR_FIELD_VAL_TYPE 61
#define UF_SF_LANG_LBCREF_ARRAY_VAL_TYPE 62
/* FEM Property type parameter. */
enum UF_SF_fem_value_type_t
{
UF_SF_FEM_VALUE_NIL = UF_SF_LANG_NIL_VAL_TYPE,
UF_SF_FEM_VALUE_INT = UF_SF_LANG_INT_VAL_TYPE,
UF_SF_FEM_VALUE_SCALAR = UF_SF_LANG_SCALAR_VAL_TYPE,
UF_SF_FEM_VALUE_TEXT = UF_SF_LANG_TEXT_VAL_TYPE,
UF_SF_FEM_VALUE_ENUM = UF_SF_LANG_ENUM_VAL_TYPE,
UF_SF_FEM_VALUE_COORD = UF_SF_LANG_COORD_VAL_TYPE ,
UF_SF_FEM_VALUE_MATERIAL = UF_SF_LANG_MATERIAL_VAL_TYPE,
UF_SF_FEM_VALUE_SECTION = UF_SF_LANG_SECTION_VAL_TYPE,
UF_SF_FEM_VALUE_VECTOR = UF_SF_LANG_VECTOR_VAL_TYPE,
UF_SF_FEM_VALUE_TABLE = UF_SF_LANG_TABLE_VAL_TYPE,
UF_SF_FEM_VALUE_LOAD = UF_SF_LANG_LOAD_VAL_TYPE,
UF_SF_FEM_VALUE_BNDCOND = UF_SF_LANG_BNDCOND_VAL_TYPE,
UF_SF_FEM_VALUE_BOOL = UF_SF_LANG_BOOL_VAL_TYPE,
UF_SF_FEM_VALUE_MULTI_STRING = UF_SF_LANG_MULTI_STRING_VAL_TYPE,
UF_SF_FEM_VALUE_MULTI_STRING_ITI = UF_SF_LANG_MULTI_STRING_ITI_VAL_TYPE,
UF_SF_FEM_VALUE_FILENAME_VAL_TYPE = UF_SF_LANG_FILENAME_VAL_TYPE,
UF_SF_FEM_VALUE_DIRPATH_VAL_TYPE = UF_SF_LANG_DIRPATH_VAL_TYPE,
UF_SF_FEM_VALUE_SSMO_VAL_TYPE = UF_SF_LANG_SSMO_VAL_TYPE ,
UF_SF_FEM_VALUE_PPT_VAL_TYPE = UF_SF_LANG_PPT_VAL_TYPE ,
UF_SF_FEM_VALUE_PLYMAT_VAL_TYPE = UF_SF_LANG_PLYMAT_VAL_TYPE ,
UF_SF_FEM_VALUE_FIELD_VAL_TYPE = UF_SF_LANG_FIELD_VAL_TYPE ,
UF_SF_FEM_VALUE_AXIS_VAL_TYPE = UF_SF_LANG_AXIS_VAL_TYPE ,
UF_SF_FEM_VALUE_DOF_VAL_TYPE = UF_SF_LANG_DOF_VAL_TYPE ,
UF_SF_FEM_VALUE_POINT_VAL_TYPE = UF_SF_LANG_POINT_VAL_TYPE,
UF_SF_FEM_VALUE_EDGES_ON_FACE = UF_SF_LANG_EDGES_ON_FACE_VAL_TYPE,
UF_SF_FEM_VALUE_SCALAR_ARRAY = UF_SF_LANG_SCALAR_ARRAY_VAL_TYPE,
UF_SF_FEM_VALUE_ACTION = UF_SF_LANG_ACTION_VAL_TYPE,
UF_SF_FEM_VALUE_SSMO_ARRAY = UF_SF_LANG_SSMO_ARRAY_VAL_TYPE,
UF_SF_FEM_VALUE_TIME = UF_SF_LANG_TIME_VAL_TYPE,
UF_SF_FEM_VALUE_INT_ARRAY = UF_SF_LANG_INT_ARRAY_VAL_TYPE,
UF_SF_FEM_VALUE_EXT_MENU = UF_SF_LANG_EXT_MENU_VAL_TYPE,
UF_SF_FEM_VALUE_CATALOG = UF_SF_LANG_CATALOG_VAL_TYPE,
UF_SF_FEM_VALUE_GENERAL_FIELD = UF_SF_LANG_GENERAL_FIELD_VAL_TYPE,
UF_SF_FEM_VALUE_SCALAR_FIELD = UF_SF_LANG_SCALAR_FIELD_VAL_TYPE,
UF_SF_FEM_VALUE_VECTOR_FIELD = UF_SF_LANG_VECTOR_FIELD_VAL_TYPE,
UF_SF_FEM_VALUE_COMPLEX_SCALAR_FIELD = UF_SF_LANG_COMPLEX_SCALAR_FIELD_VAL_TYPE,
UF_SF_FEM_VALUE_MATRIX = UF_SF_LANG_MATRIX_VAL_TYPE,
UF_SF_FEM_VALUE_REGION = UF_SF_LANG_REGION_VAL_TYPE,
UF_SF_FEM_VALUE_GROUPREF = UF_SF_LANG_GROUPREF_VAL_TYPE,
UF_SF_FEM_VALUE_SELECTREF = UF_SF_LANG_SELECTREF_VAL_TYPE,
UF_SF_FEM_VALUE_SECTION_ORIENT = UF_SF_LANG_CAE_SECTION_ORIENT_VAL_TYPE,
UF_SF_FEM_VALUE_SECTION_OFFSET = UF_SF_LANG_CAE_SECTION_OFFSET_VAL_TYPE,
UF_SF_FEM_VALUE_TARGETSET = UF_SF_LANG_TARGETSET_VAL_TYPE,
UF_SF_FEM_VALUE_SECTION_REF = UF_SF_LANG_CAE_SECTION_REF_VAL_TYPE,
UF_SF_FEM_VALUE_DOFSET_REF = UF_SF_LANG_DOFSETREF_VAL_TYPE,
UF_SF_FEM_VALUE_LBCREF = UF_SF_LANG_LBCREF_VAL_TYPE,
UF_SF_FEM_VALUE_PPT_ARRAY = UF_SF_LANG_PHYSICAL_ARRAY_VAL_TYPE,
UF_SF_FEM_VALUE_SOLUTIONREF = UF_SF_LANG_SOLUTIONREF_VAL_TYPE,
UF_SF_FEM_VALUE_GROUPREF_ARRAY = UF_SF_LANG_GROUPREF_ARRAY_VAL_TYPE,
UF_SF_FEM_VALUE_SCALAR_FIELD_TABLE = UF_SF_LANG_SCALAR_FIELD_TABLE_VAL_TYPE,
UF_SF_FEM_VALUE_SOLUTIONSTEPREF = UF_SF_LANG_SOLUTIONSTEPREF_VAL_TYPE,
UF_SF_FEM_VALUE_POINT_ARRAY_VAL_TYPE = UF_SF_LANG_POINT_ARRAY_VAL_TYPE,
UF_SF_FEM_VALUE_COMPONENTREF = UF_SF_LANG_COMPONENTREF_VAL_TYPE,
UF_SF_FEM_VALUE_COMPONENTREF_ARRAY = UF_SF_LANG_COMPONENTREF_ARRAY_VAL_TYPE,
UF_SF_FEM_VALUE_SOLVER_DRIVEN_STRING_ARRAY = UF_SF_LANG_SOLVER_DRIVEN_STRING_ARRAY_VAL_TYPE,
UF_SF_FEM_VALUE_IMAGE_VAL_TYPE = UF_SF_LANG_IMAGE_VAL_TYPE,
UF_SF_FEM_VALUE_COMPLEX_VECTOR_FIELD = UF_SF_LANG_COMPLEX_VECTOR_FIELD_VAL_TYPE,
UF_SF_FEM_VALUE_LBCREF_ARRAY = UF_SF_LANG_LBCREF_ARRAY_VAL_TYPE
};
typedef enum UF_SF_fem_value_type_t, * UF_SF_fem_value_type_p_t;
/* Durability Solution type parameter. */
enum UF_SF_dursol_stress_criterion_t
{
UF_SF_ULTIMATE_STRENGTH = 0,
UF_SF_YIELD_STRENGTH = 1
};
typedef enum UF_SF_dursol_stress_criterion_t, * UF_SF_dursol_stress_criterion_p_t;
enum UF_SF_dursol_stress_type_t
{
UF_SF_VON_MISES = 0,
UF_SF_TRESCA = 1,
UF_SF_MAXIMUM_PRINCIPLE = 2,
UF_SF_MINIMUM_PRINCIPLE = 3
};
typedef enum UF_SF_dursol_stress_type_t, * UF_SF_dursol_stress_type_p_t;
enum UF_SF_dursol_design_life_criterion_t
{
UF_SF_INFINITE_LIFE = 0,
UF_SF_CYCLES_TO_FAILURE = 1
};
typedef enum UF_SF_dursol_design_life_criterion_t, * UF_SF_design_life_criterion_p_t;
enum UF_SF_dursol_fatigue_life_criterion_t
{
UF_SF_SMITH_WATSON_TOPPER = 0,
UF_SF_STRAIN_LIFE_MAX_PRINCIPLE = 1,
UF_SF_STRAIN_LIFE_MAX_SHEAR = 2,
UF_SF_STRESS_LIFE = 3
};
typedef enum UF_SF_dursol_fatigue_life_criterion_t, * UF_SF_dursol_fatigue_life_criterion_p_t;
#endif /* UF_SF_TYPES__H_INCLUDED */