dpud (view source)
Defined in: uf_exit.h
Overview
CAM exit dpud
This cam exit will be invoked when creating/editing a CAM User-Defined
Drive Path in an interactive NX session.
The "char param" argument must be converted to a CAM exit id by
type casting. For example, the following line of code performs the
conversion:
UF_CAM_exit_id_t exit_id = (UF_CAM_exit_id_t)param;
Return
Return Code/Description
-1 User Exit Error
0 Successful User Exit execution
Environment
Internal
void dpud
(
char * param,
int * return_code,
int parm_len
)
char * | param | Input | - A parameter used to convert Open API param to CAM exit id. |
int * | return_code | Output | - return code |
int | parm_len | Input | - length of input "param" |
udop (view source)
Defined in: uf_exit.h
Overview
CAM exit udop
This cam exit will be invoked when creating/editing a CAM User-Defined
Operation in an interactive NX session.
The "char param" argument must be converted to a CAM exit id by
type casting. For example, the following line of code performs the
conversion:
UF_CAM_exit_id_t exit_id = (UF_CAM_exit_id_t)param;
Return
Return Code/Description
-1 User Exit Error
0 Successful User Exit execution
Environment
Internal
void udop
(
char * param,
int * return_code,
int parm_len
)
char * | param | Input | - A parameter used to convert Open API param to CAM exit id. |
int * | return_code | Output | - return code |
int | parm_len | Input | - length of input "param" |
udopcopy (view source)
Defined in: uf_exit.h
Overview
CAM exit udopcopy
This cam exit will be invoked when creating/copying a CAM User-Defined
Operation in an interactive NX session.
The "char param" argument must be converted to a CAM exit id by
type casting. For example, the following line of code performs the
conversion:
UF_CAM_exit_id_t exit_id = (UF_CAM_exit_id_t)param;
Return
Return Code/Description
-1 User Exit Error
0 Successful User Exit execution
Environment
Internal
void udopcopy
(
char * param,
int * return_code,
int parm_len
)
char * | param | Input | - A parameter used to convert Open API param to CAM exit id. |
int * | return_code | Output | - return code |
int | parm_len | Input | - length of input "param" |
udopdelete (view source)
Defined in: uf_exit.h
Overview
CAM exit udopdelete
This cam exit will be invoked when deleting a CAM User-Defined
Operation in an interactive NX session.
The "char param" argument must be converted to a CAM exit id by
type casting. For example, the following line of code performs the
conversion:
UF_CAM_exit_id_t exit_id = (UF_CAM_exit_id_t)param;
Return
Return Code/Description
-1 User Exit Error
0 Successful User Exit execution
Environment
Internal
void udopdelete
(
char * param,
int * return_code,
int parm_len
)
char * | param | Input | - A parameter used to convert Open API param to CAM exit id. |
int * | return_code | Output | - return code |
int | parm_len | Input | - length of input "param" |
uf2da (view source)
Defined in: uf_exit.h
Overview
2D Analysis Using Curves
The 2D analysis using curve user exit occurs after the
Info->Analysis...->Area Properties - Using Curves menu. This user exit
bypasses the curve analysis routine and substitutes your user exit
program. There are no return codes associated with this exit.
Environment
Internal
void uf2da
(
char * param,
int * retcode,
int rlen
)
char * | param | | |
int * | retcode | | |
int | rlen | | |
ufcams (view source)
Defined in: uf_exit.h
Overview
CAM Startup
The CAM startup user exit occurs after the Application->Manufacturing...
menu.
Return
Return Code/Description
-1 User Exit Error, abort and return to Gateway
0 Successful User Exit execution, proceed normally.
Environment
Internal
void ufcams
(
char * param,
int * retcode,
int rlen
)
char * | param | | |
int * | retcode | | |
int | rlen | | |
ufccp (view source)
Defined in: uf_exit.h
Overview
Create Component
The create component user exit occurs after the
Assemblies->Components->Create New Component->Add Object Methods menu
and before the select part dialog.
The next interactive step is determined by the return code as follows:
Return
Return Code/Description
1 Cancel current assembly operation
2 Select Part dialog with the string (from param) as the default.
Note: The full pathname must be specified in the param argument
in order for this to work.
3 Reserved for future use
n Select Part dialog with no default string. "n" is any other return
code except 1, 2 or 3.
Environment
Internal
void ufccp
(
char * param,
int * retcode,
int rlen
)
char * | param | | |
int * | retcode | | |
int | rlen | | |
ufcdp (view source)
Defined in: uf_exit.h
Overview
Change Displayed Part
The change displayed part user exit occurs before the displayed part is about to
be changed explicitly from any user interface entry point, e.g. from the Windows main menu.
It is not possible to provide a default name for the operation.
The next interactive step is determined by the return code as follows:
Return
Return Code/Description
1 Cancel current assembly operation
3 Reserved for future use
n Select Part dialog with no default string. "n" is any other return
code except 1 or 3.
Environment
Internal
void ufcdp
(
char * param,
int * retcode,
int rlen
)
char * | param | | |
int * | retcode | | |
int | rlen | | |
ufclg (view source)
Defined in: uf_exit.h
Overview
CLF Generate
The CLF Generate exit occurs after Application->Manufacturing->Toolbox->
Tool Path...->Postprocess->Generate CLF. Selecting this option executes
the USER_CL_GEN (CLF generation) exit.
You can pass the CLF name through the param argument.
If no User Function program error is returned and no active part exists,
the File Main menu displays.
If an active part exists, the next interactive step is determined by the
return code as follows:
Return
Return Code/Description
-1 User Exit Error
0 User Exit does not exist.
1 Successful User Exit execution
Environment
Internal
void ufclg
(
char * param,
int * retcode,
int rlen
)
char * | param | | |
int * | retcode | | |
int | rlen | | |
ufclso (view source)
Defined in: uf_exit.h
Overview
CLSF Open
The CLSF open user exit occurs after the Application->Manufacturing...
menu.
If an active part exists, the next interactive step is determined by the
return code as follows:
Return
Return Code/Description
0 No CLSF returned
1 CLSF returned, awaiting acceptance
2 CLSF returned and accepted. Select File dialog with the string (from
param) as the default.
Environment
Internal
void ufclso
(
char * param,
int * retcode,
int rlen
)
char * | param | | |
int * | retcode | | |
int | rlen | | |
ufclsr (view source)
Defined in: uf_exit.h
Overview
CLSF Rename
The CLSF rename exit occurs after
Application->Manufacturing->File->Save->CLSF As. Selecting this option
executes both the USER_CLS_RENAME and USER_CLS_SAVE exits in
succession.
You can pass the CLSF name through the param argument.
If no User Function program error is returned and no active part exists,
the File Main menu displays.
If an active part exists, the next interactive step is determined by the
return code as follows:
Return
Return Code/Description
-1 User Exit Error
0 User Exit does not exist.
1 Successful User Exit execution
Environment
Internal
void ufclsr
(
char * param,
int * retcode,
int rlen
)
char * | param | | |
int * | retcode | | |
int | rlen | | |
ufclss (view source)
Defined in: uf_exit.h
Overview
CLSF Save
The CLSF save exit is activated by any of the following actions:
1. File->Save->CLSF
2. File->Save->CLSF As You use this exit in succession with the
USER_CLS_RENAME exit.
3. Tool Path Acceptance: Preferences->Autofile CLSF
Toolbox->Operation->Generate->OK
You can pass the CLSF name through the param argument.
If no User Function program error is returned and no active part exists,
the File Main menu displays.
If an active part exists, the next interactive step is determined by the
return code as follows:
Return
Return Code/Description
-1 User Exit Error
0 User Exit does not exist.
1 Successful User Exit execution
Environment
Internal
void ufclss
(
char * param,
int * retcode,
int rlen
)
char * | param | | |
int * | retcode | | |
int | rlen | | |
ufcre (view source)
Defined in: uf_exit.h
Overview
New Part
The new part user exit is invoked after the File->New menu.
If no User Function program error is returned and an active part exists,
control is returned to the current module.
If no active part exists, the next interactive step is determined by the
return code as follows:
Return
Return Code/Description
1 Gateway menu
2 Choose part name file selection dialog with the string (from param)
as the default.
Environment
Internal
void ufcre
(
char * param,
int * retcode,
int rlen
)
char * | param | | |
int * | retcode | | |
int | rlen | | |
ufcwp (view source)
Defined in: uf_exit.h
Overview
Change Work Part
The change work part user exit occurs after the Assemblies->Context Control->Set Work Part
before a Component is chosen or when the work part is about to be changed from any other
explicit user interface entry point
The next interactive step is determined by the return code as follows:
Return
Return Code/Description
1 Cancel current assembly operation
2 Select Component dialog with the string (from param) as the default.
3 Reserved for future use
n Normal operation with no default strings. "n" is any other return
code except 1, 2 or 3.
Environment
Internal
void ufcwp
(
char * param,
int * retcode,
int rlen
)
char * | param | | |
int * | retcode | | |
int | rlen | | |
ufdcp (view source)
Defined in: uf_exit.h
Overview
Remove Component
The remove component user exit occurs after Edit->Delete after a component
has been selected.
It is not called after a Cut operation.
It is not possible to provide a default name for the operation.
The next interactive step is determined by the return code as follows:
Return
Return Code/Description
1 Cancel current assembly operation
3 Reserved for future use
n Normal operation with no default strings. "n" is any other return
code except 1 or 3.
Environment
Internal
void ufdcp
(
char * param,
int * retcode,
int rlen
)
char * | param | | |
int * | retcode | | |
int | rlen | | |
uffcp (view source)
Defined in: uf_exit.h
Overview
Export Part
The export part user exit occurs after the File->Export->Part menu.
The next interactive step is determined by the return code as follows:
Return
Return Code/Description
1 Cancel current assembly operation
2 If the user opts to specify part from the Export Part menu, the value returned
in param will be used for the default part name.
3 Reserved for future use
n Normal operation with no default strings. "n" is any other return
code except 1, 2 or 3.
Environment
Internal
void uffcp
(
char * param,
int * retcode,
int rlen
)
char * | param | | |
int * | retcode | | |
int | rlen | | |
uffpud (view source)
Defined in: uf_exit.h
Overview
SMD exit uffpud
This exit will be invoked when creating or updating a sheet metal
flat pattern.
The "char param" argument must be converted from character string
to tag_t (integer) form. For example, the following code performs the
conversion:
tag_t fp_group_id;
sscanf(param,"%d", &fp_group_tag);
Return
Return Code/Description
-1 User Exit Error
0 Successful User Exit execution
Environment
Internal
void uffpud
(
char * param,
int * return_code,
int parm_len
)
char * | param | Input | - Flat pattern group id. (as character string) |
int * | return_code | Output | - return code |
int | parm_len | Input | - length of input "param" |
ufgen (view source)
Defined in: uf_exit.h
Overview
Access Genius System
This exit accesses the Genius Library Management System. Genius is an
external product used by the Manufacturing Module for Tool Data
Management. The Genius exit occurs after
Application->Manufacturing->Toolbox->Tool->Genius. There are no return
codes associated with this exit.
This is a legacy application that is no longer supported.
Environment
Internal
void ufgen
(
char * param,
int * retcode,
int rlen
)
char * | param | | |
int * | retcode | | |
int | rlen | | |
ufget (view source)
Defined in: uf_exit.h
Overview
Open Part
The open part (retrieve) user exit is invoked after the File->Open menu.
If no User Function program error is returned and an active part exists,
control is returned to the current module.
If no active part exists, the next interactive step is determined by the
return code as follows:
Return
Return Code/Description
1 Gateway menu
2 Choose part name file selection dialog with the string (from param)
as the default.
Environment
Internal
void ufget
(
char * param,
int * retcode,
int rlen
)
char * | param | | |
int * | retcode | | |
int | rlen | | |
ufgrp (view source)
Defined in: uf_exit.h
Overview
Execute GRIP
The execute GRIP user exit occurs after the File->Execute->GRIP menu.
The next interactive step is determined by the return code as follows:
Return
Return Code/Description
1 Runs the GRIP program using the string passed from param. The Motif
file dialog is not displayed
2 Disables the Execute GRIP option. The system adminstrator has the
option of making this option (and the use of a GRIP license)
unavailable.
Environment
Internal
void ufgrp
(
char * param,
int * retcode,
int rlen
)
char * | param | | |
int * | retcode | | |
int | rlen | | |
ufgrpd (view source)
Defined in: uf_exit.h
Overview
Debug GRIP
The execute Debug GRIP user exit occurs after the File->Execute->Debug
GRIP menu.
The next interactive step is determined by the return code as follows:
Return
Return Code/Description
1 Runs the Debug GRIP program using the string passed from param. The
Motif file dialog is not displayed.
2 Disables the Execute Debug GRIP option. The system adminstrator has
the option of making this option (and the use of a GRIP license)
unavailable.
Environment
Internal
void ufgrpd
(
char * param,
int * retcode,
int rlen
)
char * | param | | |
int * | retcode | | |
int | rlen | | |
ufmcp (view source)
Defined in: uf_exit.h
Overview
Reposition Component
The reposition component user exit occurs after the Assemblies->Components->Reposition Component
menu and after the component has been selected or when a component is about to be
repositioned from any other explicit user interface entry point.
It is not possible to provide a default name for the operation.
The next interactive step is determined by the return code as follows:
Return
Return Code/Description
1 Cancel current assembly operation
3 Reserved for future use
n Normal operation with no default strings. "n" is any other return
code except 1 or 3.
Environment
Internal
void ufmcp
(
char * param,
int * retcode,
int rlen
)
char * | param | | |
int * | retcode | | |
int | rlen | | |
ufmrg (view source)
Defined in: uf_exit.h
Overview
Import Part
The import (merge) part user exit occurs after the File->Import->Part
menu.
If an active part exists, the next interactive step is determined by the
return code as follows:
Return
Return Code/Description
0 Import Part dialog
2 Import Part dialog with the string (from param) as the default filename
This filename will be used when the file selection box is brought up
after leaving the Import Part dialog.
Environment
Internal
void ufmrg
(
char * param,
int * retcode,
int rlen
)
char * | param | | |
int * | retcode | | |
int | rlen | | |
ufncp (view source)
Defined in: uf_exit.h
Overview
Rename Component
The rename component user exit occurs after the Component Name
has been changed on the Parameters tab on the Component Properties
dialog and the user has pushed either OK or Apply.
It is not possible to provide a default name for the operation.
The next interactive step is determined by the return code as follows:
Return
Return Code/Description
1 Cancel current assembly operation
3 Reserved for future use
n Normal operation with no default strings. "n" is any other return
code except 1 or 3.
Environment
Internal
void ufncp
(
char * param,
int * retcode,
int rlen
)
char * | param | | |
int * | retcode | | |
int | rlen | | |
ufnopr (view source)
Defined in: uf_exit.h
Overview
CAM New Operation:
User Function
(1) The 'new operation' exit occurs after
- Application->Manufacturing
- Select the desired Operation Template Type and SubType,
- press 'NEW' button.
The user exit number for new operation creation is 15.
OR
(2) The operation re-initialization from an Operation Template
user exit occurs after
- Application->Manufacturing
- Select existing operation(s) to be re-initialized
- press 'REINIT' button.
The user exit number for operation re-initialization is 67.
Selecting either of the above actions executes the USER_CREATE_OPER
user exit.
The user's GRIP program will use &UENUM to retrieve the user exit number.
Based on the user exit number returned by &UENUM, the user program will
know if this exit is currently invoked by new operation creation or
existing operation re-initialization.
The name of the operation is passed through the oper_name argument.
In GRIP, the user can use &UESTR to retrieve the operation name.
Use &UEXERR to set the return code upon exit from a GRIP program.
If there are more than one operation selected for re-initialization,
the user exit will be called once for each operation to be re-initialized.
Return
Return Code/Description
-1 User Exit Error, abort operation action and return to CAM Operation
Manager dialog
0 Successful User Exit execution, proceed normally.
1 Successful User Exit execution, return to CAM Operation Manager dialog.
Environment
Internal
void ufnopr
(
char * oper_name,
int * return_code,
int oper_name_length
)
char * | oper_name | Input | - operation name |
int * | return_code | Output | - return code |
int | oper_name_length | Input | - the length of the new operation name |
ufplt (view source)
Defined in: uf_exit.h
Overview
Plot File
The plot file user exit occurs at File->Plot... menu. There is no input
or output exit string.
If an active part exists, the next interactive step is determined by the
return code as follows:
Return
Return Code/Description
1 Gateway menu
n Plot dialog. "n" is any other code except 1.
Environment
Internal
void ufplt
(
char * param,
int * retcode,
int rlen
)
char * | param | | |
int * | retcode | | |
int | rlen | | |
ufpost (view source)
Defined in: uf_exit.h
Overview
CLSF Postprocess
The CLSF postprocess exit occurs after
Application->Manufacturing->Toolbox-> Tool
Path...->Postprocess->Postprocess. Selecting this option executes both
the USER_CL_GEN (CLF generation) and USER_POST (CLSF postprocessing)
exits in succession.
You can pass the CLSF name through the param argument.
If no User Function program error is returned and no active part exists,
the File Main menu displays.
If an active part exists, the next interactive step is determined by the
return code as follows:
Return
Return Code/Description
-1 User Exit Error
0 User Exit does not exist.
1 Successful User Exit execution
Environment
Internal
void ufpost
(
char * param,
int * retcode,
int rlen
)
char * | param | | |
int * | retcode | | |
int | rlen | | |
ufput (view source)
Defined in: uf_exit.h
Overview
Save Part
The save part user exit occurs after the File->Save menu.
If no User Function program error occurs and an active part exists, the
next interactive step is to continue with the last main menu (Gateway
menu).
Return
Return Code/Description
0 NX should go ahead and file the part
1 Gateway menu, user exit filed the part
Environment
Internal
void ufput
(
char * param,
int * retcode,
int rlen
)
char * | param | | |
int * | retcode | | |
int | rlen | | |
ufrcp (view source)
Defined in: uf_exit.h
Overview
Add Existing Part
The add existing part (retrieve component) user exit occurs after the
Assemblies->Components->Add Existing menu and before the select part dialog.
The next interactive step is determined by the return code as follows:
Return
Return Code/Description
1 Cancel current assembly operation
2 Select Part dialog with the string (from param) as the default provided the
part exists so that it can be loaded.
3 Component Parameters dialog with the part (from param) as the part to be added
provided the part exists so it can be loaded.
n Normal operation with no default strings. "n" is any other return
code except 1, 2 or 3.
Environment
Internal
void ufrcp
(
char * param,
int * retcode,
int rlen
)
char * | param | | |
int * | retcode | | |
int | rlen | | |
ufrrs (view source)
Defined in: uf_exit.h
Overview
Replace Reference Set
The replace reference set user exit occurs after the Format->Reference Sets
dialog has been invoked and the "Set Current" button has been pushed or when
the Reference Set is about to be changed from any other explicit user
interface entry point.
It is not possible to provide a default name for the operation.
The next interactive step is determined by the return code as follows:
Return
Return Code/Description
1 Cancel current assembly operation
3 Reserved for future use
n Normal operation with no default strings. "n" is any other return
code except 1 or 3.
Environment
Internal
void ufrrs
(
char * param,
int * retcode,
int rlen
)
char * | param | | |
int * | retcode | | |
int | rlen | | |
ufscpi (view source)
Defined in: uf_exit.h
Overview
Substitute Component In
The substitute component in user exit occurs after the Assemblies->Components->Substitute Component
menu. It is called before the component that is to be substituted in is selected.
The next interactive step is determined by the return code as follows:
Return
Return Code/Description
1 Cancel current assembly operation
2 Select Components dialog with the string (from param) as the
default.
3 Substitute component parameters menu with the part (from param) in case of the
Open As function.
In case of the Substitute function it will behave as return code 1.
n Normal operation with no default strings. "n" is any other return
code except 1,2 or 3.
Environment
Internal
void ufscpi
(
char * param,
int * retcode,
int rlen
)
char * | param | | |
int * | retcode | | |
int | rlen | | |
ufscpo (view source)
Defined in: uf_exit.h
Overview
Substitute Component Out
The substitute component out user exit occurs after the Assemblies->Components->Substitute Component
menu and after the component has been selected or when a component is about to be substituted
out from any other explicit user interface entry point.
It is not possible to provide a default name for the operation.
The next interactive step is determined by the return code as follows:
Return
Return Code/Description
1 Cancel current assembly operation
3 Reserved for future use
n Normal operation with no default strings. "n" is any other return
code except 1 or 3.
Environment
Internal
void ufscpo
(
char * param,
int * retcode,
int rlen
)
char * | param | | |
int * | retcode | | |
int | rlen | | |
ufspcl (view source)
Defined in: uf_exit.h
Overview
Close Spreadsheet
The close spreadsheet user exit occurs when you exit the spreadsheet
and return control to NX. You must be in the modeling
application and you must be using a full licensed version of the
spreadsheet. This event occurs interactively when a spreadsheet is
active by selecting either File->Exit or Connections->Disconnect from
the spreadsheet menubar. Return codes are ignored with this exit.
In order to use the full licensed version of the Xess spreadsheet along with
the integrated NX/XESS customized applications, you must do the following
prior to invoking NX:
1) Set the UGII_SPREADSHEET variable in the .ugii_env file to point to the
directory which includes the 'xess4' binary executable.
2) Set the environment variable, XESS_FULL, to anything (e.g. setenv XESS_FULL 1).
Environment
Internal
void ufspcl
(
char * param,
int * retcode,
int rlen
)
char * | param | | |
int * | retcode | | |
int | rlen | | |
ufspop (view source)
Defined in: uf_exit.h
Overview
Open Spreadsheet
The open spreadsheet user exit occurs when you activate the spreadsheet
from NX. You must be in the modeling or gateway application with
an active part and you must be using a full licensed version of the
spreadsheet. This event occurs interactively when a spreadsheet is
activated by selecting Toolbox->Spreadsheet from menubar. Return codes
are ignored with this exit.
In order to use the full licensed version of the Xess spreadsheet along with
the integrated NX/XESS customized applications, you must do the following
prior to invoking NX:
1) Set the UGII_SPREADSHEET variable in the .ugii_env file to point to the
directory which includes the 'xess4' binary executable.
2) Set the environment variable, XESS_FULL, to anything (e.g. setenv XESS_FULL 1).
Environment
Internal
void ufspop
(
char * param,
int * retcode,
int rlen
)
char * | param | | |
int * | retcode | | |
int | rlen | | |
ufspuf (view source)
Defined in: uf_exit.h
Overview
Finish Updating Spreadsheet
The finish updating spreadsheet exit occurs at the completion of
updating expressions. You must be in the modeling application.
Return
Return Code/Description
1 Perform a spreadsheet recalc after returning from the user
exit.
n No spreadsheet recalc. "n" is any other return code except 1
Environment
Internal
void ufspuf
(
char * param,
int * retcode,
int rlen
)
char * | param | | |
int * | retcode | | |
int | rlen | | |
ufspup (view source)
Defined in: uf_exit.h
Overview
Update Spreadsheet
The update spreadsheet user exit occurs at the start of updating
expressions into the NX part file. You must be in the modeling
application. First, you need to call Tools->Spreadsheet and
then, in the Spreadsheet menu call Tools->Extract Expr in
order to have some expressions. The interactive entry point is
Tools->Update Part.
Environment
Internal
void ufspup
(
char * param,
int * retcode,
int rlen
)
char * | param | | |
int * | retcode | | |
int | rlen | | |
ufsta (view source)
Defined in: uf_exit.h
Overview
NX Startup
The NX startup user exit occurs when you invoke NX. There are
no return codes for this option. If the user exit exists, your routine
executes. if the user exit does not exist, then NX starts as it
normally would.
Environment
Internal
void ufsta
(
char * param,
int * retcode,
int rlen
)
char * | param | | |
int * | retcode | | |
int | rlen | | |
ufsvas (view source)
Defined in: uf_exit.h
Overview
Save Part As
The save part user exit occurs after the File->Save As... menu.
When the mode is Design in Context and the work part to save is not
the displayed part, then for each level of the assembly that contains
the work part, the full file specification of the current part name is
passed as the string parameter (param) to the user exit. This enables
you to identify which part is to be "saved as"
If no User Function program error occurs and an active part exists, the
next interactive step is is determined by the return code as follows:
Return
Return Code/Description
1 Gateway menu. Control passes back to the Gateway menu after going
through the warnings and clean up routines of the normal NX dialogs
if required.
2 Choose part name file selection dialog with the string (from param)
as the default. For Design in Context, control passes to the normal
NX dialogs for each level of the assembly above the work part
(occurrence in an assembly tree) but with a default string for the
new part name as specified by the string from param.
n File->Save As dialog with no default string. n not equal to 1 or 2.
For Design in Context, control passes to the normal NX dialogs
for each level of the assembly above the work part (occurrence
in an assembly tree).
Environment
Internal
void ufsvas
(
char * param,
int * retcode,
int rlen
)
char * | param | | |
int * | retcode | | |
int | rlen | | |
ufuds (view source)
Defined in: uf_exit.h
Overview
User Defined Symbols
The user defined symbols user exit occurs after the
Application->Drafting->Create->User Defined Symbols menu. There are no
return codes for this option. If the user exit exists, your routine
executes and then the User Defined Symbol dialog displays. if the user
exit does not exist, the User Defined Symbol dialog displays.
Environment
Internal
void ufuds
(
char * param,
int * retcode,
int rlen
)
char * | param | | |
int * | retcode | | |
int | rlen | | |
ufufun (view source)
Defined in: uf_exit.h
Overview
User Function
The execute User Function user exit occurs after the File->Execute->User
Function menu.
The next interactive step is determined by the return code as follows:
Return
Return Code/Description
1 Runs the User Function program using the string passed from param.
The Motif file dialog is not displayed.
2 Disables the Execute User Function option. The system adminstrator
has the option of making this option (and the use of a User
Function license) unavailable.
Environment
Internal
void ufufun
(
char * param,
int * retcode,
int rlen
)
char * | param | | |
int * | retcode | | |
int | rlen | | |
ufusd (view source)
Defined in: uf_exit.h
Overview
Component Where-Used
The component where-used user exit occurs after the
Assemblies->Reports->Where Used menu and before the select components
dialog.
If no User Function program error is returned and no active part exists,
the file menu displays.
If an active part exists, the next interactive step is determined by the
return code as follows:
Return
Return Code/Description
1 Assemblies->Reports->Where Used dialog with displayed part name as
default.
2 Assemblies->Reports->Where Used dialog with the string (from param)
as the default component name.
3 Assemblies->Reports->Where Used dialog with the string (from param)
as the default directory path name.
n Assemblies->Reports->Where Used dialog with no default string. "n"
is any other code exept 1, 2, or 3.
Environment
Internal
void ufusd
(
char * param,
int * retcode,
int rlen
)
char * | param | | |
int * | retcode | | |
int | rlen | | |
wetd (view source)
Defined in: uf_exit.h
Overview
CAM exit wetd
This cam exit will be invoked when setting technology data for geometry or
operation of WEDM in an interactive NX session.
In the new API the exit object can be obtained by calling GetCamExitObject method on the CAMSetup
Return
Return Code/Description
-1 User Exit Error
0 Successful User Exit execution
Environment
Internal
void wetd
(
char * param,
int * return_code,
int parm_len
)
char * | param | Input | - A parameter used to convert Open API param to CAM exit id. |
int * | return_code | Output | - return code |
int | parm_len | Input | - length of input "param" |