UF_ASSEM_expl_status_e (view source)
Defined in: uf_assem.h
Also known as:
- UF_ASSEM_expl_status_t
- UF_ASSEM_expl_status_p_t
Data Members
UF_ASSEM_unexploded
UF_ASSEM_exploded
UF_ASSEM_revert_exploded
UF_ASSEM_level_option_e (view source)
Defined in: uf_assem_types.h
Also known as:
Overview
UF_ASSEM_level_option_t is used to control the results of an operation
to modify a part occurrence, when the part occurrence chosen
cannot be modified directly for some reason. It is currently
used for reposition.
Data Members
UF_ASSEM_use_strict_level
UF_ASSEM_use_existing_level
UF_ASSEM_establish_override
UF_ASSEM_part_load_option_e (view source)
Defined in: uf_assem_types.h
Also known as:
- UF_ASSEM_part_load_option_t
Overview
UF_ASSEM_part_load_option_t is used to control the part load option.
The first four settings are equivalent to the four possible
combinations of the partial loading and lightweight representations.
The final setting is reserved for future use.
Data Members
UF_ASSEM_part_load_option_fully_load = 0
UF_ASSEM_part_load_option_partially_load = 1
UF_ASSEM_part_load_option_fully_load_lightweight_display = 2
UF_ASSEM_part_load_option_partially_load_lightweight_display = 3
UF_ASSEM_part_load_option_minimally_load_lightweight_display = 4
UF_ASSEM_seq_playback_e (view source)
Defined in: uf_assem.h
Also known as:
- UF_ASSEM_seq_playback_t
- UF_ASSEM_seq_playback_p_t
Data Members
UF_ASSEM_seq_step_forward
UF_ASSEM_seq_step_backward
UF_ASSEM_seq_play_forward
UF_ASSEM_seq_play_backward