UF_UGMGR_part_file_info_s (view source)
Defined in: uf_ugmgr_types.h
Also known as:
- UF_UGMGR_part_file_info_t
- UF_UGMGR_part_file_info_p_t
Overview
This structure is used to represent an NX PartFile for the purpose of resolving
a part file name and used as input to the service UF_UGMGR_resolve_part_file_infos.
Note: -If fileName is specified then partId, revisionID, modelType, datasetName are ignored.
-If fileName is not provided then partID has to be provided for the input to be valid.
-If partID is provided then modelType, datasetName can be provided along with partID and revisionID.
-For unconfigured input( i.e., revision information not available) and revisionOption is UF_UGMGR_configure_none
the current revision Rule in effect will be used to resolve the NX PartFile.
Data Members
fileName
const char *
partID
const char *
revisionId
const char *
modelType
const char *
datasetName
const char *
revisionRule
const char *
revisionOption
or @DB- Command line Input name (This is what is returned from methods such as
UF_UGMGR_convert_file_name_to_cli) of the NX PartFile. If this is not specified/used,
it has to be initialized to NULL