UF_UGFONT_add_font (view source)
Defined in: uf_ugfont.h
Overview
Adds a font to the Font Table Entity (FTE) if it does not exist. If the
font already exists, the index of the existing font is returned. This
function returns the font index number for the FTE. Note that adding a font
will use the first available slot in the FTE (one that has a NULL font name).
This will only add NX fonts. Use UF_UGFONT_add_standard_font to add
Standard fonts.
Environment
Internal and External
See Also
UF_UGFONT_add_standard_font
History
Originally release in V14.0
Required License(s)
gateway
int UF_UGFONT_add_font
(
tag_t fte,
int * index,
char * font
)
tag_t | fte | Input | The tag of the Font Table Entity (FTE). |
int * | index | Output | Font index number for the specified font |
char * | font | Input | The name of the font |
UF_UGFONT_add_standard_font (view source)
Defined in: uf_ugfont.h
Overview
Adds a standard font to the Font Table Entity (FTE) if it does not exist.
If the font already exists, the index of the existing font is returned. This
function returns the font index number for the FTE. Note that adding a font
will use the first available slot in the FTE (one that has a NULL font name).
Environment
Internal and External
History
Originally release in NX 7.5
Required License(s)
gateway
int UF_UGFONT_add_standard_font
(
tag_t fte,
int * index,
char * font
)
tag_t | fte | Input | The tag of the Font Table Entity (FTE). |
int * | index | Output | Font index number for the specified font |
char * | font | Input | The name of the font |
UF_UGFONT_ask_font_header (view source)
Defined in: uf_ugfont.h
Overview
Fills in the UF_UGFONT_font_header_s structure with font information
for a given font.
This only works for NX fonts.
Environment
Internal and External
History
This function was originally released in V15.0.
Required License(s)
gateway
int UF_UGFONT_ask_font_header
(
tag_t fte,
int font,
UF_UGFONT_font_header_t * header
)
UF_UGFONT_ask_font_name (view source)
Defined in: uf_ugfont.h
Overview
Returns the font name of the specified font index number. The font name
may be NULL. This can happen if part cleanup has removed a font as being
unused. The font index number still exists, but since there is not a font
name, the output font_name will be NULL. If a font returns a NULL font name,
then it is not a valid font to use.
The user must call UF_free to free the resulting font name.
Environment
Internal and External
History
Originally released in V14.0
Required License(s)
gateway
int UF_UGFONT_ask_font_name
(
tag_t fte,
int index,
char * * font_name
)
tag_t | fte | Input | The tag of the Font Table Entity (FTE). |
int | index | Input | The font index number |
char * * | font_name | Output to UF_*free* | The font name. Use UF_free to deallocate memory when done. |
UF_UGFONT_ask_font_styles (view source)
Defined in: uf_ugfont.h
Overview
UF_UGFONT_ask_font_styles
Return the font styles available for a font in the Font Table Entry (FTE)
Environment
Internal and External
History
This function was originally released in NX 8.0
Required License(s)
gateway
int UF_UGFONT_ask_font_styles
(
tag_t fte,
int index,
int * num_styles,
char * * * styles
)
tag_t | fte | Input | The tag of the Font Table Entity (FTE) |
int | index | Input | Font index number of the font to check on |
int * | num_styles | Output | The number of style names in the style_names array. This will be zero if the index input is not that of a font in the Font Table Entity, or if the index is that of an NX Legacy font (not that of a Standard Font). |
char * * * | styles | Output to UF_*free* | An array of the names of available styles for the given font. This must be freed by the caller, using UF_free. |
UF_UGFONT_ask_font_type (view source)
Defined in: uf_ugfont.h
Overview
UF_UGFONT_ask_font_type
Return the type of a font in the Font Table Entry (FTE)
Environment
Internal and External
History
This function was originally released in NX 7.5
Required License(s)
gateway
int UF_UGFONT_ask_font_type
(
tag_t fte,
int index,
UF_UGFONT_type_t * type
)
tag_t | fte | Input | The tag of the Font Table Entity (FTE) |
int | index | Input | Font index number of the font to check on |
UF_UGFONT_type_t * | type | Output | The type of the font |
UF_UGFONT_ask_number_of_fonts (view source)
Defined in: uf_ugfont.h
Overview
Returns the number of entries in the Font Table Entity (FTE). Each entry
may be a valid font or an entry that has been previously deleted. The only way
to validate if a font number is usable is to call UF_UGFONT_ask_font_name.
If that returns a non-NULL name, then the font number is valid and can be used.
If UF_UGFONT_ask_font_name returns NULL for the name, then the font number
is not valid (it has been deleted using part cleanup).
Environment
Internal and External
History
Originally release in V14.0
Required License(s)
gateway
int UF_UGFONT_ask_number_of_fonts
(
tag_t fte,
int * num
)
tag_t | fte | Input | The tag of the Font Table Entity (FTE). |
int * | num | Output | The number of font entries in the FTE. Some of the font entries may be currently unused, if part cleanup has been run on the part. |
UF_UGFONT_replace_font (view source)
Defined in: uf_ugfont.h
Overview
UF_UGFONT_replace_font
Change the particular font number to a new name in the Font Table Entry (FTE)
To replace the font type as well as the font name, use UF_UGFONT_replace_font_1.
Environment
Internal and External
See Also
UF_UGFONT_replace_font_1
History
This function was originally released in NX3.0
Required License(s)
gateway
int UF_UGFONT_replace_font
(
tag_t fte,
int index,
const char * const font
)
tag_t | fte | Input | The tag of the Font Table Entity (FTE) |
int | index | Input | Font index number for the old font to replace |
const char * const | font | Input | The name of the new font |
UF_UGFONT_replace_font_1 (view source)
Defined in: uf_ugfont.h
Overview
UF_UGFONT_replace_font_1
Change the particular font number to a new name and new type in the
Font Table Entry (FTE)
Environment
Internal and External
History
This function was originally released in NX 7.5
Required License(s)
gateway
int UF_UGFONT_replace_font_1
(
tag_t fte,
int index,
UF_UGFONT_type_t type,
const char * const font
)
tag_t | fte | Input | The tag of the Font Table Entity (FTE) |
int | index | Input | Font index number for the old font to replace |
UF_UGFONT_type_t | type | Input | The type of the new font |
const char * const | font | Input | The name of the new font |