/*
uf_trns.h
File Description:
This is the Open C API interface to transformations. Using these subroutines you
can:
. change coordinates
. map positions
. perform compound transformations
. perform translation, scaling, and rotation
. mirror through a line or plane
. perform transformation
***************************************************************************/
#ifndef UF_TRNS_INCLUDED
#define UF_TRNS_INCLUDED
/***************************************************************************
***************************************************************************/
#include <uf_defs.h>
#include <libufun_exports.h>
/*******************************************************************************
Returns a matrix to map coordinates from one coordinate system to another.
Note: rp1 and rp2 are invalid when they contain a zero direction vector, or
the X and Y vectors are parallel.
Return:
void.
Environment: Internal & External
See Also:
History:
*******************************************************************************/
extern UFUNEXPORT void uf5940(
double ref_csys[9], /* <I>
Real Data For Reference Coordinate System
rp1[0-2] is the origin in absolute coordinates.
rp1[3-8] are the X and Y vectors in absolute coordinates.
*/
double dest_csys[9], /* <I>
Real Data For Destination Coordinate System
rp2[0-2] is the origin in absolute coordinates.
rp2[3-8] are the X and Y vectors in absolute coordinates.
*/
double matrix[12], /* <O>
Resulting Matrix. This must be declared to hold 12 doubles.
*/
int *status /* <O>
Status Code
0 = Success
1 = rp1 Is Invalid
2 = rp2 Is Invalid
*/
); /* <WRAPAS:UF_TRNS_create_csys_mapping_matrix> */
/*******************************************************************************
Returns the transformation of a position. No new objects are created here.
When rp2 is the "Change Coordinate" matrix (from UF5940), ra1 should be a
position with respect to the reference coordinate system in the input in order
to get back ra1 as a position with respect to the destination coordinate system
in the output. When rp2 is any other type of transformation matrix, ra1 should
be a position in the absolute coordinates. The output in ra1 is then a
transformed position in absolute coordinates as well.
Note: The array for the transformation matrix was changed to be 12 instead of
16. The code only uses the first 12 elements of the array to do the transformation
so the last 4 elements were not necessary.
Return: void.
Environment: Internal & External
See Also:
History:
*******************************************************************************/
extern UFUNEXPORT void uf5941(
double ra1[3], /* <I/O>
Position/ Transformed Position
*/
double rp2[12] /* <I>
Defined Transformation Matrix. This must be declared
to hold 12 doubles.
*/
); /* <WRAPAS:UF_TRNS_map_position> */
/*******************************************************************************
Returns a product of two previously defined transformation matrices.
This is not a math routine to multiply any 2 matrices. The input matrices are
transformation matrices only, and the product is the compound transformation
matrix.
Note: The array for matrix1, matrix2 and product were changed to be 12 instead of
16. The code only uses the first 12 elements of the array to do the transformation
so the last 4 elements were not necessary.
Return: void.
Environment: Internal & External
See Also:
History:
*******************************************************************************/
extern UFUNEXPORT void uf5942(
double matrix1[12], /* <I>
Matrix Number 1. This must be a 12 element
array.
*/
double matrix2[12], /* <I>
Matrix Number 2. This must be a 12 element
array.
*/
double product[12] /* <O>
Product Matrix. This must be a 12 element
array.
*/
); /* <WRAPAS:UF_TRNS_multiply_matrices> */
/*******************************************************************************
Returns a matrix to perform a linear transformation a delta distance along the
X-, Y-, and Z- axes of the absolute coordinate system.
Note: The array for the translation matrix was changed to be 12 instead of
16. The code only uses the first 12 elements of the array to do the transformation
so the last 4 elements were not necessary.
Return: void.
Environment: Internal & External
See Also:
History:
*******************************************************************************/
extern UFUNEXPORT void uf5943(
double translation[3], /* <I>
Distance To Translate
rp1[0-2] contains Dx, Dy and Dz respectively.
*/
double matrix[12] /* <O>
Translation Matrix. This must be a 12 element
array.
*/
); /* <WRAPAS:UF_TRNS_create_translation_matrix> */
/*******************************************************************************
Returns a matrix to perform a scaling, uniform or non-uniform, about an
arbitrary origin.
Note: The array for the scaling matrix was changed to be 12 instead of
16. The code only uses the first 12 elements of the array to do the transformation
so the last 4 elements were not necessary.
Return: void.
Environment: Internal & External
See Also:
History:
*******************************************************************************/
extern UFUNEXPORT void uf5944(
int *type, /* <I>
Type
1 - Uniform
2 - Non-Uniform
*/
double scales[3], /* <I>
Scaling Factors.
rp2[0] is Sx (or factors when type=1)
rp2[1] is Sy (not used when type=1)
rp2[2] is Sz (not used when type=1).
*/
double origin[3], /* <I>
Scaling Origin (Absolute Coordinates)
*/
double matrix[12], /* <O>
Scaling Matrix. This must be declared to hold
12 doubles.
*/
int *status /* <O>
Status Code
0 - Success
1 - Scaling Factor Is Not Greater Than Zero
2 - Invalid Option
*/
); /* <WRAPAS:UF_TRNS_create_scaling_matrix> */
/*******************************************************************************
Returns a matrix to perform a rotation around an arbitrary axis.
Note: The array for the rotation matrix was changed to be 12 instead of
16. The code only uses the first 12 elements of the array to do the transformation
so the last 4 elements were not necessary.
Return: void
Environment: Internal & External
See Also:
History:
*******************************************************************************/
extern UFUNEXPORT void uf5945(
double origin[3], /* <I>
Origin Of The Axis - Absolute Coordinates
*/
double direction[3], /* <I>
Direction Vector - Absolute Coordinates
*/
double *degrees_rotation, /* <I>
Rotation Angle In Degrees
*/
double matrix[12], /* <O>
Rotation Matrix. This must be declared to hold
12 doubles.
*/
int *status /* <O>
Status Code
0 - Success
1 - Direction Vector Is A Zero Vector
*/
); /* <WRAPAS:UF_TRNS_create_rotation_matrix> */
/*******************************************************************************
Returns a matrix to perform a reflection through a line or a plane.
This function will not work with a datum plane. If a datum plane is passed in as
input, an error will be returned.
When the line is perpendicular to the XY plane there is an infinite number of
planes that pass through the line and are perpendicular to the XY plane;
therefore, error code = 2.
Note: The array for the mirror matrix was changed to be 12 instead of
16. The code only uses the first 12 elements of the array to do the transformation
so the last 4 elements were not necessary.
Return: void
Environment: Internal & External
See Also:
History:
*******************************************************************************/
extern UFUNEXPORT void uf5946(
tag_t *object, /* <I>
Line Or Plane Object Identifier
*/
double matrix[12], /* <O>
Mirror matrix. This must be declared to hold 12
doubles.
*/
int *status /* <O>
Status Code
0 - Success
1 - Invalid Line Or Plane Object Identifier
2 - Unique Plane Through Line Cannot Be Defined
*/
); /* <WRAPAS:UF_TRNS_create_reflection_matrix> */
/*******************************************************************************
Transform objects according to a previously defined matrix. The matrix should
be defined by calls to uf5942-uf5946.
The upper limit on the number of objects to transform is 32767. The object
types supported for non-uniform scaling are the same as those supported by
non-uniform scaling in interactive NX.
This function will not move objects when their parents need to be transformed.
Use UF_MODL_transform_entities to transform objects and their parents.
Note: The array for the transformation matrix was changed to be 12 instead of
16. The code only uses the first 12 elements of the array to do the transformation
so the last 4 elements were not necessary.
Return: void
Environment: Internal & External
See Also:
History:
*******************************************************************************/
extern UFUNEXPORT void uf5947(
const double rp1[12], /* <I>
Defined Transformation Matrix. This must be
a 12 element array. This array should be
initialized using the functions uf5942-uf5946
to produce the required transformation.
*/
const tag_t objects[], /* <I>
Array of object identifiers.
*/
const int *n_objects, /* <I>
Number of objects in objects array.
*/
const int *move_or_copy, /* <I>
Move/Copy Status
1 - Move
2 - copy.
*/
const int *dest_layer, /* <I>
Destination Layer,
0 - the original layer,
-1 - the work layer
1 - 256 - the specified layer
*/
const int *trace_curves, /* <I>
Trace Curve Status, 1 means on, 2 means off.
*/
tag_t *copies, /* <O>
List of copied object identifiers. This is
not used when move_or_copy is equal to 1 (move).
When move_or_copy is 2 (copy), this must be dimensioned
by the caller as large enough to contain the same number
of objects that are in the objects array.
*/
tag_t *trace_curve_group, /* <O>
Group of trace curves. This is not used when
the trace_curves input is set to 2 (off).
*/
int *status /* <O>
Status Code
0 - Success
1 - Too Many Or Too Few Entities To
Transform
2 - Invalid Parameter
3 - Invalid Object (Not Alive Or Not
Transformable)
4 - Shear Matrix With Non-shearable
Objects In The List
5 - Modeling update error
6 - Error adding modeling data to copied solid
7 - Cannot scale parametric solid
8 - Transformation is unsuitable for the object
9 - Cannot scale developed curve
10 - Cannot mirror solid
11 - Cannot transform occurrence
12 - Cannot transform sketches or sketch curves
*/
); /* <WRAPAS:UF_TRNS_transform_objects> */
/*******************************************************************************
The following function will transform the input entities
and all of its parents.
It supports input entities from diffferent components in assembly context.
The component of input entity will be fully loaded after transforming if it's partially loaded.
Return: Error code
Environment: Internal & External
See Also:
History: Originally released in NX502
*******************************************************************************/
extern UFUNEXPORT int UF_MODL_transform_entities
(
int num_entities, /* <I> - number of entries in following array */
tag_t *entities, /* <I> - array of entities to transform */
double matrix[16] /* <I> - matrix defining transform */
);
/*******************************************************************************
The following function will check if there are any parents with input entities.
If input entities have parents, the parent entities will be collected
Return: Error code
Environment: Internal & External
See Also:
History: Originally released in NX502
*******************************************************************************/
extern UFUNEXPORT int UF_MODL_ask_entity_parents
(
int num_entities, /* <I> - number of entries in following array */
tag_t *entities, /* <I> - array of entities to transform */
logical *found_parent, /* <O> - if found_parent = false, found no parents
if found_parent = true, found parents */
int *num_parent_entities, /* <O> - if found_parent = true, the number of parent entities will be output*/
tag_t **parent_entities /* <OF>- if found_parent = true, the parent entities will be output
call UF_free to free parent_entities only if found_parent = true*/
);
#undef EXPORTLIBRARY
#endif /* END UF_TRNS_INCLUDED */