UF_STYLER_item_value_type_s (view source)
Defined in: uf_styler.h
Also known as:
- UF_STYLER_item_value_type_t
- UF_STYLER_item_value_type_p_t
Overview
The following structure is used for callbacks and Ask/Set methods. Reason,
item_id, subitem_index, and item_attr are used as descriptive fields to
describe the ownership of the attribute. Count, indicator, and value are
used to represent the value of the attribute. Note that not all fields in
this structure are relevant at one time. Depending on the item type and
attribute type, zero or more additional fields may become relevant.
Data Members
reason
int
item_id
const char *
subitem_index
int
count
int
item_attr
int
indicator
int
value
UF_STYLER functions. This indicates the type of
action, that triggers the callback, e.g.
UF_STYLER_ACTIVATE_CB. Open API callbacks
can rely on this field to determine what user
interaction has occurred. Programs should not
modify this value.