Object associativity type: UF_SKET_end_point; UF_SKET_arc_center - object must be an arc; UF_SKET_tangency - object must be an arc; UF_SKET_curve_point - object must be a spline UF_SKET_anchor_point - object must be a sketch conic
object_assoc_mod_value
int
Object associativity modifier: UF_SKET_first_end_point or UF_SKET_last_end_point if object_assoc_type = UF_SKET_end_point; Not Used if object_assoc_type = UF_SKET_arc_center or UF_SKET_anchor_point; parameter percentage (0 - 100) (used to find approx tgt pt) if object_assoc_type = UF_SKET_tangency; the index number of the defining point of the spline(starting from 1) if object_assoc_type = UF_SKET_curve_point;
datum plane, datum axis, NX curves