/*
uf_sf_ugs_mesh.h
File description:
Internal type definitions for UF_SF_UGS_MESH (Scenario UGS Mesher)
module.
*******************************************************************************/
#ifndef UF_SF_UGS_MESH_H_INCLUDED
#define UF_SF_UGS_MESH_H_INCLUDED
#include <uf_sf_types.h>
/***************************************************************************
* Enumeration:-UF_SF_ugs_mesher_midnode_option_t
*
* This enumeration allows the specification of how midnodes should be
* placed during meshing.
*************************************************************************** */
enum UF_SF_ugs_mesher_midnode_option_e
{
UF_SF_UGS_MESHER_straight_midnodes = 2, /* All midnodes will be placed
at straight line linear
location between corner
nodes. */
UF_SF_UGS_MESHER_curved_midnodes = 1, /* All midnodes will be project
to underlying geometry. */
UF_SF_UGS_MESHER_mixed_midnodes = 0 /* All midnodes will be projected
to underlying geometry, unless
doing so would input Jacobian
error threshold. */
};
typedef enum UF_SF_ugs_mesher_midnode_option_e UF_SF_ugs_mesher_midnode_option_t;
enum UF_SF_ugs_tet_mesh_fillet_type_option_e
{
UF_SF_UGS_TET_MESH_FILLET__all = 0, /* Both concave as well as convex fillets */
UF_SF_UGS_TET_MESH_FILLET__inside = 1, /* Inside radius fillets. */
UF_SF_UGS_TET_MESH_FILLET__outside = 2 /* Outside radius fillets */
};
typedef enum UF_SF_ugs_tet_mesh_fillet_type_option_e UF_SF_ugs_tet_mesh_fillet_type_option_t;
/***************************************************************************
* Enumeration:-UF_SF_ugs_2d_mesher_elem_type_t
*
* This enumeration allows the specification of what 2d shell element type
* should be generated by a shell mesher.
*************************************************************************** */
enum UF_SF_ugs_2d_mesher_elem_type_e
{
UF_SF_UGS_MESHER_tri3 = 0,
UF_SF_UGS_MESHER_tri6 = 1,
UF_SF_UGS_MESHER_quad4 = 2,
UF_SF_UGS_MESHER_quad8 = 3
};
typedef enum UF_SF_ugs_2d_mesher_elem_type_e UF_SF_ugs_2d_mesher_elem_type_t;
/***************************************************************************
* Structure :- UF_SF_ugs_tet_mesh_parms_s
*
* This structure allows specification of tetrahedral meshing parameters.
*
* Initialization :- This structure can be initialized with the
* UF_SF_ugs_tet_mesh_parms_INIT macro.
*************************************************************************** */
struct UF_SF_ugs_tet_mesh_parms_s
{
UF_SF_element_type_t element_type; /* Desired element type. */
int midnodes; /* TRUE for tet10s,
FALSE for tet4s. */
double element_size; /* Desired element size. If
zero or negative, then mesher
will choose element size
internally. */
UF_SF_ugs_mesher_midnode_option_t midnode_option; /* Whether to project midnodes or not. */
int geometry_tolerance_toggle; /*Geometry Tolerance for midnode straightening*/
double geometry_tolerance_value; /*Geometry Tolerance value for midnode straightening*/
double maximum_midnode_jacobian; /* If midnode_option =
UF_SF_UGS_MESHER_mixed_midnodes,
any element with a jacobian
value higher than
maximum_midnode_jacobian will
have its midnodes
straightened. */
double minimum_face_angle; /* Minimum angle at corner of a
face that can support element.
corners smaller than this will
be pinched out. This angle is
measured in degrees. */
int surf_mesh_size_variation; /* This controls how much variation
in element size is
desired/permitted in the mesh on
the surface of the bodies being
meshed. Valid values go from 0
to 100. This number does not
coorespond directly to any
actual meshing parameter, but
rather is a relative scale that
the user can use to indicate
their tolerance for mesh
variation. It is used
internally in the mesher to
calculate expansion factors and
a minimum element size. 0
means that there will be
minimumal element size
variation. 100 means that there
will be maximum element size
variation. */
int tet_mesh_size_variation; /* This controls whether the tets
are permitted to expand as you
progress into the interior of
the body. Valid values go from
0 to 100. 0 means that
element sizes must remain
relatively constant. 100 means
that the elements can expand
very rapidly. */
int multi_block_decomposition; /* Attempt MultiBlock Decomposition 0=OFF,1=ON */
int mesh_transition; /* Mesh transition 0=OFF,1=ON */
int remesh_toggle; /* Avoid failing elements by reducing element size
0=OFF,1=ON */
int create_pyramids; /* Create pyramid transition elements. Only for ANSYS
0=OFF,1=ON */
double small_feature; /* % of element length for abstraction */
int attempt_mapped_meshing;
int two_element_through_thickness_toggle;
int auto_fix_failed_elements_toggle;
int edge_merge_toggle; /* Edge merge toggle 0 or 1 */
double edge_angle; /* Edge merge angle */
int fillet_toggle; /* true => Filler detection ON
false=> Fillet detection OFF */
UF_SF_ugs_tet_mesh_fillet_type_option_t fillet_type; /* Used only if fillet_toggle == true
Fillet type */
int fillet_num_elem; /* No of elements on a quarter arc of fillet */
double fillet_min_rad; /* Min radius */
double fillet_max_rad;
};
typedef struct UF_SF_ugs_tet_mesh_parms_s UF_SF_ugs_tet_mesh_parms_t, *UF_SF_ugs_tet_mesh_parms_p_t;
#define UF_SF_ugs_tet_mesh_parms_INIT( mesh_parms ) \
{ \
(mesh_parms)->element_type = UF_SF_TET4; \
(mesh_parms)->midnodes = TRUE; \
(mesh_parms)->element_size = -1.0; \
(mesh_parms)->midnode_option = UF_SF_UGS_MESHER_mixed_midnodes;\
(mesh_parms)->maximum_midnode_jacobian = 20.0; \
(mesh_parms)->minimum_face_angle = 20.0; \
(mesh_parms)->surf_mesh_size_variation = 0; \
(mesh_parms)->tet_mesh_size_variation = 0; \
(mesh_parms)->mesh_transition = 0; \
(mesh_parms)->remesh_toggle = 0; \
(mesh_parms)->create_pyramids = 0; \
(mesh_parms)->small_feature = 50.0; \
(mesh_parms)->attempt_mapped_meshing = true; \
(mesh_parms)->two_element_through_thickness_toggle = false; \
(mesh_parms)->auto_fix_failed_elements_toggle = false; \
(mesh_parms)->edge_merge_toggle = 0; \
(mesh_parms)->edge_angle = 15.0; \
(mesh_parms)->fillet_toggle = false; \
(mesh_parms)->fillet_type = UF_SF_UGS_TET_MESH_FILLET__all; \
(mesh_parms)->fillet_num_elem = 4; \
(mesh_parms)->fillet_min_rad = 0.0; \
(mesh_parms)->fillet_max_rad = 0.0; \
}
/***************************************************************************
* Enumeration:-UF_SF_ugs_abstraction_fillet_type_option_t
*
* This enumeration allows the specification of fillet types to be
* considered during abstraction.
*************************************************************************** */
enum UF_SF_ugs_abstraction_fillet_type_option_e
{
UF_SF_UGS_ABSTRACTION_FILLET__all = 0, /* Both concave as well as convex fillets */
UF_SF_UGS_ABSTRACTION_FILLET__inside = 1, /* Inside radius fillets. */
UF_SF_UGS_ABSTRACTION_FILLET__outside = 2 /* Outside radius fillets */
};
typedef enum UF_SF_ugs_abstraction_fillet_type_option_e UF_SF_ugs_abstraction_fillet_type_option_t;
/* ================================================================
Parameter settings for tet mesh with abstraction control
================================================================ */
struct UF_SF_ugs_mesh_abstraction_params_s
{
double small_feature; /* % of element length for abstraction */
int edge_merge_toggle; /* Edge merge toggle 0 or 1 */
double edge_angle; /* Edge merge angle */
int fillet_toggle; /* true => Filler detection ON
false=> Fillet detection OFF */
UF_SF_ugs_abstraction_fillet_type_option_t fillet_type; /* Used only if fillet_toggle == true
Fillet type */
int fillet_num_elem; /* No of elements on a quarter arc of fillet */
double fillet_min_rad; /* Min radius */
double fillet_max_rad; /* Max radius */
};
typedef struct UF_SF_ugs_mesh_abstraction_params_s UF_SF_ugs_mesh_abstraction_params_t, *UF_SF_ugs_mesh_abstraction_params_p_t;
/* Macro to initialize the parameters */
#define UF_SF_ugs_mesh_abstraction_parms_INIT( abs_parms ) \
{ \
(abs_parms)->small_feature = 50.0; \
(abs_parms)->edge_merge_toggle = 0; \
(abs_parms)->edge_angle = 15.0; \
(abs_parms)->fillet_toggle = false; \
(abs_parms)->fillet_type = UF_SF_UGS_ABSTRACTION_FILLET__all; \
(abs_parms)->fillet_num_elem = 4; \
(abs_parms)->fillet_min_rad = 0.0; \
(abs_parms)->fillet_max_rad = 0.0; \
}
/***************************************************************************
* Structure :- UF_SF_ugs_2d_mesh_parms_s
*
* This structure allows specification of 2d shell meshing parameters.
*
* Initialization :- This structure can be initialized with the
* UF_SF_ugs_2d_mesh_parms_INIT macro.
*************************************************************************** */
struct UF_SF_ugs_2d_mesh_parms_s
{
UF_SF_ugs_2d_mesher_elem_type_t element_type;
/* Desired element type. */
double element_size; /* Desired element size. If
zero or negative, then mesher
will choose element size
internally. */
int edge_match_toggle; /* Edge merge toggle 0 or 1 */
double edge_match_tolerance; /* edge matching tolerance. */
int suppress_hole_toggle; /* Suppress Hole toggle 0 or 1 */
double suppress_hole_diameter_value; /* Suppress Hole Diameter value. */
int suppress_hole_point_type; /* 0- NONE, 1-POINT, 2-MESHPOINT */
int target_minimum_element_edge_length; /* Target Minimum Element Edge Length toggle 0 or 1 */
int format_mesh; /* TRUE if 2d mesh is a shell
mesh that should be formatted
to the solver. FALSE if 2d
mesh is a seed mesh and not to
be formated out to solver. */
int attempt_quad_mapping; /* TRUE if map mesher should be
tried on faces for quad meshes
or if free mesher should be
called regardless of face
shape. */
int quad_only_option; /* Applies only when attempt_quad_mapping=FALSE
Values are:
0 => Allow triangles OFF.
1 => Allow triangles ON & 0 Triangle
2 => Allow triangles ON & 1 Triangle
If attempt_quad_mapping==TRUE does not
apply.*/
int split_poor_quads; /* TRUE if poorly shaped quads
should be split into
triangles.
FALSE if quads should be kept
regardless of quality. */
double maximum_quad_warp; /* if split_poor_quads == TRUE,
this is the warp quality
threshold. Any quad with
greater warp than this will
be split. */
UF_SF_ugs_mesher_midnode_option_t midnode_option; /* Whether to project midnodes
or not. */
int geometry_tolerance_toggle; /*Geometry Tolerance for midnode straightening*/
double geometry_tolerance_value; /*Geometry Tolerance value for midnode straightening*/
double maximum_midnode_jacobian; /* If midnode_option =
UF_SF_UGS_MESHER_mixed_midnodes,
any element with a jacobian
value higher than
maximum_midnode_jacobian will
have its midnodes
straightened. */
double minimum_face_angle; /* Minimum angle at corner of a
face that can support element.
corners smaller than this will
be pinched out. This angle is
measured in degrees. */
int surf_mesh_size_variation; /* This controls how much variation
in element size is
desired/permitted in the mesh on
the surface of the bodies being
meshed. Valid values go from 0
to 100. This number does not
coorespond directly to any
actual meshing parameter, but
rather is a relative scale that
the user can use to indicate
their tolerance for mesh
variation. It is used
internally in the mesher to
calculate expansion factors and
a minimum element size. 0
means that there will be
minimumal element size
variation. 100 means that there
will be maximum element size
variation. */
double small_feature; /* % of element length for abstraction */
int edge_merge_toggle; /* Edge merge toggle 0 or 1 */
double edge_angle; /* Edge merge angle */
int mesh_transition; /* Mesh transition 0=OFF,1=ON */
int multi_block_decomposition; /* Attempt MultiBlock Decomposition 0=OFF,1=ON */
int mesh_individual_faces; /* Mesh Individual Faces 0=OFF,1=ON */
int CAD_curvature_abstraction; /* CAD Curvature Abstraction 0=OFF,1=ON */
double minimum_feature_length; /* Desired element size. If
zero or negative, then mesher
will choose element size
internally. */
int mesh_method; /* 0 - Automatic, 1 - Paver */
int fillet_toggle; /* true => Filler detection ON
false=> Fillet detection OFF */
UF_SF_ugs_abstraction_fillet_type_option_t fillet_type; /* Used only if fillet_toggle == true
Fillet type */
int fillet_num_elem; /* No of elements on a quarter arc of fillet */
double fillet_min_rad; /* Min radius */
double fillet_max_rad; /* Max radius */
int max_included_angle_quad_toggle; /* Max Angle for quad Toggle state */
int min_included_angle_quad_toggle; /* Min Angle for quad Toggle state */
int max_included_angle_tria_toggle; /* Max Angle for tria Toggle state */
int min_included_angle_tria_toggle; /* Min Angle for tria Toggle state */
double max_included_angle_quad_value; /* Max Angle for quad value */
double min_included_angle_quad_value; /* Min Angle for quad value */
double max_included_angle_tria_value; /* Max Angle for tria value */
double min_included_angle_tria_value; /* Min Angle for tria value */
int move_nodes_off_geometry; /*Move Nodes Off Geometry*/
int max_warp_toggle;
};
typedef struct UF_SF_ugs_2d_mesh_parms_s UF_SF_ugs_2d_mesh_parms_t, *UF_SF_ugs_2d_mesh_parms_p_t;
#define UF_SF_ugs_2d_mesh_parms_INIT( mesh_parms ) \
{ \
(mesh_parms)->element_type = UF_SF_UGS_MESHER_quad4; \
(mesh_parms)->element_size = -1.0; \
(mesh_parms)->edge_match_toggle = 0; \
(mesh_parms)->edge_match_tolerance = 0.508; \
(mesh_parms)->format_mesh = TRUE; \
(mesh_parms)->attempt_quad_mapping = TRUE; \
(mesh_parms)->split_poor_quads = TRUE; \
(mesh_parms)->maximum_quad_warp = 10.0; \
(mesh_parms)->midnode_option = UF_SF_UGS_MESHER_mixed_midnodes;\
(mesh_parms)->maximum_midnode_jacobian = 5.0; \
(mesh_parms)->minimum_face_angle = 20.0; \
(mesh_parms)->surf_mesh_size_variation = 0; \
(mesh_parms)->mesh_transition = 0; \
(mesh_parms)->mesh_method = 0; \
(mesh_parms)->quad_only_option = 0; \
(mesh_parms)->edge_merge_toggle = 0; \
(mesh_parms)->edge_angle = 15.0; \
(mesh_parms)->small_feature = 50.0; \
(mesh_parms)->fillet_toggle = false; \
(mesh_parms)->fillet_type = UF_SF_UGS_ABSTRACTION_FILLET__all; \
(mesh_parms)->fillet_num_elem = 4; \
(mesh_parms)->fillet_min_rad = 0.0; \
(mesh_parms)->fillet_max_rad = 0.0; \
(mesh_parms)->max_included_angle_quad_toggle = false; \
(mesh_parms)->min_included_angle_quad_toggle = false; \
(mesh_parms)->max_included_angle_tria_toggle = false; \
(mesh_parms)->min_included_angle_tria_toggle = false; \
(mesh_parms)->max_included_angle_quad_value = 150.0; \
(mesh_parms)->min_included_angle_quad_value = 30.0; \
(mesh_parms)->max_included_angle_tria_value = 140.0; \
(mesh_parms)->min_included_angle_tria_value = 20.0; \
}
/***************************************************************************
* Structure :- UF_SF_ugs_solid_from_shell_mesh_parms_s
*
* This structure allows specification of solid from shell meshing parameters.
*
* Initialization :- This structure can be initialized with the
* UF_SF_ugs_solid_from_shell_mesh_parms_INIT macro.
*************************************************************************** */
struct UF_SF_ugs_solid_from_shell_mesh_parms_s
{
int midnodes; /* TRUE for tet10s,
FALSE for tet4s. */
int tet_mesh_size_variation; /* This controls whether the tets
are permitted to expand as you
progress into the interior of
the body. Valid values go from
0 to 100. 0 means that
element sizes must remain
relatively constant. 100 means
that the elements can expand
very rapidly. */
int fill_holes; /* TRUE if the interior holes
should be filled */
};
typedef struct UF_SF_ugs_solid_from_shell_mesh_parms_s UF_SF_ugs_solid_from_shell_mesh_parms_t, *UF_SF_ugs_solid_from_shell_mesh_parms_p_t;
#define UF_SF_ugs_solid_from_shell_mesh_parms_INIT( mesh_parms ) \
{ \
(mesh_parms)->midnodes = FALSE; \
(mesh_parms)->tet_mesh_size_variation = 0; \
(mesh_parms)->fill_holes = FALSE; \
}
#endif /* UF_SF_COMPOSITE_H_INCLUDED */