/*
uf_sf_legend.h
File description:
Internal type definitions for UF_SF_LEGEND (Scenario Legend) module.
The LEGEND module uses an attribute structure in order to define what
is displayed in the legend. The attribute structure should be built
by the application using the functions provided in the LEGEND API. The
functions assist in allocating and freeing the attribute structure and
in adding text strings in order to display. Assigning simple values to
the attribute structure is left to the application.
It is not necessary for applications to define each and every attribute
for the legend if the default is what is wanted. This is the reason for
attribute masks for each structure in the attribute structure.
Application code sets the desired attributes to define and then sets the
corresponding value in the attribute structure. For adding text strings,
convenience functions are provided.
The best way to learn how to use this API is some example code which is
provided below. The examples both show the use of the LEGEND API as
well as the CGP_PART API since the latter is an integral part of
display scalar fringes and such.
*******************************************************************************/
#ifndef UF_SF_LEGEND_H_INCLUDED
#define UF_SF_LEGEND_H_INCLUDED
#include <uf_defs.h>
#include <uf_sf_types.h>
#ifdef LEGEND_COMPILE_EXAMPLE_CODE
/************************************************************************
* Example - Generate a 3 color fringe legend using user defined *
* color index labeling. The labeling is wanted in the middle of the *
* discreate color index band instead of at the threshold point of each *
* color range. This index is for a safety factor so the color range *
* values are predefined. Negative values are used so that a top to *
* bottom "red", "yellow", "green" can be used with "red" values close *
* to zero. This is a cgp_part restriction. *
************************************************************************/
int num_colors = 3;
tag_t legend_view = NULL_TAG;
char displ_str[256];
char real_str[MAX_LINE_BUFSIZE];
char *displ_title_1 = "Structural";
char *displ_title_2 = "Performance";
char *safe_title = "Safety Factor =";
char *index_title_1 = "Safe";
char *index_title_2_1 = "Exceeds";
char *index_title_2_2 = "Safety";
char *index_title_2_3 = "Factor";
char *index_title_3 = "Failure";
double max_res, min_res;
UF_SF_COLOR_attr_t color_attr;
UF_SF_LEGEND_attr_p_t legend_attr_p = NULL;
UF_SF_LEGEND_title_p_t title_p;
/* Get extreme result values */
UF_SF_get_extreme_mesh_results (&max_res, &min_res);
/***************************************
* fill the color attribute structure *
***************************************/
color_attr.num_ranges = num_colors;
color_attr.ranges = UF_allocate_memory( sizeof(double) * (num_colors+1), &error) ;
if (error ) UF_get_fail_message(error, fail_message ) ;
color_attr.ranges[0] = -100.0;
color_attr.ranges[1] = -2.0;
color_attr.ranges[2] = -1.0;
color_attr.ranges[3] = 0.0;
color_attr.rgb_values = UF_allocate_memory( sizeof(double) * num_colors * 3, &error) ;
if (error ) UF_get_fail_message(error, fail_message ) ;
color_attr.rgb_values[0] = 0.0; /*green*/
color_attr.rgb_values[1] = 1.0;
color_attr.rgb_values[2] = 0.0;
color_attr.rgb_values[3] = 1.0; /*yellow*/
color_attr.rgb_values[4] = 1.0;
color_attr.rgb_values[5] = 0.0;
color_attr.rgb_values[6] = 1.0; /*red*/
color_attr.rgb_values[7] = 0.0;
color_attr.rgb_values[8] = 0.0;
/***************************************
* setup the color fringing attributes *
***************************************/
error = UF_SF_LEGEND_set_colors(&color_attr);
if (error) UF_get_fail_message(error, fail_message );
/*******************************
* setup the legend attributes *
*******************************/
UF_SF_LEGEND_new_attr(&legend_attr_p);
legend_attr_p->attr_mask = UF_LEGEND_WIDTH_ATTR | UF_LEGEND_HEADER_ATTR | UF_LEGEND_INDEX_ATTR;
legend_attr_p->width_percent = 15;
/* header */
UF_SF_LEGEND_add_title_line (&legend_attr_p->header, displ_title_1);
UF_SF_LEGEND_add_title_line (&legend_attr_p->header, displ_title_2);
UF_SF_LEGEND_add_title_line (&legend_attr_p->header," ");
UF_SF_LEGEND_add_title_line (&legend_attr_p->header, safe_title);
UF_SF_LEGEND_format_real_to_str (-min_res, real_str);
sprintf(displ_str, " %s+", real_str);
UF_SF_LEGEND_add_title_line (&legend_attr_p->header, displ_str);
/* overall index */
legend_attr_p->index_attr.attr_mask = UF_LEGEND_INDEX_HEIGHT_ATTR |
UF_LEGEND_INDEX_COLOR_ATTR |
UF_LEGEND_INDEX_TEXT_ATTR;
legend_attr_p->index_attr.height_percent = 60;
/* color index */
legend_attr_p->index_attr.color_attr.attr_mask = UF_LEGEND_INDEX_COLOR_WIDTH_ATTR |
UF_LEGEND_INDEX_COLOR_SMOOTH_ATTR;
legend_attr_p->index_attr.color_attr.width_percent = 30;
legend_attr_p->index_attr.color_attr.smooth_sw = FALSE;
legend_attr_p->index_attr.color_attr.num_values = num_colors;
legend_attr_p->index_attr.color_attr.values = color_attr.ranges;
/* text index */
legend_attr_p->index_attr.text_attr.attr_mask = UF_LEGEND_INDEX_TEXT_JUSTIFY_ATTR;
legend_attr_p->index_attr.text_attr.justify = UF_LEGEND_CENTER_JUSTIFIED_TEXT;
/* since the legend titles are wanted in the middle of the color index
there are 3 color indicies so specify 7 index titles with the
2nd, 4th and 6th titles with text */
UF_SF_LEGEND_add_index_text_title (legend_attr_p, &title_p); /*one*/
UF_SF_LEGEND_add_index_text_title (legend_attr_p, &title_p); /*two*/
UF_SF_LEGEND_add_title_line (title_p, index_title_1);
UF_SF_LEGEND_add_index_text_title (legend_attr_p, &title_p); /*three*/
UF_SF_LEGEND_add_index_text_title (legend_attr_p, &title_p); /*four*/
UF_SF_LEGEND_add_title_line (title_p, index_title_2_1);
UF_SF_LEGEND_add_title_line (title_p, index_title_2_2);
UF_SF_LEGEND_add_title_line (title_p, index_title_2_3);
UF_SF_LEGEND_add_index_text_title (legend_attr_p, &title_p); /*five*/
UF_SF_LEGEND_add_index_text_title (legend_attr_p, &title_p); /*six*/
UF_SF_LEGEND_add_title_line (title_p, index_title_3);
UF_SF_LEGEND_add_index_text_title (legend_attr_p, &title_p); /*seven*/
/* do the deed */
error = UF_SF_LEGEND_create_legend(legend_attr_p,&legend_view);
.
.
UF_SF_LEGEND_free_attr (legend_attr_p);
#endif /* LEGEND_COMPILE_EXAMPLE_CODE */
/***************************************************************************
UF_SF_LEGEND_REAL_STR_SZ is being deprecated. It was
used to define the string length of a character string in the
LEGEND_format_real_to_str function. Use MAX_LINE_BUFSIZE declared in
uf_defs.h instead
***************************************************************************/
/* */
#define UF_SF_LEGEND_REAL_STR_SZ (MAX_LINE_BUFSIZE-1)
/* */
/***************************************************************************
Text justification for titles in the user defined color index text.
***************************************************************************/
enum UF_SF_LEGEND_text_justification_e
{
UF_LEGEND_LEFT_JUSTIFIED_TEXT = 1,
UF_LEGEND_CENTER_JUSTIFIED_TEXT = 2,
UF_LEGEND_RIGHT_JUSTIFIED_TEXT = 3
};
typedef enum UF_SF_LEGEND_text_justification_e UF_SF_LEGEND_text_justification_t;
/***************************************************************************
Title structures are used for text so that multiple lines of text
can be defined for headers, footers, and user defined index text.
***************************************************************************/
struct UF_SF_LEGEND_title_s
{
int num_strs; /* Number of strings in the title */
char **strs; /*
Array of strings */
};
typedef struct UF_SF_LEGEND_title_s UF_SF_LEGEND_title_t, *UF_SF_LEGEND_title_p_t;
/***************************************************************************
The following are the definitions used to define user defined color
index text. The application can directly set the text justification
value but should use the functions: UF_SF_LEGEND_add_index_text_title,
UF_SF_LEGEND_add_title_line, in order to build the index text.
***************************************************************************/
#define UF_LEGEND_INDEX_TEXT_JUSTIFY_ATTR 0x0001
struct UF_SF_LEGEND_index_text_attr_s
{
unsigned int attr_mask; /* This field is set to one or more of the following
symbols OR'd together to indicate which of the
remaining fields of the structure are set.
UF_LEGEND_INDEX_TEXT_JUSTIFY_ATTR */
UF_SF_LEGEND_text_justification_t justify;
/* Justification of text in the legend
default: UF_LEGEND_RIGHT_JUSTIFIED_TEXT */
int num_titles;
/* Number of title structures */
UF_SF_LEGEND_title_p_t *titles;
/*
Pointer to instances of title structures */
};
typedef struct UF_SF_LEGEND_index_text_attr_s UF_SF_LEGEND_index_text_attr_t, *UF_SF_LEGEND_index_text_attr_p_t;
/***************************************************************************
The following are the definitions used to define the color index of
the legend. This is main part of most legend areas.
***************************************************************************/
#define UF_LEGEND_INDEX_COLOR_WIDTH_ATTR 0x0001
#define UF_LEGEND_INDEX_COLOR_SMOOTH_ATTR 0x0002
struct UF_SF_LEGEND_index_color_attr_s
{
unsigned int attr_mask; /* This field is set to one or more of the following
symbols OR'd together to indicate which of the
remaining fields of the structure are set.
UF_LEGEND_INDEX_COLOR_WIDTH_ATTR
UF_LEGEND_INDEX_COLOR_SMOOTH_ATTR */
int width_percent; /* The percentage of the legend area which the color
index fills. The index is always on the right side
default value: 30% */
logical smooth_sw; /* Switch indicating whether or not the color index
represents smooth continuous colors or
discrete color bands as follows:
= TRUE -> smooth color index (default)
= FALSE -> discrete color index. */
int num_values; /* Number of colors in index. Must be >= 2.
Mandatory if color index is specified */
double *values; /*
Array[num_values] in size. Scalar value associated
as the starting value of each color in the index.
Memory should not be freed until legend is deleted.
Mandatory if color index is specified. */
};
typedef struct UF_SF_LEGEND_index_color_attr_s UF_SF_LEGEND_index_color_attr_t, *UF_SF_LEGEND_index_color_attr_p_t;
/***************************************************************************
The following are the definitions used to define the overall
attributes of the index area.
***************************************************************************/
#define UF_LEGEND_INDEX_HEIGHT_ATTR 0x0001
#define UF_LEGEND_INDEX_COLOR_ATTR 0x0002
#define UF_LEGEND_INDEX_TEXT_ATTR 0x0004
struct UF_SF_LEGEND_index_attr_s
{
unsigned int attr_mask; /* This field is set to one or more of the following
symbols OR'd together to indicate which of the
remaining fields of the structure are set.
UF_LEGEND_INDEX_HEIGHT_ATTR
UF_LEGEND_INDEX_COLOR_ATTR
UF_LEGEND_INDEX_TEXT_ATTR */
int height_percent; /* The percentage of the legend area which the
index fills. The index is placed in the
middle of the legend unless there is a long
header in which case the index follows
directly after. default: 50% */
UF_SF_LEGEND_index_color_attr_t color_attr;
/* The attributes of the color index
default: none specified */
UF_SF_LEGEND_index_text_attr_t text_attr;
/* The attributes of the text index
If not specified, default labeling will be used
for the color index. default: none specified */
};
typedef struct UF_SF_LEGEND_index_attr_s UF_SF_LEGEND_index_attr_t, *UF_SF_LEGEND_index_attr_p_t;
/***************************************************************************
The following are the definitions used to define parameters of the
scalar-to-color mapping that is used in rendering fringe displays.
****************************************************************************/
struct UF_SF_COLOR_attr_s
{
int num_ranges; /* Number of of discrete ranges of scalar
values in the scalar-to-color mapping. */
double *ranges; /*
Array of size num_ranges defining
ranges of scalar values, each of which
maps to a different color.
It is an array of (num_ranges + 1) double
scalar values, where the minimum and
maximum scalar value for the ith range
are given by ranges[i] and
and ranges[i + 1], respectively.
The scalar ranges map to the colors in the
rgb_values field, if specified, or to linear
increments of the HSV blue-to-red model,
otherwise. */
double *rgb_values; /*
Array of RGB triples where each triple
consists of red, green, and blue
double-precision numbers.
Scalar values in the ith range map to the
ith RGB triple, given by:
{ rgb_values[(i], <-- RED
rgb_values[(i + 1], <-- GREEN
rgb_values[(i + 2] } <-- BLUE
The size of the array of triples is num_ranges*3 */
};
typedef struct UF_SF_COLOR_attr_s UF_SF_COLOR_attr_t, *UF_SF_COLOR_attr_p_t;
/***************************************************************************
The following are the definitions used to define the overall legend
attributes.
****************************************************************************/
#define UF_LEGEND_WIDTH_ATTR 0x0001
#define UF_LEGEND_BORDER_ATTR 0x0002
#define UF_LEGEND_FONT_SIZE_ATTR 0x0004
#define UF_LEGEND_HEADER_ATTR 0x0008
#define UF_LEGEND_INDEX_ATTR 0x0010
#define UF_LEGEND_FOOTER_ATTR 0x0020
struct UF_SF_LEGEND_attr_s
{
unsigned int attr_mask; /* This field is set to one or more of the following
symbols OR'd together to indicate which of the
remaining fields of the structure are set.
UF_LEGEND_WIDTH_ATTR
UF_LEGEND_BORDER_ATTR
UF_LEGEND_FONT_SIZE_ATTR
UF_LEGEND_HEADER_ATTR
UF_LEGEND_INDEX_ATTR
UF_LEGEND_FOOTER_ATTR */
int width_percent; /* The percentage of the display which the
legend occupies. The legend takes up the full
height of the display. default: 20% */
logical border_sw; /* Switch indicating whether or not the border
of the legend gets displayed.
= TRUE -> display border
= FALSE -> do not display border. (default) */
double font_size; /* The size in inches of an individual character.
If not specified, the font is automatically
calculated so that 15 characters can be
displayed in the full width of the legend.
The auto size also is constrained by a maximum
size of .12" and a minimum size of .04".
default: automatic */
int font_color; /* font color */
UF_SF_LEGEND_title_t header;
/* The header text of the legend area
default: none defined. */
UF_SF_LEGEND_index_attr_t index_attr;
/* The index area's attributes if defined.
default: none defined. */
UF_SF_LEGEND_title_t footer;
/* The footer text of the legend area
default: none defined. */
int layout_type; /* IViewManager::LayoutType */
int view_port_id; /* viewport */
};
typedef struct UF_SF_LEGEND_attr_s UF_SF_LEGEND_attr_t, *UF_SF_LEGEND_attr_p_t;
#endif /* UF_SF_LEGEND_H_INCLUDED */