/*
uf_part_types.h
File Description:
Open C API typedefs and defines for the UF_PART module
***************************************************************************/
#ifndef UF_PART_TYPES_INCLUDED
#define UF_PART_TYPES_INCLUDED
/***************************************************************************
***************************************************************************/
#include <uf_defs.h>
/*
* UF_PART error and warning codes.
*/
#define ERROR_PART_base 640000
#define UF_PART_ERROR_BASE (ERROR_PART_base)
#define UF_PART_warn_objects_not_copied (UF_PART_ERROR_BASE + 1075)
#define UF_PART_err_read_only_modified (UF_PART_ERROR_BASE + 1058)
/*
* Data structure to return the part names and statuses of all parts retrieved
* into the session by either
* UF_PART_open or
* UF_ASSEM_add_part_to_assembly
*
* Starting NX3: The utility routine UF_PART_free_load_status has been provided
* to free the allocated memory below. This may be used as an alternative to
* calling UF_free_string_array and UF_free directly.
*/
struct UF_PART_load_status_s
{ logical failed; /* Output: True if the load failed and was
rolled back
*/
logical user_abort; /* Output: True if the only 'failure' was user abort
*/
int n_parts; /* Output: Length of the following two
allocated arrays. Number of parts that had
errors or warnings when loading. This is the
number (dimension) of entries in the file_names
and statuses arrays.
*/
char **file_names; /* <OF>
Allocated array of file names
*/
int *statuses; /* <OF>
Allocated array of associated status codes
for each file name. Use UF_get_fail_message
on each status code in the array to get
the associated message string.
The allocated array must be freed.
*/
};
typedef struct UF_PART_load_status_s UF_PART_load_status_t,
*UF_PART_load_status_p_t;
/*
* Data structure and constants used in part import
* History:
* NX2: plist_mode is no longer used.
*/
struct UF_import_part_modes_s
{
int layer_mode; /* 0 = Merge on work layer
1 = Merge on original layers
*/
int group_mode; /* 0 = Merge ungrouped
1 = Merge grouped
*/
int csys_mode; /* Not used by Open API applications */
int plist_mode; /* NOTE: plist_mode is no longer used */
int view_mode; /* 0 = do not retrieve views and layouts.
1 = retrieve views and layouts.
*/
logical cam_mode; /* If true, merge in tools and parameter
sets, if false do not.
*/
logical use_search_dirs; /* This is not used by Open API applications. */
};
typedef struct UF_import_part_modes_s UF_import_part_modes_t,
*UF_import_part_modes_p_t;
/*
* Data structure used by the part history routines
*/
typedef struct UF_PART_history_list_s *UF_PART_history_list_p_t;
#define IP_WORK 0
#define IP_ORIG 1
#define IP_NOGROUP 0
#define IP_GROUP 1
#define IP_USE_WCS 0
#define IP_CSYS_MENU 1
#define IP_NONE 0
#define IP_FORMAT 1
#define IP_ADD_TO 2
#define IP_ALL 3
#define IP_NO_VIEW 0
#define IP_VIEW 1
#define UF_PART_METRIC 1
#define UF_PART_ENGLISH 2
#define UF_PART_CDP_BEGIN_TEXT 0
#define UF_PART_CDP_END_TEXT 1
#define UF_PART_CDP_CONTAIN_TEXT 2
#define UF_PART_CDP_EXACT_TEXT 3
/*****************************************************************************
*
* Type which describes how solid parameters should be processed during
* an export operation,
* NOTE: UF_PART_maintain_all_params is a newly introduced option in V15.0.
*
* The behaviours of UF_PART_maintain_params and UF_PART_remove_params
* are the same in V15.0 as in earlier releases.
*
******************************************************************************/
enum UF_PART_export_params_mode_e
{
UF_PART_maintain_params, /* Solid parameters should be maintained
during the export operation. Note that
with this option, solid parameters will
NOT be copied if they depend upon other
objects for their validity unless those
other objects are going to be copied
anyway.
*/
UF_PART_remove_params, /* Solid parameters will be removed during
the export operation. Solids copied
into the destination part will have no
solid parameters.
*/
UF_PART_maintain_all_params /* All solid parameters should be
maintained during the export
operation. All solid parameters in
the source objects will be copied into
the destination objects. Note that
extra objects which are required to
maintain the validity of the
parameters will be copied too.
*/
};
typedef enum UF_PART_export_params_mode_e UF_PART_export_params_mode_t,
*UF_PART_export_params_mode_p_t;
/*****************************************************************************
*
* Type which describes how expressions should be processed during an
* export operation:
******************************************************************************/
enum UF_PART_export_exp_mode_e
{
UF_PART_copy_exp_deeply, /*Expressions will be copied deeply.
If an expression references another
expression in the same part, then
that referenced expression will also
be copied. (However any referenced
expressions in a different part will
not be copied.)
*/
UF_PART_copy_exp_shallowly /*Expressions will be copied shallowly.
If an expression references another
expression, the copy of the
referencing expression will reference
the same referenced expression. This
happens for both inter-part and
intra-part references to expressions.
*/
} ;
typedef enum UF_PART_export_exp_mode_e UF_PART_export_exp_mode_t,
*UF_PART_export_exp_mode_p_t;
/*****************************************************************************
*
* Type which describes the options provided to an export operation.
******************************************************************************/
struct UF_PART_export_options_s
{
logical new_part; /* Determines whether the objects should be exported
into a new part.
*/
UF_PART_export_params_mode_t params_mode; /* Determines how solid
parameters will be copied.
*/
UF_PART_export_exp_mode_t expression_mode; /* Determines how expressions
will be copied.
*/
};
typedef struct UF_PART_export_options_s UF_PART_export_options_t,
*UF_PART_export_options_p_t;
/*****************************************************************************
*
* Type which describes the compression options available
******************************************************************************/
struct UF_PART_compress_flags_s
{
logical standard; /* Specifies the standard compression option state
*/
};
typedef struct UF_PART_compress_flags_s UF_PART_compress_flags_t,
*UF_PART_compress_flags_p_t;
/*
Search types for UF_PART_cdp_params_t
*/
#define UF_PART_CDP_BEGIN_TEXT 0
#define UF_PART_CDP_END_TEXT 1
#define UF_PART_CDP_CONTAIN_TEXT 2
#define UF_PART_CDP_EXACT_TEXT 3
#define UF_PART_cleanup_highlight (1U << 0)
#define UF_PART_cleanup_all_groups (1U << 1)
#define UF_PART_cleanup_unnamed_groups (1U << 2)
#define UF_PART_cleanup_unreferenced (1U << 3)
#define UF_PART_cleanup_feature (1U << 4)
#define UF_PART_cleanup_parts_all (1U << 5)
#define UF_PART_cleanup_parts_components (1U << 6)
#define UF_PART_cleanup_spreadsheet (1U << 7)
#define UF_PART_cleanup_mating (1U << 8) /* Note: This operation may load parts */
#define UF_PART_cleanup_CAM_cleanup (1U << 9)
#define UF_PART_cleanup_fonts (1U << 10)
#define UF_PART_cleanup_unreferenced_exps (1U << 11)
#define UF_PART_cleanup_occurrences (1U << 12)
#define UF_PART_cleanup_visual_editor (1U << 13)
#define UF_PART_cleanup_hwo_force_demoting (1U << 14) /* Beware that if both UF_PART_cleanup_hwo_force_demoting *
* and UF_PART_cleanup_occurrences are specified, then *
* UF_PART_cleanup_occurrences takes precedence. */
#define UF_PART_cleanup_drafting (1U << 15)
#define UF_PART_cleanup_sketch (1U << 16)
#define UF_PART_cleanup_delete_broken_interpart (1U << 17)
#define UF_PART_cleanup_delete_all_materials (1U << 18)
#define UF_PART_cleanup_assembly_constraints (1U << 19)
#define UF_PART_cleanup_delete_duplicate_lights (1U << 20)
#define UF_PART_cleanup_routing (1U << 21)
#define UF_PART_cleanup_delete_invalid_attributes (1U << 22)
#define UF_PART_cleanup_unused_extract_refs (1U << 23)
#define UF_PART_cleanup_units (1U << 24)
#define UF_PART_cleanup_motion (1U << 25)
#define UF_PART_cleanup_part_family_data (1U << 26)
#define UF_PART_cleanup_all ((~0U) & (~UF_PART_cleanup_sketch))
#endif /* UF_PART_TYPES_INCLUDED */