/*
uf_oper.h
File description:
This module allows the user to perform functions which are particular to
Operations as compared to the functions which can be performed on Operations
when an Operation is viewed as a UF_PARAM object (which it is). See the
prototypes in this file for examples of what these functions are.
UF_OPER items are found in templates. In particular, they are found in
Groups contained inside of a Setup. They are typically accessed via their
template or as a member of a Group.
*******************************************************************************/
#ifndef UF_OPER_H_INCLUDED
#define UF_OPER_H_INCLUDED
/***************************** Include Files **********************************/
#include <uf_defs.h>
#include <uf_oper_spec.h>
#include <uf_cam_errors.h>
#include <libufun_cam_exports.h>
#include <uf_cutter.h>
/******************************** Defines *************************************/
/*
UF_OPER_MAX_NAME_LEN is being deprecated because NX is moving to support
multibyte characters. User written programs should start using the
new definitions:
UF_OPER_MAX_NAME_BUFSIZE should be used for buffer allocations and memory
allocations, e.g. char my_fspec[UF_OPER_MAX_NAME_BUFSIZE];
UF_OPER_MAX_NAME_NCHARS should be used to limit the number of characters in
a buffer. NX code will enforce these limits.
New routines have been added which will help in this transition:
UF_TEXT_count_characters() will count the number of characters in a
buffer.
UF_TEXT_terminate_chars() will terminate a C string after the given
number of characters.
*/
#define UF_OPER_MAX_NAME_NCHARS UF_OPER_OPNAME_NCHARS
#define UF_OPER_MAX_NAME_BUFSIZE NX_BUFSIZE(UF_OPER_MAX_NAME_NCHARS)
/* */
#define UF_OPER_MAX_NAME_LEN (UF_OPER_MAX_NAME_BUFSIZE-1)
/* */
/***************************** Public Typedefs ********************************/
/* Operation Status: for all bit fields if the bit == 0 then the condition
* represented by that bit is FALSE, otherwise it is TRUE
*/
struct UF_OPER_status_s
{
unsigned int is_edited :1; /* Has operation been edited ? */
unsigned int toolpath_exists :1; /* Does tool path exist ? */
unsigned int toolpath_edited :1; /* Has tool path been edited since
* the last time it was posted ?
*/
unsigned int open :29;
};
typedef struct UF_OPER_status_s UF_OPER_status_t, *UF_OPER_status_p_t;
/*
Operation Status: for all structure fields if it is == 0 then the condition
* represented by that field is FALSE, otherwise it is TRUE
*/
struct UF_OPER_status1_s
{
unsigned int is_edited; /* Has operation been edited ? */
unsigned int toolpath_exists; /* Does tool path exist ? */
unsigned int toolpath_edited ; /* Has tool path been edited since
* the last time it was posted ?
*/
};
typedef struct UF_OPER_status1_s UF_OPER_status1_t, *UF_OPER_status1_p_t;
/*
*/
/* Machining Modes */
enum UF_OPER_mach_mode_e
{
UF_OPER_MACH_MODE_UNDEF, /* Undefined */
UF_OPER_MACH_MODE_MILL,
UF_OPER_MACH_MODE_LATHE,
UF_OPER_MACH_MODE_DRILL,
UF_OPER_MACH_MODE_WEDM,
UF_OPER_MACH_MODE_TURN,
UF_OPER_MACH_MODE_LAST /*** This must be the last item ***/
};
typedef enum UF_OPER_mach_mode_e UF_OPER_mach_mode_t;
/************************* Public Function Definitions ************************/
/*******************************************************************************
This function returns in 'group' the tag of the program group object that the
specified 'oper' is contained in.
Environment: Internal and External
See Also:
History: Originally released in V16.0
*******************************************************************************/
extern UFUN_CAMEXPORT int UF_OPER_ask_program_group
(
tag_t oper, /* <I> - see above */
tag_t *group /* <O> - see above */
);
/*******************************************************************************
This function returns in 'group' the tag of the method group object that the
specified 'oper' is contained in.
Environment: Internal and External
See Also:
History: Originally released in V16.0
*******************************************************************************/
extern UFUN_CAMEXPORT int UF_OPER_ask_method_group
(
tag_t oper, /* <I> - see above */
tag_t *group /* <O> - see above */
);
/*******************************************************************************
This function returns in 'group' the tag of the geometry group object that the
specified 'oper' is contained in.
Environment: Internal and External
See Also:
History: Originally released in V16.0
*******************************************************************************/
extern UFUN_CAMEXPORT int UF_OPER_ask_geom_group
(
tag_t oper, /* <I> - see above */
tag_t *group /* <O> - see above */
);
/*******************************************************************************
This function returns in 'group' the tag of the cutter group object that the
specified 'oper' is contained in.
Environment: Internal and External
See Also:
History: Originally released in V16.0
*******************************************************************************/
extern UFUN_CAMEXPORT int UF_OPER_ask_cutter_group
(
tag_t oper, /* <I> - see above */
tag_t *group /* <O> - see above */
);
/*******************************************************************************
This function returns in 'status' the status of the specified Operation 'oper'.
See the definition of UF_OPER_status_t in this file for a description of the
status.
Environment: Internal and External
See Also:
History: Originally released in V16.0
*******************************************************************************/
extern UFUN_CAMEXPORT int UF_OPER_ask_status
(
tag_t oper, /* <I> - see above */
UF_OPER_status_t *status /* <O> - see above */
);/**/
/*******************************************************************************
In order to provide appropriate .NET binding for UF_OPER_ask_status,
UF_OPER_ask_status1 is introduced.
Note: C/C++ users can continue to use UF_OPER_ask_status.
For documentation, refer to documentation of UF_OPER_ask_status.
Environment: Internal and External
See Also:
History: Originally released in NX10.0
*******************************************************************************/
extern UFUN_CAMEXPORT int UF_OPER_ask_status1
(
tag_t oper, /* <I> - tag of the Operation */
UF_OPER_status1_t *status /* <O> - status of specified operation */
);
/*******************************************************************************
This function returns the NX entity subtype (as found in uf_object_types.h)
of the specified 'oper'. It is returned in 'type'.
Environment: Internal and External
See Also:
History: Originally released in V16.0
*******************************************************************************/
extern UFUN_CAMEXPORT int UF_OPER_ask_oper_type
(
tag_t oper, /* <I> - see above */
int *type /* <O> - see above */
);
/*******************************************************************************
This function returns in 'mode' the machining mode of the specified 'oper'.
Environment: Internal and External
See Also:
History: Originally released in V16.0
*******************************************************************************/
extern UFUN_CAMEXPORT int UF_OPER_ask_machining_mode
(
tag_t oper, /* <I> - see above */
UF_OPER_mach_mode_t *mode /* <O> - see above */
);
/*******************************************************************************
This function determines if the tool path in the specified 'oper' gouges
any geometry in the operation.
Environment: Internal and External
See Also:
History: Originally released in V16.0
*******************************************************************************/
extern UFUN_CAMEXPORT int UF_OPER_is_path_gouged
(
tag_t oper, /* <I> - see above */
logical *result /* <O> - TRUE if the if the tool path gouges any geometry.
FALSE otherwise. */
);
/*******************************************************************************
This function returns in 'name' the name of the specified 'oper'.
Environment: Internal and External
See Also:
History: Originally released in V16.0
*******************************************************************************/
extern UFUN_CAMEXPORT int UF_OPER_ask_name_from_tag
(
tag_t oper, /* <I> - see above */
char name[UF_OPER_MAX_NAME_BUFSIZE+1] /* <O> - see above */
);
/******************************************************************************
Does the operation have an In-Process-Workpiece or not.
Environment: Internal and External
See Also:
History: Originally released in V16.0
*******************************************************************************/
extern UFUN_CAMEXPORT int UF_OPER_has_self_ipw
(
tag_t oper, /* <I> The tag of the operation to be checked. */
logical *result /* <O> The result, TRUE if the operation has an
in-process-workpiece, FALSE otherwise.
*/
);
/*******************************************************************************
This function deletes the internal path associated with the specified 'oper'.
Environment: Internal and External
See Also:
History: Originally released in V16.0
*******************************************************************************/
extern UFUN_CAMEXPORT int UF_OPER_delete_tool_path
(
tag_t oper /* <I> - see above */
);
/*******************************************************************************
This function creates an operation based upon the specified operation template
type and subtype. All parameters of the newly created operation are derived
from the specified template object.
Environment: Internal and External
See Also:
History: Originally released in V16.0
*******************************************************************************/
extern UFUN_CAMEXPORT int UF_OPER_create
(
char *type_name, /* <I> - the operation template type name */
char *subtype_name, /* <I> - the operation template subtype name */
tag_t *new_object /* <O> - the tag of the newly created operation */
);
/***************************************************************
* Query the number of selected tracking points in an Operation.
*
* Return :
* UF_CUTTER_ERROR_TAG_NOT_CORRECT_TYPE
* The input tag is not an operation
*
* Environment: Internal and External
*
* See Also:
* History: Released in NX2.0
*************************************************************/
extern UFUN_CAMEXPORT int UF_OPER_ask_selected_tracking_point_count
(
tag_t object_tag, /* <I> the tag of the operation of the points */
int *count /* <O> the number of selected tracking points */
);
/***************************************************************
* Select a tracking point in an Operation
*.
* Note:
* Specifying a tracking point for an operation will result in setting the Z-offset,
* Adjust and Cutcom data for the operation from that of the selected tracking
* point. If a local override for this data is desired, it must be specified after
* selecting the tracking point.
*
* Return :
* UF_CUTTER_ERROR_TAG_NOT_CORRECT_TYPE
* The input tag is not an operation
*
* Environment: Internal and External
*
* See Also:
* History: Released in NX2.0
*************************************************************/
extern UFUN_CAMEXPORT int UF_OPER_select_tracking_point
(
tag_t object_tag, /* <I> the tag of the operation */
char name[] /* <I> the name of the selected tracking point */
);
/***************************************************************
* Deselect a tracking point in an Operation.
*
* Return :
* UF_CUTTER_ERROR_TAG_NOT_CORRECT_TYPE
* The input tag is not an operation
*
* Environment: Internal and External
*
* See Also:
* History: Released in NX2.0
*************************************************************/
extern UFUN_CAMEXPORT int UF_OPER_deselect_tracking_point
(
tag_t object_tag, /* <I> the tag of the operation */
char name[] /* <I> the name of the tracking point to deselect */
);
/***************************************************************
* Query the data of a selected tracking point in an Operation.
*
* Return :
* UF_CUTTER_ERROR_TAG_NOT_CORRECT_TYPE
* The input tag is not an operation
*
* Environment: Internal and External
*
* See Also:
* History: Released in NX2.0
**************************************************************/
extern UFUN_CAMEXPORT int UF_OPER_ask_selected_point_data
(
tag_t object_tag, /* <I> the tag of the operation of the points */
int index, /* <I> index of tracking point in parent (from 0 to the
number of selected points - 1) */
UF_CUTTER_tracking_point_data_t *data /* <O> the data of the point */
);
/***************************************************************
* Query the data of a selected turn tracking point in an Operation.
*
* Return :
* UF_CUTTER_ERROR_TAG_NOT_CORRECT_TYPE
* The input tag is not an operation
*
* Environment: Internal and External
*
* See Also:
* History: Released in NX5.0
**************************************************************/
extern UFUN_CAMEXPORT int UF_OPER_ask_selected_turn_point_data
(
tag_t object_tag, /* <I> the tag of the operation of the points */
int index, /* <I> index of turn tracking point in parent (from 0 to the
number of selected points - 1) */
UF_CUTTER_turn_tracking_point_data_t *data /* <O> the data of the point */
);
/******************************************************************
*
* This function queries the reference cutter of an operation.
*
* Return :
* Return code :
* = 0 : sucessful
* > 0 : failing error number
* < 0 : failing error number
*
* Environment: Internal and External
*
* See Also: UF_OPER_set_ref_cutter
*
* History: Released in NX 2.0
******************************************************************/
extern UFUN_CAMEXPORT int UF_OPER_ask_ref_cutter
(
tag_t oper_tag, /* <I> the operation tag */
tag_t *ref_cutter_tag /*<O>the tag of the reference cutter of the operation*/
);
/******************************************************************
*
* This function set the reference cutter for an operation. Currently,
* only Cavity and Zlevel operations are allowed to set reference cutter.
*
* Return :
* Return code :
* = 0 : sucessful
* > 0 : failing error number
* < 0 : failing error number
*
* Environment: Internal and External
*
* See Also: UF_OPER_ask_ref_cutter
*
* History: Released in NX 2.0
******************************************************************/
extern UFUN_CAMEXPORT int UF_OPER_set_ref_cutter
(
tag_t oper_tag, /* <I> the operation tag */
tag_t ref_cutter_tag /*<I>the tag of a reference cutter to the operation*/
);
/***************************************************************
* Set the Machining Data parameters in an operation.
*
* Return :
* UF_CAM_ERROR_TAG_NOT_CORRECT_TYPE
* The input tag is not an operation
*
* UF_OPER_ERROR_QUERY_FAILED
* No match in the Machining Data library was found for the Cut Method,
* Part Material and Tool Material defined for this operation.
*
* UF_CAM_ERROR_INSUFFICIENT_DATA
* At least one of the following is not defined for the operation:
* Cut Method, Part Material or Tool Material.
*
* Environment: Internal and External
*
* See Also:
* History: Released in NX3.0
*************************************************************/
extern UFUN_CAMEXPORT int UF_OPER_set_machining_data
(
tag_t oper_tag /* <I> tag of the operation */
);
/***************************************************************
* Reset the Feeds and Speeds data in an operation.
*
* Return :
* UF_CAM_ERROR_TAG_NOT_CORRECT_TYPE
* The input tag is not an operation
*
* UF_OPER_ERROR_QUERY_FAILED
* No match in the Machining Data library was found for the Cut Method,
* Part Material and Tool Material defined for this operation.
*
* UF_CAM_ERROR_INSUFFICIENT_DATA
* At least one of the following is not defined for the operation:
* Cut Method, Part Material or Tool Material.
*
* Environment: Internal and External
*
* See Also:
* History: Released in NX3.0.3
*************************************************************/
extern UFUN_CAMEXPORT int UF_OPER_reset_from_table
(
tag_t oper_tag /* <I> tag of the operation */
);
/***************************************************************
* Unload Tool Path of an Operation.
*
* Return :
* UF_CAM_ERROR_TAG_NOT_CORRECT_TYPE
* The input tag is not an operation
*
* Environment: Internal and External
*
* See Also:
* History: Released in NX5.0.2
*************************************************************/
extern UFUN_CAMEXPORT int UF_OPER_unload_path
(
tag_t oper_tag /* <I> tag of the operation */
);
#undef EXPORTLIBRARY
#endif /* UF_OPER_H_INCLUDED */