/*
uf_motion_ugopenint.h
File description:
Open C API motion interface
*****************************************************************************/
#ifndef UF_MOTION_UGOPENINT_H_INCLUDED
#define UF_MOTION_UGOPENINT_H_INCLUDED
/*****************************************************************************
******************************************************************************/
#include <uf_defs.h>
#include <libugopenint_cae_exports.h>
/*****************************************************************************
This function runs animation using the motion data in the specified
spreadsheet. Last argument decides whether the animation will be run
interactively by bringing up the user interface or not.
Environment: Internal and External
See Also: UF_MOTION_spreadsheet_run_from_file
History: Released in NX3
******************************************************************************/
extern UGOPENINT_CAEEXPORT int UF_MOTION_spreadsheet_run_from_file
(
const char * spreadsheet_file, /* <I> Full path and name of spreadsheet file
containing motion data */
int start_step, /* <I> Step number in spreadsheet to start
animation at */
int end_step, /* <I> Step number in spreasheet till which to
animate */
logical invoke_ui /* <I> TRUE if spreadsheet run should be
interactive FALSE if animation should be
run without the user interface */
);
/*****************************************************************************
This function runs the articulation solve in interactive mode using the existing user interface.
Environment: Internal and External
See Also: UF_MOTION_animation_run
History: Released in NX801
******************************************************************************/
extern UGOPENINT_CAEEXPORT int UF_MOTION_articulation_run
(
void
);
/*****************************************************************************
This function runs animation in interactive mode using the existing user interface.
Environment: Internal and External
See Also: UF_MOTION_articulation_run
History: Released in NX801
******************************************************************************/
extern UGOPENINT_CAEEXPORT int UF_MOTION_animation_run
(
void
);
#undef EXPORTLIBRARY
#endif /* UF_MOTION_UGOPENINT_H_INCLUDED */