/*
uf_modl_legacy.h
File description:
These routines are the Modeling legacy routines. These routines are in
the process of being replaced with other modeling functionality.
Work Part Restrictions
For those functions/subroutines that perform an operation on an
object, the object must not be an occurrence and the object must be in
the same part as the work part. If either one of these requirements are
not met, then a NULL_TAG is returned for the object on which the
operation is performed. These restrictions apply to the following older
solids routines:
UF6506
UF6507
UF6508
UF6511
UF6523
UF6524
UF6525
UF6526
UF6527
NOTE
UF6560 does NOT return an error message in this case.
*****************************************************************************/
#ifndef UF_MODL_LEGACY_H_INCLUDED
#define UF_MODL_LEGACY_H_INCLUDED
/***************************************************************************
***************************************************************************/
#include <uf_defs.h>
#include <uf_modl_types.h>
#include <libufun_exports.h>
/* uf5300 create cylinder */
extern UFUNEXPORT void uf5300(double *ra1, double *ra2, double *rp3,
int *ip4, tag_t *nr5);
/* uf5301 read cylinder data */
extern UFUNEXPORT void uf5301(tag_t *np1, double *rar2, double *rar3,
double *rr4);
/* uf5303 read cylinder endpoint and vector */
extern UFUNEXPORT void uf5303(tag_t *np1, double *rar2, double *rar3);
/* uf5305 read cylinder radius */
extern UFUNEXPORT void uf5305(tag_t *np1, double *rr2);
/* uf5309 read cylinder real data */
extern UFUNEXPORT void uf5309(tag_t *np1, double *rar2);
/* uf5310 create cone */
extern UFUNEXPORT void uf5310(double *rp1, double *rp2,
double *ra3, double *ra4, double *rp5,
int *ip6, tag_t *nr7);
/* uf5311 read cone data */
extern UFUNEXPORT void uf5311(tag_t *np1, double *rr2, double *rr3,
double *rar4, double *rar5);
/* uf5313 read cone axis vector */
extern UFUNEXPORT void uf5313(tag_t *np1, double *rar2);
/* uf5315 read cone vertex coordinate */
extern UFUNEXPORT void uf5315(tag_t *np1, double *rar2);
/* uf5317 read cone angle */
extern UFUNEXPORT void uf5317(tag_t *np1, double *rr2);
/* uf5319 read cone real data */
extern UFUNEXPORT void uf5319(tag_t *np1, double *rar2);
/* uf5320 create sphere */
extern UFUNEXPORT void uf5320(double *ra1, double *rp2,
int *ip3, tag_t *nr4);
/* uf5321 read sphere data */
extern UFUNEXPORT void uf5321(tag_t *np1, double *rar2, double *rr3);
/* uf5323 read sphere axis vector */
extern UFUNEXPORT void uf5323(tag_t *np1, double *rar2);
/* uf5325 read sphere center */
extern UFUNEXPORT void uf5325(tag_t *np1, double *rar2);
/* uf5327 read sphere radius */
extern UFUNEXPORT void uf5327(tag_t *np1, double *rr2);
/* uf5329 read sphere real data */
extern UFUNEXPORT void uf5329(tag_t *np1, double *rar2);
/* uf5374 create plane
Replaced by UF_MODL_create_plane */
extern UFUNEXPORT void uf5374(double *rp1, double *rp2,
double *rp3, tag_t *nr4);
/* uf5375 read plane data
Replaced by UF_MODL_ask_plane */
extern UFUNEXPORT void uf5375(tag_t *np1, double *rr2, double *rr3);
/* uf5376 edit plane data
Replaced by UF_MODL_edit_plane */
extern UFUNEXPORT void uf5376(tag_t *np1, double *rp2, double *rp3);
/** Face Modeling **/
/* uf5400 read face grid counts
Replaced by UF_MODL_ask_face_grid_count */
extern UFUNEXPORT void uf5400(tag_t *np1, int *iar2);
/* uf5401 edit face grid counts
Replaced by UF_MODL_edit_face_grid_count */
extern UFUNEXPORT void uf5401(tag_t *np1, int *ia2);
/* uf5404 read face u-v minimum/maximum -- replaced by UF_MODL_ask_face_uv_minma
x */
extern UFUNEXPORT void uf5404(tag_t *np1, double *rar2);
/* uf5406 read face normal direction */
extern UFUNEXPORT void uf5406(tag_t *np1, int *ir2);
/* uf5407 edit face normal direction */
extern UFUNEXPORT void uf5407(tag_t *np1, int *ip2);
/* uf5408 read face generating curve */
extern UFUNEXPORT void uf5408(tag_t *np1, int *ip2, tag_t *nr3);
/* uf5409 trim sheet by loops */
extern UFUNEXPORT void uf5409(tag_t *np1, double *rp2, int *ip3,
int *ip4, int *ip5, int *ip6,
tag_t *np7, int *ip8, int *ir9);
/* uf5410 remove face trim */
extern UFUNEXPORT void uf5410(tag_t *np1, int *ir9);
/* uf5411 read face trim status */
extern UFUNEXPORT int uf5411(tag_t *np1);
/* uf5412 trim face by curves and points */
extern UFUNEXPORT void uf5412(tag_t *np1, double *rp2, int *ip3,
int *ip4, tag_t *np5, int *ip6,
int *ip7, double *rp8, int *ir9);
/** Freeform Modeling **/
/* uf5330 create body of revolution */
extern UFUNEXPORT void uf5330(tag_t *np1, double *ra2, double *ra3,
double *ra4, tag_t *nr5);
/* uf5331 read body of revolution axis vector */
extern UFUNEXPORT void uf5331(tag_t *np1, double *rar2);
/* uf5333 read body of revolution point on axis */
extern UFUNEXPORT void uf5333(tag_t *np1, double *rar2);
/* uf5339 read body of revolution real data */
extern UFUNEXPORT void uf5339(tag_t *np1, double *rar2);
/* uf5340 create tabulated cylinder */
extern UFUNEXPORT void uf5340(tag_t *np1, double *ra2, double *ra3,
tag_t *nr4);
/* uf5341 read tabulated cylinder axis vector */
extern UFUNEXPORT void uf5341(tag_t *np1, double *rar2);
/* uf5349 read tabulated cylinder real data */
extern UFUNEXPORT void uf5349(tag_t *np1, double *rar2);
/* uf5350 create ruled sheet */
extern UFUNEXPORT void uf5350(tag_t *np1, tag_t *np2,
int *ip3, tag_t *nr4);
/* uf5360 create bounded plane */
extern UFUNEXPORT void uf5360(int *ip1, int ip2[], tag_t np3[],
double *rp4, tag_t *nr5, int *ir6);
/* uf5363 read face anchor counts */
extern UFUNEXPORT void uf5363(tag_t *np1, int *ir2,
int *ir3, int *ir4);
/* uf5364 read face anchor object */
extern UFUNEXPORT void uf5364(tag_t *np1, int *ip2,
tag_t *nr3, int *ir4);
/* uf5368 read face edge curve data */
extern UFUNEXPORT void uf5368(tag_t *np1, int *ip2,
int *ip3, tag_t *nr4, double *rr5,
int *ir6, int *ir7);
/* uf5380 create curve mesh sheet */
extern UFUNEXPORT void uf5380(tag_t *na1, tag_t *na2,
int *ip3, int *ip4,
tag_t *nr5);
/* uf5381 read curve mesh sheet primary and */
extern UFUNEXPORT void uf5381(tag_t *np1, int *ir2, int *ir3);
/* uf5382 read curve mesh sheet primary curve */
extern UFUNEXPORT void uf5382(tag_t *np1, int *ip2, tag_t *nr3);
/* uf5384 read curve mesh sheet cross curve */
extern UFUNEXPORT void uf5384(tag_t *np1, int *ip2, tag_t *nr3);
/* uf5405 create bounding box for a face */
extern UFUNEXPORT void uf5405(tag_t *np1, double *rr2, int *ir3);
/* uf5440 create b-surface sheet */
extern UFUNEXPORT void uf5440(int *ip1, int *ip2, int *ip3,
int *ip4, int *ip5, int *ip6,
int *ip7, double *rp8, int *ip9,
double *rp10, double *rp11, double *rp12,
double *rp13, tag_t *nr14);
/* uf5441 read b-surface sheet data
Replaced by UF_MODL_ask_bsurf */
extern UFUNEXPORT void uf5441(tag_t *np1, int *ir2, int *ir3,
int *ir4, int *ir5, int *ir6,
int *ir7, int *ir8, double *rr9,
int *ir10, double *rr11, double *rr12,
double *rr13, double *rr14);
/* uf5442 create b-surface sheet from body of */
extern UFUNEXPORT void uf5442(tag_t *np1, double *rp2, double *rp3,
double *rp4, tag_t *nr5);
/* uf5443 create b-surface sheet from list of curves */
extern UFUNEXPORT void uf5443(int *ip1, tag_t *np2,
int *ip3, int *ip4,
int *ip5, tag_t *nr6);
/* uf5444 approximate a face with a b-surface */
extern UFUNEXPORT void uf5444(tag_t *np1, double *rp2, double *rp3,
tag_t *nr4, int *ir5);
/* uf5448 create b-surface sheet from
Replaced by UF_MODL_create_bsurf_thru_pts */
extern UFUNEXPORT void uf5448(int *ip1, int *ip2,
int *ip3, int *ip4,
int *ip5, int *ip6,
int *ip7, double *rp8,
double *rp9, tag_t *nr10,
int *ir11);
/* uf5449 create free form feature by cubic fit from */
extern UFUNEXPORT void uf5449(int *ip1, tag_t *np2, int *ip3,
int *ip4, double *rp5, tag_t *np6,
int *ip7, int *ip8, int *ip9,
double *rp10, tag_t *nr11, int *ir12);
/* uf5450 create offset face.
Edge curve tolerance controls how accurately the edge curves lie on
the face. The tolerance value cannot be less than .0001 inches or
.00254 mm. The offset distance (RP2) must be nonzero.
Geometry edits made to a base face are reflected in the associated
offsets. Therefore, be extremely careful when modifying base faces.
If an error occurs, NR5 = NULL. Call UF/uc6560 to get the
appropriate error message.
CAUTION:
The option to create a non-associative offset surface
with LP4 is no longer supported as of the V10 release.
*/
extern UFUNEXPORT void uf5450(
tag_t *np1, /* <I> Object identifier of the base face */
double *rp2, /* <I> Offset Distance */
double *rp3, /* <I> Edge Curve Tolerance */
int *lp4, /* <I> Not used. */
tag_t *nr5 /* <O> Object identifier of the offset surface. Set to
NULL if the offset surface was unable to be created. */
);
/* uf5451 read offset distance */
extern UFUNEXPORT void uf5451(tag_t *np1, double *rr2, int *ir3);
/* uf5452 edit offset distance */
extern UFUNEXPORT void uf5452(tag_t *np1, double *rp2, double *rp3);
/* uf5453 base face type */
extern UFUNEXPORT void uf5453(tag_t *np1, int *ir2);
/* uf5460 create free form feature using conic face */
extern UFUNEXPORT void uf5460(int *ip1, tag_t *np2, tag_t *np3,
int *ip4, double *rp5, int *ip6,
int *ip7, double *rp8, int *ir9,
tag_t *nr10, tag_t *nr11, double *rr12);
/* uf5461 create free form feature using sweeping */
extern UFUNEXPORT void uf5461(int *ip1, tag_t *np2, int *ip3,
int *ip4, tag_t *np5, int *ip6,
int *ip7, tag_t *np8, int *ip9,
int *ip10, tag_t *np11, int *ip12,
double *rp13, int *ip14, tag_t *np15,
int *ip16, int *ip17, double *rp18,
double *rp19, int *ir20, tag_t *nr21);
/* uf5462 create b-surface face */
extern UFUNEXPORT void uf5462(int *ip1, tag_t *np2, int *ip3,
tag_t *np4, int *ip5, double *rp6,
int *ir7, tag_t *nr8);
/* uf5464 reads the count of poles */
extern UFUNEXPORT void uf5464(tag_t *np1, int *ir2,
int *ir3, int *ir4, int *ir5);
/* uf5465 create a b-surface face from a face */
extern UFUNEXPORT void uf5465(tag_t *np1, double *rp2, tag_t *nr3);
/* uf6500 create a block */
extern UFUNEXPORT void uf6500(double *rp1, double *rp2, double *rp3,
tag_t *nr4);
/* uf6501 create a sphere */
extern UFUNEXPORT void uf6501(double *rp1, double *rp2, tag_t *nr3);
/* uf6502 create a cylinder */
extern UFUNEXPORT void uf6502(double *rp1, double *rp2, double *rp3,
double *rp4, tag_t *nr5);
/* uf6503 create a torus */
extern UFUNEXPORT void uf6503(double *rp1, double *rp2,
double *rp3, tag_t *nr4);
/* uf6504 create a cone */
extern UFUNEXPORT void uf6504(double *rp1, double *rp2,
double *rp3, double *rp4,
tag_t *nr5);
/* uf6505 create a prism */
extern UFUNEXPORT void uf6505(double *rp1, double *rp2,
double *rp3, int *ip4, double *rp5,
tag_t *nr6);
/* uf6506 create a sewn solid from a series of sheets */
extern UFUNEXPORT void uf6506(tag_t *np1, int *ip2, int *ip3,
tag_t *nr4);
/* uf6507 create an extruded body */
extern UFUNEXPORT void uf6507(tag_t *np1, int *ip2, double *rp3,
double *rp4, tag_t *nr5);
/* uf6508 create a body of revolution */
extern UFUNEXPORT void uf6508(tag_t *np1, int *ip2, double *rp3,
double *rp4, double *rp5, tag_t *nr6);
/* uf6509 convert a face to a sheet */
extern UFUNEXPORT void uf6509(tag_t *np1, int *ip2,
double *rp3, tag_t *nr4);
/* uf6511 copy a body */
extern UFUNEXPORT void uf6511(tag_t *np1, tag_t *nr2);
/* uf6520 unite, intersect, or subtract solids */
extern UFUNEXPORT void uf6520(int *ip1, tag_t *np2,
tag_t *np3, int *ip4,
int *ip5, int *ir6,
int *ir7, tag_t *nr8);
/* uf6523 split solids
Replaced by UF_MODL_split_body */
extern UFUNEXPORT void uf6523(tag_t *np1, int *ip2,
tag_t *np3, int *ip4,
int *ir5, int *ir6, tag_t *nr7);
/* uf6524 section solids */
extern UFUNEXPORT void uf6524(tag_t *np1, int *ip2,
tag_t *np3, int *ip4,
int *ir5, int *ir6, tag_t *nr7);
/* uf6525 cut solids
uf6525 can be replaced by UF_MODL_split_bo
Note: UF_MODL_split_body does similar work but uses a
different parasolid call. It can handle the splitting of bodies
other than solids or planes.
*/
extern UFUNEXPORT void uf6525(tag_t *np1, int *ip2,
tag_t *np3, int *ip4,
int *ir5, int *ir6, tag_t *nr7,
int *ir8);
/* uf6526 add blends to a solid */
extern UFUNEXPORT void uf6526(tag_t *np1, int *ip2,
double *rp3, tag_t *np4,
int *ip5, tag_t *np6,
int *ip7, int *ir8);
/* uf6540 inquire box containing the specified body
Replaced by UF_MODL_ask_bounding_box */
extern UFUNEXPORT void uf6540(tag_t *np1, int *ir2, double *rr3);
/* uf6541 inquire containment of the specified point
Replaced by UF_MODL_ask_point_containment */
extern UFUNEXPORT void uf6541(double *rp1, tag_t *np2,
int *ir3, int *ir4);
/* uf6542 check the validity of bodies
Replaced by UF_MODL_validate_body */
extern UFUNEXPORT void uf6542(tag_t *np1, int *ip2,
int *ir3, int *ir4);
/* uf6543 return the mass properties of a body */
extern UFUNEXPORT void uf6543(tag_t *np1, double *rp2,
int *ip3, int *ir4,
double *rr5, double *rr6);
/* uf6544 check the interference of bodies
Replaced by UF_MODL_check_inteference */
extern UFUNEXPORT void uf6544(tag_t *np1, tag_t *np2,
int *ip3, int *ir4,
int *ir5);
/* uf6545 intersect a ray with a list of bodies
Replaced by UF_MODL_trace_a_ray */
extern UFUNEXPORT void uf6545(const tag_t *np1, const int *ip2,
const double *rp3, const double *rp4,
const int *ip5, const double *rp6,
const double *rp7, int *ir8,
int *ir9, double *rr10, double *rr11,
int *ir12);
/* uf6546 read number of faces */
extern UFUNEXPORT void uf6546(tag_t *np1, int *ir2,
int *ir3);
/* uf6547 read density of solid */
extern UFUNEXPORT void uf6547(tag_t *np1, int *ip2,
int *ir3, double *rr4);
/* uf6548 edit density of solid */
extern UFUNEXPORT void uf6548(tag_t *np1, double *rp2,
int *ip3, int *ir4);
/* Read global (default) solid density
Replaced by UF_MODL_ask_default_density */
extern UFUNEXPORT void uf6549
(int *ip1, /* units of denisty
* 1 - lb/cu in
* 2 - lb/cu ft
* 3 - g /cu cm
* 4 - kg/cu m */
int *ir2, /* error code
* 0 - success
* 1 - fail */
double *rr3); /* global solid
* density */
/* Edit global (default) solid density
Replaced by UF_MODL_set_default_density */
extern UFUNEXPORT void uf6550
(double *rp1, /* new density */
int *ip2, /* units of denisty
* 1 - lb/cu in
* 2 - lb/cu ft
* 3 - g /cu cm
* 4 - kg/cu m */
int *ir3); /* error code
* 0 - success
* 1 - fail */
/**************************************************************************
Error Handler:
Returns the Error message from the last call to a solids routine. The
error message from the previous solid routine called is lost if UF6560
is not called right after that solid routine.
Environment: Internal and External
See Also:
History:
*************************************************************************/
extern UFUNEXPORT int uc6560(
char cr1[300] /* <O>
Returned Error Message (40 char max)
*/
);
/********************************************************************
Gets the parameters of a torus.
Environment: Internal and External
See Also:
History:
********************************************************************/
extern UFUNEXPORT int UF_MODL_ask_torus_parms(
tag_t feature_tag, /* <I>
Feature object identifier
*/
int edit, /* <I>
Unused flag
*/
char **major_diameter, /* <OF>
Torus major diameter. This must be
freed by calling UF_free.
*/
char **minor_diameter /* <OF>
Torus minor diameter This must be
freed by calling UF_free.
*/
);
/********************************************************************
Gets the parameters of a prism.
Environment: Internal and External
See Also:
History:
********************************************************************/
extern UFUNEXPORT int UF_MODL_ask_prism_parms(
tag_t feature_tag, /* <I>
Feature object identifier
*/
int edit, /* <I>
Unused flag
*/
char **diameter, /* <OF>
Prism diameter. This must be freed
by calling UF_free.
*/
char **height, /* <OF>
Prism height. This must be freed
by calling UF_free.
*/
char **number_of_sides /* <OF>
Number of sides in prism . This must
be freed by calling UF_free.
*/
);
#undef EXPORTLIBRARY
#endif /* UF_MODL_LEGACY_H_INCLUDED */