UF_MB_add_actions (view source)
Defined in: uf_mb.h
Overview
Registers custom Internal Open API applications for the NX
menubar.
Environment
Internal
Required License(s)
gateway
int UF_MB_add_actions
(
UF_MB_action_t action_table [ ]
)
UF_MB_action_t | action_table [ ] | Input | NULL terminated array of UF_MB_action_t records containing action name, function address, and callback argument. |
UF_MB_add_styler_actions (view source)
Defined in: uf_mb.h
Overview
Associates a UIStyler dialog to an associated action specified in a Menuscript
file. The dialog file must be generated from the UIStyler and must be located
in the "application" directory underneath the directory which has been added to
the file $UGII_BASE_DIR/ugii/menu/custom_dirs.dat.
For example, on an NT system, you could specify d:\my_application
as your directory.
The actions structure provides the binding of callbacks and client data
to the dialog. You may associate multiple dialogs in your actions
structure provided that the list is NULL terminated.
Environment
Internal
Required License(s)
gateway
int UF_MB_add_styler_actions
(
UF_MB_styler_actions_p_t actions
)
UF_MB_ask_button_id (view source)
Defined in: uf_mb.h
Overview
Gets the button's ID.
Environment
Internal
Required License(s)
gateway
int UF_MB_ask_button_id
(
char * button_name,
int * button_id
)
char * | button_name | Input | Name of the button |
int * | button_id | Output | Button Identification |
UF_MB_ask_button_sensitivity (view source)
Defined in: uf_mb.h
Overview
Gets the button's sensitivity. Note that this function is intended for customized
Menuscript buttons only. The NX buttons are insensitive when running any NXOpen program and
are returned to their normal sensitivity state when the NXOpen program completes.
Environment
Internal
Required License(s)
gateway
int UF_MB_ask_button_sensitivity
(
int button_id,
UF_MB_state_p_t state
)
int | button_id | Input | Button Identification |
UF_MB_state_p_t | state | Output | Button sensitivity can be one of the following: UF_MB_ON UF_MB_OFF |
UF_MB_ask_button_type_name (view source)
Defined in: uf_mb.h
Overview
Returns the name of a button type. If the specified type corresponds
to the type of a menubar button, type_name is returned as a pointer to
the button type name, and the function returns 0; otherwise the
function type_name points to the string "UNKNOWN" and the return
value is UF_err_bad_parameter_number_1.
Environment
Internal
Required License(s)
gateway
int UF_MB_ask_button_type_name
(
UF_MB_button_type_t type,
char * * type_name
)
UF_MB_button_type_t | type | Input | The type of a menu bar button. |
char * * | type_name | Output to UF_*free* | The name of the button type. |
UF_MB_ask_double_resource (view source)
Defined in: uf_mb.h
Overview
Locates the requested resource in the X Resource Database. If it is
found, its value is set to the value found. If the resource is not found,
value is set to the default. 0 is returned unless there are any argument
or exception errors.
NOTE: This function is only available on Unix.
Environment
Internal
Required License(s)
gateway
int UF_MB_ask_double_resource
(
const char * name,
double defvalue,
double * value
)
const char * | name | Input | The name of the resource to be located. |
double | defvalue | Input | The default value for the resource if not found. |
double * | value | Output | The value of the resource. |
UF_MB_ask_int_resource (view source)
Defined in: uf_mb.h
Overview
Locates the requested resource in the X Resource Database. If it is
found, its value is set to the value found. If the resource is not found,
value is set to the default. 0 is returned unless there are any argument
or exception errors.
NOTE: This function is only available on Unix.
Environment
Internal
Required License(s)
gateway
int UF_MB_ask_int_resource
(
const char * name,
int defvalue,
int * value
)
const char * | name | Input | The name of the resource to be located. |
int | defvalue | Input | The default value for the resource if not found. |
int * | value | Output | The value of the resource. |
UF_MB_ask_logical_resource (view source)
Defined in: uf_mb.h
Overview
Locates the requested resource in the X Resource Database. If it is
found, its value is set to the value found. If the resource is not found,
value is set to the default. 0 is returned unless there are any argument
or exception errors.
NOTE: This function is only available on Unix.
Environment
Internal
Required License(s)
gateway
int UF_MB_ask_logical_resource
(
const char * name,
logical defvalue,
logical * value
)
const char * | name | Input | The name of the resource to be located. |
logical | defvalue | Input | The default value for the resource if not found. |
logical * | value | Output | The value of the resource. |
UF_MB_ask_string_resource (view source)
Defined in: uf_mb.h
Overview
Locates the requested resource in the X Resource Database. If it is
found, its value is set to the value found. If the resource is not found,
value is set to the default. 0 is returned unless there are any argument
or exception errors.
NOTE: This function is only available on Unix.
Environment
Internal
Required License(s)
gateway
int UF_MB_ask_string_resource
(
const char * name,
const char * defvalue,
char value [ ]
)
const char * | name | Input | The name of the resource to be located. |
const char * | defvalue | Input | The default value for the resource if not found. |
char | value [ ] | Output | The value of the resource. |
UF_MB_ask_toggle_state (view source)
Defined in: uf_mb.h
Overview
Gets a toggle button's current state.
Environment
Internal
Required License(s)
gateway
int UF_MB_ask_toggle_state
(
int button_id,
UF_MB_state_t * state
)
int | button_id | Input | Button ID |
UF_MB_state_t * | state | Output | The button's sensitivity can be one of the following: UF_MB_ON UF_MB_OFF |
UF_MB_init_application_data (view source)
Defined in: uf_mb.h
Overview
Initializes the custom application data. This routine should be called
before calling UF_MB_register_application.
Return
void
Environment
Internal
History
Introduced in V18.0
Required License(s)
gateway
int UF_MB_init_application_data
(
UF_MB_application_p_t app_data
)
UF_MB_load_resource_file (view source)
Defined in: uf_mb.h
Overview
Loads a resource file. Locates the requested resource file in the
vendor, site, or user application directory (specified by one of the
following environment variables: UGII_UGOPEN_VENDOR_DIR,
UGII_UGOPEN_SITE_DIR, or UGII_UGOPEN_USER_DIR), loads it into a new,
temporary XrmDatabase, and then merges it into the master XrmDatabase
for the display connection (i.e. the application session). The merge
automatically destroys the temporary database.
NOTE: This function is only available on Unix.
Environment
Internal
Required License(s)
gateway
int UF_MB_load_resource_file
(
const char * resource_file
)
const char * | resource_file | Input | The name of the vendor resource file to be loaded. The name does not include the path. |
UF_MB_register_application (view source)
Defined in: uf_mb.h
Overview
Register the user application defined by the application button.
Environment
Internal
Required License(s)
gateway
int UF_MB_register_application
(
UF_MB_application_p_t app
)
UF_MB_set_button_sensitivity (view source)
Defined in: uf_mb.h
Overview
Sets the button's sensitivity.
Environment
Internal
Required License(s)
gateway
int UF_MB_set_button_sensitivity
(
int button_id,
UF_MB_state_t state
)
int | button_id | Input | Button ID |
UF_MB_state_t | state | Input | The button's sensitivity can be set to one of the following states: UF_MB_ON UF_MB_OFF |
UF_MB_set_toggle_state (view source)
Defined in: uf_mb.h
Overview
Sets the state of a toggle button.
Environment
Internal
Required License(s)
gateway
int UF_MB_set_toggle_state
(
int button_id,
UF_MB_state_t state
)
int | button_id | Input | Button ID |
UF_MB_state_t | state | Input | Sets the toggle buttons state on or off. Use one of the following constants: UF_MB_ON UF_MB_OFF |