UF_GDT_characteristic_e (view source)
 
Defined in: uf_gdt.h
 
Also known as:
 
Overview
Defines the set of valid feature control frame characteristic GD&T types


Data Members

UF_GDT_STRAIGHTNESS_TYPE
GDT form type - straightness

UF_GDT_FLATNESS_TYPE
GDT form type - flatness

UF_GDT_CIRCULAR_TYPE
GDT form type - circular

UF_GDT_CYLINDRICAL_TYPE
GDT form type _ cylindrical

UF_GDT_LINE_PROFILE_TYPE
GDT profile type - line profile

UF_GDT_SURFACE_PROFILE_TYPE
GDT profile type - surface profile

UF_GDT_ANGULAR_TYPE
GDT orientation type - angular

UF_GDT_PERPENDICULAR_TYPE
GDT orientation type - perpendicular

UF_GDT_PARALLEL_TYPE
GDT orientation type - parallel

UF_GDT_POSITION_TYPE
GDT position type - position

UF_GDT_CONCENTRIC_TYPE
GDT position type - concentric

UF_GDT_SYMMETRIC_TYPE
GDT position type - symmetric

UF_GDT_CIRCULAR_RUNOUT_TYPE
GDT runout type - circular runout

UF_GDT_TOTAL_RUNOUT_TYPE
GDT runout type - total runout

 


 
UF_GDT_data_type_e (view source)
 
Defined in: uf_gdt.h
 
Also known as:
 
Overview
Defines an enumerated type for each data structure inside the GD&T module
used in the UF_GDT_free routine


Data Members

UF_GDT_DATA_FRAME_TYPE
UF_GDT_data_frame_t

UF_GDT_DATUM_IDENT_TYPE
UF_GDT_datum_identifier_t

UF_GDT_DATUM_REF_TYPE
UF_GDT_datum_reference_t

UF_GDT_DESCRIPT_TYPE
UF_GDT_description_t

UF_GDT_DIRECTED_DIM_TYPE
UF_GDT_directed_dimension_t

UF_GDT_FCF_TYPE
UF_GDT_fcf_t

UF_GDT_MOD_DATA_TYPE
UF_GDT_modifier_data_t

UF_GDT_MULTI_DATUM_TYPE
UF_GDT_multiple_datum_t

UF_GDT_SIZE_TOL_TYPE
UF_GDT_size_tolerance_t

UF_GDT_STATISTICAL_TYPE
UF_GDT_statistical_info_t

UF_GDT_SURFACE_PARMS_TYPE
UF_GDT_surface_parms_t

UF_GDT_TARGET_POINT_TYPE
UF_GDT_datum_target_point_t

UF_GDT_TARGET_LINE_TYPE
UF_GDT_datum_target_line_t

UF_GDT_TARGET_AREA_TYPE
Obsolete in V15.0

UF_GDT_TOL_VALUE_TYPE
UF_GDT_tolerance_value_t

UF_GDT_TOL_ZONE_TYPE
UF_GDT_tolerance_zone_t

UF_GDT_FEAT_PARMS_TYPE
UF_GDT_feature_parms_t

UF_GDT_DIA_AREA_TYPE
UF_GDT_target_dia_area_t

UF_GDT_RECT_AREA_TYPE
UF_GDT_target_rect_area_t

UF_GDT_CYL_AREA_TYPE
UF_GDT_target_cyl_area_t

UF_GDT_UDEF_AREA_TYPE
UF_GDT_target_udef_area_t

UF_GDT_ANNOTATION_TAGS_TYPE
UF_GDT_annotation_tags_t

UF_GDT_CALLOUT_STR_TYPE
UF_GDT_callout_strings_t

UF_GDT_DEPTH_TOL_TYPE
UF_GDT_depth_tolerance_t

UF_GDT_LIM_FITS_TOL_TYPE
UF_GDT_limits_and_fits_tolerance_t

UF_GDT_DATUM_REF_FRAME_TYPE
UF_GDT_drf_data_t

UF_GDT_THREAD_TYPE
UF_GDT_thread_data_t

UF_GDT_MODL_DATA_TYPE
UF_GDT_modl_data_t

UF_GDT_PRODUCT_ATT_TYPE
UF_GDT_product_attribute_t

 


 
UF_GDT_datum_assoc_type_e (view source)
 
Defined in: uf_gdt.h
 
Also known as:
 
Overview
Defines an enumerated type for each method of associating a datum
display instance to the model.


Data Members

UF_GDT_FEATURE_EDGE
datum is attached to a feature edge

UF_GDT_DOTTED_DATUM
datum is attached to stub of dotted leader

UF_GDT_ATTACHED_TO_FCF
datum is attached to an fcf

UF_GDT_ATTACHED_TO_STUB
datum is attached to a leader stub

UF_GDT_DIRECTED_DATUM
datum is part of a directed datum instance

UF_GDT_EXTENSION_LINE
datum is attached to a dimension ext. line

 


 
UF_GDT_default_gage_type_e (view source)
 
Defined in: uf_gdt.h
 
Also known as:
 
Overview
The following enumerated type defines the restrained condition
for a GD&T part


Data Members

UF_GDT_SEPARATE_GAGE = 1


UF_GDT_SIMULTANEOUS_GAGE = 2


 


 
UF_GDT_directed_dimension_type_e (view source)
 
Defined in: uf_gdt.h
 
Also known as:
 
Overview
The following enumerated type defines the directed dimension types
available in the tolerancing module.


Data Members

UF_GDT_LINEAR_DIRECTED_DIMENSION
Linear directed dimension

UF_GDT_ANGULAR_DIRECTED_DIMENSION
Angular directed dimension

 


 
UF_GDT_edge_select_type_e (view source)
 
Defined in: uf_gdt.h
 
Also known as:
 
Overview
The following enumerated type defines the different feature edge
selection methods for GD&T,


Data Members

UF_GDT_EDGE_SELECT_ON = 1


UF_GDT_EDGE_SELECT_OFF = 2


UF_GDT_EDGE_SELECT_ALWAYS = 3


 


 
UF_GDT_feature_type_e (view source)
 
Defined in: uf_gdt.h
 
Also known as:
 
Overview
Defines the valid set of feature types which can describe the geometry
of a tolerance feature


Data Members

UF_GDT_GENERAL_FEATURE
General feature type

UF_GDT_SLOT_FEATURE
Slot feature type

UF_GDT_TAB_FEATURE
Tab feature type

UF_GDT_HOLE_FEATURE
Hole feature type

UF_GDT_PIN_FEATURE
Pin feature type

UF_GDT_SOCKET_FEATURE
Socket feature type

UF_GDT_BALL_FEATURE
Ball feature type

UF_GDT_ELONGATED_HOLE_FEATURE
Elongated hole feature type

UF_GDT_PLANE_FEATURE
Plane feature type

UF_GDT_BOUNDED_FEATURE
Bounded feature type

UF_GDT_TAPERED_HOLE_FEATURE
Tapered hole feature type

UF_GDT_TAPERED_PIN_FEATURE
Tapered pin feature type

UF_GDT_HOLLOW_TORUS_FEATURE
Hollow torus feature type

UF_GDT_SOLID_TORUS_FEATURE
Solid torus feature type

UF_GDT_HOLLOW_REVOLVED_FEATURE
Hollow revolved feature type

UF_GDT_SOLID_REVOLVED_FEATURE
Solid revolved feature type

UF_GDT_COUNTERBORE_HOLE_FEATURE
Counterbore hole feature type

UF_GDT_COUNTERSINK_HOLE_FEATURE
Countersink hole feature type

UF_GDT_EDGE_BLEND_FEATURE
Edge blend feature type

UF_GDT_THICKNESS_GAP_FEATURE
Thickness/Gap feature type

UF_GDT_STEPPED_SHAFT_FEATURE
Stepped shaft feature type

UF_GDT_STEPPED_HOLE_FEATURE
Stepped hole feature type

UF_GDT_COMPLEX_ELONGATED_HOLE_FEATURE
Complex elongated hole feature type

UF_GDT_OPPOSED_POINT_FEATURE
Opposed point element feature type

UF_GDT_OPPOSED_LINE_FEATURE
Opposed line element feature type

UF_GDT_THREAD_FEATURE
Thread Feature Type

UF_GDT_MODEL_AXIS_FEATURE
Modeling Axis Feature Type

UF_GDT_MODEL_PLANE_FEATURE
Modeling Plane Feature Type

UF_GDT_SPLINE_FEATURE
Spline feature type

UF_GDT_GEAR_FEATURE
Gear feature type

UF_GDT_CIRCULAR_TOOTH_THICKNESS_FEATURE
Circular tooth thickness type

UF_GDT_CIRCULAR_SPACE_WIDTH_FEATURE
Circular space width type

UF_GDT_PIN_MEASUREMENT_FEATURE
Pin measurement feature

 


 
UF_GDT_geometric_definition_type_e (view source)
 
Defined in: uf_gdt.h
 
Also known as:
 
Overview
The following enumerated type defines the orientation and region types
available in the tolerancing module.


Data Members

UF_GDT_ALL_GEOMETRY
No Definition

UF_GDT_PLANAR_ORIENTATION
Planar Orientation

UF_GDT_PLANAR_CROSS_SECTION
Planar Cross Section

UF_GDT_REGION
Region

UF_GDT_POINT
Point

UF_GDT_RECTANGULAR_REGION
Rectangular Bounded Region

UF_GDT_CIRCULAR_REGION
Circular Bounded Region

 


 
UF_GDT_index_display_type_e (view source)
 
Defined in: uf_gdt.h
 
Also known as:
 
Overview
The following enumerated type defines the valid index display
methods for GD&T,


Data Members

UF_GDT_UNIQUE = 0


UF_GDT_PART_BASED


 


 
UF_GDT_leader_type_e (view source)
 
Defined in: uf_gdt.h
 
Also known as:
 
Overview
The following enumerated type defines the leader terminator symbols


Data Members

UF_GDT_LEADER_NON_TERMINATED = 0


UF_GDT_LEADER_DATUM


UF_GDT_LEADER_ARROWHEAD


UF_GDT_LEADER_DOT


 


 
UF_GDT_limits_and_fits_display_type_e (view source)
 
Defined in: uf_gdt.h
 
Also known as:
 
Overview
The following data structures are defined for limits and fits tolerance,
These are used by the limits and fits tolerance ask, set routines.

Functions affected by the modification of these structure are:
UF_GDT_ask_depth_tolerance_parms
UF_GDT_set_depth_tolerance_parms
UF_GDT_set_depth_tolerance_parms


Data Members

UF_GDT_DEFAULT_DISPLAY_TYPE = 0


UF_GDT_LIMITS_DISPLAY_TYPE


UF_GDT_TOLERANCE_DISPLAY_TYPE


UF_GDT_NORMAL_DISPLAY_TYPE


 


 
UF_GDT_material_modifier_e (view source)
 
Defined in: uf_gdt.h
 
Also known as:
 
Overview
Defines the allowable material condition modifiers for feature control
frame and datum specifications


Data Members

UF_GDT_MMC
Maximum material condition modifier

UF_GDT_LMC
Least material condition modifier

UF_GDT_RFS
Regardless of feature size modifier

UF_GDT_TANGENTIAL
Tangential zone modifier NOTE: The
tangential modifier may only be used
to modify the tolerance zone of feature
control frames. It may not be used to
modify datum identifiers, targets, or
references

UF_GDT_NO_MOD
No material modifier. NOTE: The
UF_GDT_NO_MOD type should be used in
place of the RFS type for ASME 1994 and
ISO applications

 


 
UF_GDT_modifier_types_e (view source)
 
Defined in: uf_gdt.h
 
Also known as:
 
Overview
Defines the allowable zone modifiers for a feature control frame


Data Members

UF_GDT_FREE_STATE
Free state zone refinement (all)

UF_GDT_UNIT_BASIS_LENGTH
Unit basis length refinement
(straightness)

UF_GDT_UNIT_BASIS_AREA
Unit basis area refinement (flatness)

UF_GDT_PROJECTED_ZONE
Projected zone refinement (position)

UF_GDT_STATISTICAL
Statistical refinement (many)

UF_GDT_NO_MODIFIERS
No modifiers

UF_GDT_MAX_BONUS
MAX bonus tolerance specification

UF_GDT_PATTERN_COUNT
Obsolete in V16.0

UF_GDT_INDIVIDUAL_COUNT
Obsolete in V16.0

UF_GDT_SEP_REQT
Obsolete in V16.0

UF_GDT_SIM_REQT
Obsolete in V16.0

UF_GDT_BOUNDARY
Obsolete in V16.0

UF_GDT_ALL_OVER
Obsolete in V16.0

UF_GDT_AVG_DIA
Obsolete in V16.0

UF_GDT_COAX_HOLE_COUNT
Obsolete in V16.0

UF_GDT_NON_MANDATORY_MFG_DATA
Obsolete in V16.0

UF_GDT_NO_PERFECT_MMC_FORM
Obsolete in V16.0

UF_GDT_PERFECT_MMC_ORIENTATION
Obsolete in V16.0

UF_GDT_PERFECT_MMC_COAXIALITY
Obsolete in V16.0

UF_GDT_PERFECT_MMC_SYM_FEAT_LOC
Obsolete in V16.0

UF_GDT_SURFACE_COUNT
Obsolete in V16.0

UF_GDT_THRU
Obsolete in V16.0

UF_GDT_THRU_HOLE
Obsolete in V16.0

 


 
UF_GDT_modl_parameter_e (view source)
 
Defined in: uf_gdt.h
 
Also known as:
 
Overview
The following enumerated type defines the parameter used to map the
faces of the modeling feature to the tolerance feature.
Following describes each enum type, how it is related to the modeling
feature parameter and how to use it to create tolerance features based
on modeling features -

UF_GDT_MODL_PARAM_INVALID:
This enum type is resereved by the system for inernal use. It is not
available for use.

UF_GDT_MODL_PARAM_NONE:
When this enum type is used, the system knows exactly how to map the
faces of modeling feature to tolerance features.

Use with following modeling features -
1. Simple Hole
Modeling Feature Parameter: Hole Diameter
Tolerance feature will reference face defined by Hole Diameter parameter
2. Extrude/Revolve
Tolerance feature will reference cylindrical face in the modeling feature
and create GDT pin/hole type tolerance features
3. Cylindrical Pocket
Modeling Feature Parameter: Pocket Diameter
Tolerance feature will reference face defined by Pocket Diameter parameter
4. Counterbore Hole
System will create complex tolerance features/subfeatures -
Complex feature - References hole and counterbore faces
Complex subfeature 1 - References hole face
Complex subfeature 2 - References counterbore face
5. Countersink Hole
System will create complex tolerance features/subfeatures -
Complex feature - References countersink and hole faces
Complex subfeature 1 - References hole face
Complex subfeature 2 - References countersink face
Cross-section definition subfeature for complex subfeature 2
6. Symbolic Thread
System will create complex tolerance features/subfeatures -
Complex feature - References cylindrical face on which thread resides
Complex subfeature - References modeling thread feature
7. Boss
Modeling Feature Parameter: Boss Diameter
Tolerance feature will reference face defined by Boss Diameter
parameter
8. Edge Blend
Modeling Feature Parameter: Radius
Tolerance feature will reference faces defined by Radius parameter


UF_GDT_MODL_PARAM_ALL:
Use this enum type to create a GDT general type tolerance feature that
references all the faces of the modeling feature. Currently, this is not
enabled.


UF_GDT_MODL_PARAM_HOLE:
Use this enum type when creating tolerance feature that will reference
cylindrical face of the modeling feature.

Use with following modeling features -
1. Counterbore Hole, Countersink Hole
Modeling Feature Parameter: Hole Diameter
Tolerance feature will reference faces defined by Hole Diameter parameter


UF_GDT_MODL_PARAM_COUNTERBORE:
Use this enum type when creating tolerance feature that will reference
cylindrical face of the Counterbore Hole modeling feature.
Modeling Feature Parameter: Counterbore Diameter
Tolerance feature will reference faces defined by Counterbore Diameter
parameter


UF_GDT_MODL_PARAM_COUNTERSINK:
Use this enum type when creating tolerance feature that will reference
conical face of the Countersink Hole modeling feature.
Tolerance feature will reference conical faces


UF_GDT_MODL_PARAM_X_LENGTH:
Use this enum type when creating tolerance feature that will reference
faces of the modeling feature along the X-axis of the feature.

Use with following modeling features -
1. Rectangular Slot, Ball End Slot, U Slot, T Slot
Modeling Feature Parameter: Length
Tolerance feature will reference faces that are defined by Length
parameter
2. Rectangular Pad, Rectangular Pocket
Modeling Feature Parameter: X Length
Tolerance feature will reference faces that are defined by X Length
parameter


UF_GDT_MODL_PARAM_Y_LENGTH:
Use this enum type when creating tolerance feature that will reference
faces of the modeling feature along the Y-axis of the feature.

Use with following modeling features -
1. Rectangular Slot, U Slot
Modeling Feature Parameter: Width
Tolerance feature will reference faces that are defined by Width
parameter
2. Ball End Slot
Modeling Feature Parameter: Ball Diameter
Tolerance feature will reference faces separated by distance equal to
the ball diameter
3. T Slot
Modeling Feature Parameter: Bottom Width
Tolerance feature will reference faces that are defined by Bottom Width
parameter
4. Rectangular Pad, Rectangular Pocket
Modeling Feature Parameter: Y Length
Tolerance feature will reference faces that are defined by Y Length
parameter


UF_GDT_MODL_PARAM_X_LENGTH_TOP:
Use this enum type when creating tolerance feature that will reference
top faces of the T Slot modeling feature along the X-axis of the feature.
Modeling Feature Parameter: None


UF_GDT_MODL_PARAM_Y_LENGTH_TOP:
Use this enum type when creating tolerance feature that will reference
top faces of the T Slot modeling feature along the Y-axis of the feature.
Modeling Feature Parameter: Top Width


Data Members

UF_GDT_MODL_PARAM_INVALID


UF_GDT_MODL_PARAM_NONE


UF_GDT_MODL_PARAM_ALL


UF_GDT_MODL_PARAM_HOLE


UF_GDT_MODL_PARAM_COUNTERBORE


UF_GDT_MODL_PARAM_COUNTERSINK


UF_GDT_MODL_PARAM_X_LENGTH


UF_GDT_MODL_PARAM_Y_LENGTH


UF_GDT_MODL_PARAM_X_LENGTH_TOP


UF_GDT_MODL_PARAM_Y_LENGTH_TOP


 


 
UF_GDT_pattern_type_e (view source)
 
Defined in: uf_gdt.h
 
Also known as:
 
Overview
Defines the valid pattern types for a tolerance feature


Data Members

UF_GDT_NO_PATTERN


UF_GDT_RADIAL_PATTERN
Obsolete in V16

UF_GDT_RECTANGULAR_PATTERN
Obsolete in V16

UF_GDT_ARBITRARY_PATTERN


 


 
UF_GDT_precedence_e (view source)
 
Defined in: uf_gdt.h
 
Also known as:
 


Data Members

UF_GDT_PRECEDENCE_NONE = 0
No Precedence

UF_GDT_PRECEDENCE_PRIMARY
Primary datum reference

UF_GDT_PRECEDENCE_SECONDARY
Secondary datum reference

UF_GDT_PRECEDENCE_TERTIARY
Tertiary datum reference

 


 
UF_GDT_profile_type_e (view source)
 
Defined in: uf_gdt.h
 
Also known as:
 
Overview
Defines the allowable types of profile tolerances.
Outside if defined to be the direction away from material and
inside the direction into material.


Data Members

UF_GDT_PROFILE_EQ_BILATERAL
equally disposed bilateral

UF_GDT_PROFILE_UNILATERAL_OUT
unilateral outside

UF_GDT_PROFILE_UNILATERAL_IN
unilateral inside

UF_GDT_PROFILE_UNEQ_BILATERAL
unequally disposed bilateral

 


 
UF_GDT_relation_type_e (view source)
 
Defined in: uf_gdt.h
 
Also known as:
 
Overview
The following enumerated type is used to specify the type of master
model link which is to be broken from the "break relationship" function.


Data Members

UF_GDT_PULL_RELATION_TYPE
link between pulled feature and component

 


 
UF_GDT_restrained_condition_e (view source)
 
Defined in: uf_gdt.h
 
Also known as:
 
Overview
The following enumerated type defines the default part gaging
standards for GD&T


Data Members

UF_GDT_FREE_STATE_CONDITION = 1


UF_GDT_RESTRAINED_CONDITION = 2


 


 
UF_GDT_size_value_type_e (view source)
 
Defined in: uf_gdt.h
 
Also known as:
 
Overview
The following enumerated type defines the size tolerance value
types available in the tolernacing module.


Data Members

UF_GDT_NO_SIZE
No size tolerance value

UF_GDT_LINEAR_SIZE
Linear size tolerance

UF_GDT_RADIAL_SIZE
Radial size tolerance

UF_GDT_DIAMETRAL_SIZE
Diametral size tolerance

UF_GDT_ANGULAR_MAJOR_SIZE
Angular major size tolerance

UF_GDT_ANGULAR_MINOR_SIZE
Angular minor size tolerance

 


 
UF_GDT_standard_e (view source)
 
Defined in: uf_gdt.h
 
Also known as:
 
Overview
Defines the standards that are supported by the Geometric Tolerancing
module


Data Members

UF_GDT_NO_STANDARD
Standard not specified

UF_GDT_ANSI_1982
ANSI Y14.5M - 1982 standard

UF_GDT_ASME_1994
ASME Y14.5M - 1994 standard

UF_GDT_ISO_1983
ISO 1101 : 1983 standard

 


 
UF_GDT_standard_keyword_id_e (view source)
 
Defined in: uf_gdt.h
 
Also known as:
 
Overview
Defines the standard keyword ids


Data Members

UF_GDT_PATTERN_COUNT_KEYWORD
Pattern Count (3X, etc)

UF_GDT_INDIVIDUAL_COUNT_KEYWORD
INDIVIDUALLY applied

UF_GDT_SEP_REQT_KEYWORD
SEP REQT applied

UF_GDT_SIM_REQT_KEYWORD
SIM REQT applied

UF_GDT_BOUNDARY_KEYWORD
BOUNDARY condition applied

UF_GDT_ALL_OVER_KEYWORD
ALL OVER applied to surfaces

UF_GDT_AVG_DIA_KEYWORD
AVG DIAM applied to size
tolerances

UF_GDT_COAX_HOLE_COUNT_KEYWORD
nX COAXIAL HOLES applied

UF_GDT_NON_MANDATORY_MFG_DATA_KEYWORD
NON-MANDATORY MFG DATA applied

UF_GDT_NO_PERFECT_MMC_FORM_KEYWORD
NON-PERFECT FORM AT MMC applied

UF_GDT_PERFECT_MMC_ORIENTATION_KEYWORD


UF_GDT_PERFECT_MMC_COAXIALITY_KEYWORD


UF_GDT_PERFECT_MMC_SYM_FEAT_LOC_KEYWORD


UF_GDT_SURFACE_COUNT_KEYWORD
n SURFACES applied

UF_GDT_THRU_KEYWORD
THRU applied to feature

UF_GDT_THRU_HOLE_KEYWORD
THRU HOLE applied to feature

UF_GDT_SIM_REQT_N_KEYWORD
SIM REQT N applied to feature

UF_GDT_MAJOR_DIA_KEYWORD
MAJOR DIA applied to thread feature

UF_GDT_MINOR_DIA_KEYWORD
MINOR DIA applied to thread feature

UF_GDT_PITCH_DIA_KEYWORD
PITCH DIA applied to thread feature

UF_GDT_INTERRUPTED_KEYWORD


 


 
UF_GDT_stub_direction_e (view source)
 
Defined in: uf_gdt.h
 
Also known as:
 
Overview
The following enumerated type defines the leader stub direction


Data Members

UF_GDT_STUB_LEFT = 1


UF_GDT_STUB_RIGHT


UF_GDT_STUB_UP


UF_GDT_STUB_DOWN


 


 
UF_GDT_text_location_e (view source)
 
Defined in: uf_gdt.h
 
Also known as:
 
Overview
The following enumerated type defines the allowable types of appended text
locations.


Data Members

UF_GDT_ABOVE
above appended text

UF_GDT_BELOW
below appended text

UF_GDT_BEFORE
before appended text

UF_GDT_AFTER
after appended text

 


 
UF_GDT_tol_format_e (view source)
 
Defined in: uf_gdt.h
 
Also known as:
 
Overview
Defines the valid tolerance display formats for a size tolerance


Data Members

UF_GDT_LIM_MINUS_BEFORE_PLUS
Limits minus before plus

UF_GDT_LIM_PLUS_BEFORE_MINUS
Limits plus before minus

UF_GDT_LIM_MINUS_OVER_PLUS
Limits minus over plus

UF_GDT_LIM_PLUS_OVER_MINUS
Limits plus over minus

UF_GDT_PLUS_OVER_MINUS
Tolerance plus over minus

UF_GDT_MINUS_OVER_PLUS
Tolerance minus over plus

UF_GDT_PLUS_MINUS
Tolerance plus minus

UF_GDT_NO_TOLERANCE
No tolerance defined

 


 
UF_GDT_tolerance_type_e (view source)
 
Defined in: uf_gdt.h
 
Also known as:
 
Overview
Defines the type of tolerances that can be part of a tolerance feature
Tolerance features may include a number of these different types


Data Members

UF_GDT_DATUM_TARGET_POINT_TYPE = 0
Datum target point tolerance type

UF_GDT_DATUM_TARGET_LINE_TYPE = 1
Datum target line tolerance type

UF_GDT_DATUM_IDENTIFIER_TYPE = 3
Datum identifier type

UF_GDT_DATUM_MULTIPLE_TYPE = 4
Special Multiple datum type

UF_GDT_GEOMETRIC_TOLERANCE_TYPE = 5
Geometric tolerance type

UF_GDT_SIZE_TOLERANCE_TYPE = 6
Size Tolerance type

UF_GDT_DATUM_TARGET_DIA_TYPE = 7
Circular datum target areas

UF_GDT_DATUM_TARGET_RECT_TYPE = 8
Rectangular datum target areas

UF_GDT_DIRECTED_DIMENSION_TYPE = 9
Directed dimension type

UF_GDT_DATUM_TARGET_CYL_TYPE = 10
Cylindrical datum target areas

UF_GDT_WALL_THICKNESS_TYPE = 11
Wall thickness tolerance type

UF_GDT_DEPTH_TOLERANCE_TYPE = 12
Depth Tolerance type

UF_GDT_LIMITS_AND_FITS_TOLERANCE_TYPE = 13
Limits and fits tolerance type

UF_GDT_THREAD_TOLERANCE_TYPE = 14
Thread tolerance type

UF_GDT_DATUM_TARGET_USER_DEFINED_TYPE = 15
User defined datum target type

 


 
UF_GDT_zone_shape_e (view source)
 
Defined in: uf_gdt.h
 
Also known as:
 
Overview
Defines the possible tolerance zone shapes for a feature control frame


Data Members

UF_GDT_SHAPE_PLANAR
Planar tolerance zone - Planar zones
define a tolerance zone which runs
parallel to a flat or complex plane.

UF_GDT_SHAPE_CYLINDRICAL
Cylindrical tolerance zone - Cylindri-
cal zones define a tolerance zone which
surrounds the AXIS of a cylindrical
feature.

UF_GDT_SHAPE_SPHERICAL
Spherical tolerance - Spherical zones
define a tolerance zone surrounding
the center of a spherical feature.

UF_GDT_SHAPE_OFFSET
Profile zone - Offset zones define
unilateral or bilateral tolerance zones
used for profile tolerances.