/*
uf_disp_ugopenint.h
File Description :
This include file contains the prototypes and descriptions of the display
functions. The functions include temporary display, color table access and
model bounds access.
In addition, this file contains the prototypes for the public functions in the
UF_DISP module. This module is to be used to display UDO geometry. These
functions should be called from the user program. The user program can be
registered with the display, selection, fit and attention point callbacks.
This provides routines for:
Coneheads - describes the functions that enable you to display coneheads and
objects. The coneheads section describes the C include files, data
structures, and C functions available to you which enable you to
temporarily display coneheads, and get and set conehead attributes.
Features and Dimensions - describes the functions that enable you to display
sketch and rpo dimensions.
Batch Shade - describes the batch shade function.
Color Table Access - describes the functions that enable you to read and modify
colors or the value of any color.
Model Bounds - are functions that enable you to query model bounds.
Name Display - are functions that enable you to set/query the name view status
or the name display status.
Object Display - are routines that enable you to display temporary graphics
objects, regenerate the display, and display objects.
Overlay Graphics Primitives - are routines to render geometry using Overlay
Graphics Primitives (OGP). These functions are
intended to be used exclusively from motion
callbacks. Please see the discussion and example
provided with UF_UI_specify_screen_position. Note
that these functions do not create NX
objects, and the geometry they define is not
associated with any existing objects.
Overlay Graphics primitives give the appearance of being drawn on a transparent
overlay. That is, they are displayed on top of any previously displayed
geometry, and when they are erased, the display of the underlying geometry is
not affected. Overlay Graphics primitives are drawn in the same color as the
crosshair: either white or black, whichever will contrast better with
the current background color.
Because of the method used internally to render Overlay Graphics primitives,
on most workstation configurations, when a portion of one primitive overlaps
another primitive, the overlapping portion will not display at all. Visually,
it is as if they cancel each other out. Therefore, in the course of defining
the primitives, care should be taken to avoid overlapping geometry.
User Defined Object Display - are routines that display, fit, and perform
attention point/selection computations. Each routine is overloaded with these
operations. The overloading of multiple functions allows you to call the
routine once from an Open API program. You can control which operation the
routine participates in by selectively registering an Open API program using
the registration methods in uf_udobj.h.
Work Plane Emphasis is a mode where all objects that are not on the work plane
are dimmed through a color change. These de-emphasized objects are filtered
out of selection operations.
The work plane emphasis set consists of points, lines, arcs, conics splines,
planes datum planes, datum axes, coordinate systems (except the WCS and GFEM
coordinate systems), and edges. This option also employs an exclusion object
set, which consists of those objects not affected by work plane emphasis. The
exclusion object set consists of sketcher datums and degree of freedom
indicators, the WCS, and the Grid.
***************************************************************************/
#ifndef UF_DISP_UGOPENINT_INCLUDED
#define UF_DISP_UGOPENINT_INCLUDED
/***************************************************************************
***************************************************************************/
#include <uf_defs.h>
#include <uf_disp.h>
#include <uf_disp_types.h>
#include <libugopenint_exports.h>
/*
Function prototypes
*/
/*****************************************************************
* Export a PNG/JPEG/TIFF/GIF/XWD/BMP full window area image
* Creates an image file with the file type you specify using the image
* currently displayed in the graphics window.
*
* Return:
* Return code:
* = 0 No error
* = not 0 Error code, including:
* UF_DISP_err_failed_to_create_image_file
* Standard UF error codes
*
* Environment: Internal
* See Also: See example
* History: Original release was in V13.0.
*****************************************************************/
extern UGOPENINTEXPORT int UF_DISP_create_image(
char* filename , /* <I>
Name of output image file
*/
UF_DISP_image_format_t format , /* <I>
Image type to produce:
UF_DISP_PNG
UF_DISP_JPEG
UF_DISP_TIFF
UF_DISP_COMPRESSED_TIFF
UF_DISP_GIF
UF_DISP_XWD (Only on UNIX workstations)
UF_DISP_BMP (Only on Windows workstations)
*/
UF_DISP_background_color_t color /* <I>
Back ground color:
UF_DISP_ORIGINAL
UF_DISP_WHITE
*/
);
/*****************************************************************
* Creates an image file with the file type and rectangular frame you
* specify using the image currently displayed in the graphics window.
* Export a PNG/JPEG/TIFF/GIF/XWD/BMP full window or rectangular area image
* Full window image: set width and height to zero
* Rectangular area image: set width, height greater than zero and set
* upper left point window coordinate
*
* Return:
* Return code:
* = 0 No error
* = not 0 Error code, including:
* UF_DISP_err_failed_to_create_image_file
* Standard UF error codes
*
* Environment: Internal
* See Also:
* History: Original release was in V15.0.
*****************************************************************/
extern UGOPENINTEXPORT int UF_DISP_create_framed_image(
char* filename , /* <I>
Name of output image file
*/
UF_DISP_image_format_t format , /* <I>
Image type to produce:
UF_DISP_PNG
UF_DISP_JPEG
UF_DISP_TIFF
UF_DISP_COMPRESSED_TIFF
UF_DISP_GIF
UF_DISP_XWD (Only on UNIX workstations)
UF_DISP_BMP (Only on Windows workstations)
*/
UF_DISP_background_color_t color , /* <I>
Back ground color:
UF_DISP_ORIGINAL - original background
color
UF_DISP_WHITE - white background color.
*/
int upper_left_corner[2] , /* <I>
The Image's upper left corner in the
window. Set both x and y to 0 (zero)
for a full screen image.
upper_left_corner[0] = x position
upper_left_corner[1] = y position
*/
int width , /* <I>
Image width in pixels. Set to 0 (zero)
for full screen image.
*/
int height /* <I>
Image height in pixels. Set to 0
(zero) for full screen image.
*/
);
/*****************************************************************************
* Displays all or some rpo dimensions which belong to the specified
* feature. The dimensions are specified indirectly by an array of
* expression tags. If the count of the array is -1 then the array is
* ignored and all rpo dimensions of the feature are displayed. If the
* count is 0 then nothing is displayed. The display is temporary and can
* be removed by a display refresh operation. The background color can
* also be used to erase the dimensions but it may leave gaps on the
* display. There must be a part loaded when this function is called. Any
* specified expression which does not tie directly to a dimension of the
* specified feature is considered invalid.
*
* Environment: Internal
* See Also:
* History:
***************************************************************************/
extern UGOPENINTEXPORT int UF_DISP_display_rpo_dimensions(
tag_t feature_tag , /* <I>
Tag of the feature to which the
dimensions belong
*/
int exp_count , /* <I>
>=0 = Number of expression tags
in exp_tags array
-1 = all rpo dimensions of the
feature
*/
tag_t* exp_tags , /* <I> exp_count
Array of expression tags of which
the dimensions need to be
displayed.(is ignored if count <=0)
*/
int view_option , /* <I>
Option for the view, the constants
are in uf_disp.h:
UF_DISP_ALL_VIEWS_BUT_DRAWING
UF_DISP_VIEW_OF_LAST_CURSOR
UF_DISP_ALL_ACTIVE_VIEWS
UF_DISP_WORK_VIEW_ONLY
*/
int color_option , /* <I>
Option for the color, the constants
are in uf_disp.h:
UF_DISP_USE_SYSTEM_COLOR
UF_DISP_USE_BACKGROUND_COLOR
UF_DISP_USE_ORIGINAL_COLOR
UF_DISP_USE_SPECIFIED_COLOR
*/
int color /* <I>
Color used to display the
dimensions if color_option=
UF_DISP_USE_SPECIFIED_COLOR.
Use the color constants listed
in uf_obj.h.
*/
);
/*****************************************************************************
* Displays all or some sketch dimensions which belong to a specified
* sketch. The dimensions are specified indirectly by an array of
* expression tags. If the count of the array is -1 then the array is
* ignored and all dimensions of the sketch are displayed. If the count is
* 0 then nothing is displayed. The display is temporary and can be
* removed by a display refresh operation. The background color can
* also be used to erase the dimensions but it may leave gaps on the
* display. There must be a part loaded when this function is called. Any
* specified expression which does not tie directly to a dimension of the
* specified feature is considered invalid.
*
* Environment: Internal
* See Also:
* History:
*****************************************************************************/
extern UGOPENINTEXPORT int UF_DISP_display_sket_dimensions(
tag_t sketch_tag , /* <I>
Tag of the sketch to which the
dimensions belong
*/
int exp_count , /* <I>
>= 0 = Number of expression tags in
exp_tags array
-1 = all dimensions of the sketch
*/
tag_t* exp_tags , /* <I> exp_count
Array of expression tags of which
the dimensions need to be displayed.
(is ignored if count <= 0)
*/
int view_option , /* <I>
Option for the view, the constants
are in uf_disp.h:
UF_DISP_ALL_VIEWS_BUT_DRAWING
UF_DISP_VIEW_OF_LAST_CURSOR
UF_DISP_ALL_ACTIVE_VIEWS
UF_DISP_WORK_VIEW_ONLY
*/
int color_option , /* <I>
Option for the color, the constants
are in uf_disp.h:
UF_DISP_USE_SYSTEM_COLOR
UF_DISP_USE_BACKGROUND_COLOR
UF_DISP_USE_ORIGINAL_COLOR
UF_DISP_USE_SPECIFIED_COLOR
*/
int color /* <I>
Color used to display the
dimensions if color_option=
UF_DISP_USE_SPECIFIED_COLOR.
Use the color constants listed in
uf_obj.h.
*/
);
/*****************************************************************************
* Displays a temporary conehead vector with either the base of the staff,
* the arrow tip or the base of the arrow head at the reference point
* in the specified view.
* Return: void
* Environment: Internal
* See Also: See example
* History:
*****************************************************************************/
extern UGOPENINTEXPORT void UF_DISP_conehead(
int display_flag , /* <I>
Display views to draw the conehead vector in.
UF_DISP_ALL_VIEWS_BUT_DRAWING
UF_DISP_VIEW_OF_LAST_CURSOR
UF_DISP_ALL_ACTIVE_VIEWS
UF_DISP_WORK_VIEW_ONLY
>0 = View sequence number
*/
double coord[3] , /* <I>
3D absolute coordinates of anchor.
*/
double vector[3] , /* <I>
3D vector which gives conehead direction
*/
int anchor_flag /* <I>
Denotes the anchor point
0 = Anchor point at base of staff
1 = Anchor point at tip of arrowhead
2 = Anchor point at base of arrowhead
*/
);/**/
/*****************************************************************************
* Displays a temporary, labeled conehead vector with either the base of
* the staff, the arrow tip or the base of the arrowhead at the reference
* point in the specified view(s). A label will be placed at the cone's tip.
* Environment: Internal
* Return: void
* See Also:
* History:
*****************************************************************************/
extern UGOPENINTEXPORT void UF_DISP_labeled_conehead(
int display_flag , /* <I>
Display views to draw the conehead
vector in.
UF_DISP_ALL_VIEWS_BUT_DRAWING
UF_DISP_VIEW_OF_LAST_CURSOR
UF_DISP_ALL_ACTIVE_VIEWS
UF_DISP_WORK_VIEW_ONLY
>0 = View sequence number
*/
double coord[3] , /* <I>
3D absolute coordinates of anchor or
reference point in absolute space.
*/
double vector[3] , /* <I>
3D vector which gives conehead direction
in absolute space.
*/
int anchor_flag , /* <I>
Denotes the anchor point's location:
0 = Anchor point at base of staff
1 = Anchor point at tip of arrowhead
2 = Anchor point at base of arrowhead
*/
char * label /* <I>
Labels the conehead at its tip.
*/
);
/*****************************************************************************
* Gets the current attribute settings with which the conehead vector
* displays by a call to UF_DISP_conehead. You can then obtain the
* values of the fields of the UF_DISP_conehead_attrb_s structure (see
* the example below).
* Return:void
* Environment: Internal
* See Also: See example
* History:
*****************************************************************************/
extern UGOPENINTEXPORT void UF_DISP_get_conehead_attrb(
UF_DISP_conehead_attrb_s * attributes /* <O>
Pointer to the attributes structure.
*/
);
/*****************************************************************************
* Allows changes to the current attribute settings with which the
* conehead vector displays by a call to UF_DISP_conehead.
* Note that it is best to get the current attribute settings and then
* adjust the ones you need, as shown in the example.
* Return:void
* Environment: Internal
* See Also: See example
* History:
*****************************************************************************/
extern UGOPENINTEXPORT void UF_DISP_set_conehead_attrb(
UF_DISP_conehead_attrb_s * attributes /* <I>
Pointer to attributes structure.
*/
);/**/
/*****************************************************************************
* Resets the conehead attributes to the default values.
* Return: void
* Environment: Internal
* See Also:
* History:
*****************************************************************************/
extern UGOPENINTEXPORT void UF_DISP_reset_conehead_attrb(void);/**/
/*****************************************************************************
* Adds an object to the display. You can use this routine to update the
* display of a new or modified object, if UF_DISP_set_display has been
* used to turn off the display update.
* Environment: Internal
* See Also:
* History:
*****************************************************************************/
extern UGOPENINTEXPORT int UF_DISP_add_item_to_display(
tag_t object_id /* <I>
Object identifier of the object to
be added to display
*/
);
/****************************************************************************
* Downloads the color table to the graphics display, so that all geometry
* displayed in the graphics window will now use the current contents of
* the Color Table object (of the Display part); this is equivalent to
* selecting Apply from the color palette dialog in interactive
* NX. There must be a part loaded before calling this function.
* Environment: Internal
* See Also: Please see the example
* History:
*****************************************************************************/
extern UGOPENINTEXPORT int UF_DISP_load_color_table(
void
);
/*****************************************************************************
*
* Overlay Graphics related prototypes follow
*
*****************************************************************************/
/***************************************************************************
* This function defines a simple line to be rendered in the specified
* view. The "ogp" in the name indicates that the line is drawn as an
* Overlay Graphics primitive (please see the Overview to this section); as
* such, it neither creates, nor is directly associated with, an NX
* object. UF_DISP_display_ogp_* functions are intended to be used
* exclusively from motion callback functions. Please see the discussion
* and example provided with UF_UI_specify_screen_position.
* Environment: Internal Only
* See Also: See example
* History:
****************************************************************************/
extern UGOPENINTEXPORT int UF_DISP_display_ogp_line(
tag_t view_tag , /* <I>
Tag of the view in which the line is to
be rendered
*/
double pos1[3] , /* <I>
1st endpoint (Work Part Abs Coords)
*/
double pos2[3] /* <I>
2nd endpoint (Work Part Abs Coords)
*/
);
/***************************************************************************
* This function defines a polyline to be rendered in the specified view.
* The "ogp" in the name indicates that the polyline will be drawn as an
* Overlay Graphics primitive (please see the Overview to this section); as
* such, it neither creates, nor is directly associated with, an NX
* object. * UF_DISP_display_ogp_* functions are intended to be used
* exclusively from motion callback functions. Please see the discussion
* and example provided with UF_UI_specify_screen_position.
*
* Environment: Internal and External
* See Also: See example
* History:
****************************************************************************/
extern UGOPENINTEXPORT int UF_DISP_display_ogp_polyline(
tag_t view_tag , /* <I>
Tag of the view in which the polyline
is to be rendered
*/
double pos_array[][3] , /* <I>
Array of positions [pos_count][3]
each position is an (x,y,z) triplet in
Work Part Absolute Coordinates.
*/
int pos_count /* <I>
count of positions in pos_array
*/
);
/***************************************************************************
* This function defines a circle to be rendered in the specified view.
* The "ogp" in the name indicates that the arc will be drawn as an
* Overlay Graphics primitive (please see the Overview to this section); as
* such, it neither creates, nor is directly associated with, an NX
* object. The orientation matrix must be ortho-normal. (If necessary, use
* UF_MTX3_initialize to create the matrix from X and Y vectors.)
* UF_DISP_display_ogp_* functions are intended to be used
* exclusively from motion callback functions. Please see the discussion
* and example provided with UF_UI_specify_screen_position.
*
* Environment: Internal and External
* See Also: See example
* History:
****************************************************************************/
extern UGOPENINTEXPORT int UF_DISP_display_ogp_circle(
tag_t view_tag , /* <I>
Tag of the view in which the circle is to
be rendered
*/
double orientation[9] , /* <I>
The rotation matrix of the circle
(relative to the Work Part Absolute
Coordinate System). The matrix must be
ortho-normal. If necessary, use
UF_MTX3_initialize to create the matrix
from X and Y vectors.
*/
double center[3] , /* <I>
The circle center in the coordinate
system of the arc (as defined by
"orientation" above).
*/
double radius /* <I>
The radius of the circle (Work Part
Absolute units)
*/
);
/***************************************************************************
* This function defines an arc to be rendered in the specified view. The
* "ogp" in the name indicates that the arc will be drawn as an Overlay
* Graphics primitive (please see the Overview to this section); as such, it
* neither creates, nor is directly associated with, an NX object.
* The arc is drawn in a positive angular direction ("counterclockwise")
* from the start angle to the end angle.
* The orientation matrix must be ortho-normal. (If necessary, use
* UF_MTX3_initialize to create the matrix from X and Y vectors.)
* This function returns an error if the absolute value of the difference
* between the start and end angle is greater than two pi (plus the system
* tolerance). An error is also returned if the start angle is greater than
* the end angle.
* UF_DISP_display_ogp_* functions are intended to be used
* exclusively from motion callback functions. Please see the discussion
* and example provided with UF_UI_specify_screen_position.
*
* Environment: Internal and External
* See Also: See example
* History:
****************************************************************************/
extern UGOPENINTEXPORT int UF_DISP_display_ogp_arc(
tag_t view_tag , /* <I>
Tag of the view in which the arc is to be
rendered
*/
double orientation[9] , /* <I>
The rotation matrix of the arc (relative to
the Work Part Absolute Coordinate System).
The matrix must be ortho-normal. If
necessary, use UF_MTX3_initialize to create
the matrix from X and Y vectors.
*/
double start_angle , /* <I>
Start angle in radians; the zero degree
vector is the positive x-axis of the space
described by the orientation matrix.
*/
double end_angle , /* <I>
End angle in radians; the zero degree
vector is the positive x-axis of the space
described by the orientation matrix.
*/
double center[3], /* <I>
The arc center in the coordinate system of
the arc (as defined by "orientation" above).
*/
double radius /* <I>
The radius of the arc (Work Part Absolute
units)
*/
);
/*****************************************************************************
*
* Prints the contents of the graphics window to the default printer.
* This function is available only on Windows workstations and returns
* an error if called on a non-Windows workstation.
*
* Environment: Internal
* See Also:
* History: Originally released in V16.0.
* Second parameter redefined in V18.0.
*****************************************************************************/
extern UGOPENINTEXPORT int UF_DISP_print_window_ug_image (
int format, /* <I> Specifies the format of the printed image.
0: A vector-format image is printed.
1: A raster-format (bitmap) image is printed.
If only wireframe views are displayed, then a
vector-format image is printed even if the
format parameter is set to 1. */
int color_usage /* <I> Specifies how color is used in the printed
image.
0: If a vector image is printed, line color is
determined by the setting of the Black Lines Only
option in the File->Print dialog. If a raster image
is printed, the image background is the same as the
background of the graphics window.
1: If a vector image is printed, line color is
determined by the setting of the Black Lines Only
option in the File->Print dialog. If a raster image
is printed, the image background is white.
2: If a vector image is printed, lines are printed
in color (or shades of gray on a monochrome printer).
If a raster image is printed, the image background
is the same as the background of the graphics
window.
3: If a vector image is printed, all lines are
printed in black. If a raster image is printed,
the image background is white. */
);
#undef EXPORTLIBRARY
#endif /* END UF_DISP_UGOPENINT_INCLUDED */