UF_DIE_wrap_binder_s (view source)
Defined in: uf_dieeng.h
Also known as:
- UF_DIE_binder_wrap_t
- UF_DIE_binder_wrap_p_t
Overview
The following structure is utilized in the functions:
UF_DIE_create_binder_wrap
UF_DIE_edit_binder_wrap
UF_DIE_ask_binder_wrap
UF_DIE_free_binder_wrap
NOTES:
The value character strings in the below structure can be a numeric value (e.g., "25"),
a fully defined expression (e.g., "p5 = 25"), an existing expression name (e.g., "p5"), or
an expression string (e.g., "p5+p7"). If the fully defined expression exists then an error
is returned. If the expression name does not exist an error is returned. In all other cases
an expression is created. When this value is returned from UF_CURVE_ask_trim, the character
string is a fully defined expression (e.g., "p5=25").
Environment
Internal and External
See Also
History
Originally released in V16.0
Data Members
input_type
defined_by
union UF_DIE_wrap_binder_union
material_thickness
char*
distance_tol
double
angle_tol
double
output_sw
Can be either UF_DIEENG_POINTS,
UF_DIEENG_BOUNDARY, or UF_DIEENG_SHEET.