/*
uf_dbc_mld.h
* File Description:
*
* This file contains the documentation required for using the User
* Function Interface to DBC_MOLD. DBC_MOLD is the module that allows
* NX MOLD to interface with the external database that stores the
* user's data. Note that this is not a UF layer for DBC; it only handles
* DBC_MOLD.
*
******************************************************************************/
#ifndef UF_DBC_MLD_H_INCLUDED
#define UF_DBC_MLD_H_INCLUDED
#include <uf_defs.h>
#include <uf_cam.h>
#include <libufun_cam_exports.h>
/********************************** Defines ***********************************/
/********************************** TypeDefs **********************************/
/* UF_DBC_MLD_id_t is the identifier for referring to a UF_DBC_MLD object */
typedef void *UF_DBC_MLD_id_t;
/* UF_DBC_MLD_sheet_t - the data structure into which a spreadsheet is read */
typedef void *UF_DBC_MLD_sheet_t;
/******************************* Prototypes **********************************/
/*****************************************************************************
* This function returns the UF_DBC_MLD_id_t that corresponds to the
* UF_CAM_exit_id_t passed to the User Exit from NX.
*
* Environment: Internal and External
*
* See Also:
*
* History: Originally released in V16.0
******************************************************************************/
extern UFUN_CAMEXPORT int UF_DBC_MLD_ask_dbc_mld
(
UF_CAM_exit_id_t exit_id, /* <I> - exit_id passed to exit from NX */
UF_DBC_MLD_id_t *dbc_mld_id /* <O> - the dbc_mld of this exit_id */
);
/*****************************************************************************
* This function creates an UF_DBC_MLD object. The 'object' returned is
* used in the other public functions of UF_DBC_MLD to identify the
* object to process.
*
* Environment: Internal and External
*
* See Also:
*
* History: Originally released in V16.0
******************************************************************************/
extern UFUN_CAMEXPORT int UF_DBC_MLD_create
(
UF_DBC_MLD_id_t *object /* <O> - the id of the created object */
);
/*****************************************************************************
* This function will execute the specified command in the interpreter
* associated with the specified UF_DBC_MLD object.
*
* Environment: Internal and External
*
* See Also:
*
* History: Originally released in V16.0
******************************************************************************/
extern UFUN_CAMEXPORT int UF_DBC_MLD_exec_command
(
UF_DBC_MLD_id_t dbc_mld_id, /* <I> - see above description */
const char *command /* <I> - the command to execute */
);
/*****************************************************************************
* Returns the sheet associated with the specified UF_DBC_MLD_id_t.
*
* Environment: Internal and External
*
* See Also:
*
* History: Originally released in V16.0
******************************************************************************/
extern UFUN_CAMEXPORT int UF_DBC_MLD_ask_sheet
(
UF_DBC_MLD_id_t object, /* <I> - see above description */
UF_DBC_MLD_sheet_t *sheet /* <O> - see above description */
);
/*****************************************************************************
* Assign the specified sheet to the specified UF_DBC_MLD_id_t.
*
* Environment: Internal and External
*
* See Also:
*
* History: Originally released in V16.0
******************************************************************************/
extern UFUN_CAMEXPORT int UF_DBC_MLD_set_sheet
(
UF_DBC_MLD_id_t object, /* <I> - see above description */
UF_DBC_MLD_sheet_t sheet /* <I> - see above description */
);
/*****************************************************************************
* Assign the specified string to the result in the interpreter associated
* with the specified UF_DBC_MLD_id_t. This will be the return value of
* the last TCL command executed in the interpreter.
*
* Environment: Internal and External
*
* See Also:
*
* History: Originally released in V16.0
******************************************************************************/
extern UFUN_CAMEXPORT int UF_DBC_MLD_set_interp_result
(
UF_DBC_MLD_id_t object, /* <I> - see above description */
const char *result /* <I> - see above description */
);
/*****************************************************************************
* Delete the specified UF_DBC_MLD object.
*
* Environment: Internal and External
*
* See Also:
*
* History: Originally released in V16.0
******************************************************************************/
extern UFUN_CAMEXPORT int UF_DBC_MLD_delete
(
UF_DBC_MLD_id_t object /* <I> - the object to delete */
);
#undef EXPORTLIBRARY
#endif /* UF_DBC_MLD_H_INCLUDED */