UF_CURVE_trim_incr_length_s (view source)
Defined in: uf_curve.h
Also known as:
- UF_CURVE_trim_incr_length_t
Overview
use the following structure when
trim_type == UF_CURVE_TRIM_TO_INCR_LENGTH
Data Members
string_trim_extend_end
value [ MAX_LINE_BUFSIZE ]
char
the string should be
trimmed or extended to the
bounding object, this
should be set to one of
the following values:
UF_CURVE_TRIM_EXTEND_START
UF_CURVE_TRIM_EXTEND_END