UF_CURVE_offset_draft_data_s (view source)
 
Defined in: uf_curve.h
 
Also known as:
 


Data Members

draft_height
char *
Distance between the plane of the input
curves (reference plane) to the plane of
the offset curves (offset plane)

draft_angle
char *
The angle from the offset vector to a line
perpendicular to the reference plane.

rough_type
int
1 for rough type, 0 otherwise
rough_type = 1 will produce a spline or
splines that approximate the offset curve(s).
The approximation may not be as accurate as
for the regular offset, but should be faster.