UF_CLONE_convert_cb_t | cb | Input | the callback reason indicating the answer needed |
const char * | input_part_specifier | Input | The name of a part in the current clone operation for which the specified answer is required; for import, an O/S filename; for export, a CLI name |
char * * | answer | Output | space should be allocated with UF_allocate_memory, user must free |
UF_CLONE_notify_cb_t | cb | Input | callback reason |
const char * | input_part_specifier | Input | The name of a part in the current clone operation; for import, an O/S filename; for export, a CLI name may be null if the cb applies to a whole clone operation |
const void* | data | Input | data, e.g. the name of the name about to be applied, or a pointer to an action type or a naming type, or a checkout action/cb pair |