/*
uf_cfi.h
File Description:
A set of Open C API subroutines is available for accessing files. These
routines provide a "C" interface to NX Open C API routines and
native files.
CAUTION
We recommend that you use standard C functions for file and directory
manipulations in lieu of the cfi routines in this file. These routines
will all be impacted by the UGII_OPTION environment variable. In
particular file specifications returned by functions such as uc4576
may be converted to lower case if UGII_OPTION=lower is set.
NOTE
These functions would not work with file names and folder names of
NX Manager and Teamcenter Engineering.
Use routines from uf_ugmgr
for this purpose.
File types are used to identify the contents of a file and are also used
to determine the default extension for a file. Note that for many cases
several files will have different extensions but the same contents
(e.g. text files). Note that many types do not have a name. These are
usually variations on a different file format but with a different
extension.
The following are the restrictions on the length of various items:
File Names are limited to UF_CFI_MAX_FILE_NAME_NCHARS characters
File Extensions are limited to 4 characters
Directory specifications are limited to MAX_FSPEC_NCHARS
characters
Full file specifications are limited to MAX_FSPEC_NCHARS
characters
Many of the Open C API CFI routines request a file type (ftype) as
input. This type is used to determine the default extension for a file
if none is supplied. The system does not add an extension if one is
included in the filespec. A file type of zero does not use any
extension.
For description of file formats see table
Many of the Open C API CFI routines return negative error numbers.
For description of these errors see table
******************************************************************************/
#ifndef UF_CFI_INCLUDED
#define UF_CFI_INCLUDED
#define UF_MAXWORD 32768 /*value of UF_MAXWORD is same as MAXWORD.*/
/***************************************************************************
***************************************************************************/
#include <uf_defs.h>
#include <uf_cfi_types.h>
/* The following must be the last include file */
#include <libufun_exports.h>
/* */
#define UF_MAX_UNIQUE_FILE_NAME_NCHARS 16
#define UF_MAX_UNIQUE_FILE_NAME_BUFSIZE NX_BUFSIZE(UF_MAX_UNIQUE_FILE_NAME_NCHARS)
/* */
#define UF_MAX_UNIQUE_FILE_NAME_SIZE (UF_MAX_UNIQUE_FILE_NAME_BUFSIZE)
/* */
/*******************************************************************************
Open a file for binary buffered I/O. The open mode
is used to indicate how the file is to be accessed.
The file format is used both to specify a default extension to use and
for the write modes, the type to be stored in the file's header. For the
read mode, a format of zero may be specified indicating no default
extension.
A native operating system file may be opened by using the
appropriate file type. For example, a format of 4 opens a text file in
the native file system.
A successful open returns a simple integer channel number. This
channel number is to be passed to the routines for reading, writing,
skipping, and closing the file.
uc4510 (read characters), uc4511 (read integers), uc4512 (read reals),
and uc4513 (read bytes) are used to read primitive data types from a
file open with uc4500. Combinations of these types may be used to
create more complex data types. The I/O channel number returned by uc4500
is passed to these other routines.
uc4520 (write characters), uc4521 (write integers), uc4522 (write
reals), and uc4523 (write bytes) are used to write primitive data types
to a file opened with uc4500. Combinations of these calls are used to
create more complex types. The I/O channel number returned by uc4500
is passed to these other routines.
uc4530 (skip characters), uc4531 (skip integers), uc4532 (skip reals),
and uc4533 (skip bytes) are used to bypass primitive data types in a
file opened with uc4500. A combination of these may be used to skip
over more complex types. Skips may be backward by using negative
skip counts.
For characters, the count will be rounded up to the next integer
boundary (e.g. a write/read/skip of 5 will actually write/read/skip 8
characters).
Return:
Return code:
<0 = error
>= 0 = i/o channel number
Environment: Internal and External
See Also:
uc4510
uc4511
uc4512
uc4513
uc4520
uc4521
uc4522
uc4523
For description of modes see table
For description of file formats see table
History:
*******************************************************************************/
extern UFUNEXPORT int uc4500(
const char * fspec ,/* <I>
File To Open
*/
int omode ,/* <I>
Open Mode
1 = Read
2 = Write
3 = Write, Replace
5 = Update
7 = Scratch
*/
int ftype /* <I>
File Format
*/
);
/*******************************************************************************
Open a text file for I/O. Only the routines uc4514,
uc4524, and uc4525 for reading and writing lines may be used on text
file. See the description of uc4500 for a description of the parameters.
For omode = 4, the file must exist and will be opened for write. The
file pointer will be initially positioned at the end of file.
For omode = 6, a printer is opened. If the filespec is blank, the
default printer will be opened.
Return:
Return code:
< 0 = error
>= 0 = I/O Channel Number
Environment: Internal and External
See Also:
uc4514a
uc4524
uc4525
For description of file types see table
History:
******************************************************************************/
extern UFUNEXPORT int uc4504(
const char * fspec ,/* <I>
File To Open
*/
int omode ,/* <I>
Open Mode
1 = Read
2 = Write
3 = Write, Replace
4 = Append
6 = Printer
*/
int ftype /* <I>
File Type
*/
);
/*******************************************************************************
Open a binary file for block I/O. Only the routines
uc4516 and uc4526 for reading and writing blocks may be used on a
file opened with uc4506. See the description of uc4500 for a
description of the parameters.
Return:
Return code:
> 0 = error
<= 0 = I/O Channel Number
Environment: Internal and External
See Also:
uc4516
uc4526
For description of file types see table
History:
*******************************************************************************/
extern UFUNEXPORT int uc4506(
const char * fspec ,/* <I>
File To Open
*/
int omode ,/* <I>
Open Mode
1 = Read
2 = Write
3 = Write, Replace
5 = Update
7 = Scratch
*/
int ftype /* <I>
File Type
*/
);
/*******************************************************************************
Open a file for record oriented I/O. Only the
routines uc4517 and uc4527 may be used to read and write records.
Record I/O is generally only supported for native files.
Return:
Return code:
< 0 = error
>= 0 = I/O Channel Number
Environment: Internal and External
See Also:
uc4517
uc4527
For description of file types see table
History:
*******************************************************************************/
extern UFUNEXPORT int uc4507(
const char * fspec ,/* <I>
File Specification
*/
int omode ,/* <I>
Open Mode
1 = Read
2 = Write
3 = Replace
5 = Update
7 = Scratch
*/
int ftype ,/* <I>
File Type
*/
int rectype /* <I>
Record Format
= 0 = Variable Length Records
> 0 = Fixed Record Length
*/
);
/*******************************************************************************
Open a directory for reading. Directory entries are read
using uc4518 with the fields picked out using uc4600 to uc4609.
Sub-directories may be opened using uc4509.
The dmode bit-mask is used to indicate the intention of the
application in using the directory. Bits zero through seven indicate
which fields from the file header to read and bits ten through thirteen
specify special directory options.
You can specify which bits to set by using the left shift operator in
conjuction with the bit wise or. For example, to set bits 11 and 13, you
would use the following declaration:
int dmode = (1 << 11) | (1 << 13);
A wildcard template may be used and is specified when the directory
is opened. It may be passed separate from the directory filespec or as
part of the directory filespec. For example:
dmode(bit 11) = 1, fspec = "disk/manager", wcard = "*.prt" will
return out all parts in the manager's directory.
If neither dmode(bit 11) or dmode(bit 12) is set then all files will be
returned. dmode(bit 11) and dmode(bit 12) should not be
set at the same time.
If dmode(bit 13) is set then the caller is only interested in the names
of the files and none of the header attributes. If this is set then none
of the parameter dmode(bit 0) through dmode(bit 7) should be set.
If dmode(bit 10) is set then the caller is intending to open
sub-directories. If it is not set then uc4509 should not be called.
Return:
Return code:
< 0 = error
>= 0 = I/O Channel Number
Environment: Internal and External
See Also:
uc4518
uc4600
uc4609
uc4509
For description of file types see table
History:
*******************************************************************************/
extern UFUNEXPORT int uc4508(
const char * fspec ,/* <I>
Directory Specification
*/
int dmode ,/* <I>
Bit-mask Of Open Options
bit 0 = Read Owner Field
0 = No
1 = Yes
bit 1 = Read Protection Classfield
0 = No
1 = Yes
bit 2 = Read Status Field
0 = No
1 = Yes
bit 3 = Read Length Field
0 = No
1 = Yes
bit 4 = Read Dates
0 = No
1 = Yes
bit 5 = Read Description Field
0 = No
1 = Yes
bit 6 = Read Customer Area Field
0 = No
1 = Yes
bit 7 = Read Machine Field
0 = No
1 = Yes
bit 8-9 = *Reserved*
bit 10 = Enable Sub-trees
0 = No
1 = Yes
bit 11 = Template Given
0 = No
1 = Yes, Template In wcard
bit 12 = Directory Contains Wildcards
0 = No
1 = Yes
bit 13 = Read Filenames Only
0 = No
1 = Yes
bit 14-15 = *Reserved*
*/
int ftype ,/* <I>
This argument is no longer used.
*/
const char * wcard /* <I>
Wildcard Template
*/
);
/*******************************************************************************
Open a subdirectory of the currently open directory.
The previous directory entry read by uc4518 must have been of type
directory (format 100-112) otherwise the error 'not a directory'
is returned. Subdirectories are closed using uc4549.
Environment: Internal and External
See Also:
uc4518
uc4549
History:
*******************************************************************************/
extern UFUNEXPORT int uc4509( void);
/*******************************************************************************
Read characters from a file opened with uc4500.
For characters, the count will be rounded up to the next integer
boundary (e.g. a read of 5 will actually read 8 characters).
Integer variables are used for storing the characters in byte format.
Environment: Internal and External
See Also:
uc4500
History:
*******************************************************************************/
extern UFUNEXPORT int uc4510(
int chan ,/* <I>
I/O Channel Number returned from uc4500.
*/
int len ,/* <I>
Number Of Characters To Read
*/
char cbuf[UF_MAXWORD] /* <O>
Array To Read Characters Into
*/
);
/*******************************************************************************
Read integers from a file opened with uc4500.
Environment: Internal and External
See Also:
uc4500
History:
*******************************************************************************/
extern UFUNEXPORT int uc4511(
int chan ,/* <I>
I/O Channel Number returned from uc4500.
*/
int len ,/* <I>
Number Of Integers To Read
*/
int * sibuff /* <O>
Array To Read Integers Into
*/
);
/*******************************************************************************
Read reals from a file opened with uc4500.
Environment: Internal and External
See Also:
uc4500
History:
*******************************************************************************/
extern UFUNEXPORT int uc4512(
int chan ,/* <I>
I/O Channel Number returned from uc4500
*/
int len ,/* <I>
Number Of Reals To Read
*/
double rbuff[] /* <O>
Array To Read Reals Into
*/
);
/*******************************************************************************
Read bytes from a file opened with uc4500.
Environment: Internal and External
See Also:
History:
*******************************************************************************/
extern UFUNEXPORT int uc4513(
int chan ,/* <I>
I/O Channel Number returned by uc4500
*/
int len ,/* <I>
Number Of Bytes To Read
*/
char bbuf[UF_MAXWORD] /* <O>
Array To Read Bytes Into
*/
);
/*******************************************************************************
Read a line of text from a file opened with uc4504.
Return:
Return code
< 0 = Error
>= 0 = Length Of Line Read
Environment: Internal and External
See Also:
uc4504
History:
*******************************************************************************/
extern UFUNEXPORT int uc4514a(
int chan ,/* <I>
I/O channel number returned by uc4504
*/
char **cbuf /* <OF>
Line read. The buffer must be freed with UF_free()
*/
);
/*******************************************************************************
Randomly read blocks from a file opened with
uc4506. Data is always read on a block boundary.
Return:
Return code
< 0 = Error
> 0 = Number of bytes actually read
Environment: Internal and External
See Also:
uc4506
History:
*******************************************************************************/
extern UFUNEXPORT int uc4516(
int chan ,/* <I>
I/O channel number returned by uc4506
*/
int block ,/* <I>
Starting block number to read (from 0)
*/
int bytes ,/* <I>
Number of bytes to read
*/
char *cbuf /* <O>
Data read
*/
);
/*******************************************************************************
Read the next record from a file opened using uc4507.
Environment: Internal and External
See Also:
uc4507
History:
*******************************************************************************/
extern UFUNEXPORT int uc4517(
int chan ,/* <I>
I/O channel number returned by uc4507
*/
int * bytes ,/* <O>
Length of record read in bytes
*/
char *cbuf /* <O>
Array to read record into
*/
);
/*******************************************************************************
Read the next directory entry and save the entry's
information in memory. This information may then be accessed by the
routines uc4600 through uc4609.
Return:
Return code
< 0 = Error
0 = Entry Read
1 = End Of Subdirectory
2 = End Of Directory
Environment: Internal and External
See Also:
uc4508
History:
*******************************************************************************/
extern UFUNEXPORT int uc4518( void );
/*******************************************************************************
Returns the full filespec of the last directory entry
read. This is provided so the Open C API program need not be
concerned with the syntax of filespecs in forming them.
Environment: Internal and External
See Also:
uc4508
History:
*******************************************************************************/
extern UFUNEXPORT int uc4519(
char fspec[MAX_FSPEC_BUFSIZE] /* <O>
Full file specification of the last directory
entry read.
*/
);
/*******************************************************************************
Write characters to a file opened with uc4500.
The count will be rounded up to the next integer
boundary (e.g. a write of 5 will actually write 8 characters).
Environment: Internal and External
See Also:
uc4500
History:
*******************************************************************************/
extern UFUNEXPORT int uc4520(
int chan ,/* <I>
I/O channel number returned by uc4500.
*/
long len ,/* <I>
Number of characters to write
*/
const char * cbuff /* <I>
Character data to write
*/
);
/*******************************************************************************
Write integers to a file opened with uc4500.
Environment: Internal and External
See Also:
uc4500
History:
*******************************************************************************/
extern UFUNEXPORT int uc4521(
int chan ,/* <I>
I/O channel number returned by uc4500
*/
long len ,/* <I>
Number of integers to write
*/
int * sibuff /* <I>
Integer data to write
*/
);
/*******************************************************************************
Write reals to a file opened with uc4500.
Environment: Internal and External
See Also:
History:
*******************************************************************************/
extern UFUNEXPORT int uc4522(
int chan ,/* <I>
I/O channel number returned by uc4500
*/
long len ,/* <I>
Number of reals to write
*/
double rbuff[] /* <I>
Real data to write
*/
);
/*******************************************************************************
Write bytes to a file opened with uc4500.
Environment: Internal and External
See Also:
uc4500
History:
*******************************************************************************/
extern UFUNEXPORT int uc4523(
int chan ,/* <I>
I/O channel number returned by uc4500
*/
long len ,/* <I>
Number of bytes to write
*/
const void * bbuff /* <I>
Byte data to write
*/
);
/*******************************************************************************
Write a line to a text file. Only complete lines may
be written to a text file. The addition of any delimiters (e.g. newline)
is done automatically.
Environment: Internal and External
See Also:
uc4504
History:
*******************************************************************************/
extern UFUNEXPORT int uc4524(
int chan ,/* <I>
I/O channel number returned by uc4504
*/
const char * cbuf /* <I>
Line to write
*/
);
/*******************************************************************************
uc4525 is used to write a page break to a text file.
Environment: Internal and External
See Also:
uc4504
History:
*******************************************************************************/
extern UFUNEXPORT int uc4525(
int chan /* <I>
I/O channel number returned by uc4504
*/
);
/*******************************************************************************
Randomly write to a file opened with uc4506. The
data is always written on a block boundary.
Environment: Internal and External
See Also:
uc4506
History:
*******************************************************************************/
extern UFUNEXPORT int uc4526(
int chan ,/* <I>
I/O channel number returned by uc4506
*/
int block ,/* <I>
Starting block number to write (from 0)
*/
int bytes ,/* <I>
Number of bytes to write
*/
const char * buf /* <I>
Data to write
*/
);
/*******************************************************************************
Write a record to a file opened with uc4507. For fixed
length record files, the parameter bytes is ignored.
Environment: Internal and External
See Also:
uc4507
History:
*******************************************************************************/
extern UFUNEXPORT int uc4527(
int chan ,/* <I>
I/O channel number returned by uc4507
*/
int bytes ,/* <I>
Length of record to write in bytes
*/
const char * cbuf /* <I>
Buffer containing data to write
*/
);
/*******************************************************************************
Skip characters in a file opened with uc4500.
Skips may be backward by using negative skip counts.
Environment: Internal and External
See Also:
uc4500
History:
*******************************************************************************/
extern UFUNEXPORT int uc4530(
int chan ,/* <I>
I/O channel number returned by uc4500
*/
long len /* <I>
Number of characters to skip over
*/
);
/*******************************************************************************
Skip integers in a file opened with uc4500.
Skips may be backward by using negative skip counts.
Environment: Internal and External
See Also:
History:
*******************************************************************************/
extern UFUNEXPORT int uc4531(
int chan ,/* <I>
I/O channel number returned by uc4500
*/
long len /* <I>
Number of integers to skip over
*/
);
/******************************************************************************
Skip reals in a file opened with uc4500.
Skips may be backward by using negative skip counts.
Environment: Internal and External
See Also:
History:
*******************************************************************************/
extern UFUNEXPORT int uc4532(
int chan ,/* <I>
I/O channel number returned by uc4500
*/
long len /* <I>
Number of reals to skip over
*/
);
/*******************************************************************************
Skip bytes in a file opened with uc4500.
Skips may be backward by using negative skip counts.
Environment: Internal and External
See Also:
History:
*******************************************************************************/
extern UFUNEXPORT int uc4533(
int chan ,/* <I>
I/O channel number returned by uc4500
*/
long len /* <I>
Number of bytes to skip over
*/
);
/******************************************************************************
Find the current position within a file opened with
uc4500. That position may then be restored using uc4535.
Return:
Return code:
< 0 = Error
>= 0 = File position
Environment: Internal and External
See Also:
uc4500
uc4535
History:
*******************************************************************************/
extern UFUNEXPORT long uc4534(
int chan /* <I>
I/O channel number returned by uc4500
*/
);
/*******************************************************************************
Restore the read/write position within a file
previously saved using uc4534. The file must have been opened with
uc4500.
Environment: Internal and External
See Also:
uc4500
uc4534
History:
*******************************************************************************/
extern UFUNEXPORT int uc4535(
int chan ,/* <I>
I/O channel number returned by uc4500
*/
long pos /* <I>
File position returned by uc4534
*/
);
/*******************************************************************************
Reposition a file back to the beginning. This may be
used for binary, text, and record I/O files.
Environment: Internal and External
See Also:
History:
*******************************************************************************/
extern UFUNEXPORT int uc4536(
int chan /* <I>
I/O channel number
*/
);
/******************************************************************************
Close a file opened with either uc4500, uc4504,
uc4506, or uc4507. The close disposition is used to indicate whether a
file opened for write is to be saved or not. A normal close will make
the file permanent and delete any previous file with the same name.
An abort close will delete the file and retain any previous file with the
same name.
Environment: Internal and External
See Also:
History:
*******************************************************************************/
extern UFUNEXPORT int uc4540(
int chan ,/* <I>
I/O channel number
*/
int disp /* <I>
Disposition
0 = Normal close
1 = Abort close
*/
);
/*******************************************************************************
Determine characteristics of an open file given its I/O channel number.
The integer date/times in qreslt (if qreslt = 6) can be converted to
character strings using uc4582.
Starting in NX 11 a query type of 5 is no longer supported.
Environment: Internal and External
See Also:
For description of file types see table
History:
*******************************************************************************/
extern UFUNEXPORT int uc4544(
int chan ,/* <I>
I/O channel number
*/
int qitem ,/* <I>
Item to inquire:
1 = File System
2 = File Type
3 = Last Error
4 = Record Format
6 = Creation, Modify, Access
Dates
*/
int * qreslt /* <O>
Query result:
For qreslt = 1,
2 = NATIVE
For qreslt = 2,
See File Types
For qreslt = 3, Last read or write error
For qreslt = 4,
= 0 = Variable length records
> 0 = Fixed record length
For qreslt = 6, qreslt is an array of 6 integers
(0)-(1) = Creation Date,Time
(2)-(3) = Modification Date,Time
(4)-(5) = Last Access Date,Time
*/
);
/*******************************************************************************
Determines the file length (in bytes) of
an open file given its I/O channel number.
Environment: Internal and External
See Also:
History:
*******************************************************************************/
extern UFUNEXPORT int uc4547(
int chan ,/* <I>
I/O channel number
*/
int qitem ,/* <I>
Item to query
1 = File length in bytes
*/
int * qreslt /* <O>
Query result
*/
);
/*******************************************************************************
Close any directories opened with uc4508. If any
subdirectories are open, they will be closed as well.
Environment: Internal and External
See Also:
uc4508
History:
*******************************************************************************/
extern UFUNEXPORT int uc4548( void );
/*******************************************************************************
Close a subdirectory opened with uc4509. Directory
reads will then continue with the previous directory.
Environment: Internal and External
See Also:
uc4509
History:
*******************************************************************************/
extern UFUNEXPORT int uc4549( void );
/*******************************************************************************
Checks whether the specified file of the given type exists.
NOTE: Mixed or upper case file names may not be found if the
environment variable UGII_OPTION = LOWER is set.
Passing an ftype of 0 will look for a file but does not work for a directory.
To check for a directory the ftype must be set to 100.
Return:
Return code:
< 0 = Error
= 0 = File Exists
= 1 = File Does Not Exist
Environment: Internal and External
See Also:
For description of file types see table
History:
*******************************************************************************/
extern UFUNEXPORT int uc4560(
const char * fspec ,/* <I>
File to check
*/
int ftype /* <I>
File type
0 will check for files
100 will check for directories
*/
);
/*******************************************************************************
Remove a given file from the file system.
Environment: Internal and External
See Also:
For description of file types see table
History:
*******************************************************************************/
extern UFUNEXPORT int uc4561(
const char * fspec ,/* <I>
File to delete
*/
int ftype /* <I>
File type
*/
);
/*******************************************************************************
Change the name of a given file. The new file name
should be a simple name (e.g. no directory specification).
Environment: Internal and External
See Also:
For description of file types see table
History:
*******************************************************************************/
extern UFUNEXPORT int uc4562(
const char * fspec ,/* <I>
Old file name
*/
int ftype ,/* <I>
File type
*/
const char * fspec2 /* <I>
New file name
*/
);
/*******************************************************************************
Create an empty directory.
Environment: Internal and External
See Also:
History:
*******************************************************************************/
extern UFUNEXPORT int uc4563(
const char * fspec ,/* <I>
Directory to create
*/
int ftype /* <I>
File type
*/
);
/******************************************************************************
Retrieve the header information of a single file and
store it in memory. The information may then be retrieved using
uc4600 through uc4609.
Environment: Internal and External
See Also:
uc4600
uc4601
uc4602
uc4603
uc4605
uc4606
uc4607
uc4608
uc4609
For description of file types see table
History:
*******************************************************************************/
extern UFUNEXPORT int uc4564(
const char * fspec ,/* <I>
File specification from which to read header
*/
int ftype ,/* <I>
File type
*/
int fmode /* <I>
Bit-mask Specifying Header Fileds Desired
bit 0 = Read Owner Field
0 = No
1 = Yes
bit 1 = Read Protection Class Field
0 = No
1 = Yes
bit 2 = Read Status Field
0 = No
1 = Yes
bit 3 = Read Length Field
0 = No
1 = Yes
bit 4 = Read Dates
0 = No
1 = Yes
bit 5 = Read Description Field
0 = No
1 = Yes
bit 6 = Read Customer Area Field
0 = No
1 = Yes
bit 7 = Read Machine Field
0 = No
1 =yes
bit 8-15 = *Reserved*
*/
);
/*******************************************************************************
Read the current default value for a directory.
Environment: Internal and External
See Also:
History:
*******************************************************************************/
extern UFUNEXPORT int uc4565(
int def ,/* <I>
Default to read:
1 = Current directory
2 = '$' directory
3 = '!' directory
*/
char fspec[MAX_FSPEC_BUFSIZE] /* <O>
Current Setting
*/
);
/******************************************************************************
Change the current user's directory.
Environment: Internal and External
See Also:
History:
*******************************************************************************/
extern UFUNEXPORT int uc4566(
int def ,/* <I>
Default to change:
1 = Current directory
2 = '$' directory
3 = '!' directory
*/
const char * fspec /* <I>
New default value
*/
);
/*******************************************************************************
Copies or moves a file from a source file specification to a destination file
specification. When any move option is used, the source file will only be
deleted after it has been successfully copied to the destination file.
Using a file type of -1 indicates "any file type" so changing extensions
during the copy or move operation will work correctly.
Environment: Internal and External
See Also:
For description of file types see table ENDSAMPLE
History:
*******************************************************************************/
extern UFUNEXPORT int uc4567(
const char * srcspc ,/* <I>
Source file specification
*/
const char * dstspc ,/* <I>
Destination file specification
*/
int cmode ,/* <I>
Specifies Copy/Move Options:
= UF_CFI_COPY_NEVER_REPLACE
= UF_CFI_COPY_ALWAYS_REPLACE
= UF_CFI_COPY_REPLACE_IF_NEWER
= UF_CFI_COPY_LEGACY (same as UF_CFI_COPY_NEVER_REPLACE)
= UF_CFI_MOVE_NEVER_REPLACE
= UF_CFI_MOVE_ALWAYS_REPLACE
= UF_CFI_MOVE_REPLACE_IF_NEWER
= UF_CFI_MOVE_LEGACY (same as UF_CFI_MOVE_NEVER_REPLACE)
*/
int stype ,/* <I>
Source file type
*/
int dtype /* <I>
Destination file type
*/
);
/*******************************************************************************
Examine a filespec and make sure it conforms to the syntax of the file
system.
Environment: Internal and External
See Also:
For description of file types see table
History:
*******************************************************************************/
extern UFUNEXPORT int uc4570(
const char * fspec ,/* <I>
File specification to validate
*/
int ftype /* <I>
File type
*/
);
/*******************************************************************************
Examine a filespec and make sure it is a valid directory specification for
the file system. A "directory file spec" is a path to a file which is a
directory.
Environment: Internal and External
See Also:
For description of file types see table
History:
*******************************************************************************/
extern UFUNEXPORT int uc4571(
const char * fspec ,/* <I>
Directory File Specification To Validate
*/
int ftype /* <I>
File Type
*/
);
/*******************************************************************************
Examine a filespec and make sure it is a valid wildcard directory specification
for the file system. This will also indicate whether there were any
wildcard characters in the filespec. To find all files that match the wildcard
filespec, open the directory with uc4508 and supply the wildcard filespec,
then read (uc4518) each matching entry and the corresponding filespec (uc4519).
Return:
Return code:
= 0 = Valid file specification
= 1 = Valid with wildcards
Anything else is an error
Environment: Internal and External
See Also:
For description of file types see table
History:
*******************************************************************************/
extern UFUNEXPORT int uc4572(
const char * fspec ,/* <I>
File specification to validate
*/
int ftype /* <I>
File type
*/
);
/*******************************************************************************
Given a filespec return its fully qualified equivalent. If
a non-zero file type is given, the extension will also be set. For
example, the native system with a default directory DISK2/JOE
fspec = "foo", type = 2 will produce expfspec = "DISK2/JOE/FOO.PRT"
Environment: Internal and External
See Also:
For description of file types see table
History:
*******************************************************************************/
extern UFUNEXPORT int uc4573(
const char * fspec ,/* <I>
File specification to expand
*/
int ftype ,/* <I>
File type
*/
char expfspec[MAX_FSPEC_BUFSIZE] /* <O>
Expanded file specification
*/
);
/*******************************************************************************
Accept a filespec and removes any directory path, extension,
and any system specific information and returns the resultant simple
filename. For example:
fspec = "/DISK1/JOE/FOO.PRT", ftype = 2 will produce fname = "FOO".
Environment: Internal and External
See Also:
For description of file types see table
History:
*******************************************************************************/
extern UFUNEXPORT int uc4574(
const char * fspec ,/* <I>
File specification from which to extract name
*/
int ftype ,/* <I>
File type
*/
char fname[UF_CFI_MAX_FILE_NAME_BUFSIZE] /* <O>
Simple file name
*/
);
/*******************************************************************************
Combine a directory with a filename producing a file specification (filespec).
For example:
dspec = "/manager", ftype = 2, fname = "bar"
will produce fspec = "/MANAGER/BAR.PRT".
If the file name is a directory, using a filetype of 100 will merge the
directories. For example:
dspec = "/manager", ftype = 100, fname = "bar"
will produce fspec = "/MANAGER/BAR".
Environment: Internal and External
See Also:
For description of file types see table
History:
*******************************************************************************/
extern UFUNEXPORT int uc4575(
const char * dspec ,/* <I>
Directory
*/
int ftype ,/* <I>
File type
*/
const char * fname ,/* <I>
File name
*/
char fspec[MAX_FSPEC_BUFSIZE] /* <O>
Resultant file specification
*/
);
/*******************************************************************************
Take a filespec and returns its directory and filename components. For example:
fspec = "/Manager/Work/BENCH", ftype = 2
Note that this routine is impacted by the UGII_OPTION environment variable,
so if UGII_OPTION=lower is set, then the above example will produce:
dspec = "/manager/work" and fname = "bench.prt".
Environment: Internal and External
See Also:
For description of file types see table
History:
*******************************************************************************/
extern UFUNEXPORT int uc4576(
const char * fspec ,/* <I>
File specification to split up
*/
int ftype ,/* <I>
File type
*/
char dspec[MAX_FSPEC_BUFSIZE] ,/* <O>
Directory component
*/
char fname[UF_CFI_MAX_FILE_NAME_BUFSIZE] /* <O>
File name component
*/
);
/*******************************************************************************
The name returned is a unique name for a temporary file. The resultant
filename is unique from other processes at the time. From a single
process, filenames will begin duplicating after the first 1,679,615 calls
to uc4577. Temporary files should be deleted when no longer needed by an
application. If the files are not deleted, there is a chance that the same
name may come up again if the same user happens to get the same process id
on a later date.
The maximum number of characters which will be returned is 12.
Environment: Internal and External
See Also:
History:
*******************************************************************************/
extern UFUNEXPORT int uc4577(
char fname[UF_MAX_UNIQUE_FILE_NAME_BUFSIZE] /* <O>
Unique filename
*/
);/* <WRAPAS:UF_CFI_get_unique_filename> */
/*******************************************************************************
Remove the file extension from a given file specification and
returns the resultant file specification.
Environment: Internal and External
See Also:
For description of file types see table
History:
*******************************************************************************/
extern UFUNEXPORT int uc4578(
const char * fspec ,/* <I>
File specification
*/
int ftype ,/* <I>
File type
*/
char dspec[MAX_FSPEC_BUFSIZE] /* <O>
Resultant file specification
*/
);
/*******************************************************************************
Form the full filespec, given a simple name of a file
in the UGII_UTIL directory.
Environment: Internal and External
See Also:
For description of file types see table
History:
*******************************************************************************/
extern UFUNEXPORT int uc4579(
const char * fname ,/* <I>
File name
*/
int ftype ,/* <I>
File type
*/
char fspec[MAX_FSPEC_BUFSIZE] /* <O>
Resultant file specification
*/
);
/*******************************************************************************
return the four character symbolic name for a given ftype
code (e.g.: 'PART' for ftype code 2). Many ftype codes will return
'TEXT' which indicates the file's contents may be displayed as ascii
data. Unnamed ftypes will have their numeric code returned in ascii.
Return:
Return code:
< 0 = Error
= 0 = Format Returned
= 1 = Format Undefined
Environment: Internal and External
See Also:
For description of file types see table
History:
*******************************************************************************/
extern UFUNEXPORT int uc4580(
int ftype ,/* <I>
File type
*/
char symb[5] /* <O>
Symbolic name
*/
);
/******************************************************************************
Convert the symbolic character representation of a file type
into its numeric equivalent. For example, "PART" translates to a 2.
Return:
Return code:
= 0 = Unknown Symbolic Name
> 0 = File Type
Environment: Internal and External
See Also:
History:
*******************************************************************************/
extern UFUNEXPORT int uc4581(
const char * symb /* <I>
Symbolic file type
*/
);
/*******************************************************************************
Convert NX computational time to display form. Two forms are available
for the date and two forms are available for the time.
A date or time of -1 returns the current date and/or time.
NOTE: In option 9 of the dtype argument, "formatted for the locale"
means that the date and time string is appropriate for the language in
which the user's operating system environment runs under.
Return:
Return code:
0 = No error
not 0 = Error code
Environment: Internal and External
See Also:
uc4583
History:The dtype argument was modified in V13.0 to
increase the number of options from 4 to 9.
*******************************************************************************/
extern UFUNEXPORT int uc4582(
int date[2] ,/* <I>
Computational time:
[0] Date
[1] Time
*/
int dtype ,/* <I>
Date And time representation:
1 = mm/dd/yy, hh:mm
2 = mm/dd/yy, hh:mm xM
3 = dd-mmm-yy, hh:mm
4 = dd-mmm-yy, hh:mm xM
5 = mm/dd/yyyy, hh:mm
6 = mm/dd/yyyy, hh:mm xM
7 = dd-mmm-yyyy, hh:mm
8 = dd-mmm-yyyy, hh:mm xM
9 = Formatted for the locale
where 'mm' = numeric month,
'dd' = day,
'yy' = two digit year,
'yyyy' = four digit year,
'mmm' = symbolic month,
'hh' = hour,
'mm' = minute,
'x' = 'A' or 'P'
When a blank is passed in for 'x', dtype = 8 will default to
12 hour time format where dtype = 7 will display a 24 hour time format.
Note: On Windows any string can be specified as AM/PM by using
Control Panel -> Regional and Language Options -> Customize -> Regional Options -> Time
*/
char date_string[21] ,/* <O>
Date (20 characters max)
*/
char time[21] /* <O>
Time (20 characters max)
*/
);
/*******************************************************************************
Convert a character date and time to NX computational date and time.
Return:
Return Code:
0 = Success
1 = Failure
Environment: Internal and External
See Also:
uc4582
History:
*******************************************************************************/
extern UFUNEXPORT int uc4583(
const char * date ,/* <I>
Date in any of the following forms
MM/DD/YY
DD-MMM-YY
DDMMMYY
MM/DD/YYYY
DD-MMM-YYYY
DDMMMYYYY
If date is blank, the current date is used
*/
const char * time ,/* <I>
Time in either of the following forms
HH:MM
HH:MM xM (x = 'A' or 'P')
If time is blank, the current time is used
*/
int* dandt /* <O>
Date And Time
(1) = Computational Date
(2) = Computational Time
*/
);
/******************************************************************************
Query the user name, String Result
Environment: Internal and External
See Also:
History:
*******************************************************************************/
extern UFUNEXPORT int uc4595(
int qitem ,/* <I>
Item to query:
1 = Username
*/
char str[17] /* <O>
Query result. This must be a buffer big enough to hold the user
name.
*/
);
/******************************************************************************
Query a set of characteristics. The result for each item code follows:
Login Status: (qitem = 1)
bit 0 = Login Status
0 = NOT LOGGED IN
1 = LOGGED IN
bit 1 = Username Status
0 = DO NOT NEED A USERNAME TO LOGIN
1 = USERNAME NEEDED FOR LOGIN
bit 2 = Password Status
0 = DO NOT NEED A PASSWORD TO LOGIN
1 = PASSWORD NEEDED FOR LOGIN
bits 3-15 = *Reserved*
File Header Support: (qitem = 2)
bit 0 = Owner Supported
0 = NO
1 = YES
bit 1 = Protection Classes Supported
0 = NO
1 = YES
bit 2 = Status Word Supported
0 = NO
1 = YES
bit 3-4 = *Reserved*
bit 5 = Description Supported
0 = NO
1 = YES
bit 6 = Customer Area Supported
0 = NO
1 = YES
bit 7 = Non-Native Files Supported
0 = NO
1 = YES
bits 8-15 = *Reserved*
Environment: Internal and External
See Also:
History:
*******************************************************************************/
extern UFUNEXPORT int uc4596(
int qitem ,/* <I>
Item to query
1 = Login status
2 = File header fields supported
*/
int * qreslt /* <O>
Query result
*/
);
/******************************************************************************
Translate an error code to the text associated with it.
Due to the way error handling is done in the file system routines, the
error text should be retrieved before another error occurs otherwise
the error message might be lost.
Environment: Internal and External
See Also:
History:
******************************************************************************/
extern UFUNEXPORT int uc4599(
int ug_errorno ,/* <I>
Error Code
*/
char errstg[ MAX_LINE_BUFSIZE ] /* <O>
Error Text
*/
);
/******************************************************************************
Return the simple file name of the last file read with uc4518 or uc4564..
To obtain the full file specification, including the directory use uc4519.
Environment: Internal and External
See Also:
uc4518
uc4564
uc4519
History:
*******************************************************************************/
extern UFUNEXPORT int uc4600(
char fname[UF_CFI_MAX_FILE_NAME_BUFSIZE] /* <O>
Filename
*/
);
/******************************************************************************
Return the file type of the last file read with uc4518 or uc4564..
You may use uc4581 to translate the file type to a character string.
Return:
Return code:
< 0 = error
>= 0 = file type
Environment: Internal and External
See Also:
uc4518
uc4564
uc4581
History:
*******************************************************************************/
extern UFUNEXPORT int uc4601( void );
/******************************************************************************
Return the status word of the last file read with uc4518 or uc4564..
Environment: Internal and External
See Also:
uc4518
uc4564
History:
*******************************************************************************/
extern UFUNEXPORT int uc4602(
int * fsts /* <O>
Status word
*/
);
/******************************************************************************
Return the owner of the last file read with uc4518 or uc4564..
Environment: Internal and External
See Also:
uc4518
uc4564
History:
*******************************************************************************/
extern UFUNEXPORT int uc4603(
char owner[17] /* <O>
Owner of file (16 characters max)
*/
);
/******************************************************************************
Return the length of the last file read with uc4518 or uc4564..
Return:
Return code:
>= 0 = File Length In Bytes
< 0 = error code
Environment: Internal and External
See Also:
uc4518
uc4564
History:
******************************************************************************/
extern UFUNEXPORT long uc4605( void );
/******************************************************************************
Return the creation, modification, and last access date/time
of the last file read with uc4518 or uc4564..
Use uc4582 to convert the date/time to character strings.
Environment: Internal and External
See Also:
uc4518
uc4564
uc4582
History:
*******************************************************************************/
extern UFUNEXPORT int uc4606(
int * cdate ,/* <O>
Two word array containing the creation date and time
*/
int * mdate ,/* <O>
Two word array containing the modification date and time
*/
int * ldate /* <O>
Two word array containing the last access date and time
*/
);
/******************************************************************************
Return the descriptions area of the last file read with uc4518 or uc4564..
Environment: Internal and External
See Also:
uc4518
uc4564
History:
*******************************************************************************/
extern UFUNEXPORT int uc4607(
char darea[ MAX_LINE_BUFSIZE ] /* <O>
Description Area (132 characters max)
*/
);
/******************************************************************************
Return the customer area of the last file read with uc4518 or uc4564..
Environment: Internal and External
See Also:
uc4518
uc4564
History:
*******************************************************************************/
extern UFUNEXPORT int uc4608(
char carea[ MAX_LINE_BUFSIZE ] /* <O>
Customer area (132 characters max)
*/
);
/******************************************************************************
Return the machine field of the last file read with uc4518 or uc4564.
These values are available for part files only. Parts filed in
V10.0 or earlier return unknown values.
Return:
Return code:
< 0 = error
1 = APOLLO
2 = DEC VAX/VMS
3 = HP CISC
4 = HP RISC
5 = SUN 3
6 = SUN SPARC
7 = DEC RISC (ULTRIX)
8 = SGI
9 = DATA GENERAL
10 = IBM MVS
11 = IBM AIX
12 = AXP/OSF
13 = AXP/VMS
Environment: Internal and External
See Also:
uc4518
uc4564
History:
*******************************************************************************/
extern UFUNEXPORT int uc4609( void );
/******************************************************************************
Modify the status header field of a file. An error returns if the file
system does not support a status field or the user does not have the privilege
to change it.
Environment: Internal and External
See Also:
For description of file types see table
History:
*******************************************************************************/
extern UFUNEXPORT int uc4612(
const char * fname ,/* <I>
File name
*/
int ftype ,/* <I>
File type
*/
int fsts /* <I>
New status value
*/
);
/******************************************************************************
Modify the owner header field of a file. An error returns if the file system
does not support an owner field or the user does not have the privilege to
change it (some operating systems may require root privilege to change file
ownership).
Environment: Internal and External
See Also:
For description of file types see table
History:
*******************************************************************************/
extern UFUNEXPORT int uc4613(
const char * fname ,/* <I>
File name to change the owner of
*/
int ftype ,/* <I>
File type
*/
const char * owner /* <I>
New owner value
*/
);
/******************************************************************************
Change the description header field of a file. An
error is returned if the file system does not support a description field or
the user does not have the privilege to change it.
Environment: Internal and External
See Also:
For description of file types see table
History:
*******************************************************************************/
extern UFUNEXPORT int uc4617(
const char * fname ,/* <I>
File name to change description of
*/
int ftype ,/* <I>
File type
*/
const char * desc /* <I>
New description value
*/
);
/******************************************************************************
Change the customer area header field of a file. An
error will be returned if the file system does not support a customer
area field or the user does not have the privilege to change it.
This function modifies the part file on disk and should not
be used on a part file that has already been opened in NX. If this
occurs, the part cannot be saved. Use UF_PART_set_customer_area to
modify the customer area of a loaded part.
Environment: Internal and External
See Also: UF_PART_set_customer_area
For description of file types see table
History:
*******************************************************************************/
extern UFUNEXPORT int uc4618(
const char * fname ,/* <I>
File name to change the customers area of
*/
int ftype ,/* <I>
File type
*/
const char * carea /* <I>
New customer area value
*/
);
/******************************************************************************
Read a switch from the program command line given the name of the switch.
All switches are global switches; they may appear anywhere on the command line.
Switches may have a value or no value. For example:
/LIST=FOO.LIS switch with a value
/LIST switch with no value
The characters that must match should be specified using upper case characters.
The user entered switch must completely match, but matching is case insensitive.
So if the program passes:
"PARTfile"
as the switch, then the following user entries will match:
-part=abc
-partfi=abc
-partfile=abc
-PARTFILE=abc
And the following user entries will not match:
-p=abc // Not enough characters
-parti=abc // the i does not match the specified f
Under UNIX, switches take the form:
-name no value
-name=value switch with a value
Switches are separated by blanks on UNIX. For example:
ugraf -user=manager -pass=frogs
Under WNT, switches take the form:
-name no value
-name:value switch with a value
-name=value switch with a value
NOTE: Use uc4624 in conjunction with this function. You must call
uc4624 before calling either uc4620 or uc4621.
Return:
Return code:
< 0 = Error
0 = Switch Not Present
1 = Switch Found With No Value
3 = Switch Found With A Value
Environment: External
See Also:
uc4624
uc4621
History:
*******************************************************************************/
extern UFUNEXPORT int uc4620(
const char * sname ,/* <I>
Switch name
*/
char swstg[ MAX_LINE_BUFSIZE ] /* <O>
Switch value
*/
);
/******************************************************************************
Read arguments from the command line. Each argument may be read only once.
NOTE: Use uc4624 in conjunction with this function. You must call
uc4624 before calling either uc4620 or uc4621.
Return:
Return code:
< 0 = Error
0 = Argument Not Present
1 = Argument Found
Environment: External
See Also:
uc4624
uc4620
History:
*******************************************************************************/
extern UFUNEXPORT int uc4621(
char nxtarg[MAX_FSPEC_BUFSIZE] /* <O>
Argument Value
*/
);
/*******************************************************************************
Returns an argument list to the GRIP xspawn command. The returned string
can not exceed 132 characters.
Environment: Internal and External
See Also:
History:
*******************************************************************************/
extern UFUNEXPORT int uc4622(
char *ip1 /* <I>
The return argument list
*/
);
/******************************************************************************
Returns a pointer to a string which is the release number of the
specified part file. Some of the possible values are shown for the
description of cr2. You must allocate sufficient size for the relnum
array. For example, you could use MAX_FSPEC_BUFSIZE (prototyped in
uf_defs.h) for the size of the array.
Environment: Internal and External
See Also:
History:
******************************************************************************/
extern UFUNEXPORT int uc4623(
const char * fspec ,/* <I>
Part file name
*/
char relnum[133] /* <O>
Release number
An example of possible Return Values are: V8, V9,
V10, V10.1, V10.2, V10.3 etc.
*/
);
/******************************************************************************
Save argument names for use with uc4620 and uc4621. The prog
parameter is not used. It is only present for backward compatibility.
You must use uc4624 before calling uc4620 or uc4621.
Note that uc4624 expects to receive the argc and argv values passed to the
program from main, and so the values in argv are assumed to be in the current
users locale not UTF8 data. As such this routine does not honor the setting of the text
mode made by calling UF_TEXT_set_text_mode().
Environment: External
See Also:
uc4620
uc4621
History:
*******************************************************************************/
extern UFUNEXPORT int uc4624(
int prog ,/* <I>
Not used
*/
int argc ,/* <I>
Argument count
*/
char ** argv /* <I>
array of argument names. This data is always assumed to be in
the users current locale.
*/
);
/*******************************************************************************
Outputs a sorted directory listing to the Information Window if it has
been opened. Use UF_UI_open_listing_window to open the
Information Window. Dates in cbuf must be in the format
DD-MMM-YY (eg. 04-JUL-89).
Return:
Return code:
< 0 = Error code
0 = No files listed
> 0 = Number of files listed
Environment: UF_UI_open_listing_window
See Also:
History:
*******************************************************************************/
extern UFUNEXPORT int uc4650(
const char * dir ,/* <I>
Input directory
*/
int fmode ,/* <I>
File selection mode
1 = Select all files
2 = File template specified in cbuf
3 = Select file created/modified/ accessed
after date specified in cbuf according to
field specified in ibuf
4 = Select file created/modified/ accessed
before date specified in cbuf according to
field specified in ibuf
5 = Select file by owner specified in cbuf
6 = Select file by protection class specified in
cbuf
7 = Select files of type specified in ibuf
8 = Select files by status specified in ibuf
*/
int smode ,/* <I>
Sort mode
1 = Alphabetic
2 = Creation date
3 = Modified date
4 = Access date
5 = Owner
*/
int * pbuf ,/* <I>
Print Field Selection Array,
Set Array Element = 1 To Print Desired Field
(1) = Print format
(2) = Print owner
(3) = Print pclass
(4) = Print length
(5) = Print status
(6) = Print creation date
(7) = Print creation time
(8) = Print modification date
(9) = Print modification time
(10) = Print access date
(11) = Print access time
(12) = Print machine type
(13) = Print description area
(14-16) = Reserved
*/
int * ibuf ,/* <I>
Integer Parameter Array
IF fmode=3 or fmode=4, ibuf show date type
IF ibuf(1) = 1 : use file creation date
IF ibuf(1) = 2 : use file modified date
IF ibuf(1) = 3 : use file accessed date
IF fmode=7, ibuf selects file type set array element
= 1 to select desired file type
(1) = Part
(2) = Symbol
(3) = Text
(4) = GRIP
(5) = Customer
(6) = UNISOLIDS
(7) = UGI
(8) = Communications
(9) = Keystroke
(10) = Display
(11) = CL file
(12) = Directory
(13-16) = Reserved
IF fmode=8, ibuf(1) = File Status
*/
const char * cbuf /* <I>
Character Parameter
IF fmode=2, cbuf contains file template
IF fmode=3, cbuf contains file date
IF fmode=4, cbuf contains file date
IF fmode=5, cbuf contains owner name
IF fmode=6, cbuf contains protection class
*/
);
/******************************************************************************
Return the language name stored in the native binary file.
You can use the returned language name string
to differentiate languages that use the same character set.
NOTE: If a Native Binary File has not been loaded then uc4901
returns "ENGLISH".
Return:
Return code
0 = No error
not 0 = Error code
Environment: Internal and External
See Also:
History:
*******************************************************************************/
extern UFUNEXPORT int uc4901(
char lname[MAX_FSPEC_BUFSIZE] /* <O>
Returns The Language Name Stored In The Native
Binary File
*/
);
/******************************************************************************
Test if a file exists.
Note: This function only works with files - not directories. To check if a
directory exists use uc4560 and pass a file type of 100.
Return:
0 - No error
Otherwise - Error Code
Environment: Internal and External
See Also:
History: Originally released in V16.0
*******************************************************************************/
extern UFUNEXPORT int UF_CFI_ask_file_exist(
const char *file_spec , /* <I>
The file to check
*/
int *status /* <O>
File existence status.
0 - file exists
1 - file does not exist
*/
);
/******************************************************************************
Spawn a subprocess. The return code will indicated the status of the
process creation. If the status from the actual command is needed, use
UF_CFI_spawn_check_status.
Environment: Internal and External
See Also: UF_CFI_spawn_check_status
History: Originally released in V18.0
*******************************************************************************/
extern UFUNEXPORT int UF_CFI_spawn(
const char *program , /* <I>
The command to be executed. This command must either be
a full path name, or the program must be found on the
path.
*/
int num_args, /* <I>
The number of arguments in the next array. These
arguments will be passed to the command.
*/
char *arguments[], /* <I>
An array of character pointers for the arguments to
be passed to the program. You may pass in a NULL if
there are not any arguments. These arguments will be
added in the order they are stored, so the command
will be:
program argument[0] argument[1] ...
Switches must be formatted by the caller. On NT,
switches take the form "-switch:value", where on Unix
switches take the form "-switch=value".
*/
logical is_concur, /* <I>
If TRUE, the command will be run at the same time
as the NX Open program, if FALSE, then UF_CFI_spawn
will wait for the completion of the command prior
to returning to the caller.
*/
int *process_id /* <O>
The process ID of the spawned process.
This process ID can be used to check the status of
the spawned process using UF_CFI_spawn_check_status.
*/
);
/******************************************************************************
Check the status of a spawned subprocess.
Environment: Internal and External
See Also: UF_CFI_spawn
History: Originally released in V18.0
*******************************************************************************/
extern UFUNEXPORT int UF_CFI_spawn_check_status(
int process_id , /* <I>
The process id returned by UF_CFI_spawn for the
command that was run. Note that this is only returned
for processes that are run concurrently.
*/
logical *still_running, /* <O>
If TRUE, the command is still running. If FALSE,
the command has completed.
*/
int *return_status /* <O>
If still_running is FALSE, then this is the return
status from the child process. If still_running
is TRUE, then this will be set to zero. A
return_status of 127 is set when the spawned
command could not be found.
*/
);
#undef EXPORTLIBRARY
#endif